Introduction to Inductive Reactance

Inductive Reactance Explained
Catalog
| Ⅰ Introduction |
| Ⅱ Detailed description |
| Ⅲ Calculation formula |
| Ⅳ Role of inductive reactance in the circuit |
Ⅰ Introduction
When a current flows through the coil, an induced electromagnetic field will be formed in the coil, and the induced electromagnetic field will generate an induced current in the coil to resist the current passing through the coil. Therefore, we call the interaction between this current and the coil the electrical inductance, which is the inductance in the circuit.
Alternating current can also pass through the coil, but the inductance of the coil has an obstructive effect on the alternating current. This obstruction is called inductive reactance. The more difficult it is for alternating current to pass through the coil, the greater the inductance, the greater the obstructive effect of the inductance. The higher the frequency of the alternating current, the more difficult it is to pass through the coil, and the obstructive effect of inductance is also greater. Experiments have proved that inductive reactance is proportional to inductance and also proportional to frequency. If the inductive reactance is represented by XL, the inductance is represented by L, and the frequency is represented by f, then the calculation formula is:
XL= 2πfL=ωL
The unit of inductive reactance is the ohm. Knowing the frequency f (Hz) of the alternating current and the inductance L (H) of the coil, the inductive reactance can be calculated using the above formula. The unit of inductance is "Henry (H)". We can use the special properties of current and coil to make inductance devices of different sizes and values to form a circuit system network with different functions.
XL is the inductive reactance, the unit is ohms, ω is the angular velocity of the alternator, the unit is radians/second, f is the frequency, the unit is Hertz, and L is the coil inductance, the unit is Henry.
Ⅱ Detailed description
① When the alternating current passes through the circuit of the inductance coil, the self-induced electromotive force is generated in the circuit, which hinders the change of current and forms inductive reactance. The greater the self-inductance coefficient, the greater the self-inductance electromotive force, and the greater the inductive reactance. If the frequency of the alternating current is large, the rate of change of the current is also large, and the self-induced electromotive force must also be large, so the inductive reactance also increases with the frequency of the alternating current. The inductance in the alternating current is proportional to the frequency of the alternating current and the self-inductance of the inductance coil. In practical applications, the inductance plays the role of "blocking and passing through", so the characteristics of inductance are often used in AC circuits to bypass low-frequency and direct current and prevent high-frequency alternating current.

The curve of inductive reactance and capacitive reactance
② In a purely inductive circuit, the relationship between the alternating voltage (u) at both ends of the inductor and the self-induced electromotive force (εL) is u=-εL and εL =-Ldi/dt, so u=Ldi/dt. The sinusoidal alternating current changes periodically, and the self-induced electromotive force in the coil is constantly changing. When the current of sinusoidal alternating current is zero, the current rate of change is the largest, so the voltage is the largest. When the current is at the maximum, the current rate of change is the smallest, so the voltage is zero. It can be concluded that the voltage phase across the inductor leads the current phase by π/2.
In a purely inductive circuit, the frequency of current and voltage are the same. The impedance of an inductive component is the inductive reactance (XL=ωL=2πfL), which is proportional to both ω and L. When ω=0, XL =0, so the inductor plays the role of "passing DC and blocking AC" or "passing low frequency and blocking high frequency".
③ In a purely inductive circuit, the inductive reactance does not consume electric energy, because during any 1/4 cycle when the current increases from zero to the maximum value, the current in the circuit will generate a magnetic field near the coil. And the electric energy will be converted into magnetic field energy storage stored in a magnetic field. But in the next 1/4 cycle, the current changes from large to small, the magnetic field gradually weakens, and the stored magnetic field energy is converted into electrical energy and returned to the power supply, so the inductive reactance does not consume electrical energy (the resistance heating is ignored ).
Ⅲ Calculation formula
Winding small voltage transformer, the calculation formula of inductive reactance is derived as follows:
2πfL=R primary load (1)
The primary load of R includes the impedance and inductive reactance of the primary coil of the transformer. Because I only need to wind about 10 turns, the impedance can be regarded as approximately 0; so the primary load of R is mainly caused by inductive reactance. Know the magnitude of R primary load and f (the frequency is known to be 500KHz), then:
L = R primary load/(2πf) (2)
So how to get the value of R primary load? This value is derived from the quiescent current and the primary voltage:
R primary load = V primary / I static (3)
The primary voltage is known, and the empirical value of the quiescent current (the current in the primary coil when the secondary is open) is:
I static=5%*I primary full load (4)
I primary full load * V primary = I secondary full load * V secondary (5)
Because the primary and secondary voltage ratios are known quantities, the full load value of the I primary can be known as long as the full load value of the I secondary is known. The voltage ratio between the primary and secondary voltages of the transformer I want to do is 1:1.2, and the I secondary full load is 200 mA. Then I primary full load = 240 mA, put this value into equation (4), you can find that I static is about 10 mA. V primary is a known quantity, where the primary voltage of my transformer is V primary = 5V. Substituting V primary = 5V and I static = 10 mA into equation (3), we get R primary load = 500 ohms. Substituting R primary load=500 ohms into equation (2), you can find:
L=500/(2πf)=500/(2π*500000)=159 (microhenry)
Ⅳ Role of inductive reactance in the circuit
Inductance: "pass DC, block AC; pass low frequency, block high frequency"
From the causes of inductive reactance, we know: the inductance coil has no hindrance to the DC current, that is, it "passes DC and blocks AC".
From the expression of inductive reactance XL= 2πfL, it is known that an inductance coil with a large self-inductance coefficient will have obvious inductive reactance to an alternating current with a small frequency, let alone a high-frequency alternating current. We call this kind of inductance coil a low-frequency choke. As long as the AC passes through the low-frequency choke, there will be a greater inductance, and there is no hindrance to the DC. That is, the low-frequency choke "passes DC and blocks AC".
Inductance coils with a small self-inductance coefficient have very small inductance to alternating currents with small frequencies. Only when high-frequency alternating currents pass through can they have obvious inductive reactance. We call this type of coil a high-frequency choke. The high-frequency choke "passes low frequency and blocks high frequency".
1.What is XC and XL?
Now when you type a reactance and frequency, you can calculate L and C at that frequency. XL is called inductive reactance and Xc is called capacitive reactance. and the formulae[ XL = 2∏fL, XC = 1/2∏fC ] is given in that website. At resonance the reactence will be the same for both capacitance and inductance.
2.What are inductance and inductive reactance?
Inductance is the ability to create a voltage within a conductor or a nearby conductor by changing the current flow in that the first conductor. The larger the inductance the greater the voltage induced per change in current. Inductive reactance is an opposition to a change in current.
3.What is inductive reactance Class 12?
Inductive reactance is the name given to the opposition by an inductor to a changing current flow in the circuit. This impedance value is measured in ohms, just like the resistance. The inductive reactance is represented by XL and measured in ohms (Ω).
4.What is the reactance formula?
Reactance formula The total reactance (X) is equal to the difference between the two: Total Reactance, X =XL – Xc. a. Capacitive Reactance Xc. The reactance, which is large at low frequencies and small at high frequencies is known as capacitive reactance (Xc).
5.What is XL in the LCR circuit?
The formula for finding Q (the voltage magnification) uses the ratio of the inductive reactance to the total circuit resistance. Where XL is the inductive reactance at resonance, given. by 2πƒrL and R is the TOTAL circuit resistance.
What is a Fixed Inductor?UTMEL15 April 202113662Fixed inductors are a classification of inductors according to their structure, and fixed inductors are commonly used inductive devices. An inductor with a fixed inductance is called a fixed inductor (or a fixed coil), and it can be a coil with a single layer, multiple layers, honeycomb type, or a magnetic core. These coils are winded on the magnetic core using a wire of corresponded diameter and they are packaged with epoxy resin or plastic according to the inductance and the maximum DC operating current.
Read More
Introduction to Inductive ReactanceUTMEL16 April 202115335Alternating current can also pass through the coil, but the inductance of the coil has an obstructive effect on the alternating current. This obstruction is called inductive reactance.
Read More
Inductance Basis: Definition, Structure and ApplicationsUTMEL18 April 202210099Hello everyone, I am Rose. Today I will introduce inductance to you. Inductance is a property of a closed loop and a physical quantity. It is a circuit parameter that describes the induced electromotive force effect in this coil or in another coil due to changes in coil current. Inductance is a general term for self-inductance and mutual inductance. A device that provides an inductance is called an inductor.
Read More
What is Color Ring Inductor? How to Read Inductor Color Code?UTMEL01 April 202517034Hello everyone, I am Rose. Today I will introduce color ring inductor to you. A color ring inductor, also known as a color code inductor or a color ring inductor, is a self-inducting component. Together with a capacitor, the inductance coil (color ring inductance) frequently creates a resonant and filter circuit in the circuit.
Read More
What is inductor: Symbol, Applications and TypesUTMEL04 January 202211251As we begin our studies in 2022, we will work together to decode inductance today. What is an inductor? What enables it to work normally? The answer is the existence of this induced current.
Read More
Subscribe to Utmel !
MC74LCX16373DTGON Semiconductor
SN74LVC573APWRTexas Instruments
SGTL5000XNAA3R2NXP USA Inc.
M2GL005-VFG256Atmel (Microchip Technology)
MC14044BDR2GON Semiconductor
APA150-FG144Microchip Technology
SN74ABT273DBRTexas Instruments
TLV320AIC10IPFBTexas Instruments
A3P1000-FG144IAtmel (Microchip Technology)
A3PE1500-FGG484IAtmel (Microchip Technology)


Product
Brand
Articles
Tools