What are the Types of Camera Lenses?

Ultimate Guide to Camera Lenses
Catalog
| Ⅰ Introduction |
| Ⅱ Camera Lens Classification |
| Ⅲ Camera Lens Parameters |
Ⅰ Introduction
A camera lens, generally called lens for short, is a kind of optical lens. Its function is optical imaging. The lens is an important component in the machine vision system and has a key role in imaging quality. It has an impact on several of the most important indicators of imaging quality, including resolution, contrast, depth of field, and various aberrations.
For cameras, the quality of the lens has always been a key factor affecting the image quality, and digital cameras are of course no exception. The CCD resolution of digital cameras is limited, in principle, the requirements for the optical resolution of the lens are lower. Because the imaging area of digital cameras is small (because the digital camera is imaging on the CCD, the area of the CCD is relatively small. The film of a traditional 35mm camera is much smaller), the lens is required to ensure a certain imaging quality. For example, for a certain subject, 200 pixels are needed in the horizontal direction to perfectly reproduce its details. If the imaging width is 10mm, a lens with an optical resolution of 20 lines/mm can do the job. If the imaging width is 1mm, the optical resolution of the lens must be above 200 lines/mm. On the other hand, the traditional film is more sensitive to ultraviolet rays, and it is often necessary to install a UV lens for outdoor shooting, while CCDs are more sensitive to infrared rays. The addition of special coatings or additional filters to the lens will greatly improve the image quality. The physical aperture of the lens must also be considered, and regardless of its relative aperture, the larger the physical aperture, the greater the luminous flux, the better the digital camera's acceptance and control of light, and the better the image quality.

camera lens
In traditional digital cameras, a wide-angle lens is a photographic lens with a focal length shorter than a standard lens, a viewing angle larger than a standard lens, a distance longer than a fisheye lens, and a viewing angle smaller than a fisheye lens. Wide-angle lenses are divided into two types: ordinary wide-angle lenses and ultra-wide-angle lenses. The focal length of the ordinary wide-angle lens of the 135 camera is generally 38-24 mm, and the angle of view is 60-84 degrees. The focal length of the ultra-wide-angle lens is 20-13 mm, and the angle of view is 94-118 degrees. Due to the short focal length of the wide-angle lens and the large viewing angle, a larger area of scenery can be captured within a shorter shooting distance. Therefore, it is widely used in the shooting of large-scale photography works.
In photography creation, using a wide-angle lens to shoot can achieve the following effects: 1. It can increase the spatial depth of the photographic picture; 2. The depth of field is longer, which can ensure that the subject's front and back scenes are clear on the screen. Therefore, most modern pocket-sized automatic cameras use ordinary wide-angle lenses of 38-35 mm; 3. The lens covers a large area and the shooting range is wide; 4. It is the scenes shot at the same shooting distance and the image in the screen is smaller than that of a scene taken with a standard lens; 5. The defects of perspective distortion and image distortion are prone to appear in the screen. The shorter the focal length of the lens and the closer the shooting distance, the more obvious this defect is.
Ⅱ Camera Lens Classification
1.By structure
Fixed aperture fixed focus lens
This lens has only one focus adjustment ring that can be adjusted manually, which can be rotated left and right. This ring can make the image imaged on the CCD target surface the clearest. It doesn’t have the aperture adjustment ring, so the aperture cannot be adjusted, and the luminous flux entering the lens cannot be changed by changing the lens factor, but can only be adjusted by changing the illuminance of the field of view. The structure is simple and the price is cheap.
Manual iris fixed focus lens
Compared with fixed-aperture fixed-focus lenses, manual aperture fixed-focus lenses have an aperture adjustment ring. The aperture range is generally from F1.2 or F1.4 to fully closed, which can easily adapt to the illuminance of the subject site. The illuminance is more uniform and the price is cheaper.
Auto iris fixed focus lens
Auto iris fixed focus lens adds a gear-driven micro-motor to the iris adjustment ring of the manual iris fixed-focus lens, and draw a 3 or 4-core shielded wire from the drive circuit, and connect it to the camera's automatic iris interface seat. When the luminous flux entering the lens changes, the charge generated by the CCD target surface of the camera changes accordingly, so that the video signal level changes. Then a control signal is generated, which is transmitted to the automatic iris lens so that the motor in the lens performs the corresponding correction.

optical lens
Manual iris zoom lens
The focal length of a manual iris zoom lens is variable. There is a focal length adjustment ring, which can adjust the focal length of the lens within a certain range. The variable-ratio is generally 2 to 3 times, and the focal length is generally 3.6 to 8mm. In practical applications, you can manually adjust the zoom ring of the lens to easily select the market angle of the monitored market. But after the camera installation position is fixed, it is very inconvenient to manually adjust the zoom frequently. Therefore, after the completion of the project, the focal length of the manual zoom lens is generally seldom adjusted.
Auto iris motorized zoom lens
Compared with the automatic iris fixed focus lens, two micromotors are added. One of the motors is connected with the zoom ring of the lens and can control the focal length of the lens when it rotates. The other motor is connected with the focus ring of the lens and when it rotates in a controlled manner. The focus of the lens can be completed at the time. However, due to the addition of two motors and an increase in the number of lens groups, the size of the lens has also increased accordingly.
Motorized three variable lens
Compared with the automatic iris electric zoom lens, it only changes the control of the iris adjustment motor from automatic control to manual control by the controller.
2.By focal length
Standard lens
The angle of view is about 50 degrees, which is also the angle that a person can see without turning his head and eyes, so it is also called a standard lens. The focal length of the standard lens of a 5mm camera is mostly 40mm, 50mm, or 55mm. The focal length of the standard lens of the 120 camera is mostly 80mm or 75mm. The larger the CCD chip, the longer the focal length of the standard lens.
Wide-angle lens
The angle of view is above 90 degrees, which is suitable for shooting close-up and large-scale scenery and can deliberately exaggerate the foreground to show a strong sense of perspective. The typical wide-angle lens of a 35mm camera has a focal length of 28mm and an angle of view of 72 degrees. The 50 and 40mm lens of the 120 camera is equivalent to the 35 and 28mm lens of the 35mm camera.

smartphone with dual cams
Long focal length lens
It is suitable for subjects with a long shooting distance. The small depth of field can easily make the background blurred and the subject stands out, but it is bulky and difficult to focus on dynamic subjects. 35mm camera long focal length lenses are usually divided into three levels, 135mm or less is called medium focal length, 135-500mm is called long focal length, and above 500mm is called the ultra-long focal length. The 150mm lens of the 120 camera is equivalent to the 105mm lens of the 35mm camera. Because the long focal length lens is too bulky, there is a telephoto lens design. That is, a negative lens is added behind the lens, and the main plane of the lens is moved forward. A shorter lens body can be used to obtain the effect of a long focal length.
Reflective telescope lens
It is another super-telescopic lens design that uses a reflective mirror to form an image, but due to the design, the aperture cannot be installed, and only the shutter can be used to adjust the exposure.
Macro lens
In addition to close-up macro photography, it can also be telephoto.
3.By interface
C Type lens
Flange focal length is the distance between the mounting flange and the convergent point of the incident lens parallel light. The flange focal length is 17.526mm or 0.690in. The lens can be used on line sensors with a length of 0.512in (13mm) or less. However, due to geometric distortion and market angle characteristics, it is necessary to identify whether short-focus lenses are suitable. For example, a lens with a focal length of 12.6mm should not use a linear array with a length greater than 6.5mm. If the flange focal length size is used to determine the distance from the lens to the array, the lens adapter should be increased when the magnification of the object side is less than 20 times. The adapter ring is added behind the lens to increase the distance from the lens to the image, assuming that the focus range of most lenses is 5-10%. The lens extension distance is the focal length/object side magnification.
CS type lens
With a 5 mm adapter ring, a C lens can be used on a CS-mount camera.
U lens
A variable focal length lens, the flange focal length is 47.526mm or 1.7913in, and the mounting rib is M42×1. It is mainly designed for 35mm photo applications, and can be used for any array less than 1.25in (38.1mm) in length. It is recommended not to use a short focal length lens.
4.Special lenses
There are special lenses such as a micro-magnification system. Pay special attention to the difference between CS and C. When connecting different types of cameras and different types of Lens, you must customize the adapter ring. The main parameters and evaluation of optical lens are focal length, field of view, object distance, aperture, shutter, and so on. The most complete evaluation of the lens is MTF (Modulation Transfer Function). However, due to aberrations (due to calibration), each range of the lens has an MTF value. These ranges refer to: (1) the paraxial part, (2) the off-axis part, and (3) the sub-parts of the above two parts in different directions when there is asymmetric distortion in the optical system. Each part has its own corresponding MTF value for different radiation energy wavelength ranges. MTF is the most commonly used and optimal index for evaluating imaging systems, and it is also the optimal index for guiding the integration of machine vision systems.
Ⅲ Camera Lens Parameters
1.Focus and aperture
Depth of field: The moderately sharp focus around the subject plays a vital role in the appearance of the final image. In order to make full use of all the apertures provided on the lens, the camera can be fixed on a tripod to prevent camera shake.
2.f/aperture number and aperture size
Any kind of lens set at a certain f/aperture number can transmit images with almost the same amount of light, because the diaphragm diameter is directly related to the focal length. For example, when an 80 mm lens uses a 5 mm diaphragm diameter, the aperture must be adjusted at f/16. Therefore, the focal length of the lens is divided by the diaphragm diameter to obtain the corresponding f/aperture number.
3.Focal length mark
Adjust the thread of the focusing ring, the lens extends from the camera. As the focusing ring rotates, you can find the focal length being adjusted by looking at the mark of the fixed reference symbol.
4.Aperture adjustment
Rotate the aperture ring upward to the next f/aperture number (for example, from f/4 to f/5.6), the aperture size is halved (that is, the light quantity of the film is halved); rotate the aperture ring down to the next f/aperture number ( For example, from f/4 to f/2.8). The aperture size is doubled.
5.Depth of Field
As the lens focuses on the subject, you can find the f/number corresponding to (or close to) the adjusted aperture on both sides of the fixed reference symbol, and identify the relative value under the focal length mark to determine the effective depth of field.
6.The role of the depth of field
Change of aperture size: Focusing on a subject at the same distance through a lens of the same focal length. This indicator shows how the adjustment of aperture size changes the depth of field. Generally speaking, the foreground depth of the subject is enlarged by 1/3, and the back depth of field is enlarged by 2/3. The smaller the aperture, the greater the depth of field. The depth of field at an aperture of F/2 is much smaller than that at an aperture of f/16.
The distance from the subject to the camera: Even if the same focal length and aperture are used, the depth of field is limited to a certain extent by the distance from the subject to the camera. The closer the subject is to the camera, the smaller the depth of field. The depth of field produced by the lens focusing at 15 feet (4.5 meters) is much greater than the depth of field produced by the lens focusing at 5 feet (1.5 meters).
Lens change: In the case of the same object distance and aperture, using different focal length lenses can change the depth of field. The shorter the focal length of the lens, the greater the maximum depth.
1.What are optical lenses used for?
Lens, in optics, a piece of glass or other transparent substance that is used to form an image of an object by focusing rays of light from the object.
2.How do optical lenses work?
A lens works by refraction: it bends light rays as they pass through it so they change direction. That means the rays seem to come from a point that's closer or further away from where they actually originate—and that's what makes objects seen through a lens seem either bigger or smaller than they really are.
3.What is the difference between optical and digital zoom?
In short, with the optical zoom you first get the subject close before you capture it. With digital zoom, your camera uses part of the image and later brings it to the correct size. With digital zoom, you, therefore, have more chance of quality loss.
4.What are the 3 types of lenses?
Macro Lenses. Telephoto Lenses. Wide Angle Lenses. Standard Lenses. Specialty Lenses
5.What's the difference between camera lenses?
Focal length is expressed in mm and a higher number means a bigger zoom, while a lower number means the lens can be used for wider shots. ... A number lower than 30-50 mm will take in a bigger view than you naturally see, while higher numbers mean focus will be on a smaller aspect of your view.
The Introduction to Common Tools and Using Methods of Fiber OpticUTMEL07 January 20227109The building and maintenance of optical cables in the intelligent industry has gradually expanded with the rapid expansion of the Internet of Things and 5G technologies, resulting in an increase in demand for various optical fiber tools. Cutting shears, for example, come in a variety of shapes and sizes, and each tool serves a different purpose. Do you have any experience with them? When should you utilize certain fiber optic tools?
Read More
What are Fiber Optic Patch Cables?UTMEL11 February 20228157Hello everyone, I am Rose. Today I will introduce fiber optic patch cables to you. Optical fiber communication, as an emerging technology, has become one of the main pillars of modern communication and plays a critical role in modern telecommunication networks, thanks to the rapid growth of traffic data.
Read More
Basis of Fiber Optic and Fiber Optic CommunicationUTMEL22 October 20215093Hello everyone, I am Rose. Today I will introduce fiber optic to you. Fiber Optic is a type of glass or plastic fiber that can be utilized to transmit light. It is mostly used for communication. This article will show you the basic knowledge of fiber optic and fiber optic communication.
Read More
The History of MicroscopeUTMEL21 October 20217976Hello, everyone. I am Rose. Today I will show you the history of microscopes. The microscope is used to magnify tiny objects into instruments that can be seen by human eyes. Microscopes are divided into optical microscopes and electron microscopes.
Read More
What is VCSEL?UTMEL28 October 202111734Hello everyone, I am Rose. I welcome you on board, today I will introduce VCSEL to you. The Vertical-Cavity Surface-Emitting Laser (VCSEL, or Vertical-Cavity Surface-Emitting Laser) is a semiconductor whose laser is emitted perpendicular to the top surface. It differs from an edge-fired laser, which emits the laser from the edge.
Read More
Subscribe to Utmel !
204-10UYT/S530-A3Everlight Electronics Co Ltd
QTLP670C3TREverlight Electronics Co Ltd
OP240BTT Electronics/Optek Technology
CLP6B-WKW-CC0E0233Cree Inc.
SFH 4258SOSRAM Opto Semiconductors Inc.
AA4040SRCGKC-RKingbright
SMP4-SBC-RBBivar Inc.
HLMP-3301-F0002Broadcom Limited
AFBR-1549SZBroadcom Limited
ZB5AV05Schneider Electric


Product
Brand
Articles
Tools