web counter

Results: ( 29,342 )

Isolators

Isolators definition

What is an Isolator

Isolators are devices used to ensure that a circuit is completely powered down in order for it to be serviced or maintained. Digital Isolator Switches isolate a given part of the circuit by cutting off its electrical supply, making it safe for service or maintenance. As one of switch circuit types, the electrical isolator is generally used to involve high voltage devices like transformers.

Types of Isolators

Due to different application requirements, there are several isolator types, such as Pantograph isolator, single break isolator and double break isolator. Among them, Pantograph isolators include 3 types of isolators: Line Side Isolator, Bus Side Isolator and Transfer Bus Side Isolator.

Recommended Manufacturers

Advanced PhotonixAmerican BrightAnalog Devices, Inc.BroadcomCEL (California Eastern Laboratories)Central Semiconductor
Frequently Asked Questions

What are fused switch disconnectors used for?

Isolators protect workers performing maintenance on part of an electrical circuit, as well as preventing damage to the circuit itself.

What is an RF isolator?

An RF isolator is a two-port device that only transfers microwave or radio frequency power in one direction while blocking the signal in the other. It prevents a microwave source from being detuned by a mismatched load by shielding your RF components from excessive power reflection.

How does an RF isolator work?

In terms of functionality, an RF isolator is similar to a diode, however unlike a diode, which only transmits current in one way, an isolator only transfers RF energy in one direction.
It becomes an isolator when one of the three ports of a three-port circulator is terminated with 50 Ohm.
The gadget has two ports, port-1 and port-2, as illustrated. It permits signal from port-1 to port-2 to be attenuated as little as possible, and signal from port-2 to port-1 to be attenuated as much as possible.
Furthermore, any RF energy entering through port-2 will be directed to a matching termination on port-3. This is converted to heat and dispersed. As a result, any reflections from port-2 to port-1 are removed. This protects any signal source or equipment connected to port-1 from being damaged.

Where do we use isolators?

The isolator is a switch that separates a circuit system component when it is needed. Electrical isolators are a distinct component of a system designed to ensure safe maintenance. Isolators are typically used at the breaker's end to repair or replace it.

What does a microwave isolator do?

A microwave or radio frequency isolator is a two-port device that exclusively sends power in one way. Internal behavior allows propagation in one direction while blocking propagation in the other.

What is an optocoupler used for?

Optocouplers can be used as a switching device on their own or in conjunction with other electrical components to create isolation between low and high voltage circuits. These gadgets are commonly used for the following purposes: Switching input/output on a microprocessor. Controlling both DC and AC electricity.

How do optoisolators work?

An opto-isolator uses a beam of light controlled by input current to link the input and output sides. It converts a useful input signal into light, delivers it through a dielectric channel, and catches light on the output side before converting it back to an electric signal.

What is an Optoisolator?

A semiconductor device called an optoisolator (also known as an optical coupler, photocoupler, or optocoupler) exchanges an electrical signal across isolated circuits using light.

These electronic components are utilized in a variety of communications and monitoring systems where electrical isolation is needed to prevent high voltage emitters from impacting lower power circuits receiving a signal.

What types of uses do optoisolators have?

Optoisolators are best for isolating voltage from digital signals, although they can also transmit analog signals.

High speed refers to the isolation of any data rate greater than 1 megabit per second (Mbps). The most common digital and analog optoisolator speed is 1 Mbps, though digital speeds of 10 Mbps and 15 Mbps are also available.