web counter
Current Divider Calculator

The current flow through each of up to ten parallel-linked resistances connected to a current source is calculated with this method.

Current Divider Calculator

Current Source
Formula
R= The total equivalent parallel resistance of the resistor array across the current source.
Introduction

Current Divider Calculator

Use this calculator to determine how a known total current divides among two or more parallel resistive branches. Enter the source current and the resistance of each connected branch. The calculator returns the current through every branch and can be checked by confirming that all branch currents add up to the total current.

The basic calculation assumes ideal resistors connected across the same two nodes and a known current entering the parallel network. For AC circuits containing capacitors or inductors, use complex impedance rather than resistance and account for phase.

How to Use the Current Divider Calculator

  1. Enter the total current flowing into the parallel network.

  2. Select or enter the current unit, such as A, mA, or µA.

  3. Enter the resistance of each active branch using consistent resistance units.

  4. Leave unused branch fields blank rather than entering zero.

  5. Calculate the branch currents.

  6. Verify that the sum of the calculated branch currents equals the entered total current, allowing for rounding.

If every resistance is entered in the same unit, the resistance unit cancels in the divider ratio. The output current uses the same current unit as the entered total current.

What Is a Current Divider?

A current divider is a parallel network in which an incoming current splits among multiple branches. Components are in parallel when both terminals of every branch connect to the same two nodes. Consequently, each branch has the same voltage across it.

For resistive branches, Ohm's law gives I = V/R. Because the branch voltage is common, a lower resistance carries more current and a higher resistance carries less current. Current is therefore proportional to branch conductance, where conductance is the reciprocal of resistance.

Kirchhoff's Current Law

Kirchhoff's current law follows conservation of electric charge: the sum of currents entering a junction equals the sum of currents leaving it. For a current divider with n outgoing branches:

IT = I1 + I2 + ... + In

where IT is the current entering the parallel network and I1 through In are the branch currents. This equation provides a useful check on every current-divider result.

General Current Divider Formula

For branch k in a parallel network of resistors, the branch current is:

Ik = IT × (1/Rk) ÷ Σ(1/Rj)

In conductance form, with Gk = 1/Rk:

Ik = IT × Gk ÷ ΣGj

The equivalent resistance of all parallel branches is:

Req = 1 ÷ Σ(1/Rj)

Therefore, the current-divider rule may also be written as:

Ik = IT × Req/Rk

Two-Resistor Current Divider Formula

For two parallel resistors R1 and R2 carrying a total current IT:

I1 = IT × R2/(R1 + R2)

I2 = IT × R1/(R1 + R2)

Notice that the current through one resistor uses the other resistor in the numerator. This is sometimes called the opposite-resistance form of the current-divider rule.

Current Divider Variables

SymbolMeaningTypical Unit
ITTotal current entering the parallel networkA, mA, or µA
IkCurrent through branch kA, mA, or µA
RkResistance of branch kΩ, kΩ, or MΩ
ReqEquivalent resistance of all parallel branchesΩ, kΩ, or MΩ
GkConductance of branch k, equal to 1/RkS
VVoltage shared by all parallel branchesV

Current Divider Calculation Examples

Example 1: Two Parallel Resistors

A total current of 6 A enters two parallel resistors, R1 = 4 Ω and R2 = 12 Ω.

I1 = 6 A × 12 Ω/(4 Ω + 12 Ω) = 4.5 A

I2 = 6 A × 4 Ω/(4 Ω + 12 Ω) = 1.5 A

KCL check: 4.5 A + 1.5 A = 6 A. The 4 Ω branch carries three times the current of the 12 Ω branch because its resistance is one third as large.

The equivalent resistance is 3 Ω, so the voltage across both branches is 6 A × 3 Ω = 18 V. Ohm's law confirms 18 V/4 Ω = 4.5 A and 18 V/12 Ω = 1.5 A.

Example 2: Three Parallel Resistors

A total current of 12 mA enters R1 = 1 kΩ, R2 = 2 kΩ, and R3 = 3 kΩ in parallel.

Req = 1 ÷ (1/1 kΩ + 1/2 kΩ + 1/3 kΩ) = 0.545455 kΩ

The branch currents are:

  • I1 = 12 mA × 0.545455/1 = 6.54545 mA

  • I2 = 12 mA × 0.545455/2 = 3.27273 mA

  • I3 = 12 mA × 0.545455/3 = 2.18182 mA

KCL check: 6.54545 mA + 3.27273 mA + 2.18182 mA = 12 mA after rounding.

Example 3: Equal Branch Resistances

If n equal resistors are connected in parallel, the total current divides equally:

Ibranch = IT/n

For four equal branches carrying a total of 20 mA, each branch carries 5 mA.

Current Ratio Between Two Branches

Because the voltage is the same across parallel resistors:

I1/I2 = R2/R1

Branch current is inversely proportional to branch resistance. If R2 is twice R1, then I1 is twice I2.

Branch Voltage and Power

After finding the equivalent resistance, calculate the common branch voltage with:

V = ITReq

Power dissipated in branch k can then be calculated using any consistent form:

Pk = V Ik = Ik2Rk = V2/Rk

Select resistors with suitable resistance tolerance, voltage rating, and power rating for the real circuit. A calculated nominal current does not include component tolerance, self-heating, source limits, wiring resistance, or temperature effects.

DC Resistance and AC Impedance

The resistance formulas above apply directly to ideal resistive DC networks. In sinusoidal steady-state AC analysis, replace each resistance with its complex impedance:

Ik = IT × Yk/ΣYj

where Yk = 1/Zk is complex admittance. The branch currents are phasors and may have different phase angles. Using impedance magnitudes alone can produce an incorrect result when reactive branches are present.

Open Circuits and Short Circuits

  • An open branch has effectively infinite resistance and carries zero current in the ideal model.

  • A branch with zero resistance is an ideal short circuit. If it is the only ideal short, the ideal model directs all current through it.

  • Multiple ideal zero-resistance branches do not provide enough information to determine how current shares; real parasitic resistances or impedances are required.

  • Leave unused calculator inputs blank. Do not use zero to represent an unused or open branch.

When the Current Divider Rule Applies

Use the current-divider rule when all branch elements are connected between the same two nodes and the total current entering that parallel group is known. The simple resistor form assumes linear resistors.

Do not apply the shortcut unchanged to a circuit with dependent sources, active components, nonlinear devices, or branches that are not truly in parallel. Such circuits may require nodal analysis, Kirchhoff's laws, or a device-specific model.

Common Current Divider Mistakes

  • Using the voltage-divider formula for a parallel current-divider circuit.

  • Putting the same branch resistance in the numerator of the two-resistor shortcut.

  • Assuming current divides equally when branch resistances are unequal.

  • Mixing Ω and kΩ without converting or using consistent units.

  • Entering zero resistance for an unused branch.

  • Forgetting to check that branch currents sum to the total current.

  • Using resistance instead of complex impedance in a reactive AC circuit.

  • Ignoring resistor power dissipation and source compliance limits.

Current Divider FAQ

Why does the smaller resistor carry more current?

Parallel branches share the same voltage. From I = V/R, current increases as resistance decreases, so the lower-resistance branch carries more current.

Does current always divide equally in parallel?

No. It divides equally only when all branch resistances or impedances are equal. Otherwise, each branch receives a share proportional to its conductance or admittance.

Can this calculator handle more than two branches?

Yes, when the interface provides additional resistance fields. Enter each connected branch and leave unused fields blank. The general conductance formula applies to any number of ideal parallel resistors.

Can I use different resistance units?

Convert all branch values to the same unit before calculating. For example, 500 Ω is 0.5 kΩ. Once the units are consistent, they cancel in the current ratio.

Can current divider calculations be used for capacitors and inductors?

Yes, in sinusoidal steady-state analysis, but the calculation must use complex impedances or admittances and phasor currents. The simple real-resistance calculator is not sufficient for branches with different phase angles.

How can I verify a current-divider result?

Add all branch currents and compare the sum with the total current. You can also calculate the common voltage from each branch using V = IkRk; every branch should produce the same voltage within rounding tolerance.

Current Divider Video

Watch the original current-divider video on YouTube.

References

Frequently Asked Questions

What is meant by current dividers?

Current dividers or current division is the process of finding the individual branch currents in a parallel circuit were each parallel element has the same voltage. Kirchhoff's current law, (KCL) states that the algebraic sum of the individual currents entering a junction or node will equal the currents leaving it.

What is voltage and current divider rule?

Current Division Rule A parallel circuit acts as a current divider as the current divides in all the branches in a parallel circuit, and the voltage remains the same across them. The current division rule determines the current across the circuit impedance.

What is voltage divider formula?

A voltage divider is applying a voltage across a series of two resistors. We may draw in a few different ways, but they should always essentially be the same circuit. Thus formula is given as follows: V o u t = R b R a + R b × V i n V_{out} = \frac{R_b}{R_a+R_b} \times V_{in} Vout=Ra+RbRb×Vin.

How do I calculate current?

Ohms Law and Power To find the Voltage, ( V ) [ V = I x R ] V (volts) = I (amps) x R (Ω) To find the Current, ( I ) [ I = V ÷ R ] I (amps) = V (volts) ÷ R (Ω) To find the Resistance, ( R ) [ R = V ÷ I ] R (Ω) = V (volts) ÷ I (amps) To find the Power (P) [ P = V x I ] P (watts) = V (volts) x I (amps)

Does a voltage divider affect current?

Application Dont's. As tempting as it may be to use a voltage divider to step down, say, a 12V power supply to 5V, voltage dividers should not be used to supply power to a load. Any current that the load requires is also going to have to run through R1.

Is current divided in a parallel circuit?

"A parallel circuit has two or more paths for current to flow through." Simply remember that PARALLEL means two paths up to thousands of paths. The flow of electricity is divided between each according to the resistance along each route.

How do you calculate amps in a parallel circuit?

Divide the voltage by R1 to get I1. V/R1 = I1. I1 will be measured in amps. Divide the voltage by R2 to get I2.

What is the voltage divider equation?

Using the voltage divider ratio rule, we can see that the largest resistor produces the largest I*R voltage drop. Thus, R1 = 4V and R2 = 8V. Applying Kirchhoff's Voltage Law shows that the sum of the voltage drops around the resistive circuit is exactly equal to the supply voltage, as 4V + 8V = 12V.

Can you measure current in parallel?

A multimeter set to measure current can only measure the current going through it. ... Devices in parallel must have the same voltage across them, although the currents through each can be different.
Hot products

ImagePart NumberManufacturerCategoryPackage/CaseDescriptionPriceQuantityBuy/Quote
BLM18PG121SN1DBLM18PG121SN1DMurata ElectronicsFerrite Beads and Chips0603 (1608 Metric)MURATA - BLM18PG121SN1D - Ferrite Bead, 0603 [1608 Metric], 120 ohm, 2 A, BLM18P Series, 0.05 ohm, ± 25%-

In stock : 355131

Minimum: 1

TP3420AV309TP3420AV309Texas InstrumentsInterface - Telecom20-LCC (J-Lead)IC TELECOM INTERFACE 20PLCC-

In stock

Minimum: 1

19-217/R6C-AL1M2VY/3T19-217/R6C-AL1M2VY/3TEverlight Electronics Co LtdLED Indication - Discrete0603 (1608 Metric)LED RED CLEAR 2SMD-

In stock : 6070

Minimum: 1

MPZ2012S102AT000MPZ2012S102AT000TDK CorporationFerrite Beads and Chips0805 (2012 Metric)TDK - MPZ2012S102AT000 - FERRITE BEAD, 0.15OHM, 1.5A, 0805-

In stock : 51745

Minimum: 1

SE2537L-RSE2537L-RSkyworks Solutions Inc.RF Amplifiers16-VFQFN Exposed PadRF Amplifier 5GHz Gain 30 dB 3.3Volt -10C 85C-

In stock : 10000

Minimum: 1

SKY81294-14-001SKY81294-14-001Skyworks Solutions Inc.PMIC - LED Drivers9-BGA, WLCSPIC LED FLASH DVR 1.2V 9CSP
  • 1:$0.465882
  • 10:$0.439511
  • 100:$0.414633
  • 500:$0.391163

In stock : 1000

Minimum: 1

HMC588LC4BTRHMC588LC4BTRAnalog Devices Inc.RF Misc ICs and Modules24-TFQFN Exposed PadIC OSC VCO WIDEBAND 24SMD-

In stock : 5

Minimum: 1

80HCPS1432CRM80HCPS1432CRMRenesas Electronics America Inc.Specialized ICs576-BBGA, FCBGAIC SER RAPIDIO SWITCH 576FCBGA-

In stock

Minimum: 1

DS21Q48NDS21Q48NMaxim IntegratedInterface - Telecom144-BBGAIC LIU E1/T1/J1 4X 5V LONG144BGA-

In stock

Minimum: 1

ALT6702RM45Q7ALT6702RM45Q7Skyworks Solutions Inc.RF Amplifiers-IC RF AMP CELLULAR SMD-

In stock

Minimum: 1

EEF-CS1E150REEF-CS1E150RPanasonic Electronic ComponentsAluminum - Polymer Capacitors2917 (7343 Metric)Aluminum Organic Polymer Capacitors 15uF 25volt
  • 1:$0.593588
  • 10:$0.559988
  • 100:$0.528291
  • 500:$0.498388

In stock : 28000

Minimum: 1

AFBR-2418TZAFBR-2418TZBroadcom LimitedFiber Optics - Receivers-Fiber Optic Transmitters, Receivers, Transceivers RX DC-50MBd ML 820nm ST Thrd-

In stock : 660

Minimum: 1

SFH 4713ASFH 4713AOSRAM Opto Semiconductors Inc.Infrared, UV, Visible Emitters3-SMD, No LeadEMITTER IR 860NM 1A-

In stock : 6000

Minimum: 1

TZY2Z060AC01R00TZY2Z060AC01R00Murata ElectronicsTrimmers, Variable Capacitors-2.5 ~ 6pF Trimmer Capacitor 25V Top Adjustment-

In stock : 4636

Minimum: 1

SML-S13RTT86SML-S13RTT86ROHM SemiconductorInfrared, UV, Visible Emitters1206 (3216 Metric)EMITTER IR 850NM 30MA 1206-

In stock : 1

Minimum: 1

TZY2Z100AC01R00TZY2Z100AC01R00Murata ElectronicsTrimmers, Variable Capacitors-3 ~ 10pF Trimmer Capacitor 25V Top Adjustment-

In stock : 22000

Minimum: 1

DGD2136S28-13DGD2136S28-13Diodes IncorporatedPMIC - Gate Drivers28-SOIC (0.295, 7.50mm Width)HV GATE DRIVER SO-28-

In stock : 2799

Minimum: 1

TEN-HS5TEN-HS5Traco PowerAccessoriesAluminumTRACOPOWER TEN-HS5 Power Supply Accessory, Heat Sink, DC/DC Converter, TEN25, TEN25WI Series
  • 1:$3.808917
  • 10:$3.593318
  • 100:$3.389922
  • 500:$3.198040

In stock : 255

Minimum: 1

HEF4044BT,652HEF4044BT,652NXP USA Inc.Logic - Latches16-SOIC (0.154, 3.90mm Width)IC R/S LATCH 3-STATE QUAD 16SOIC-

In stock

Minimum: 1

T9GV5L14-22T9GV5L14-22TE ConnectivityRelays-Power Relays, Standard, Monostable, DC, 900 mW Coil Power Rating DC, 538 Ω Coil Resistance, UL Coil Insulation Class F, Potter & Brumfield T9G-

In stock

Minimum: 1