Sort by
How to Use the Oscilloscope's X-Y Display Correctly19 September 2022
Hello everyone, I am Rose. Welcome to the new post today. This post will tell you how to use the oscilloscope's X-Y display directly.
FPGA vs ASIC: Comprehensive Comparison Guide09 May 2025
A Comprehensive Comparison Guide for Choosing the Right Hardware Solution (2025)
DVI Connector: Types, Advantages, Distiguishment And Development18 November 2020
A DVI connector, that is, digital video interface connector, is an interface standard launched in 1999 by the DDWG (Digital Display Working Group) formed by Silicon Image, Intel, Compaq, IBM, HP, NEC, Fujitsu and other companies.
The 2026 Memory Super-Cycle: Navigating the 500% Surge in DRAM and NAND Flash Prices17 August 2026
Driven by massive AI capital expenditures, the 2026 semiconductor market is experiencing a historic memory super-cycle, sending DRAM and NAND Flash prices soaring. With manufacturers prioritizing high-margin AI memory like HBM, severe shortages have spilled over to mature nodes, impacting automotive and IoT sectors. To navigate this volatility, procurement teams must secure long-term agreements, diversify suppliers, and optimize designs to mitigate rising BOM costs.
Linear Induction Motor: Working Principle, Characteristics, and Applications02 March 2021
LIM stands for Linear Induction Motor, and it is an improved version of the rotary induction motor that produces linear translational motion instead of rotating motion. Other than rotating torque, this device generates linear movement and force. By cutting a radically shaped cut in the revolving induction and thus leveling the section, the design and functionality of the linear induction motor can be demonstrated in the diagram below.
Bridge Rectifier: Functions, Circuits and Applications03 November 2020
Bridge rectifiers are the most commonly used circuits for rectifying AC to DC using the single conductance of a diode. A bridge rectifier consists of four rectifier silicon chips connected by a bridge and encapsulated in insulating plastic. There is a zinc metal shell over an insulating layer to enhance heat dissipation in a high power bridge rectifier.
Introduction to Pi Filter19 February 2021
A Pi filter is a type of filter with a two-port, three-terminal block consisting of three elements with two terminals in each element: the first element is connected to the GND terminal via i/p, the second terminals are connected to the terminals from i/p to o/p and the third element is connected to the terminals from o/p to GND. The circuit model is going to be like a 'Pi' symbol. Capacitors and one inductor are the elements used in the circuit.
What is Visible Light Communication(VLC)?13 October 2021
In some situations, visible light communication (VLC) has considerable advantages over the more generally utilized radio frequency (RF). VLC has gained a lot of attention because of its ability to provide a very accurate and safe indoor positioning system, in addition to the obvious usage of data transmission from one location to another. Implementing a VLC system poses unique hurdles in terms of system integration and power management, particularly for people unfamiliar with the technology. This article will look at some of the uses of VLC, as well as the fundamentals of the VLC positioning system, and how the most recent devices offer a low-risk design approach.
What is an ASIC Chip?07 January 2026
ASIC (Application Specific Integrated Circuit) is a special-purpose integrated circuit, which is an integrated circuit designed and manufactured in response to specific user requirements and the needs of a specific electronic system.
Introduction to Semiconductor Devices17 October 2025
Semiconductor devices are electronic devices with conductivity between a good conductor and an insulator. It uses the special electrical characteristics of semiconductor materials to accomplish specific functions such as generate, control, receive, transform, and amplify signals, and convert energy.
An Overview of Development Board18 December 2025
The development board is a circuit board used for embedded system development. Development boards are generally customized by embedded system developers according to development needs.
What is a Projector?14 October 2021
Hi, fellas. I am Rose. Welcome to the new post today. A projector is an electronic device that can display images or videos on a screen. Through various interfaces, it may be connected to PCs, VCDs, DVDs, BDs, gaming consoles, DVs, and other devices to play video signals. This article introduces the basis of projectors.


Product
Brand
Articles
Tools