What is LCD? Working Principle, Features, and Future Trends

Published: 02 April 2021 | Last Updated: 05 January 202613276
LCD is a liquid crystal display. The LCD structure is to place a liquid crystal cell between two parallel glass substrates. LCD has replaced CRT as the mainstream, and the price has dropped a lot, and it has become fully popular.
In this video, working principle and construction of liquid crystal display is discussed.

Construction and Working of Liquid Crystal display

Catalog

Ⅰ LCD Features
Ⅱ LCD advantages
Ⅲ LCD types
LCD working principle
Ⅴ Future Trends

 

Ⅰ LCD Features

(1) Low-voltage and energy efficiency: Modern LCDs utilizing LED backlights operate on significantly lower voltages (IC circuits) compared to legacy display technologies, making them ideal for battery-operated devices.

(2) Ultra-slim profile: The physical footprint is minimal. Modern panels are often less than 10mm thick, with high-end models achieving widths under 5mm.

(3) Non-emissive technology: Unlike OLEDs or CRTs, LCDs function by modulating light rather than emitting it directly from the liquid crystal layer. This often results in reduced eye strain during prolonged use (flicker-free backlights).

(4) High Pixel Density: The technology allows for extremely small pixel pitch, enabling high-definition resolutions (4K and 8K) on relatively small screens.

(5) Accurate Color Reproduction: With the integration of IPS (In-Plane Switching) and Quantum Dot technology, modern LCDs cover wide color gamuts (sRGB, DCI-P3).

(6) Minimal Radiation: LCDs produce negligible electromagnetic radiation compared to CRT monitors, ensuring safety for users and security for information sensitive to TEMPEST attacks.

(7) Long Lifespan: LED-backlit LCDs typically offer a lifespan of 30,000 to 60,000 hours before brightness degradation becomes noticeable.

Ⅱ LCD advantages

(1) Geometric Accuracy: Historically, CRT displays relied on electromagnetic deflection, which often caused geometric distortion (pincushion effects) at the screen edges. LCDs rely on a fixed pixel grid, ensuring zero geometric distortion and perfect linear alignment across the entire screen area.

(2) Environmental Safety: Compared to legacy CRT (which contained lead) and early CCFL-backlit LCDs (which contained mercury), modern LED-backlit LCDs are environmentally friendly. They do not emit X-rays and are generally compliant with modern RoHS (Restriction of Hazardous Substances) standards.

(3) Power Efficiency: The most significant advantage of LCD technology is power consumption. A traditional 17-inch CRT monitor could consume over 80W. In contrast, a modern 24-inch LED-backlit LCD typically consumes between 20W and 30W. This drastic reduction in wattage translates to lower thermal output and significant electricity savings in corporate environments.

Ⅲ LCD types

Based on the backlight source technology, LCDs are primarily categorized into two generations: CCFL (Legacy) and LED (Standard/Modern).

Common Misconception: LED vs. LCD

Consumers often mistake "LED" and "LCD" for two entirely different display technologies. This confusion stems from marketing terminology used by TV manufacturers.

LCD

LCD display

Technically, the "LED TVs" sold on the market are actually LED-backlit Liquid Crystal Displays. The panel itself remains an LCD (utilizing liquid crystals to block or pass light). The difference lies solely in the backlighting: earlier generations used CCFL (fluorescent tubes), while modern displays use LEDs (Light Emitting Diodes). High-end variations for 2025 include Mini-LED and Quantum Dot (QLED), which are advanced forms of LED-backlit LCDs.

In summary: LCD is the overarching technology. LED refers to the specific method of lighting that LCD panel.

(1) CCFL (Cold Cathode Fluorescent Lamp)

This is the legacy standard. CCFL displays offer good color consistency but are thicker, run hotter, and consume more power. They also contain small amounts of mercury, making them harder to recycle. These are rarely produced in 2025.

(2) LED (Light Emitting Diode)

This is the current industry standard. WLED (White LED) backlighting allows displays to be incredibly thin and energy-efficient. While early LEDs struggled with color accuracy compared to CCFL, modern IPS and VA panels with LED backlighting provide superior brightness and contrast. Advanced iterations like Mini-LED use thousands of tiny LEDs to provide "local dimming," rivaling OLED contrast levels.

Ⅳ LCD working principle

The fundamental principle of an LCD is that liquid crystals change their molecular alignment when an electrical voltage is applied, thereby modulating the passage of light. Liquid crystals do not emit light themselves; they act as "light valves" that block or allow light from the backlight to pass through color filters.

LCD basic structure

LCD basic structure

The most common modern structure is the TFT (Thin Film Transistor) Active Matrix. In this architecture, every pixel is controlled by a transistor acting as a switch. The transistor controls the voltage stored in a capacitor at each sub-pixel (Red, Green, Blue). This voltage determines the angle of the liquid crystal molecules, which in turn dictates how much light passes through the polarizing filters to reach the viewer.

(1) Passive-matrix type (TN/STN)

Note: This technology is largely obsolete for high-resolution displays but explains the foundational physics.

In a Twisted Nematic (TN) LCD, the panel consists of two glass substrates with alignment films and polarizers. Without voltage, the liquid crystal molecules twist 90 degrees, guiding light from the rear polarizer through to the front polarizer, making the pixel appear "white" (or transparent).

When voltage is applied, the liquid crystals untwist and align vertically. This breaks the light path—the polarized light is blocked by the front polarizer, causing the pixel to appear black. By varying the voltage, the degree of twist changes, allowing different amounts of light to pass (grayscale).

IPS LCD and TN LCD

IPS LCD vs TN LCD pixel structure

(2) Active-matrix type (TFT)

TFT-LCD improves upon passive matrix by placing a transistor at every pixel location. In a 1080p display (1920x1080), there are over 6 million sub-pixels, each with its own tiny transistor.

The TFT acts as an active switch. When a row of pixels is addressed, the TFTs turn on to charge a capacitor. When the row is deselected, the TFT turns off, trapping the charge in the capacitor. This holds the liquid crystal in the correct state until the next refresh cycle. This "sample and hold" method prevents the "ghosting" and low contrast issues seen in older passive displays, allowing for the high frame rates and sharp images required for modern video and gaming.

Ⅴ Future Trends in LCD Technology

While emerging technologies like OLED and Micro-LED are gaining traction, LCD technology continues to dominate the market through significant evolution. In 2025, several key trends are ensuring the relevance of LCDs in computing, automotive, and industrial applications.

(1) Mini-LED Backlighting

The most significant upgrade to LCDs is the transition to Mini-LED. By replacing traditional edge-lit LED strips with thousands of microscopic LEDs behind the panel, manufacturers can create hundreds or thousands of "local dimming zones." This allows LCDs to achieve true blacks and HDR (High Dynamic Range) performance that rivals OLED, without the risk of screen burn-in.

(2) Quantum Dot Enhancement (QLED)

Quantum Dot layers are now being standardly integrated into premium LCDs. These microscopic particles emit light at very precise wavelengths when hit by the blue LED backlight, resulting in a significantly wider color gamut and higher brightness efficiency than standard LCD filters.

(3) Ultra-High Refresh Rates

For the gaming and esports sector, LCD technology (specifically "Fast IPS" panels) remains superior in speed. Monitors reaching 500Hz and even 540Hz are becoming available, providing motion clarity that other display technologies currently struggle to match at consumer price points.

(4) Automotive Smart Cockpits

The automotive industry relies heavily on LCDs for durability and temperature resistance. The trend is shifting toward "pillar-to-pillar" screens—single, massive curved LCD units that span the entire dashboard, integrating instrument clusters and infotainment into a seamless interface.

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1.What is better LED or LCD?

While a standard LCD monitor uses fluorescent backlights, an LED monitor uses light-emitting diodes for backlights. LED monitors usually have superior picture quality, but they come in varying backlight configurations. And some backlight configurations create better images than others.

2.What does an LCD screen look like?

In an LCD TV screen, much smaller pixels colored red, blue, or green make a brightly colored moving picture. For many people, the most attractive thing about LCD TVs is not the way they make a picture but their flat, compact screen. Unlike an old-style TV, an LCD screen is flat enough to hang on your wall.

3.Is LCD better for your eyes?

Both LCD and LED make use of Liquid crystal display, but the difference lies in the backlight, which is majorly responsible for the effect on the eyes. The regular LCDs use a cold fluorescent cathode display backlight, and the LED uses Light Emitting diodes. The LED backlighting is smaller and much safer for the eyes.

4.What are the advantages of LCD?

1) Energy Efficient. LCDs are known for their energy-efficient properties.   2) Long-Lasting. Another advantage of LCDs is their ability to last for a very long time.   3) LED Backlighting.   4) No Screen Burn-In.   5) Supports Small and Low-Profile Sizes.

5.What is the function of LCD?

LCD uses a liquid crystal to produce a visible image. Liquid crystal displays are super-thin technology display screens that are generally used in laptop computer screens, TVs, cell phones, and portable video games.

6.Can an LCD screen be fixed?

It may cost $100 or more to repair a cracked LCD TV screen. It is possible to replace TV screens, but it is a major repair. It usually means replacing the entire display panel. The cost of a replacement screen is almost as high, or higher than the cost of a new TV.

7.What is the liquid in an LCD screen?

The basis of LCD technology is the liquid crystal, a substance made of complicated molecules. Like water, liquid crystals are solid at low temperatures. Also like water, they melt as you heat them. But when the ice melts, it changes into a clear, easily flowing liquid.

8.What happens when the LCD is broken?

Because the LCD and Digitizer are fused together, damaging the LCD will cause the touch function no to work. LCD damage will usually show colored spots around the screen and or lines. You can get a broken LCD by simply dropping the phone or even sitting on it.

9.Is IPS LCD good for the eyes?

IPS LCD screens have good viewing angles and are better for outdoor use compared to AMOLED displays. However, none of them are necessarily better for your eyes. In other words, both can be equally dangerous for your eyes.

10.How is LCD made?

Liquid crystal display (LCD) screens are manufactured by assembling a sandwich of two thin sheets of glass. On one of the sheets are transistor “cells” formed by first depositing a layer of indium tin oxide (ITO), an unusual metal alloy that you can actually see through.
Related Articles

  • The Introduction to Common Tools and Using Methods of Fiber Optic
    The Introduction to Common Tools and Using Methods of Fiber Optic
    UTMEL07 January 20227106

    The building and maintenance of optical cables in the intelligent industry has gradually expanded with the rapid expansion of the Internet of Things and 5G technologies, resulting in an increase in demand for various optical fiber tools. Cutting shears, for example, come in a variety of shapes and sizes, and each tool serves a different purpose. Do you have any experience with them? When should you utilize certain fiber optic tools?

    Read More
  • What are Fiber Optic Patch Cables?
    What are Fiber Optic Patch Cables?
    UTMEL11 February 20228155

    Hello everyone, I am Rose. Today I will introduce fiber optic patch cables to you. Optical fiber communication, as an emerging technology, has become one of the main pillars of modern communication and plays a critical role in modern telecommunication networks, thanks to the rapid growth of traffic data.

    Read More
  • Basis of Fiber Optic and Fiber Optic Communication
    Basis of Fiber Optic and Fiber Optic Communication
    UTMEL22 October 20215091

    Hello everyone, I am Rose. Today I will introduce fiber optic to you. Fiber Optic is a type of glass or plastic fiber that can be utilized to transmit light. It is mostly used for communication. This article will show you the basic knowledge of fiber optic and fiber optic communication.

    Read More
  • The History of Microscope
    The History of Microscope
    UTMEL21 October 20217973

    Hello, everyone. I am Rose. Today I will show you the history of microscopes. The microscope is used to magnify tiny objects into instruments that can be seen by human eyes. Microscopes are divided into optical microscopes and electron microscopes.

    Read More
  • What is VCSEL?
    What is VCSEL?
    UTMEL28 October 202111731

    Hello everyone, I am Rose. I welcome you on board, today I will introduce VCSEL to you. The Vertical-Cavity Surface-Emitting Laser (VCSEL, or Vertical-Cavity Surface-Emitting Laser) is a semiconductor whose laser is emitted perpendicular to the top surface. It differs from an edge-fired laser, which emits the laser from the edge.

    Read More