Sort by
What is speaker?08 October 2021
Hi, fellas. Welcome back to the new post today. The speaker is a type of transducer that converts electrical signals to auditory signals. The sound quality is greatly influenced by the speaker's performance. This article introduces some basic knowledge of the speaker.
What is a Switched Reluctance Motor?09 July 2024
Switched reluctance motor is a type of speed-regulating motor developed after DC motor and brushless DC motor. Product power levels range from several watts to hundreds of kilowatts, and are widely used in household appliances, aviation, aerospace, electronics, machinery, and electric vehicles.
What are Proximity Sensors?24 October 2025
The proximity sensor is a general term for a sensor that replaces contact detection methods such as limit switches. It aims to detect without contacting the detection object. It can detect the movement information and presence information of the object into electrical signals.
Introduction to UFS (Universal Flash Storage)23 July 2021
UFS (Universal flash storage) is a flash storage specification designed for use in consumer electronic products such as digital cameras and smartphones. Its design goal is to develop a unified flash memory card format. While providing high data transmission speed and stability, it can also reduce consumer confusion about various memory card formats on the market.
Basic Introduction to RF Connector30 October 2025
The RF connector is a component that connects to the coaxial cable, microstrip line or other RF transmission line to realize the electrical connection and separation of the transmission line, or to transfer different types of transmission lines. It belongs to the electromechanical integration product and acts as a bridge.
Antenna: Principles, Performance Parameters and Classification15 November 2021
An antenna is a transducer that takes a guided wave propagating on a transmission line and transforms it into an electromagnetic wave propagating in an unbounded medium (usually free space) or vice versa. It is a component used in radio equipment to transmit or receive electromagnetic waves.
RF Mixer: Types, Applications, and Practical Guide12 May 2025
Comprehensive guide to RF mixers covering their types, functionality, applications in wireless communications, performance metrics, and comparisons of top products.
Fiber Optic Connectors Explained: LC, SC, ST, FC and How to Choose14 July 2026
This guide walks through what the connector actually does, the families you will meet in the field, the difference between UPC and APC endfaces, how to tell similar plugs apart, and a practical way to choose for your own link.
What is Gallium Nitride(GaN)?19 January 2021
GaN is a very stable compound and a hard high melting point material with a melting point of about 1700°C. GaN has a high degree of ionization, which is the highest (0.5 or 0.43) among III-V compounds. Under atmospheric pressure, GaN crystals generally have a hexagonal wurtzite structure. It has 4 atoms in a cell, and the atomic volume is about half of GaAs. Because of its high hardness, it is also a good coating protection material.
RF Modulator: Working Principle and Development Trend21 April 2021
An RF modulator is an electronic device that provides a baseband signal, which is used to convert radio frequency resources.There are many RF modulators available, but all functions work in a similar way.
Everything You Need to Know about Connectors07 September 2021
Electrical connectors, as key components for current or signal connections, are also an important part of the industrial system. Connectors can be as huge as airplanes and rockets or as small as mobile phones and televisions, forming bridges between circuits or other components and serving as electric current or signal links.
nF Capacitors: Definition, Conversion, Circuit Applications, and Selection11 August 2026
This article will serve as a detailed roadmap, guiding you through the fundamental concepts, practical identification methods, essential conversion techniques, and diverse applications of nF capacitors. We’ll also touch upon common failure modes and provide strategies for effective selection, ensuring you’re well-equipped to integrate these vital components into your designs.


Product
Brand
Articles
Tools