Sort by
How to Test and Diagnose CAN Bus Transceiver Failures07 June 2025
Learn how to test and diagnose CAN bus transceiver failures, identify common issues like communication errors, and ensure reliable network performance.
What is RF Switch?16 November 2021
Hello everyone, I am Rose. Welcome back to the new post today. The microwave switch, also known as a radio frequency switch, performs the conversion function required to regulate the microwave transmission channel. An RF (Radio Frequency) or microwave switch is a device that allows high-frequency signals to be routed across a transmission line.
PCB Design Guidelines21 December 2021
Hello everyone, I am Rose. Today I will provide you a comprehensive guideline of PCB design.
RF Front End in the 5G Era25 October 2021
The RF front end is a core component of wireless communication equipment and is the basic component that converts wireless electromagnetic wave signals and binary digital signals into each other.
What are Tilt Sensors?19 December 2020
Tilt sensors are often used to measure changes in the horizontal angle of the system. The level from the simple bubble level in the past to the current electronic level is the result of the development of automation and electronic measurement technology.
Differential Amplifier vs Current Sense Amplifier07 April 2022
Hello everyone, I am Rose. Welcome to the new post today. Today I will compare two amplifier to you. Differential amplifier and current sense amplifier.
Utmel, China's Leading Overseas Component Distributor, at PCIM Europe 202310 November 2023
PCIM Europe 2023, a 3-day event, was held in Nuremberg, Germany from May 9 to 11, 2023.
Types and Application of Position Sensors31 October 2025
A position sensor is a sensor that can sense the position of the measured object and convert it into a usable output signal. There are mainly two types of position sensors: the contact type and proximity type. They’re usually applied in brushless DC motors or as Crankshaft and Camshaft position sensors in automobiles.
What is Band Pass Filter?17 November 2021
Hello everyone, I am Rose. Today I will introduce band pass filter to you. A band pass filter is defined as a circuit that permits a signal to flow between two frequencies.
What is 4G Router?27 September 2021
Hello, I am Rose. Welcome to the new post today. The 4G Router is a high-speed industrial Internet of Things router, which is fully compatible with 4G/3.5G/3G networks, supports VPN links, industrial-grade protection, and a wide-temperature design. This article will introduce 4G Router in 6 aspects.
Semiconductor Material Industry Guide21 January 2022
This article mainly introduces the classification of semiconductor materials and the characteristics of the semiconductor material industry.
What is a DC-to-DC Converter?23 April 2021
DC-DC converter, also known as a DC-to-DC converter or DC transformer, is a circuit or electromechanical device that converts electrical energy. It can convert a direct current (DC) power source into a direct current power source (or approximate DC) of different voltages. Its power range is from very low (small batteries) to very high (high-voltage power transmission). The output voltage of some DC-DC converters has the same reference point as the input voltage, while the output voltage of some DC-DC converters is isolated from the input voltage.


Product
Brand
Articles
Tools