Sort by
CR2450 vs CR2032 Batteries18 June 2025
CR2450 vs CR2032: CR2450 offers higher capacity and is larger, ideal for high-drain devices, while CR2032 suits compact, low-power gadgets. Learn more.
What is Digital Power Supply?10 November 2020
The digital power supply is mainly the external characteristics of switching power supply. One is the "communication" function of the digital power supply, the second refers to the "NC" function of the digital power supply, and the third refers to the “monitoring” function of the digital power supply, for example, to temperature and other parameters.
AI Server MLCCs: Why NVIDIA Rubin Racks Require Over 600,000 Capacitors02 June 2026
Next-generation AI servers like NVIDIA's Rubin architecture require over 600,000 MLCCs per rack due to extreme power densities exceeding 120kW. This transition from GB300 demands high-capacitance, low-ESR capacitors with X7R/X7S dielectrics to handle intense transient responses and thermal loads, forcing procurement teams to navigate extended 24-week lead times for these specialized components.
Top-Rated AG13 Battery Equivalent Substitutes22 August 2025
Find the best AG13 battery equivalent options like LR44, SR44, and A76, plus where to buy trusted substitutes for your devices in 2025.
LPDDR5 Memory 2026: Lead Times, HBM Impact, and Procurement Strategies17 July 2026
Global semiconductor fabrication facility managing advanced memory production. In Q2 2026, contract prices for 12GB LPDDR5X modules surged 89% quarter-over-quarter, jumping from $77.10 to $145.90, while lead times for advanced memory components stretched to 40–58 weeks. A vehicle platform designed in 2023 with specific memory requirements must ship in 2026, regardless of spot market conditions.
Semiconductor Market Predicted to Witness Significant Growth by 202319 September 2023
A recent report by The Express Wire predicts significant growth in the global Semiconductor market by 2023. The market has already witnessed growth from USD million to USD million from 2017 to 2022. W
Apple Will Help TSMC to Be in the Leading Position in the Next Era16 March 2022
On March 16, Apple reportedly launched its latest computer, the Mac Studio, last week, and the hot product at the launch was the processor chip that serves as the core.
A76 Battery Equivalent Pros and Cons Explained29 August 2025
Compare a76 battery equivalent options like LR44, AG13, 357, and SR44. See pros, cons, and which type fits your device’s needs best.
A brief Analysis of the 555 Timer Circuit and its Project Applications15 March 2024
This blog is a brief introduction of 555 Timer, it will show up its project applications and circuit diagram.
What is a Vibration Sensor?24 October 2025
The vibration sensor is used to detect the impact force or acceleration of the sensor. It usually uses piezoelectric devices which will generate charge under a stress. The vibration sensor can be used for long-term monitoring of vibration and displacement, thermal expansion amount of rotor, and chassis.
Top Batteries That Can Replace LR4409 June 2025
Find the best LR44 equivalent batteries like SR44, 357, AG13, and A76. Compare their voltage, capacity, and performance for your device's needs.
STMicroelectronics: The European Powerhouse in Silicon Carbide Semiconductor Technology05 October 2023
STMicroelectronics (NYSE:STM), a leading semiconductor manufacturer in Europe, is making significant strides in the realm of silicon carbide technology.


Product
Brand
Articles
Tools