Sort by
What is PWM "Dead Band"?21 April 2022
Hello everyone, I am Rose. Today I will introduce PWM dead band to you. This article includes its definition.
Nearly 60% of the Industry Believes That the Chip Shortage Will Be Solved in 2023 at the Earliest21 April 2022
When will the chip shortage be solved? According to the "2022 Global Semiconductor Industry Survey" released by KPMG Anhou & Associates, 56% of leaders believe the chip shortage will not end until 2023, while 42% believe the shortage will end by the end of 2022.
Foreign Media Burst Samsung: DRAM, Foundry and Chip Defeat on All Fronts20 April 2022
According to industry media EMI analysis, Samsung Electronics, and more specifically Samsung's various semiconductor divisions are on fire.
Towards an Optoelectronic Chip That Mimics the Human Brain20 April 2022
How does the human brain, made up of some 86 billion neurons connected in neural networks, perform extraordinary feats of computation, but consume only a dozen watts?
Semiconductor Cleaning: Processes, Methods and Reasons20 April 2022
Hello everyone, I am Rose. Today I will introduce semiconductor cleaning to you. Including how to clean semiconductor, what method we use to clean semiconductor and why we need to clean semiconductor.
TinyML Takes a Major Step Forward as Israeli Company Releases New Chip19 April 2022
TinyMCE, or optimizing machine learning (ML) models to run on resource-constrained devices, is one of the fastest-growing subfields of ML. To achieve this ultra-low-power, high-performance computing required by TinyML (or sometimes called TinyAI), engineers have explored a number of exciting new technologies.
Samsung: 3nm Yield Rate of 20%19 April 2022
According to foreign media Phonearena, Samsung foundry is the second-largest independent foundry in the world after the giant TSMC. In other words, in addition to manufacturing its own designs for Exynos chips, Samsung also makes chips based on designs submitted by third-party companies such as Qualcomm and other foundry customers.
Does the Terminal Resistance of the CAN Bus Have to be 120Ω?19 April 2022
Hello everyone, I am Rose. Today I will introduce Controller Area Network(CAN)to you. Knowing the function of terminal resistor will help us better understand causes of waveform instability and other problems in daily work.
Inductance Basis: Definition, Structure and Applications18 April 2022
Hello everyone, I am Rose. Today I will introduce inductance to you. Inductance is a property of a closed loop and a physical quantity. It is a circuit parameter that describes the induced electromotive force effect in this coil or in another coil due to changes in coil current. Inductance is a general term for self-inductance and mutual inductance. A device that provides an inductance is called an inductor.
Selection and Optimization of Peripheral Components for DC-DC Boost Regulator15 April 2022
Hello everyone, I am Rose. Welcome to the new post today. This article will introduce the features of boost regulator and how to choose peripheral components for the dc-dc boost converter.
Gartner: Hysis Revenue Plunges 81%, Samsung Holds on to Semiconductor Leadership15 April 2022
Worldwide semiconductor revenues total $595 billion in 2021, up 26.3 percent from 2020, according to final statistics from Gartner, Inc. "The events behind the current chip shortage continue to impact original equipment manufacturers (OEMs) globally, but the rise of 5G smartphones and strong demand and rising logistics/raw material prices are driving semiconductor average selling prices (ASPs) higher, said Andrew Norwood, research vice president at Gartner.
What is Tantalum Capacitor: Structure, Failure and Application Guide14 April 2022
Hello everyone, I am Rose. Welcome to the new post today. Today I will introduce tantalum capacitors to you. This article includes its structure, production process,failure mode, precautions and application guide and so on.


Product
Brand
Articles
Tools