web counter

Samsung: 3nm Yield Rate of 20%

Published: 19 April 2022 | Last Updated: 19 April 20225748
According to foreign media Phonearena, Samsung foundry is the second-largest independent foundry in the world after the giant TSMC. In other words, in addition to manufacturing its own designs for Exynos chips, Samsung also makes chips based on designs submitted by third-party companies such as Qualcomm and other foundry customers.
Intel has rebranded their manufacturing process nodes. What was once 10nm is now 7nm, through the power of a press release. To be fair to Intel, their 10nm is competitive with the 7nm processes from Samsung and TSMC, the other big players in the chip-making space, and the rename realigns each companies nodes to be roughly comparable. In addition to the rename, Intel also gave us info on their upcoming CPU tech, including EMIB in the planned Meteor Lake CPUs, and two new styles of Foveros stacked / 3D chips. Intel's plan goes as a far as ambitious 18 angstrom (or 1.8nm) node that they plan to be producing by 2026. That sounds awfully fast to me, but hey, we all need goals.

Intel has a plan to go beyond 3nm chips | Upscaled

According to foreign media Phonearena, Samsung foundry is the second-largest independent foundry in the world after the giant TSMC. In other words, in addition to manufacturing its own designs for Exynos chips, Samsung also makes chips based on designs submitted by third-party companies such as Qualcomm and other foundry customers.

The Snapdragon 865 application processor (AP) is built by TSMC using its 7nm process node. With the 5nm Snapdragon 888 chipset, Qualcomm went back to Samsung and continues to rely on the Korean foundry to produce the 4nm Snapdragon 8 Gen 1. This is the AP that currently powers high-end Android phones made by Samsung, Xiaomi, and Motorola.


Samsung-3nm-gaa-image.png


Samsung Foundry Continues to Struggle with Yield Rates


But in February, it was reported that Samsung Foundry's yield at its 4nm process node was only 35%. That means only 35 percent of the die-cut from wafers will pass quality control. By comparison, TSMC achieved a 70% yield on its 4nm Snapdragon 8 Gen 1 Plus. In other words, all things being equal, TSMC manufactured twice as many chips as Samsung foundries in the same period.

This results in TSMC eventually receiving orders from Qualcomm to build its remaining Snapdragon 8 Gen 1 chipset as well as the Snapdragon 8 Gen 1 Plus SoC. We also assume that TSMC will be licensed to build the 3nm Snapdragon 8 Gen 2, even though Qualcomm will need to pay a premium to TSMC to allow the exclusive manufacturer of that chipset to build enough chips in a short period of time to make enough chips.

Although Samsung has recently said its yields have been increasing, a Business Post report says Samsung's 3nm process node yields are still well below the company's target. While Samsung Foundry's all-ring gate (GAA) transistor architecture debuted its 3nm node, putting it ahead of TSMC (which will launch its GAA architecture for its 2nm node), Samsung Foundry's yields in its early 3nm production have been in the 10 to 20 percent range.

Not only is this a very low yield that Samsung needs to improve, but it is worse than the aforementioned 35% yield that Sammy experienced in the 4nm Snapdragon 8 Gen 1.

Wccftech said that according to sources, the first "performance version" of the 3nm GAA chipset that Samsung will ship to customers starting next year could actually be the new internal Exynos chip. Samsung has reportedly been developing a new family of Exynos chips for its smartphones, but it's unclear at this stage whether they will be manufactured using the 3nm GAA process node.


Samsung 3nm Yield Rate of 20%.png


TSMC and Samsung Will Soon Have New Challengers For Process Leadership


TSMC and Samsung will soon have new challenges as Intel has said it aims to take over the industry's process leadership by the end of 2024. It has also been the first to acquire a more advanced extreme ultraviolet (EUV) lithography machine.

The second-generation EUV machines are called High NA or high numerical aperture. The current EUV machine has an NA of 0.33, but the new machine has an NA of 0.55. The higher the NA, the higher the resolution of the circuit pattern etched on the wafer. This will help chip designers and foundries make new chipsets that contain even more transistors than the billions of transistors used on current integrated circuits.

It will also prevent foundries from running wafers through the EUV machine again to add additional features to the chip. small said that the higher resolution patterns produced by the second generation EUV machine will provide higher resolution will make the chip features 1.7 times smaller and the chip density 2.9 times higher.

By getting this machine first, Intel will be able to take a big step toward its goal of reclaiming process leadership from TSMC and Samsung.

 

Samsung 3nm Yield Rate of 20%.jpg


Related News

1、Chip Packaging Lead Time Has Grown to 50 Weeks

2、Eight Internet of Things (IoT) Trends for 2022

3、Demand for Automotive Chips Will Surge 300%

4、Volkswagen CFO: Chip Supply Shortage Will Continue Until 2024

5、BMW CEO: The Car Chip Problem Will Not Be Solved Until 2023

6、Shenzhen: This Year Will Focus on Promoting SMIC and CR Micro 12-inch Project



UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Related Articles

Subscribe to Utmel !

Featured Parts More