Classification and Working Principle of Ballast Resistor

How the Ballast Resistor Works?
Catalog
Ⅰ Introduction
A ballast resistor is a device that limits current and generates an instantaneous high voltage on fluorescent lamps. It is made by winding enameled wire on an iron core made of silicon steel. When such a coil with an iron core turns on/off in an instant, it will self-induce and generate high voltage, which is applied to the electrodes (filaments) at both ends of the fluorescent tube. This action is performed alternately. When the starter (jumping bulb) is closed, the filament of the lamp tube passes through the current limit of the ballast and conducts heat; when the starter is open, the ballast will self-induct and generate a high voltage on the filaments at both ends of the tube. The filament emits electrons to bombard the fluorescent powder on the tube wall to emit light. The starter is repeatedly turned on and off several times, and this action will be repeated several times to open the tube. When the lamp tube emits light normally, the internal resistance becomes smaller, and the starter always keeps an open circuit state. The current will stably pass through the lamp tube and the ballast to work so that the lamp tube emits light normally. Since the ballast always has current passing through when the fluorescent lamp is working, it is easy to produce vibration and heat. Ballast resistors are divided into electronic ballasts and inductance ballasts.
Ⅱ History and development
In the late 1980s, the United States applied toroidal inductive ballasts to compact energy-saving fluorescent lamps. In 1988, Midwest Toriod began mass production.
There was a worldwide energy crisis in the 1970s. The urgency of saving energy made many companies devote themselves to the research of energy-saving light sources and electronic ballasts for fluorescent lamps. With the rapid development of semiconductor technology, various high back-pressure power switching devices continue to emerge, providing conditions for the development of electronic ballasts. At the end of the 1970s, manufacturers took the lead in launching the first generation of electronic ballasts, which was a major innovation in the history of lighting development. Because of its many advantages such as energy-saving, it has attracted great attention and interest all over the world. It is considered to be an ideal product to replace inductive ballasts. Later, some famous enterprises have invested considerable manpower and material resources to carry out higher-level research and development. Due to the rapid advancement of microelectronics technology, the development of electronic ballasts in the direction of high performance and high reliability has been promoted. Many semiconductor companies have introduced a series of dedicated power switching devices and control integrated circuits. In 1984, Siemens developed TPA4812 active power factor correction electrical IC whose power factor reaches 0.99. Subsequently, some companies have successively introduced integrated electronic ballasts. In 1989, Helvali, Finland, successfully launched dimmable monolithic integrated circuit electronic ballasts. Electronic ballasts have been promoted and applied throughout the world, especially in developed countries.
Ⅲ Classification and working principle
1 Classification of the ballast resistor
From the working principle, it can be divided into inductive ballast and electronic ballast; according to the installation mode, it can be divided into independent, built-in, and integral types; from the starting method, it can be divided into preheating start, cold start (or Instant start) types.
2 Inductive ballast
As shown in the figure below, when 220V 50HZ AC power is applied to the switch closed circuit, the current flow through the ballast, and the lamp filament starter heats the filament. The starter is disconnected at the beginning. Because an AC voltage greater than 190V is applied, the gas arc discharge in the jumping bubble in the starter. Then the two metal sheets deformed by heat, and the two electrodes are close together to form a path to heat the filament. When the two electrodes of the starter are close together, because there is no arc Discharge, bimetallic cooling, and the two poles are separated. Because the inductive ballast is inductive, when the circuit is suddenly interrupted, a pulse voltage of 600V-1500V with a duration of about 1ms will be generated at both ends of the lamp. The exact voltage value depends on the lamp. In the case of discharge, the voltage across the lamp drops immediately. At this time, the ballast resistor limits the lamp current. And on the other hand, the ballast resistor makes a phase difference of 55 to 65 between the power supply voltage and the lamp operating current. The phase difference of the lamp can maintain the secondary starting voltage of the lamp so that the lamp can work more stably.

Due to its simple structure, inductive ballast, as the first type of ballast resistor to work with fluorescent lamps, has a relatively large market share. Due to its low power factor, poor low-voltage starting performance, heavy energy consumption, stroboscopic, and many other shortcomings. Its market share is gradually being replaced by electronic ballasts. The energy loss of inductive ballasts: 40W (lamp power) + 10W (inductive ballast self-heating loss) is equal to the total power consumption of the whole set of lamps and lanterns which is 50W.
3 Electronic ballast
The electronic ballast is a converter that converts power frequency AC power to high-frequency AC power. Its basic working principle is:
As shown in the figure below, after the industrial frequency power supply passes through the radio frequency interference (RFI) filter, full-wave rectification, and passive (or active) power factor corrector (PPFC or APFC), it becomes a DC power supply. Through the DC/AC converter, the output of high-frequency AC power of 20K-100KHZ is added to the LC series resonant circuit connected to the lamp to heat the filament, but the lamp is "discharged" into the "on" state, and then enters the light-emitting state. The high-frequency inductor plays a role in limiting the increase of current, ensuring that the lamp tube obtains the lamp voltage and lamp current required for normal operation. In order to improve reliability, various protection circuits are often added, such as abnormal protection, surge voltage, and current protection, temperature protection, and so on.

Schematic diagram of electronic ballast

Detailed schematic diagram of electronic ballast
1 How do we know if the ballast is broken?
(1) First of all, we can look at the appearance of lamps and ballasts. If the ballast is burned out, the shell will turn black. (2) It can also be detected with an electric pen. If there is no electricity at the incoming and outgoing ends and the incoming end of the shell, it means that the ballast is broken, causing the incoming fuse to be short-circuited. The incoming end has electricity but the outgoing end does not mean that the internal circuit of the ballast is open, and that the shell is electrified means that the ballast is leaking. (3) If both the incoming and outgoing ends have electricity, the shell is not electrified, and the light is not on, you can also judge by replacing the trigger. If you change the trigger and still don't light up, the ballast is broken. (4) It is best to use a multimeter to measure the resistance of the coil with 200 gears. If there is resistance, it means that there is no problem with the coil. If the resistance is infinite, it means that the coil is open and damaged.
2 How to connect the two wires of the ballast resistor?
We first keep the lamp energized and then use an electric pen to test the incoming wires of the fluorescent lamp. Under normal circumstances, there is no distinction between the live line and the neutral line, the details are as follows: If it is an old-fashioned ballast with an iron core, under normal circumstances, the live wire can be connected to any one of the two wires of the ballast, and the two incoming wires of the ballast are not divided into the neutral wire and the live wire. If it is an electronic ballast, then there is no distinction between the neutral wire and the live wire under normal circumstances, but if the two wires are the same color wire, there can be no distinction between the neutral wire and the live wire; but if the two wires are of two types different color wires, then at this time the red wire is connected to the live wire, and the remaining wire is connected to the neutral wire.
3 Where does a ballast resistor go?
Note: Ballast resistors are usually located bolted to the firewall if your distributor and/or coil are at the rear of the engine. If your distributor is located near the front or side of the engine in the case of an inline-4 cylinder, then it's probably right near the ignition coil or distributor.
4 Why do ignition coils need a ballast resistor?
Due to its application, such devices are called Ignition Ballast Resistor. The use of this device reduces the risk of coil failure. It is installed in the circuit between the primary voltage source for the ignition coil and the coil stud. This jumper wire provides the necessary voltage to make the engine start.
5 How many ohms should a ballast resistor have?
3.0 Ohms External Resisted Ignition Coils have an internal resistance of 1.5 Ohms, and when combined with the Ballast Resistor, you get a total resistance of 3.0 Ohms which is necessary for 12 Volt ignitions systems.
Classification and Working Principle of Ballast ResistorUTMEL18 November 20208233The ballast resistor is connected between the power source and one or more discharge lamps and is mainly used to limit the current of the lamp to a required value. It may include devices that change the supply voltage or frequency and increase the power factor, which can be used alone or together with the starter to provide the necessary conditions for the lamp to start.
Read More
What is Electronic Ballast?UTMEL28 September 202015574Electronic Ballast is a kind of ballast, which uses electronic technology to drive the electric light source to produce the required lighting. Corresponding to it is the inductive ballast. More and more modern fluorescent lamps use electronic ballasts, which are light and compact, and people can even integrate electronic ballasts with lamps.
Read More
Subscribe to Utmel !
VE2220K122R017KEMET
JK-A0100EU-2Cherry Americas LLC
![B72210S500K551]()
HC230W9B3M
VDRS10D030TSEVishay
![B72540V140K62]()
P137-06N-VGA-V2Tripp Lite
VAR-18042077M3S-XKTDK Corporation
VE1812L501R008KEMET
2920447Phoenix Contact


Product
Brand
Articles
Tools