web counter

FPGA vs. Microcontroller Technology: Similarities and Differences

Published: 22 March 2023 | Last Updated: 13 March 20245947
The article will introduce the Similarities and Differences between FPGA and Microcontroller Technology.

Field-programmable gate arrays (FPGAs) and microcontrollers share similarities but are not identical. Both are compact computing units or integrated circuits within various devices and products. The primary distinction lies in their programmability. FPGAs can be programmed at the hardware level post-manufacturing, making them "field-programmable." At the same time, the microcontroller technology offers customization on a more limited scale. Moreover, FPGAs can process parallel inputs, whereas microcontrollers execute one code line at a time.

FPGAs provide increased personalization, with higher costs and more complex programming. On the other hand, microcontrollers are affordable yet offer limited customization. To understand the nuances between microcontrollers and FPGAs, delve deeper into their similarities and differences. Choosing between them is not a matter of superiority but requires consideration of various factors.

What is the Microcontroller Technology?

A microcontroller (MCU) is a compact computer designed for a specific purpose. It shares common components with other computers, such as a CPU, RAM, and input/output devices. However, unlike a desktop computer capable of executing numerous programs, a microcontroller is engineered to perform a single task repeatedly, autonomously, or upon user command.

Microcontrollers are embedded within various devices across consumer, manufacturing, medical, and other sectors. They are energy-efficient, consuming power in milliamps, making them cost-effective. Nevertheless, the price of the devices they are integrated into can differ significantly.

ü Microcontrollers are pervasive in daily life and found in many consumer items, including keyboards, monitors, printers, photocopiers, fax machines, telephones, TV remote controls, microwave ovens, washing machines and dryers, lawn sprinklers, and children's toys.

ü Apart from consumer products, microcontrollers also serve critical functions in traffic signals, automobile engine control systems, power tools, and implantable medical devices.

The list above only scratches the surface, as microcontrollers are incorporated into many modern devices. Each microcontroller fulfills a specific, recurring function. It may operate independently using a feedback control system (traffic signals) or respond to user input (flipping a switch or pressing a button) applicable to microwaves, washing machines, and TV remote controls.

What is the FPGA Technology?

A field-programmable gate or grid array (FPGA) technology is more complex than a microcontroller technology. Typically, chips arrive with pre-installed programming. Users can modify the software but not the hardware. However, this leads to the distinguishing characteristic of an FPGA – the ability for users to customize its hardware after purchase.

This feature is particularly valuable for engineers when creating prototypes for their application-specific ICs (integrated circuits). Another advantage of FPGAs is that they allow devices incorporating them to be modified without requiring completely new hardware.

Take, for instance, a scenario where regulations require vehicle rear-view cameras to function more quickly. Suppose FPGAs power these cameras. In that situation, manufacturers can implement the necessary adjustments without resorting to costly hardware replacements. Instead, they can reprogram the FPGA within each car's rear-view camera system. This enables modifications to be made to existing vehicles without rendering them obsolete.

Field-Programmable Gate Arrays comprise integrated hardware circuits featuring programmable logic blocks that are not pre-configured for a specific function during manufacturing. Users can customize and modify these devices through a hardware description language (HDL), connecting logic blocks such as AND as well as XOR with interconnects. Modern FPGAs contain numerous logic gates and RAM blocks, which allows for intricate computations. Some even include converters that can convert analog signals to digital or digital signals to analog, similar to FPAAs.

FPGA vs. Microcontroller: How They Match?

FPGA and microcontroller technologies are examples of flexible integrated circuits that allow manufacturers and end-users to specify their devices' particular functionality. Found in various devices such as traffic lights and laundry machines, these tiny, flat, square chips are embedded within these systems to perform specialized applications, making our lives easier.

Although visually similar with programmable pins surrounding them, FPGAs and microcontrollers are miniature computers programmed for distinct purposes, focusing on performing a single function rather than acting as personal or desktop computers. These circuits cater to tasks with varying levels of complexity, following preset commands to execute their designated functions.

Building Blocks

FPGA and microcontroller devices share fundamental similarities, as both are integrated circuits that use computer logic and binary to function. Integrated circuits, composed of semiconductor material like silicon, perform calculations and store data using digital or analog technology, with some FPGAs converting between the two. Digital technology is based on binary logic, while analog technology relies on a linear function of the input to calculate the output. Understanding the basics of computer logic is crucial when programming either a microcontroller or an FPGA.

Customization

FPGAs and microcontrollers offer post-production programmability, allowing manufacturers and end-users to tailor their functions for various applications across diverse industries. FPGAs stand out due to their extensive customization capabilities, making them ideal for complex, highly technical tasks. Simultaneously, microcontrollers are better suited for simpler applications.

FPGA vs. Microcontroller: How They Differ?

The primary distinction between the FPGA and microcontroller technology lies in the degree of personalization and intricacy. Furthermore, they differ in terms of affordability and user-friendliness. In essence, FPGAs offer enhanced adaptability, the capacity to handle more complicated tasks, and the ability to make changes to hardware after the fact. Remember that utilizing an FPGA requires a higher level of expertise and knowledge.

Although FPGAs possess certain benefits, microcontrollers are more affordable and simpler to operate. The majority of enthusiasts or novices would find the microcontroller technology to be a more suitable choice. In contrast, engineering firms and manufacturers might opt for FPGAs.

FPGA vs. Microcontroller: Power Consumption

FPGAs, known for their versatility and high-speed capabilities, often consume more power than microcontrollers, making them less suitable for power-efficient systems. This increased power consumption can be attributed to various factors, like low logic utilization due to place-and-route constraints, unused transistors, inefficient clock trees, and extended signal paths. Despite their use in emulation and prototyping, FPGAs are less power-efficient than components like ASICs.

In contrast, microcontrollers operate at much lower processing speeds, typically in the range of a few MHz, and consume significantly less power than FPGAs. They often feature idle or power-saving modes, enabling more sustainable operation. Some microcontrollers even have sleep currents below 1 µA and can function at just a few µA during slow clock rates. To improve power efficiency in FPGA systems, engineers usually incorporate microcontrollers on the board.

Ultimately, the choice between the FPGA and microcontroller technology should be based on the specific requirements of the project and the user's familiarity with the technology. Please don't hesitate to contact us if you have any more inquiries about FPGA vs. microcontroller technology.


UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

What is the difference between FPGAs and microcontrollers?

A programmable logic device called an FPGA has the ability to change the hardware architecture on the fly to accommodate various application needs. On the other hand, a microcontroller is a single-chip computer with a CPU, memory, inputs/outputs, and other essential peripheral devices that may be used to control and carry out a range of functions.

Which is better for my application, FPGA or microcontroller?

Your application's requirements will determine this. FPGAs might be a better option if you require a great degree of customisation and flexibility. A microcontroller can be a better fit for your application if you need to carry out predetermined functions and need fewer peripherals.

What is the cost difference between FPGAs and microcontrollers?

Because they provide more flexibility and customizability than microcontrollers, FPGAs are often more expensive. This results in cost savings because FPGAs can be utilized again in other applications. On the other hand, because they are created expressly to carry out certain functions, microcontrollers are typically the less expensive option.
Related Articles

  • Getting Started with Arduino: What is Arduino and How to Use Arduino Boards
    Getting Started with Arduino: What is Arduino and How to Use Arduino Boards
    UTMEL28 September 20237419

    Arduino is an open-source electronics platform that includes software and programmable circuit boards, allowing beginners to build electronic projects by writing simple code. The article provides an overview of Arduino, including different board types, basic components, how to use the boards, and project ideas like an automated plant watering system.

    Read More
  • IoT Chips Lead Time 2026: Navigating MCU, PMIC, and Sensor Shortages
    IoT Chips Lead Time 2026: Navigating MCU, PMIC, and Sensor Shortages
    UTMEL15 July 20261258

    Navigating component supply and allocation challenges in the 2026 IoT market. This procurement trend brief provides electronics engineers and component sourcing teams with a data-driven analysis of the IoT chips lead time 2026 landscape, detailing supply bottlenecks and alternative design strategies.

    Read More
  • MCU with Built-in NPU: How to Pick an Edge AI Microcontroller in 2026
    MCU with Built-in NPU: How to Pick an Edge AI Microcontroller in 2026
    UTMEL30 July 20262142

    Evaluating Edge AI microcontrollers requires looking beyond vendor-quoted TOPS metrics. This guide explains how to segment candidate parts into sensor, control, or vision tiers, calculate binding SRAM constraints, verify NPU operator support to avoid CPU fallbacks, and navigate production lifecycle risks. Follow a practical five-step engineering sequence to benchmark real models on physical evaluation boards.

    Read More
  • Top 5 Microcontrollers Defining IoT, Edge AI, and Power Efficiency in 2026: Sourcing and Selection Guide
    Top 5 Microcontrollers Defining IoT, Edge AI, and Power Efficiency in 2026: Sourcing and Selection Guide
    UTMEL15 August 20261052

    This guide reviews the top five microcontrollers defining 2026 embedded designs—ESP32-S3, STM32U5, MSPM0G5187, CH32V003, and nRF54. It evaluates how contiguous SRAM limits, power duty cycling, and hardware acceleration impact edge AI and IoT performance. It also details strategic procurement methods for navigating mature-node supply chain risks, dual-footprint layouts, and component authentication.

    Read More
  • Arduino vs. Raspberry Pi: A Detailed Comparison
    Arduino vs. Raspberry Pi: A Detailed Comparison
    UTMEL24 April 20256039

    Hello everyone, welcome to the new post today.This guide is going to talk in detail about Arduino vs. Raspberry Pi to clarify their differences and help you pick the right board based on your needs.

    Read More

Subscribe to Utmel !

Featured Parts More