web counter

Arduino vs. Raspberry Pi: A Detailed Comparison

Published: 01 November 2023 | Last Updated: 24 April 20256015
Hello everyone, welcome to the new post today.This guide is going to talk in detail about Arduino vs. Raspberry Pi to clarify their differences and help you pick the right board based on your needs.
Topics covered in this article:
Ⅰ. What is Arduino?
Ⅱ. What is Raspberry Pi?
Ⅲ. Arduino vs. Raspberry Pi: Key Differences
Ⅳ. How to Choose Between Arduino vs. Raspberry Pi for Different Scenarios?
Ⅴ. Wrapping Up

Arduino vs. Raspberry Pi.png

Arduino and Raspberry Pi are two very popular boards used in the market. Both single-board computers have their own strengths and weaknesses. This makes it challenging to make one winner over the other. The Arduino board is simpler and easier to use, while the Raspberry Pi offers more processing power to handle complex projects. Therefore, this guide is going to talk in detail about Arduino vs. Raspberry Pi to clarify their differences and help you pick the right board based on your needs.

Ⅰ. What is Arduino?

Arduino is an open-source platform that provides developers an easy way to program and build electronic projects. It involves both software (Integrated Development Environment) and hardware (programmable circuit board).

The Arduino board includes digital Input/Output pins through which it can read inputs from sensors and other devices and produce corresponding outputs, such as turning on an LED, etc. It provides a simplified version of the C programming language, which makes it easy to program and design simple electronic projects.

Arduino Uno is one of the most widely used Arduino boards. So, the key features of Arduino, specific to Arduino Uno, are as follows:

· ATmega328P microcontroller

· 14 Digital Input/Output pins

· 6 Analog Input pins

· 16 MHz clock speed

· 32 KB flash memory

· 2 KB SRAM

· 1 KB EEPROM

In short, Arduino Uno or other types of Arduino boards incorporate all the components users need to create full-fledged electronic projects.

图片1.png

Ⅱ. What is Raspberry Pi?

Raspberry Pi is a fully functional single-board computer, meaning all the hardware is on a single electronics board. The main hardware components include CPU, memory, USB, LAN, micro HDMI ports, etc.

Think of Raspberry Pi as a mini computer that can connect to the computer monitor, mouse, and keyboard. It comes with its own operating system known as Raspberry Pi OS, a Linux-optimized version.

Raspberry Pi 4 Model B is one of the most commonly used Raspberry Pi boards. So, the key features of Raspberry Pi, specific to Raspberry Pi 4 Model B, are as follows:

· Quad-core 64-bit ARM-Cortex A72 processor running at 1.5GHz

· 1-8GB of LPDDR4 RAM

· Dual 4K HDMI outputs

· Two USB 3.0 and two USB 2.0 ports

· Dual-band 2.4/5.0 GHz wireless LAN, Bluetooth 5.0, BLE

· Gigabit Ethernet and PoE capability (with add-on PoE HAT)

· H.265 (4Kp60) and H.264 (1080p60) hardware decoding

· Support for Linux, Raspberry Pi OS, and other operating systems

· Raspberry Pi standard 40-pin GPIO header with various interface options

· Mature Linux software stack with recent Linux kernel support

In short, Raspberry Pi's powerful specs make it able to assist in simple to complex electronic projects that involve multiple inputs and outputs with precise functionalities, such as robotics, IoT, etc.

图片2.png

Ⅲ. Arduino vs. Raspberry Pi: Key Differences

Now that we have cleared the basics of Arduino and Raspberry Pi, let's shift our focus on what are the differential elements between them.

1. Microcontrollers vs. Microprocessors

Arduino boards use microcontrollers (e.g., ATmega series), which are not computers and are meant to mainly do tasks around I/O operations.

Raspberry Pi boards use microprocessors (e.g., ARM Cortex), which are similar to what you see in computers. They are capable of running operating systems and provide computer-like functionality.

2. Operating Systems

Arduino does not come with a dedicated operating system. It works on simple instructions provided through the Integrated Development Environment (IDE). In contrast, Raspberry Pi supports a wide range of operating systems, including its own Raspberry Pi OS.

3. Connective Options

Arduino provides limited I/O pins with limited analog and digital pins. Besides that, it provides a small number of communication ports, mostly a USB port. The communication is mostly based on SPI, UART, and analog pins. In short, you get basic connectivity options with Arduino.

Raspberry Pi offers advanced connectivity options. It comes with more I/O analog and digital pins and a wide range of communication ports, such as HDMI, Ethernet, etc. It can also connect to various USB peripherals, such as mouse, keyboard, webcams, etc.

4. RAM

Arduino boards come with limited memory, ranging around 2-8 KB RAM for different boards. On the other hand, Raspberry Pi comes with more RAM, even ranging up to 8 GB RAM. This means that Raspberry Pi is more suited for complex projects that require more memory.

5. Cost

Arduino boards are cheaper than Raspberry Pi boards. For instance, you can get Arduino UNO REV3 for around $28, while Raspberry Pi 4 Model B (4 GB) costs around $55.

6. Processor & Clock Speed

As mentioned earlier, Arduino includes a microcontroller (e.g., ATmega series) with an average 16 MHz clock speed for most boards. In contrast, Raspberry PI includes a microprocessor (e.g., ARM Cortex) with around 1.5 GHz clock speed. So, the higher clock speed with a powerful processor makes Raspberry Pi best suited for complex projects.

Features

Arduino

Raspberry Pi

License

Open-source hardware and software

Closed-source hardware and software

Processor

AVR Microcontroller

ARM Cortex-A72 (Raspberry Pi 4)

RAM

Less RAM (2 KB)

Large RAM (over 1 GB)

Clock Speed

16 MHz (Arduino UNO)

1.5 GHz (Raspberry Pi 4 B)

Operating System

No dedicated operating system. It works on simple instructions through the Integrated Development Environment (IDE)

Linux-based Raspberry Pi OS operating system, but can also install other OS

Programming Language

C or C++

C, C++, Python, Scratch, and Ruby

Internet

No built-in internet support

Built-in Ethernet port and Wi-Fi support

CPU Architecture

8-bit

64-bit

Cost

Cheaper

Expensive

Ⅳ. How to Choose Between Arduino vs. Raspberry Pi for Different Scenarios?

From the above-detailed comparison, it is evident that Arduino and Raspberry Pi have their own pros and cons. Although Raspberry Pi is a more powerful board than Arduino, it cannot simply replace the usability of Arduino. They both are useful in different scenarios. So, the next question is how to choose between Arduino and Raspberry Pi.

To better understand the different scenarios where Arduino and Raspberry Pi are effective, below we are listing a few sets of projects/tasks where they suit best.

Arduino is usable in:

· Simple robots (robot arm)

· Parking lot counter

· Repetitive tasks (reading from sensors, closing door, turning light on/off)

· Weighing machines

· Smart home devices

Raspberry Pi is usable in:

· Complex, multitasking software

· Sophisticated robots

· Media center to stream local/online content

· Smart home

· Home security

· Industrial applications

In simple words, Arduino is great for simple projects with low power consumption and may involve repetitive tasks. In contrast, Raspberry Pi should be considered as a computer capable of handling any complex project that involves the internet or complex functionalities.

Ⅴ. Wrapping Up

Arduino and Raspberry Pi are globally used due to their ability to perform specified tasks despite being compact in size. Arduino is widely used by beginners or someone working on simple projects. However, Raspberry Pi finds application in complex projects, even at the industrial level. Therefore, this guide will conclude that there is no winner in this comparison. So, it is recommended to pick between Arduino and Raspberry Pi based on the project requirements.

 


UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

Is it better to use a Raspberry Pi or an Arduino?

It all depends on the needs of your project:   The Raspberry Pi is better suited for: projects that need to run a full operating system, projects that need to handle complex calculations, projects that need networking capabilities, multimedia applications, IoT applications that need network connectivity and data processing capabilities, and projects that need a graphical interface. It is essentially a minicomputer.  Arduino is more suitable for: simple hardware control projects, real-time control applications, low-power applications, projects that require precise timing, simple sensor data acquisition, embedded projects that do not require an operating system. It is a microcontroller platform that focuses on interacting with hardware.  Translated with DeepL.com (free version)

Which is more expensive, Arduino or Raspberry Pi?

In general, the Raspberry Pi is more expensive than the Arduino:   Arduino: basic models (e.g., Arduino Uno) cost around $20-$30  Raspberry Pi: standard models (e.g., Raspberry Pi 4) cost around $35-$55 depending on RAM size  but prices vary depending on model, configuration, and availability. Raspberry Pi: Standard models (e.g., Raspberry Pi 4) cost around $35-55 depending on RAM size, but prices vary by model, configuration, and availability. In addition, Raspberry Pi may require additional accessories (e.g., SD card, power adapter, heat sink, etc.) to function properly.

Can the Arduino run Python?

The standard Arduino does not run Python directly, it mainly uses the C/C++ based Arduino programming language. However:   There are special projects such as MicroPython and CircuitPython that can be run on some advanced Arduino-compatible boards.  Some of the more powerful Arduino boards (such as the Arduino Portenta or the Arduino Nano 33 BLE) can run special versions of Python.  Traditional Arduino UNO, Mega, etc. cannot run Python directly

What are the disadvantages of the Raspberry Pi?

Weak real-time control: not suitable for applications that require precise timing due to running a full operating system  Higher power consumption: consumes more power than an Arduino and is not suitable for battery-powered long term projects  Long startup time: requires bootstrapping of the operating system  Reliability issues: the operating system may crash and the SD card may be corrupted  Limited hardware interfaces: limited number of GPIO pins, not as many as some Arduino models  Supply Problems: supply shortages have been common in recent years  Sensitive to unexpected power loss: may cause SD card corruption or system file corruption

What is Arduino best suited for?

Arduino is best suited for:   Hardware control projects: LED control, motor control, robotics projects  Sensor data acquisition: sensor monitoring for temperature, humidity, light, etc.  Real-time control systems: applications that require deterministic response times  Low-power applications: battery-powered, long-term monitoring devices  Simple automation projects: home automation, simple robotics  Learning to program an embedded system: entry-level electronics and programming Learn  Prototyping: rapid hardware prototyping  Stand-alone control systems: stand-alone control systems that do not require network connectivity

How long will the Arduino last?

Under normal usage conditions, the Arduino hardware itself can last for many years, even 10 years or more:   The ATmega microcontrollers used in the Arduino boards are designed to last 20 years or more  There are no mechanically moving parts, so there is a low rate of hardware failures  The main life-limiting factor is the physical environmental conditions (e.g., humidity, temperature fluctuations, and voltage spikes)  A properly used Arduino can operate for several years without requiring maintenance or replacement  However, the actual lifespan will be affected by the specific environment in which it is used, the quality of the power supply, how often it is used, and whether or not it has overvoltage or short-circuit protection.
Related Articles

  • Getting Started with Arduino: What is Arduino and How to Use Arduino Boards
    Getting Started with Arduino: What is Arduino and How to Use Arduino Boards
    UTMEL28 September 20237393

    Arduino is an open-source electronics platform that includes software and programmable circuit boards, allowing beginners to build electronic projects by writing simple code. The article provides an overview of Arduino, including different board types, basic components, how to use the boards, and project ideas like an automated plant watering system.

    Read More
  • IoT Chips Lead Time 2026: Navigating MCU, PMIC, and Sensor Shortages
    IoT Chips Lead Time 2026: Navigating MCU, PMIC, and Sensor Shortages
    UTMEL15 July 20261233

    Navigating component supply and allocation challenges in the 2026 IoT market. This procurement trend brief provides electronics engineers and component sourcing teams with a data-driven analysis of the IoT chips lead time 2026 landscape, detailing supply bottlenecks and alternative design strategies.

    Read More
  • MCU with Built-in NPU: How to Pick an Edge AI Microcontroller in 2026
    MCU with Built-in NPU: How to Pick an Edge AI Microcontroller in 2026
    UTMEL30 July 20262048

    Evaluating Edge AI microcontrollers requires looking beyond vendor-quoted TOPS metrics. This guide explains how to segment candidate parts into sensor, control, or vision tiers, calculate binding SRAM constraints, verify NPU operator support to avoid CPU fallbacks, and navigate production lifecycle risks. Follow a practical five-step engineering sequence to benchmark real models on physical evaluation boards.

    Read More
  • Top 5 Microcontrollers Defining IoT, Edge AI, and Power Efficiency in 2026: Sourcing and Selection Guide
    Top 5 Microcontrollers Defining IoT, Edge AI, and Power Efficiency in 2026: Sourcing and Selection Guide
    UTMEL15 August 20261018

    This guide reviews the top five microcontrollers defining 2026 embedded designs—ESP32-S3, STM32U5, MSPM0G5187, CH32V003, and nRF54. It evaluates how contiguous SRAM limits, power duty cycling, and hardware acceleration impact edge AI and IoT performance. It also details strategic procurement methods for navigating mature-node supply chain risks, dual-footprint layouts, and component authentication.

    Read More
  • Arduino vs. Raspberry Pi: A Detailed Comparison
    Arduino vs. Raspberry Pi: A Detailed Comparison
    UTMEL24 April 20256015

    Hello everyone, welcome to the new post today.This guide is going to talk in detail about Arduino vs. Raspberry Pi to clarify their differences and help you pick the right board based on your needs.

    Read More

Subscribe to Utmel !