What is a Capacitive Sensor?

Capacitive sensor, Theory, application and design
Catalog
1 Parallel plate capacitors | |
Ⅰ Introduction
Since the late 1970s, with the development of integrated circuit technology, capacitive sensors packaged with miniature measuring instruments have become widely available. This new type of sensor can greatly reduce the influence of distributed capacitance and overcome its inherent shortcomings. The capacitive sensor is a sensor with extremely wide application and continues to demonstrate great development potential in modern electronics and IoT applications.
A typical capacitive sensor consists of upper and lower electrodes, an insulator, and a substrate. When the membrane is subjected to pressure, the membrane deforms to a certain extent. Therefore, the distance between the upper and lower electrodes changes, thereby changing the capacitance. However, the relationship between the capacitance of the capacitive pressure sensor and the distance between the upper and lower electrodes is non-linear. Therefore, a measurement circuit with a compensation function should be used to compensate for the output capacitance nonlinearity. Modern digital signal processing techniques have significantly improved the accuracy and reliability of these compensation circuits.
Ⅱ Working Principle
1 Parallel Plate Capacitors
It is known from physics that the capacitor formed by two parallel metal plates, if the edge effect is not considered, the capacitance is C=εS/d
Where ε = the dielectric constant (permittivity) of the medium between the two plates;
S = the relative effective area of the two polar plates;
d = the distance between two plates
It can be seen from the above formula that there are three methods for changing the capacitance C. One is to change the dielectric constant ε of the medium; the second is to change the effective area of the capacitor; the third is to change the distance between the two plates. The output of the obtained electrical parameter is the increment ΔC of the capacitance value, which becomes a capacitive sensor.
2 Cylindrical Capacitors
Capacitive sensors are also often referred to as capacitive level gauges. The capacitance detection element of a capacitive level gauge works according to the principle of a cylindrical capacitor. The capacitor consists of two insulated coaxial cylindrical polar plates with internal electrodes and external electrode composition. When an electrolyte with a dielectric constant of ε is filled between the two cylinders, the capacitance between the two cylinders is:

Where L is the length of the part where the two cylinders overlap; D is the diameter of the outer cylinder electrode; d is the diameter of the inner cylinder electrode; ε is the dielectric constant of the intermediate medium. In actual measurement, D, d, and ε are basically unchanged, so the level of the liquid can be known by measuring C, which is also one of the reasons that the capacitive sensor has the characteristics of convenient use, simple structure, high sensitivity, and low price.
Capacitive sensors use various types of capacitors as sensing elements. Due to the measured changes, the capacitance of the capacitor will change. Through the measurement circuit, the change in capacitance can be converted into an electrical signal output. By measuring the size of the electrical signal, the measured parameter can be determined. This is the basic working principle of capacitive sensors.
Ⅲ Classification
According to the working principle of the sensor, the capacitive sensor can be divided into three types: variable pole distance type, variable area type, and variable medium type. According to the structure of the sensor, capacitive sensors can be divided into three types of structural forms. They can be divided into linear displacement and angular displacement according to the form of displacement, each of which is divided into flat (circular) plate shape and cylindrical shape according to the shape of the sensor plate. Although there are spherical shape and zigzag shape, they are rarely used. Among them, the differential type is generally better than the single group (unilateral) sensor, which has the characteristics of high sensitivity, wide linear range, and high stability.

Shapes of capacitive sensor
1. Variable Pole Distance Type Capacitive Sensor
The variable pole distance capacitive sensor is composed of a fixed pole plate and a movable pole plate: the movable pole plate is served by the metal plane under test. The distance between the plates of the capacitive sensor changes due to the measured changes.

Variable pole distance capacitive sensor structure
The change of the electrode plate spacing is not a linear relationship, indicating that there is a principle nonlinear error in this type of capacitive sensor. That is, when the range is far less than the initial distance between the two plates, it can be considered a linear relationship. Therefore, this type of sensor is generally used to measure small displacement changes. However, when the distance between the plates is too small, the flatness of the electrode surface should have an effect on the sensitivity, and at the same time, it is easy to cause capacitor breakdown. The distance between the plates cannot be infinitely small. The way to improve is to add a piece of mica or plastic film between the plates.
The relative dielectric constant of mica is approximately 7 times that of air, and its breakdown voltage is not less than 10³ kV/mm, while the breakdown voltage of air is only 3 kV/mm. Even if the mica sheet is 0.01mm thick, its breakdown voltage remains at 10 kV/mm. Therefore, after the mica sheet is placed, the initial distance between the plates can be greatly reduced. As long as the mica sheet is properly selected, a better linear relationship of the displacement sensor can be obtained. Generally, the initial capacitance of a capacitive sensor is between 20 pF and 30 pF, the distance between the plates is between 25 μm and 200 μm, and the maximum displacement should be less than 1/10 of the distance.
In actual use, in order to improve the nonlinearity, increase the sensitivity and overcome some external conditions such as the power supply ratio and the influence of environmental temperature changes, capacitive sensors often use the differential structure. When the initial state of the measurement is not started, adjust the movable plate to the middle position to make the capacitance on both sides equal; during measurement, the middle plate moves up and down with the measured object, which will cause the capacitance changes of the upper and lower parts. Therefore, the differential value of the capacitors on both sides improves the sensitivity in this way, and the linearity made near the zero point is also improved.
2. Variable Area Type Capacitive Sensor
In variable area type capacitive sensor, the flat structure is particularly sensitive to the change of the plate distance, and the measurement accuracy is affected. The cylindrical structure is nearly not affected by the radial change of the plate. It has become the most common structure in practical applications. The capacitance change of the capacitive sensor is proportional to the linear displacement when the edge effect is ignored.

Variable area type capacitive sensor
Figure a is a flat-plate linear displacement structure, in which the pole plate 1 is movable, called the moving pole plate. The polar plate 2 is fixed and is called a fixed polar plate. Figure b is a concentric cylindrical variable area sensor. The outer cylinder does not move, and the inner cylinder moves linearly up and down within the outer cylinder. Figure c is an angular displacement structure. When the axis of the polar plate 2 is driven by the object to be measured and rotates by an angular displacement of θ degrees, the covering area A of the two polar plates decreases, so the capacitance decreases accordingly.
3. Variable Dielectric Constant (ε) Type Capacitive Sensor
Variable dielectric constant (ε) type capacitive sensors are mostly used to measure the thickness and liquid level of dielectrics. They can also be used to measure the temperature and humidity of dielectric materials according to the change of the dielectric constant of the inter-electrode medium with changes in temperature and humidity. If the edge effect is ignored, the relationship between the capacitance of the single-group flat linear displacement sensor and the linear displacement of the medium is determined by the length and width of the fixed plate and the length of the measured object entering between the two plates.
Ⅳ Advantages
1) Good Temperature Stability
The capacitance value of the capacitive sensor generally has nothing to do with the electrode material, which is conducive to the selection of materials with a low-temperature coefficient, and because of the extremely small heat generated by itself, the stability is not affected. The resistance sensor has a copper loss, which is easy to generate heat and generate zero drift.
2) Simple Structure
The capacitive sensor has a simple structure and is easy to manufacture while guaranteeing high accuracy. It can be made very small to achieve some special measurements; it can work in harsh environments such as high temperature, strong radiation, and strong magnetic field, and can withstand large temperature changes, high pressure, high impact, and overload conditions; it can measure ultra-high temperature and low-pressure differences.
3) Good Dynamic Response
Capacitive sensors have very little electrostatic energy (about a few 10⁻⁵N) due to the electrostatic attraction between the electrode plates. The movable part can be made very small and thin, so its natural frequency is very high and its dynamic response time is short. It can work at a frequency of several megahertz, especially suitable for dynamic measurement. Because of its small dielectric loss, it can be powered by a higher frequency and the system operates at a higher frequency. It can be used to measure high-speed changing parameters.
4) Non-contact Measurement and High Sensitivity
Capacitive sensors can measure the vibration or eccentricity of the rotary shaft, the radial clearance of small ball bearings, etc. through non-contact measurement. When non-contact measurement is used, the capacitive sensor has an averaging effect, which can reduce the influence of the surface roughness of the workpiece on the measurement.
In addition to the above-mentioned advantages, the capacitive sensor also has a very small electrostatic attraction between the electrode plates, and the required input force and input energy are extremely small, so it can measure extremely low pressure, force, and very small acceleration, displacement, etc. It can be made very sensitive with high resolution, which can sense 0.01 μm or less displacement. Due to its low dielectric loss such as air, the zero residuals generated when connected in a bridge structure using a differential structure are extremely small, thus allowing the circuit to be amplified at high magnification and making the instrument highly sensitive.
5) Low Power Consumption
Modern capacitive sensors consume very little power, making them ideal for battery-powered and IoT applications. This characteristic has become increasingly important with the growth of wireless sensor networks and portable devices.
Ⅴ Disadvantages
① High Output Impedance and Poor Load Capacity
Regardless of the type of capacitive sensor, limited by the geometry of the electrode plate, its capacitance is very small, generally tens to hundreds of picofarads (pF), so the output impedance of the capacitive sensor is very high. Due to the high output impedance, the output power is small, the load capacity is poor, and it is susceptible to external disturbances causing instability. However, modern impedance matching circuits and buffer amplifiers have significantly mitigated this issue.
② The Influence of Parasitic Capacitance is Significant
The initial capacitance of the capacitive sensor is very small, but the parasitic capacitance of the lead cable capacitance connecting the sensor and the electronic circuit, and the stray capacitance of the electronic circuit is large. The presence of parasitic capacitance not only reduces the measurement sensitivity but also causes a nonlinear output. Because the parasitic capacitance changes randomly, the sensor is in an unstable working state which can affect the measurement accuracy. Modern design techniques including guard rings, driven shields, and integrated electronics help minimize these effects.
③ Environmental Sensitivity
Capacitive sensors can be affected by environmental factors such as humidity, contamination, and electromagnetic interference. Proper shielding and environmental compensation techniques are necessary for reliable operation in challenging conditions.
Ⅵ Applications
Capacitive sensors have the advantages of simple structure, high-temperature resistance, radiation resistance, high resolution, and good dynamic response characteristics. They are widely used in pressure, displacement, acceleration, thickness, vibration, liquid level, and other measurements. However, pay attention to the impact of the following aspects on the measurement results: ① reduce the changes in ambient temperature and humidity (which may cause changes in the dielectric constant of certain media or the geometric dimensions and relative positions of the plates); ② reduce edge effect; ③ reduce parasitic capacitance; ④ use shielding electrode and ground (protect the electric field of the sensitive electrode and isolate it from external electric field); ⑤ pay attention to the leakage resistance, excitation frequency and the insulation of the plate support material.
Modern Applications Include:
Touchscreen Technology: Capacitive touchscreens in smartphones, tablets, and industrial control panels
Automotive Systems: Proximity sensing, occupancy detection, and human-machine interfaces
Industrial Automation: Level sensing, position detection, and quality control
Consumer Electronics: Gesture recognition, fingerprint sensors, and proximity detection
Medical Devices: Respiration monitoring, pressure sensing, and diagnostic equipment
IoT Applications: Environmental monitoring, smart home devices, and wearable technology
Ⅶ Modern Developments
Recent advances in capacitive sensor technology include:
MEMS Integration: Micro-electromechanical systems (MEMS) technology has enabled the production of extremely small and precise capacitive sensors with integrated signal processing.
Smart Sensors: Integration of microcontrollers and digital signal processors directly with capacitive sensing elements for improved accuracy and self-calibration.
Multi-touch Capability: Advanced algorithms enable simultaneous detection of multiple touch points in touchscreen applications.
Flexible Sensors: Development of flexible capacitive sensors using polymer substrates for wearable and conformable applications.
AI Integration: Machine learning algorithms are being used to improve signal processing and compensate for environmental variations.
Ⅷ Frequently Asked Questions (FAQs)
Q1: What is the typical measurement range of capacitive sensors?
A: Capacitive sensors can measure displacements from nanometers to several millimeters, depending on the sensor design. For displacement sensors, typical ranges are from 0.01 μm to 10 mm. For proximity sensors, detection ranges can extend from a few millimeters to several centimeters.
Q2: How do capacitive sensors differ from resistive sensors?
A: Capacitive sensors measure changes in capacitance and typically offer higher sensitivity, better resolution, and lower power consumption than resistive sensors. They are also less affected by temperature variations and have better dynamic response. However, resistive sensors are generally simpler and less expensive.
Q3: Can capacitive sensors work through non-conductive materials?
A: Yes, capacitive sensors can detect objects through non-conductive materials such as glass, plastic, or wood. This makes them useful for applications where the sensor needs to be protected or where direct contact is not possible. The material thickness and dielectric properties will affect the sensing range and sensitivity.
Q4: What is the typical frequency range for capacitive sensor operation?
A: Modern capacitive sensors typically operate at frequencies ranging from several kHz to several MHz. Higher frequencies generally provide better sensitivity and faster response times but may be more susceptible to electromagnetic interference. The optimal frequency depends on the specific application requirements.
Q5: How can I minimize electromagnetic interference in capacitive sensors?
A: To minimize EMI: (1) Use proper shielding and grounding techniques, (2) Keep signal cables as short as possible, (3) Use twisted pair or coaxial cables for connections, (4) Implement guard rings around sensing electrodes, (5) Use differential measurement techniques, and (6) Apply appropriate filtering in the signal processing circuit.
Q6: What maintenance do capacitive sensors require?
A: Capacitive sensors generally require minimal maintenance. Regular cleaning of the sensing surface to remove dust, moisture, or contaminants is important. Periodic calibration may be necessary depending on the application. Check cable connections and shielding integrity regularly, especially in harsh environments.
Q7: Are capacitive sensors suitable for outdoor applications?
A: Yes, with proper design and protection. Outdoor applications require sensors with appropriate environmental ratings (IP ratings), temperature compensation, and protection against moisture and contamination. Sealed enclosures and conformal coatings can protect the sensor electronics from environmental factors.
Article Last Updated: October 31, 2025
This article has been updated to reflect current technology developments, correct technical terminology, and include modern applications of capacitive sensors. Information about MEMS integration, smart sensors, and IoT applications has been added to reflect advances since the original 2020 publication.
Related Articles:
What is a capacitive sensor used for?
Capacitive sensors are most often used to measure the change in position of a conductive target. But capacitive sensors can be effective in measuring presence, density, thickness, and location of non-conductors as well. Non-conductive materials like plastic have a different dielectric constant than air.
How do Capacitive sensors work?
A capacitive sensor uses the characteristics of a capacitor and its electrical field to form a sensor. Capacitive sensors work by detecting any change in the electric field the sensor can register either touch or proximity, displacement, as well as the level detection of humidity and fluids.
What do Capacitive sensors detect?
Many types of sensors use capacitive sensing, including sensors to detect and measure proximity, pressure, position and displacement, force, humidity, fluid level, and acceleration. Human interface devices based on capacitive sensing, such as touchpads, can replace the computer mouse.
Where are capacitive sensors used?
Capacitive sensors are used in the measurement of brake disc deformation. Due to the high temperature development, very few sensors are suitable for operating close to the measurement object. Capacitive transducers detect changes in the nanometer range and measure the wear on the brake disc.
What is the most common use of capacitive sensors?
The major applications include the sensors used to measure or detect proximity, position or displacement, humidity, fluid level & acceleration. Digital audio players, mobile phones & tablet computer use capacitive sensing touchscreens as input devices. Capacitive sensors can also replace mechanical buttons.
The Key Role of Electronic Components in IoT DevicesUTMEL01 September 20236423The article discusses the pivotal role of electronic components in Internet of Things (IoT) devices. IoT devices work by capturing real-world data using sensors, processing it through a microcontroller, and then sending it to the cloud for further analysis.
Read More
Accelerometer Sensors Guide: Working Principle, Circuit Design, Specifications, and ApplicationsUTMEL25 June 20261337A practical accelerometer sensor guide covering working principles, MEMS and piezoelectric types, datasheet specifications, circuit design, mounting, applications, and selection.
Read More
2026 ADAS Sensors: Supply Outlook and Alternative SourcingUTMEL18 July 20261461Automotive cleanroom assembly integrating advanced driver assistance systems. The automotive industry faces a structural semiconductor deficit in 2026, driven not by pandemic-era demand shocks but by AI data centers absorbing global foundry capacity on legacy nodes (40nm-90nm) where 95% of automotive-grade components are manufactured. Video demonstrations of these systems show a "machine view" overlay with red crosshairs tracking pedestrian movement and sudden cut-ins before traditional collision thresholds are triggered.
Read More
Magnetic Sensors for Position Detection: Hall Effect vs. AMR vs. TMR Engineering GuideUTMEL21 August 2026829This guide compares Hall effect, AMR, and TMR magnetic sensors for position detection in motor control and robotics. It explains their physical principles, key performance metrics, and selection criteria. Hall effect suits low-cost commutation, AMR offers high-speed angle sensing, and TMR provides maximum precision and low power, with practical integration advice.
Read More
Temperature Sensor Types Comparison: Thermocouple, RTD, and Semiconductor IC Selection GuideUTMEL17 August 2026701This comprehensive selection guide compares thermocouples, platinum RTDs, and semiconductor ICs across measurement range, accuracy limits, and signal conditioning complexity. It covers fundamental operating physics, mathematical transfer functions, lead-wire compensation topologies, and power budgets. Engineers will find practical design checklists, benchtop multimeter diagnostic techniques, and an architectural decision workflow to optimize system performance and bill-of-materials cost.
Read More
Subscribe to Utmel !
T0054445199Apex Tool Group
EBM7MF375Menda
ES80CH032Menda
ET70CH024Menda
50533Elesa USA Corporation
JKC8805WHTransforming Technologies
DK-GL4506PTransforming Technologies
10514Essentra Components
10513Essentra Components
DK-GL2505TTransforming Technologies


Product
Brand
Articles
Tools