web counter

Innovative Changes in Leading-Edge Chip Architectures

Published: 06 September 2023 | Last Updated: 06 September 20231890
Chipmakers are adopting both evolutionary and revolutionary technologies to gain substantial improvements in performance at the same or lower power.

Chipmakers are adopting both evolutionary and revolutionary technologies to gain substantial improvements in performance at the same or lower power. This indicates a fundamental shift from manufacturing-driven designs to those driven by semiconductor architects. The explosion in data, fueled by large language models and more sensors, as well as increased competition and international rivalries involving AI, is changing the rules dramatically at the leading edge of chip design. 

At the heart of these shifts are highly customized chip architectures, some involving chipsets developed at the most advanced process nodes. Parallel processing is almost a given, and so are accelerators aimed at specific data types and operations. These developments have been in research or sitting on the sidelines for years, and they are now being fully deployed. 

Power and thermal dissipation are persistent headaches for design teams, and they become more difficult to resolve as the speed and amount of processing increases. Memory innovations are playing a significant role in addressing these challenges. The options include in-memory/near-memory processing, as well as processing closer to the source of data. 

Furthermore, CPU improvements are speeding up the main processing elements. One way to do this is branch prediction, which predicts what the next operation will be. Another key trend on the system side is increasing domain specificity, which has disrupted the old model of developing a general-purpose processor that works across all applications. Intel unveiled a framework for integrating chiplets into an advanced package that leverages its Embedded Multi-die Interconnect Bridge to connect high-speed I/O, processor cores, and memory. The list of new approaches and technologies is unprecedented. What it shows is just how widely the industry is searching for new ways to increase power and reduce power, while still keeping an eye on area and cost. 

With all of these changes, two other issues have emerged. One is sustainability. As more data is processed by more chips, the challenge will be staying even on energy consumption, let alone reducing carbon footprints. A second issue that remains unresolved is reliability. Many of the new chip designs are also orders of magnitude more complex than previous generations of chips. 

In conclusion, the power, performance, and area/cost advances in chip architectures are a sharp departure from the gains the past. Innovation is happening everywhere, and roadmaps point to continued jumps in performance, lower energy consumption per computation, and reduced total cost of ownership.

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Related Articles

Subscribe to Utmel !

Featured Parts More