web counter
Op-Amp Voltage and Gain Calculator

Op Amp Voltage and Gain Calculator is a great opamp calculation tool, which is used to calculate the output Voltage, Inverting Gain and Non-Inverting Gain for an operational Amplifier. Before calculation, you should input the values of V1, V2, Vp, Vn and the resistance of R1, R2, R3, R4. And this operational amplifier calculator is easy-to-use and suitable for professional and newbie electricians.

Input Parameters
R1KOhms
R2KOhms
R3KOhms
R4KOhms
V1V
V2V
VpV
VnV
Outputs

Vout

Output is clipped.

V
Gain InvertingVout/V1
Gain non-invertingVout/V2
Introduction

Operational amplifiers are used in many circuits - one of the main applications is in amplifiers. Here the operational amplifier gain is of key importance.  Although there are both inverting and non-inverting amplifiers which have their own calculations, there is a generic equation for these circuits. The generic formula can be used to develop the equations for the inverting and non-inverting configurations.  The gain of these operational amplifier circuits is governed by the level of negative feedback. Applying negative feedback provides a defined level of gain, wider bandwidth, lower distortion as well as a number of other advantages. However it is often the operational amplifier gain that is of major importance.  When looking at the inverting amplifier circuit, the equation for the circuit can be calculated from the simple formula Av = R2/R1.  For the non-inverting amplifier the gain is slightly different and can be calculated from the formula Av = 1+ (R2/R1).  It is also possible to use the non-inverting amplifier as a buffer amplifier with a unity voltage gain by looping the output back to the inverting input, i.e. R1 = infinity and R2 = zero. In this way the voltage gain can be calculated to be 1.  So in summary both inverting and non-inverting amplifier gain is easy to calculate using the simple formulas.

Op Amp Gain | Details Calculations Formulas

Op-Amp Voltage and Gain Calculator Overview

The Op-Amp Voltage and Gain Calculator helps estimate the output voltage, inverting gain, and non-inverting gain of a basic operational amplifier circuit. By entering the resistor values, input voltages, and supply rail voltages, you can quickly check how an op-amp stage will amplify or invert a signal.

This calculator is useful when designing signal conditioning circuits, sensor interfaces, active filters, audio preamplifiers, comparator front-end circuits, and other analog circuits that use negative feedback around an operational amplifier.

The tool accepts resistor values R1, R2, R3, and R4, input voltages V1 and V2, and the positive and negative supply rails Vp and Vn. It then calculates the expected output voltage and indicates whether the output is clipped by the supply voltage limits.

What Is an Operational Amplifier?

An operational amplifier, or op-amp, is a high-gain differential voltage amplifier. It has a non-inverting input marked with a plus sign, an inverting input marked with a minus sign, and one output. In most linear amplifier circuits, feedback resistors are used to set a controlled closed-loop gain.

In an ideal op-amp model, the input terminals draw no current and the feedback loop drives the two input terminals to nearly the same voltage. These assumptions make it possible to calculate many op-amp circuits using simple resistor ratios.

What This Calculator Can Calculate

  • Estimated output voltage for the entered input voltages and resistor network.

  • Inverting gain, which shows how much the inverting input signal is amplified and phase-inverted.

  • Non-inverting gain, which shows how much the non-inverting input signal is amplified without phase inversion.

  • Output clipping when the calculated voltage exceeds the positive or negative supply rail.

For a differential amplifier or a more complex circuit, resistor matching and input common-mode range become especially important. Use this calculator as a first-pass design aid, then verify the result against the selected op-amp datasheet and circuit requirements.

Input Parameters Explained

InputMeaningTypical Unit
R1Input or reference resistor used in the feedback network, depending on the circuit topology.kOhm
R2Feedback resistor or gain-setting resistor paired with R1.kOhm
R3Additional input or divider resistor used by the op-amp calculator circuit.kOhm
R4Additional feedback, divider, or matching resistor used with R3.kOhm
V1Input voltage applied to one side of the op-amp circuit.V
V2Input voltage or reference voltage applied to the other side of the op-amp circuit.V
VpPositive supply rail of the op-amp.V
VnNegative supply rail of the op-amp. For a single-supply circuit, this is often 0 V.V

Basic Op-Amp Gain Formula

The general voltage gain relationship is:

Vout = A * Vin

Where:

  • Vout = output voltage

  • Vin = input voltage

  • A = closed-loop voltage gain

In practical feedback amplifiers, the closed-loop gain is usually set by resistor ratios, not by the extremely high open-loop gain of the op-amp itself.

Inverting Op-Amp Formula

For a standard inverting amplifier, the input signal is applied to the inverting input through an input resistor, and the feedback resistor connects the output back to the inverting input.

A = -R2 / R1

Vout = -(R2 / R1) * Vin

The negative sign means the output signal is inverted, or 180 degrees out of phase with the input signal. If R1 and R2 are equal, the circuit has a gain of -1 and works as an inverting buffer.

Non-Inverting Op-Amp Formula

For a standard non-inverting amplifier, the input signal is applied to the non-inverting input, while the feedback divider sets the gain.

A = 1 + R2 / R1

Vout = (1 + R2 / R1) * Vin

The output signal stays in phase with the input signal. A non-inverting amplifier has a minimum gain of 1. When the output is directly connected to the inverting input, the circuit becomes a voltage follower or buffer.

Output Voltage With Two Inputs

Many op-amp calculator circuits include two input voltages and four resistors. In a common single-op-amp topology, the output can be estimated by combining the inverting contribution from one input and the non-inverting contribution from the other input:

Vout = V2 * (R4 / (R3 + R4)) * (1 + R2 / R1) - V1 * (R2 / R1)

If the resistor ratios are matched, the circuit can behave like a difference amplifier, where the output is proportional to the voltage difference between two inputs:

Vout = Gain * (V2 - V1)

The exact formula depends on the resistor labels and circuit diagram used by the calculator. Always match the formula to the schematic before using the result in a final design.

Example Calculation

For a simple inverting amplifier:

  • R1 = 10 kOhm

  • R2 = 100 kOhm

  • Vin = 0.2 V

The gain is:

A = -100 kOhm / 10 kOhm = -10

The output voltage is:

Vout = -10 * 0.2 V = -2 V

For a simple non-inverting amplifier using the same resistor ratio:

A = 1 + 100 kOhm / 10 kOhm = 11

If Vin = 0.2 V, the output is:

Vout = 11 * 0.2 V = 2.2 V

Why Output Clipping Happens

An ideal formula may calculate an output voltage beyond the op-amp's supply rails, but a real op-amp cannot output a voltage higher than its positive rail or lower than its negative rail. When the calculated output exceeds the available output range, the signal is clipped.

For example, if an op-amp is powered from 0 V and 5 V, a calculated output of 7 V cannot be produced. The actual output will saturate near the upper supply limit. Many real op-amps also cannot swing exactly to the rails unless they are rail-to-rail output devices.

How to Use This Calculator

  1. Choose the op-amp circuit type, such as inverting, non-inverting, or a two-input configuration.

  2. Enter resistor values in kOhm according to the calculator diagram.

  3. Enter the input voltages V1 and V2.

  4. Enter the positive and negative supply rails as Vp and Vn.

  5. Calculate the output voltage and gain values.

  6. Check whether the output is clipped by the supply rails.

  7. Compare the result with the selected op-amp's input and output voltage range in the datasheet.

How to Interpret the Result

ResultMeaningWhat to Check
Positive gainThe output is in phase with the input signal.Usually associated with non-inverting operation.
Negative gainThe output is inverted relative to the input signal.Usually associated with inverting operation.
Output is within Vp and VnThe calculated output is inside the supply limits.Still verify real output swing limits in the datasheet.
Output is clippedThe calculated output exceeds the supply range.Reduce gain, lower the input signal, or use a wider supply voltage if the op-amp allows it.

Practical Design Notes

  • Use resistor values that keep input bias current errors acceptable for the selected op-amp.

  • Check the op-amp gain-bandwidth product if the signal frequency is high.

  • Make sure the input common-mode voltage range includes the expected input voltages.

  • Check output swing limits, especially in single-supply circuits.

  • Use precision resistors when gain accuracy or common-mode rejection matters.

  • Add supply decoupling capacitors close to the op-amp power pins in real hardware.

  • Confirm stability when driving capacitive loads or using high feedback resistance.

Common Mistakes to Avoid

  • Forgetting that inverting gain is negative.

  • Assuming the output can swing exactly to the supply rails.

  • Using resistor ratios correctly but ignoring the op-amp's input common-mode range.

  • Choosing very high resistor values and creating large offset errors from input bias current.

  • Using a high gain without checking bandwidth and slew rate.

  • Mixing up R1, R2, R3, and R4 compared with the circuit diagram.

  • Using ideal formulas for a precision design without checking real op-amp datasheet limits.

When This Calculator Is Not Enough

This calculator is best for quick voltage and gain estimates. More detailed analysis is needed when the circuit has high frequency signals, large output current, capacitive loads, very small input signals, high source impedance, strict noise requirements, precision DC accuracy requirements, or a single-supply input range close to ground or the positive rail.

In those cases, check the op-amp datasheet for offset voltage, input bias current, input common-mode range, output swing, slew rate, gain-bandwidth product, noise, and load-drive capability. Simulation and bench testing are recommended before final production.

Frequently Asked Questions

What is op-amp gain?

Op-amp gain is the ratio between output voltage and input voltage. In closed-loop amplifier circuits, the gain is usually controlled by external feedback resistors.

Why is the inverting gain negative?

The negative sign shows that the output voltage moves in the opposite direction from the input voltage. This means the signal is phase-inverted by 180 degrees.

Why does the non-inverting gain include 1?

In a non-inverting amplifier, the output includes the input voltage plus the voltage developed across the feedback network. This creates the gain formula 1 + R2/R1.

What does output clipping mean?

Output clipping means the calculated output voltage is beyond what the op-amp can produce from its supply rails. The real output saturates near the rail instead of following the ideal formula.

Can I use this calculator for single-supply op-amp circuits?

Yes. Enter the positive supply as Vp and enter 0 V as Vn if the circuit is powered from a single supply. Also check whether the chosen op-amp supports the required input and output voltage range.

Can this calculator replace an op-amp datasheet?

No. The calculator gives ideal or simplified results. Real op-amps have limitations such as offset voltage, input bias current, output swing, bandwidth, slew rate, noise, and load-drive capability.

Related Online Calculation Tools

Frequently Asked Questions

What parameters do I need to input for the calculation?

You need to input the resistor values (R1-R4 in kΩ), input voltages (V1 and V2 in volts), and the op-amp's power supply voltages (Vp and Vn in volts). These parameters allow the tool to calculate the output voltage and gains accurately.

Why does the output voltage sometimes show "Output is clipped"?

This occurs when the calculated Vout exceeds the op-amp's supply voltages (Vp or Vn). Real op-amps cannot output voltages beyond their supply rails, so the signal is clipped at ±Vp/Vn. Ensure your input signals and resistor ratios stay within the supply limits.

How are the inverting and non-inverting gains calculated?

Inverting Gain: Gain = -R2/R1 (negative due to signal inversion). Non-Inverting Gain: Gain = 1 + R2/R1. The tool uses these formulas to compute gains based on your resistor values.

Can I use this calculator for differential amplifier configurations?

No, this tool is designed for basic inverting/non-inverting op-amp circuits. For differential amplifiers (e.g., using R3 and R4), refer to a dedicated differential amplifier calculator, as the formula involves additional resistor ratios.

Why is the non-inverting gain formula different from the inverting gain?

In a non-inverting configuration, the input signal is applied directly to the op-amp's non-inverting terminal, resulting in a positive gain (1 + R2/R1). For inverting setups, the signal is fed through resistors to the inverting terminal, causing phase inversion and a negative gain (-R2/R1).
Hot products

ImagePart NumberManufacturerCategoryPackage/CaseDescriptionPriceQuantityBuy/Quote
BLM18PG121SN1DBLM18PG121SN1DMurata ElectronicsFerrite Beads and Chips0603 (1608 Metric)MURATA - BLM18PG121SN1D - Ferrite Bead, 0603 [1608 Metric], 120 ohm, 2 A, BLM18P Series, 0.05 ohm, ± 25%-

In stock : 355131

Minimum: 1

AD9364BBCZAD9364BBCZAnalog Devices Inc.RF Transceiver ICs144-LFBGA, CSPBGARF Transceiver 1.3V 144-Pin CSP-BGA Tray-

In stock

Minimum: 1

MPZ2012S102AT000MPZ2012S102AT000TDK CorporationFerrite Beads and Chips0805 (2012 Metric)TDK - MPZ2012S102AT000 - FERRITE BEAD, 0.15OHM, 1.5A, 0805-

In stock : 51745

Minimum: 1

SE2537L-RSE2537L-RSkyworks Solutions Inc.RF Amplifiers16-VFQFN Exposed PadRF Amplifier 5GHz Gain 30 dB 3.3Volt -10C 85C-

In stock : 10000

Minimum: 1

CYBL10162-56LQXICYBL10162-56LQXICypress Semiconductor CorpRF Transceiver ICs56-UFQFN Exposed PadMCU 32-Bit CYBL10X6X ARM Cortex M0 RISC 128KB Flash 1.8V/2.5V/3.3V/5V 56-Pin QFN EP Tray-

In stock : 48

Minimum: 1

SKY81294-14-001SKY81294-14-001Skyworks Solutions Inc.PMIC - LED Drivers9-BGA, WLCSPIC LED FLASH DVR 1.2V 9CSP
  • 1:$0.465882
  • 10:$0.439511
  • 100:$0.414633
  • 500:$0.391163

In stock : 1000

Minimum: 1

HSMS-282P-TR1GHSMS-282P-TR1GBroadcom LimitedDiodes - RF6-TSSOP, SC-88, SOT-363Diode Schottky 15V 6-Pin SOT-363 T/R-

In stock

Minimum: 1

80HCPS1432CRM80HCPS1432CRMRenesas Electronics America Inc.Specialized ICs576-BBGA, FCBGAIC SER RAPIDIO SWITCH 576FCBGA-

In stock

Minimum: 1

ALT6702RM45Q7ALT6702RM45Q7Skyworks Solutions Inc.RF Amplifiers-IC RF AMP CELLULAR SMD-

In stock

Minimum: 1

SI8261BBD-C-ISSI8261BBD-C-ISSilicon LabsIsolators - Gate Drivers6-SOIC (0.295, 7.50mm Width)4A Gate Driver Capacitive Coupling 5000Vrms 1 Channel 6-SDIP
  • 1:$7.623102
  • 10:$7.191606
  • 100:$6.784534
  • 500:$6.400503

In stock : 9020

Minimum: 1

SI8261BAD-C-ISSI8261BAD-C-ISSilicon LabsIsolators - Gate Drivers6-SOIC (0.295, 7.50mm Width)Gate Drivers 5kV Opto input Sgl channel 4.0A driver
  • 1:$4.558766
  • 10:$4.300723
  • 100:$4.057286
  • 500:$3.827628

In stock : 100000

Minimum: 1

CSR8510A06-ICXR-RCSR8510A06-ICXR-RQualcommRF Transceiver ICs6-XFBGAIC RF TXRX BLUETOOTH 6XFBGA-

In stock

Minimum: 1

FOD8333FOD8333ON SemiconductorIsolators - Gate Drivers16-SOIC (0.295, 7.50mm Width)Optocoupler AC/DC-IN 1-CH DC-OUT 16-Pin SO Rail
  • 1:$7.142559
  • 10:$6.738263
  • 100:$6.356852
  • 500:$5.997030

In stock : 50

Minimum: 1

FOD8332R2FOD8332R2ON SemiconductorIsolators - Gate Drivers16-SOIC (0.295, 7.50mm Width)OPTOISO 4.243KV GATE DRIVER 16SO-

In stock : 11

Minimum: 1

SP1004U-ULC-04UTGSP1004U-ULC-04UTGLittelfuse Inc.TVS - Diodes10-XFDFNTVS DIODE 9.2V 1004/10DFN-

In stock : 2633

Minimum: 1

ISM303DACTRISM303DACTRSTMicroelectronicsMultifunction-HIGH PERFORMANCELOW POWER COMPAC-

In stock : 4138

Minimum: 1

SLD8S36ASLD8S36ALittelfuse Inc.TVS - DiodesNonstandard SMDTVS DIODE 36.5V 58.1V SMTO-263-

In stock : 20

Minimum: 1

ACPL-302J-500EACPL-302J-500EBroadcom LimitedIsolators - Gate Drivers16-SOIC (0.295, 7.50mm Width)OPTOISO 5KV 1CH GATE DRIVER 16SO
  • 1:$6.873772
  • 10:$6.484691
  • 100:$6.117633
  • 500:$5.771352

In stock : 36800

Minimum: 1

UR020-006-RAUR020-006-RATripp LiteUSB Cables-TRIPP-LITE UR020-006-RACOMPUTER CABLE, USB, 6FT, BLACK-

In stock

Minimum: 1

SFH 4713ASFH 4713AOSRAM Opto Semiconductors Inc.Infrared, UV, Visible Emitters3-SMD, No LeadEMITTER IR 860NM 1A-

In stock : 6000

Minimum: 1