Sort by
What is an LDO (Low Dropout Regulator)?29 October 2021
Hello everyone. Today I would like to introduce you to LDO (low dropout regulator), a low dropout linear regulator. I hope it will help you understand LDO better.
Development Board vs Single-Board Computer (SBC): Differences, History, and How to Choose14 July 2026
If you have ever scoped a prototype, you have probably hit the same fork in the road: do you reach for a development board built around a specific chip, or a single-board computer that boots a full operating system? The two look similar on a bench, both arrive as a populated PCB with connectors along the edges, yet they belong to different design philosophies and solve different problems. This guide draws a clean line between them, sketches how each category grew up, lays out the real technical differences in side-by-side tables, and ends with a practical framework for picking the right one.
Weak Current Control Strong Current: How to use the Relay?28 November 2022
Hello everyone, I am Rose. Welcome to the new post today. Today I will introduce relay to you. Including its definition, parameters, working principle and so on.
Basic Knowledge of Various Types of Mixers03 January 2023
Welcome to the new post today. Today I will introduce the basic knowledge of mixer.
16 Q&A About the Secrets of Operational Amplifiers27 March 2025
Hello everyone, I am Rose. Last time, I introduce operational amplifier to you. Today, I will answer 16 questions about operational amplifier, let's see whether you have the following questions!
Using Microcontrollers in the Internet of Things (IoT) Applications27 June 2023
The Internet of Things (IoT) is a concept that connects physical devices to the Internet, enabling communication and data exchange between devices by integrating sensors, embedded systems, and networks.
Carbon Film vs Metal Film Resistors: Complete Comparison Guide19 May 2025
This comprehensive article compares carbon film and metal film resistors, explaining their structures, characteristics, and applications to help engineers and hobbyists choose the right type for their specific projects. While carbon film resistors offer cost advantages and unique characteristics for certain applications like high voltage circuits and some audio equipment, metal film resistors provide superior precision, stability, and low noise performance, making them the preferred choice for most modern precision electronics.
Introduction to Step-up Transformer01 March 2021
A step-up transformer is a transformer that is used to raise the output voltage while retaining the current flow constant and without variance. This kind of transformer is predominantly used in power transmission and generation stations. The main and secondary windings are used in this transformer. In contrast to the secondary winding, the main winding has fewer twists.
What is a Servo Motor?09 March 2021
Servo motor refers to the engine that controls the operation of mechanical components in the servo system and is a motor indirect speed change device. The servo motor can control the speed and position accuracy very accurately and can convert the voltage signal into torque and speed to drive the control object.
A Beginner's Guide to the 2N5551 Transistor and Its Uses27 May 2025
The 2N5551 transistor is a high-voltage NPN device ideal for amplification and switching. Learn its specs, uses, and 2N5551 transistor equivalent options.
Ten Smart Sensor Technology Trends for IoT Applications20 November 2021
Hello everyone, I am Rose. Welcome back to the new post today. Smart sensors are smart sensor devices that can sense, gather, judge, analyze, and process external environmental data autonomously.
What is Mini LED?08 December 2020
Mini LED is defined as an LED device with a chip size between 50~200μm. The size of the Mini LED is between the small-pitch LED and Micro LED, which is the result of further refinement of the small-pitch LED. Mini LED can be used as a backlight source in products such as large-size displays, smartphones, car panels, and gaming notebooks. It can also be used as a self-luminous display with RGB three-color LED chips.


Product
Brand
Articles
Tools