Sort by
Voltage Regulator: Types, Working, and Applications23 February 2021
A voltage regulator is a part of the power supply device that, under all operating conditions, ensures a stable, continuous voltage supply. During power changes and differences in loads, it controls voltage. As well as DC voltages, it will control AC. We will take a closer look at the idea of a voltage regulator and the different forms in this blog, and we will expand on the common voltage regulator ICs and their common implementations!
Introduction to TTL and CMOS Logic Gate Circuits24 November 2025
Electronic circuits that implement basic and common logic operations are called logic gate circuits. TTL and CMOS logic gate circuits are 2 typical types. Read this to learn their structure and features.
Characteristics and Working Principle of IGBT31 October 2025
IGBT, Insulated Gate Bipolar Transistor, is a composite fully controlled voltage-driven power semiconductor device composed of BJT (bipolar transistor) and IGFET, (Insulated Gate Field Effect Transistor). It has the advantages of both the high input impedance of MOSFET and the low on-voltage drop of GTR.
How does a Photodiode Work?15 August 2020
A photodiode is a special diode (light-receiving device) that converts optical signals into electrical signals.It has a pn junction, and its shell has a window with glass for light penetration.So how does it work and how do we use it? Read this article to find the answer.
Understanding Computer Memory: From SIMM and DIMM to DDR523 May 2025
DIMM, Dual in-line memory module, is a memory stick that appeared after the launch of Pentium CPU, which provides 64-bit data channels.
Rectifier Diode: Function and Circuit12 August 2020
Rectifier Diode is a semiconductor device used to convert alternating current to direct current.It has obvious unidirectional conductivity, and can be made of materials such as semiconductor germanium or silicon. This article gives you a brief introduction to rectifier diodes.
Is there a Limit to the Chip Process Node?02 November 2021
Process node refers to the spacing between circuits within an integrated circuit, specifically, the line width of the gate in the transistor structure, which is the value in the XXnm process. The narrower the width, the lower the power consumption.
A Comprehensive Guide to FPGA Development Boards07 September 2026
This comprehensive guide will take you on a journey through the fascinating world of FPGA development boards. We’ll explore what they are, how they differ from microcontrollers, and most importantly, how to choose the perfect board for your needs. Whether you’re a seasoned engineer or a curious hobbyist, prepare to unlock new possibilities in hardware design and accelerate your projects. We’ll cover everything from budget-friendly options to specialized boards for image processing, delve into popular learning paths, and even provide insights into essential software like Vivado. By the end of this article, you’ll have a clear roadmap to navigate the FPGA landscape and make informed decisions for your next groundbreaking endeavor.
8051 Microcontroller: History, Architecture, Applications, and Features20 February 2021
The 8051 Microcontroller Introduction and some of its basic features are discussed in this article.
Analysis of Resistors in Series and Parallel12 June 2026
Several resistors are connected at a time to form a circuit without branches in the middle, which is called a resistor in a series circuit. And a circuit that connects two or more resistors between two points in a circuit with the same voltage at both ends of the resistor is called a resistor in a parallel circuit. The following mainly focus on the circuits, calculation methods, fault characteristics and fault treatment of resistors in series and parallel. And the final part introduces a concept-- ESR, which is related to series resistors and capacitors
What is a Polypropylene Capacitor?08 November 2021
A polypropylene capacitor is a kind of capacitor with a very stable electric capacity. It is often used in applications requiring very precise capacitance and can replace most polyphenylene or mica capacitors.
Bluetooth Explained: Characteristics and Applications02 June 2021
Bluetooth is a global specification of wireless data and voice communication, which is a special close-range wireless technology for setting communication environments for fixed and mobile devices. Bluetooth allows some of the current portable mobile devices and computer devices to connect to the Internet without a cable and can be wirelessly accessing the Internet.


Product
Brand
Articles
Tools