web counter

8051 Microcontroller: History, Architecture, Applications, and Features

Published: 20 February 2021 | Last Updated: 20 February 202122567
The 8051 Microcontroller Introduction and some of its basic features are discussed in this article.
Basics of 8051 Microcontroller are introduced in this video.

Introduction to 8051 Microcontroller

Catalog

Ⅰ Introduction

Ⅱ What is a Microcontroller?

Ⅲ 8051 Microcontroller History

Ⅳ 8051 Microcontroller Architecture

Ⅴ Applications of 8051 Microcontroller

Ⅵ 8051 Microcontroller Features

 

Ⅰ Introduction

The 8051 microcontroller series, technically referred to as the Intel MCS-51 Architecture, was developed by Intel in 1980 and was very popular in the 80's (still are popular). In different fields, such as embedded systems, consumer electronics, vehicles, etc., the 8051 Microcontroller is one of the most prominent and most commonly used microcontrollers.

8051 microcontroller

8051 microcontroller

There are several features of the 8051 Microcontroller such as Serial Communication, Timers, Interrupts, etc., and thus many students and beginners begin their work on the 8051 Microcontroller principle of Microcontrollers (although this trend seems to be changed with the introduction of Arduino).

While 8051 Microcontroller can seem a bit out of date, we believe that Microcontrollers, Embedded Systems, and Programming are some of the best platforms to get started with (both C and Assembly).

So, an introduction to the 8051 microcontrollers and some of the fundamentals of the 8051 microcontrollers will be given in this article.

But before we get into the 8051 Microcontroller Introduction and Fundamentals, we need to talk a bit about what a microcontroller is and the distinction between a microprocessor and a microcontroller.

Ⅱ What is a Microcontroller?

A Microcontroller is a VLSI IC that, along with some other peripherals such as memory (RAM and ROM), I/O ports, timers/counters, communication interface, ADC, etc., contains a CPU (processor).

A microprocessor (which was built before the microcontroller) is merely a processor (CPU) and does not have the peripherals mentioned above. We need to independently interface the peripherals to make it functional or create a scheme around it.

Almost all process and control functions were performed using Microprocessors before the advent of Microcontrollers. Although the external peripherals need to operate as a device for the Microprocessor, the average expense of the control system was high.

But the situation, including the field of embedded systems, has changed entirely with the advent of the Microcontroller.

Ⅲ 8051 Microcontroller History

A short description of the 8051 Microcontroller and its past is given in the 8051 Microcontroller Introduction. The Intel 8051 Microcontroller was a successor to the 8048 Microcontroller (Intel MSC-51 Architecture) (Intel MSC-48 Architecture).

8051 Microcontrollers were initially designed using N-MOS technology, but the use of battery-powered systems and their low power consumption contribute to the use of CMOS technology (which is famous for its low power consumption).

While Intel built 8051 microcontrollers (which was discontinued in 2007), 8051 compatible microcontrollers are now being manufactured by more than 20 semiconductor manufacturers, i.e. processors based on the MSC-51 architecture.

Atmel (AT89C51, AT89S51), Phillips (S87C654), STC Micro (STC89C52), Infineon (SAB-C515, XC800), Siemens (SAB-C501), Silicon Labs (C8051), NXP (NXP700, NXP900), etc., are among the 8051 microcontrollers generated by various manufacturers.

Silicon IP Cores (Intellectual Property Cores) are the bulk of the modern 8051 Microcontrollers, but discrete 8051 Microcontroller ICs are also available. 8051 IP Cores are used in FPGAs (Field Programmable Gate Array) and SoCs (System on Chip) instead of Advanced ARM Architecture-based MCUs due to their low power consumption, smaller size, and basic architecture.

Ⅳ 8051 Microcontroller Architecture

8051 microcontroller <a href='https://www.utmel.com/components/top245yn-top-switch-gx-family-pin-diagram-circuit-diagram?id=2179'><strong>pin diagram</strong></a> and pin function

8051 microcontroller pin diagram and pin function

CPU (Central Processor Unit):

As you might be conscious, the brain of every processing computer is the Central Processor Unit or CPU. Both processes that are conducted in the Microcontroller are scrutinized and controlled. The operator has no control over the operation of the CPU. It interprets and carries out all of the programs printed in storage space (ROM) and executes the planned task. In the 8051 microcontrollers, the CPU monitors numerous types of registers.

Interrupts:

As the heading put forth, Interrupt is a subroutine call that reads the main function or job of the Microcontroller and allows it to execute any other program that is then extra important. 8051 Interrupt's functionality is highly constructive as it assists in emergency situations. Interrupts provide one with a mechanism for postponing or halting the current operation, executing a sub-routine job, and then restarting the execution of the regular program again.

At the time of the interrupt, the Micro-controller 8051 should be assembled in such a way that it temporarily interrupts or breaks the core program. When the sub-routine assignment is done, the main program execution immediately continues as normal. In the 8051 Microcontroller, there are 5 interrupt supplies, two out of five are peripheral interrupts, two are timer interrupts, and one is serial port interrupt.

Memory:

It is a software that is a series of commands that requires a micro-controller. This software helps the microcontroller to perform particular tasks. Such programs require a storage space on which the Microcontroller can accumulate and interpret them to operate on some particular procedure. The memory that is put into play with the Microcontroller device to generate is known as program memory or code memory. It's also known as Read-Only Memory or ROM.

The microcontroller still requires memory for the short term to amass data or operands. For this primary purpose, the disk space that is used to temporarily store data for service is known as Data Memory and we use Random Access Memory or RAM. The 8051 microcontroller includes 4K code memory or program memory, so it has 4KB ROM and 128 bytes of data memory (RAM) as well.

Bus:

Fundamentally, Bus is a set of wires that serve as a contact channel or a transfer data medium. Such buses are made up of 8, 16 or more wires. A bus will either carry 8 bits or 16 bits overall. Two types of buses exist:

Bus Address: The 8051 microcontroller consists of a 16-bit bus address. For resolving memory locations, it is brought into play. It is often used to relay to Memory the address from the Central Processing Unit.

Data bus: The 8051 microcontroller consists of an 8-bit data bus. It is used for data carting.

Oscillator:

Because we all know that the microcontroller is a piece of equipment for a digital circuit, it needs a timer for its purpose. The Microcontroller 8051 consists of an on-chip oscillator for this purpose, which toils as a CPU time source (Central Processing Unit). As the efficiency thumps of the oscillator are steady as a result, harmonized use of all 8051 Microcontroller parts is encouraged. Input/Output Port: As we know, the microcontroller is used to handle the functions of devices in embedded systems.

We require I/O (input/output) interfacing ports in the Microcontroller to collect them to other devices, gadgets, or peripherals. Micro-controller 8051 consists of 4 input/output ports to connect it to other peripherals for this purpose. Timers/Counters: With two 16 bit counters & timers, Micro-controller 8051 is compatible. The counters would be divided into 8-bit registers. Timers are used to calculate intervals, to figure out the duration of the pulse, etc.

Ⅴ Applications of 8051 Microcontroller

The 8051 Microcontroller is still used in many embedded systems and applications even with the production of many sophisticated and superior microcontrollers.

Any of the 8051 Microcontroller applications are listed below:

Consumer Appliances (TV Tuners, Remote controls, Computers, Sewing Machines, etc.)

Home Applications (TVs, VCR, Video Games, Camcorder, Music Instruments, Home Security Systems, Garage Door Openers, etc.)

Communication Systems (Mobile Phones, Intercoms, Answering Machines, Paging Devices, etc.)

Office (Fax Machines, Printers, Copiers, Laser Printers, etc.)

Automobiles (Air Bags, ABS, Engine Control, Transmission Control, Temperature Control, Keyless Entry, etc)

Aeronautical and Space

Medical Equipment

Defense Systems

Robotics

Industrial Process and Flow Control

Radio and Networking Equipment

Remote Sensing

Ⅵ 8051 Microcontroller Features

8-Bit ALU: ALU is the heart of a microcontroller or Arithmetic Logic Machine. On binary numbers, it executes arithmetic and bitwise operations. The 8051 ALU is an 8-bit ALU, meaning it can run 8-bit data operations.

8-Bit Accumulator: The Accumulator is an essential ALU-related register. An 8-bit register is an accumulator in 8051.

RAM: 8051 There is 128 bytes of RAM on the microcontroller, plus SFRs and Input/Output Port Registers.

ROM: 8051 has an on-chip ROM of 4 KB (Program Memory).

I/O ports: 8051 has four bit-addressable and bidirectional 8-bit input/output ports.

Timers / Counters: There are two 16-bit Timers / Counters in 8051.

Serial Port: Full Duplex UART Connectivity supports 8051.

External Memory: 8051 Two 16 bit address lines can be reached at once by the microcontroller: one for each RAM and ROM. The total external memory that can be accessed by an 8051 Microcontroller for RAM and ROM is 64KB (216 for each type).

Other features: Interrupts, on-chip oscillator, Power Down Mode, Boolean Processor, etc.

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1.What is the use of 8051 microcontrollers?

Application of Microcontroller 8051. The use of microcontrollers in various fields such as automobile, aeronautics, space, robotics, electronics, defense application, mobile communications, rail transport, industrial processing, and medical applications is rapidly increasing.

2.What is meant by microcontroller 8051?

8051 microcontroller is an 8-bit microcontroller created in 1981 by Intel Corporation. It has an 8-bit processor that simply means that it operates on 8-bit data at a time. It is among the most popular and commonly used microcontroller.

3.Is 8051 still used?

Despite the more limited features and old architecture, the 8051 is still used in some wireless communication products. The latest HC-10 Bluetooth modules are based on 8051 core. Although 16-bit or 32-bit MCUs can replace the functions offered by 8051s, the 8-bit MCU is sufficient for many product developers.

4.Is 8051 a RISC or CISC?

Processor 8085 is a RISC and controller 8051 is a CISC. Reduced instruction set computer. It is a type of microprocessor that has been designed to carry out few instructions at the same time. As instruction are few it can be executed in a less amount of time.

5.Why microcontroller is used?

Microcontrollers are used in automatically controlled products and devices, such as automobile engine control systems, implantable medical devices, remote controls, office machines, appliances, power tools, toys, and other embedded systems.
Related Articles

  • Getting Started with Arduino: What is Arduino and How to Use Arduino Boards
    Getting Started with Arduino: What is Arduino and How to Use Arduino Boards
    UTMEL28 September 20237393

    Arduino is an open-source electronics platform that includes software and programmable circuit boards, allowing beginners to build electronic projects by writing simple code. The article provides an overview of Arduino, including different board types, basic components, how to use the boards, and project ideas like an automated plant watering system.

    Read More
  • IoT Chips Lead Time 2026: Navigating MCU, PMIC, and Sensor Shortages
    IoT Chips Lead Time 2026: Navigating MCU, PMIC, and Sensor Shortages
    UTMEL15 July 20261233

    Navigating component supply and allocation challenges in the 2026 IoT market. This procurement trend brief provides electronics engineers and component sourcing teams with a data-driven analysis of the IoT chips lead time 2026 landscape, detailing supply bottlenecks and alternative design strategies.

    Read More
  • MCU with Built-in NPU: How to Pick an Edge AI Microcontroller in 2026
    MCU with Built-in NPU: How to Pick an Edge AI Microcontroller in 2026
    UTMEL30 July 20262048

    Evaluating Edge AI microcontrollers requires looking beyond vendor-quoted TOPS metrics. This guide explains how to segment candidate parts into sensor, control, or vision tiers, calculate binding SRAM constraints, verify NPU operator support to avoid CPU fallbacks, and navigate production lifecycle risks. Follow a practical five-step engineering sequence to benchmark real models on physical evaluation boards.

    Read More
  • Top 5 Microcontrollers Defining IoT, Edge AI, and Power Efficiency in 2026: Sourcing and Selection Guide
    Top 5 Microcontrollers Defining IoT, Edge AI, and Power Efficiency in 2026: Sourcing and Selection Guide
    UTMEL15 August 20261018

    This guide reviews the top five microcontrollers defining 2026 embedded designs—ESP32-S3, STM32U5, MSPM0G5187, CH32V003, and nRF54. It evaluates how contiguous SRAM limits, power duty cycling, and hardware acceleration impact edge AI and IoT performance. It also details strategic procurement methods for navigating mature-node supply chain risks, dual-footprint layouts, and component authentication.

    Read More
  • Arduino vs. Raspberry Pi: A Detailed Comparison
    Arduino vs. Raspberry Pi: A Detailed Comparison
    UTMEL24 April 20256014

    Hello everyone, welcome to the new post today.This guide is going to talk in detail about Arduino vs. Raspberry Pi to clarify their differences and help you pick the right board based on your needs.

    Read More

Subscribe to Utmel !