web counter

Low Temperature Drift Resistors Increase the Accuracy of Analog Circuits

Published: 11 February 2025 | Last Updated: 11 February 20251889
Analog circuits are used in many applications ranging from aerospace to medical devices. Therefore, the accuracy of these devices needs to be very high. These circuits translate real-life signals into usable electronic circuits. However, substantial challenges arise due to environmental factors, particularly due to temperature changes, as the resistivity of components changes with changes in temperature.

As analog circuits are required to perform under extreme fluctuating conditions, Low-Temperature Drift Resistors (LTDRs) can address this scenario. LTDRs are designed such that the changes in their resistance are minimal despite being subjected to a wide range of temperatures. Hence, they allow the development of technology where accuracy cannot be compromised.

Temperature Coefficient of Resistance Metrics and its Significance

The Temperature Coefficient of Resistance (TCR) tells us how much a resistor’s resistance changes with temperature. It is expressed in parts per million per degree Celsius (ppm/°C), and TCR is calculated as:

wps3.jpg

Where R and Ro are resistances and T, and To are temperatures.

TCR is very important in maintaining the accuracy of a circuit. Resistors with high TCR experience more changes in resistance as the temperature fluctuates, leading to errors in circuit performance, whereas low TCR resistors are those that do not undergo much change, keeping the system stable over a wide range of temperatures. Most industries, therefore, prefer low TCR components for reduced errors and high efficiency.

Methods of Measuring TCR

The variation in resistance that a resistor undergoes over a temperature range is measured while measuring the TCR. There exist two common techniques for measuring TCR: the four-point probe method and the Van der Pauw technique.

The four-point probe method minimizes contact resistance errors since it uses separate probes for current injection and voltage measurement. This increases the accuracy measuring of resistivity, especially for thin films. On the other hand, the Van der Pauw method is fit for samples with irregular shapes. This technique can use peripheral contacts to apply current and measure voltage, calculating resistivity and TCR. This technique often provides great value in thin-film resistors or any other material with complex geometrical characterizations. Special environmental test chambers are used to measure the accurate readings. Since, in highly precise applications, the resistors shall have definite TCRs.

LTDRs are designed to have very minimal resistance change due to temperature changes. It has a low TCR value. Applications of LTDR include industries such as aerospace, automotive, medical devices, and precision instrumentation. For example, LTDRs in automotive systems are used for very accurate measurements within engine control units despite the heat generated by the engines.

LTDRs are important because they enhance reliability and performance in electronic systems. They improve circuit accuracy, reduce maintenance needs, and prolong the life of devices.

Why LTDRs Have Low TCR

The material composition also contributes to the TCR. The material and structural characteristics of LTDRs are carefully engineered, hence they have a low TCR. Two key mechanisms contribute to this behaviour:

1. Electron Mean Free Path: The mean free path of electrons is naturally short in certain materials. For instance, in NiCr mean free path is 0.4 nm, hence scattering due to temperature change will be minimal, keeping the resistance change minimal.

2. Amorphous and Crystalline Phases: Certain materials have positive and negative TCR for their crystalline and amorphous forms respectively. A balance between these phases creates a material with near-zero TCR. Cr-Si-C films are one such material.

Current status of LTDRs in the Industry

LTDRs are utilized across a wide range of industries, including aerospace and automotive to medical technology. The demand for LTDRs has increased over the past few years due to fast-growing areas in material science and fabrication techniques. A few companies from this domain are Vishay, Rohm, and TE Connectivity. The manufacturers provide resistors for specific applications with TCR as low as 1 ppm/°C. Applications of LTDRs using NiCr-based LTDR are common in precision measurement systems, while SiCr has found its place in integrated circuits.

Other challenges to the industry include cost versus performance, in that most of the advanced LTDRs require costly materials and processes. Nevertheless, ongoing research into new materials and methods of manufacture tries to provide more cost-effective ways.

Future Scope of LTDRs

Innovation and expansion of applications mark the future of LTDRs. Research into materials such as polycrystalline ceramics and nanocomposites, will decrease the TCR values further. This helps LTDR perform at better cost-effectiveness. Fabrication techniques in atomic layer deposition and doping on an atomic scale improve manufacturing uniformity, scalability, and broader usage such as consumer electronics and IoT gadgets, among others.

LTDRs would also play a crucial part in quantum computing and space exploration, where precision really plays an important role together with stability. Sustainability seeks to make use of eco-materials, processes, or integration into energy-efficient use, like renewable energy grids. As technology in LTDRs advances, such breakthroughs in precision electronics and beyond get enabled.

Saumitra Jagdale

Saumitra Jagdale is a Backend Developer, Freelance Technical Author, Global AI Ambassador (SwissCognitive), Open-source Contributor in Python projects, Leader of Tensorflow Community India, and Passionate AI/ML Enthusiast

Related Articles

  • Current Shunt Resistor Pulse Rating Selection: Sizing for Inrush Energy, TCR Drift, and Kelvin Connections
    Current Shunt Resistor Pulse Rating Selection: Sizing for Inrush Energy, TCR Drift, and Kelvin Connections
    UTMEL12 September 20261253

    This guide explains how to size low-ohmic current shunt resistors by separating steady-state thermal design from transient pulse survivability. It covers adiabatic inrush energy calculations, manufacturer pulse curves, terminal-temperature derating, composite TCR errors from copper terminations, 4-terminal Kelvin layouts, thermal EMF suppression, ESL-induced spikes, and a dual-checklist verification workflow.

    Read More
  • What are the Differences Between Pull up and Pull down Resistors?
    What are the Differences Between Pull up and Pull down Resistors?
    UTMEL22 October 202540497

    Pull up is to clamp an uncertain signal to a high level with a resistor, and the resistor also acts as a current limiter. In the same way, pull down means to clamp the uncertain signal to a low level through a resistor. To pull up is to input current to the device, and the pull-down is to output the current.

    Read More
  • Rheostat Basics: Types, Principle and Functions
    Rheostat Basics: Types, Principle and Functions
    UTMEL25 December 202520012

    A rheostat is a device that can adjust the size of the resistance and can be connected to the circuit to adjust the size of the current. A general rheostat is composed of a wire with a larger resistance and a device that can change the contact point to adjust the effective length of the resistance wire. Rheostat can limit the current and protect the circuit, and change the voltage distribution in the circuit.

    Read More
  • Basic Introduction to Metal Film Resistor
    Basic Introduction to Metal Film Resistor
    UTMEL28 August 202014589

    Metal film resistors are a kind of film resistors. Metal film resistors are resistors in which special metals or alloys are used as resistor materials, and the resistor film layer is basically formed on ceramic or glass by vacuum evaporation or sputtering.

    Read More
  • Varistor: Definition, Function, Working and Testing
    Varistor: Definition, Function, Working and Testing
    UTMEL03 April 202586133

    A varistor is a device with a non-linear volt-ampere characteristic. When the voltage applied to the varistor is lower than its threshold value, the current flowing through it is extremely small, which is equivalent to a resistor with infinite resistance, vice versa. The most common varistor is a metal oxide varistor (MOV).

    Read More

Subscribe to Utmel !

Featured Parts More