Basic Introduction to Metal Film Resistor

Metal Film Resistors Explained
Catalog
Ⅴ The difference between carbon film resistors and metal film resistors |
Ⅵ Distinguish between carbon film resistors and metal film resistors |
Ⅰ Basic introduction
Metal film resistors are a kind of film resistors. Metal film resistors are resistors in which special metals or alloys are used as resistor materials, and the resistor film layer is basically formed on ceramic or glass by vacuum evaporation or sputtering. Because it is a lead type resistor, it is convenient for manual installation and maintenance and is used in most household appliances, communications, and instruments. Metal film resistors are widely used resistors so far, with high precision, stable performance, simple and lightweight structure. It plays an important role in the electronics industry and military aerospace under high-precision requirements.
Ⅱ Thin film resistor
There are mainly four types of thin film resistors
1.Carbon film resistor
Metal film resistors are made by depositing crystalline carbon on the ceramic rod skeleton. Carbon film resistors are low in cost. It has stable performance, a wide resistance range, and low-temperature coefficient and voltage coefficient. It is currently the most widely used resistor.
2.Metal film resistor

Metal film resistor
Metal film resistors are the main type introduced today. The alloy material is evaporated on the surface of the ceramic rod skeleton by vacuum evaporation. Metal film resistors have higher accuracy, better stability, noise and temperature coefficient calibration than carbon film resistors, and are widely used in instrumentation and communication equipment.
3.Metal oxide film resistor
The feature of a metal oxide film resistor is that a layer of metal oxide is deposited on the insulating rod. Since it is an oxide itself, it is stable at high temperatures, heat shock resistant, and has a strong load capacity.
4.Synthetic film resistor
Synthetic film resistors are made by coating a conductive composite suspension on a substrate, so it is also called paint film resistance. Because its conductive layer presents a granular structure, it has high noise and low accuracy. It is mainly used to make high voltage, high resistance, and small resistors.
Ⅲ Structure of metal film resistor
The production of metal film resistors is to deposit a nickel-chromium alloy on a round base rod to obtain excellent performance. The usual tolerance is ±1%, and tolerances of ±0.1%, ±0.2z5%, and ±0.5% can also be obtained. The temperature coefficient can be as low as ±15ppm/℃. After cycling and aging, the change will not exceed 0.25%. The typical structure is shown in the figure.

Structure of metal film resistor
Metal film resistors are resistors in which special metals or alloys are used as resistance materials, and the resistance film layer is basically formed on ceramic or glass by vacuum evaporation or sputtering. This type of resistor is generally made by a vacuum evaporation process, that is, heating the alloy in a vacuum, the alloy is evaporated, and a conductive metal film is formed on the surface of the porcelain rod. Grooving and changing the thickness of the metal film can control the resistance. Its heat resistance, noise potential, temperature coefficient, voltage coefficient, and other electrical properties are better than carbon film resistors. The manufacturing process of metal film resistors is relatively flexible. Not only can its material composition and film thickness be adjusted, but also the resistance value can be adjusted through grooves, so that a resistor with good performance and a wide resistance range can be made.
Metal film resistors generally have cap structure, cylindrical structure, chip structure, and leadless structure, as shown in the figure

Ⅳ Features of metal film resistor
①Good heat resistance, rated working temperature is 70℃, maximum working temperature can reach 155℃.
②Good voltage stability and small temperature coefficient.
③Wide working frequency range, low noise electromotive force, can be used in high-frequency circuits.
④Under the same power condition, it is much smaller than the carbon film resistor, about half of the carbon film resistor.
⑤It can adjust the precision resistance value by cutting butterfly and pattern method, and the accuracy can reach ±0.5%, ±0.05%.
⑤The resistance range is very wide, and can be made into 1Ω -1000MΩ resistors.
⑦The rated power is 0.125W, 0.25W, 0.5W, lW, 2W, lOW and 25W, etc.
③The pulse load stability is poor, not as good as carbon film resistors.
⑨The application is very wide, suitable for AC, DC, and pulse circuits.
Ⅴ The difference between carbon film resistors and metal film resistors
For carbon film resistors, it uses carbon to be deposited on a magnetic rod or ceramic tube, and at the same time, a layer of the crystalline carbon film is formed on the surface. The thickness of the carbon film and the method of notching the carbon film are used to change the degree of the carbon film resistor and finally, get the required resistance value. The surface is coated with epoxy resin to strengthen the seal. The appearance color is basically khaki, of course, there are other colors, such as pink.
The color band is four bands, the resistance range is 1Ω~10MΩ, the rated power is 0.125W, 0.25W, 0.5W, 1W, etc., the accuracy range: ±10%, ±5%, ±2%. This kind of resistor is universal larger, often used in cheap products, such as power supplies, chargers. It is not recommended for starting resistance, because the impact resistance is relatively defective.
For metal film resistor, it uses vacuum evaporation or burning infiltration to form a metal film on the ceramic tube frame. This film is attached to the surface of the white ceramic. The resistor is cut and adjusted to obtain a more precise resistance. This kind of resistor has high precision, small size, good stability, and high cost. It is usually used in wireless electronic equipment, especially on occasions with higher precision requirements.
Ⅵ Distinguish between carbon film resistors and metal film resistors
1. According to the temperature coefficient of resistor
We can distinguish the two types of resistors by carbon film resistors with negative temperature coefficient characteristics, and metal film resistors with small positive temperature coefficients, which can distinguish these two resistors well.
2. According to resistance accuracy
The manufacturing process of each type of resistor is different, and the accuracy of the resistor is also different. We know that carbon film resistors are very common resistors, and their accuracy is generally not high. The production requirements of metal film resistors are higher and the resistance accuracy is higher than that of carbon film resistors. It is also an identification method to judge the resistance accuracy.
4. According to resistor color
Common carbon film resistors have low precision and low production costs, so their appearance is mostly khaki or pink, while the appearance of metal film resistors is mostly blue. We can clearly distinguish the two resistors through color.
5. According to resistance painting
Carbon film resistors have a layer of black protective paint on the surface. We can distinguish by looking at the color of the protective paint. Metal film resistors usually use a bright white protective film. Through the protective painting of these two resistors, we can also distinguish the two well.
Related Articles:
Varistor: Definition, Function, Working and Testing
SMD Resistors: Codes, Size, Testing, Tolerance and Selection
Are metal film resistors better?
Metal Oxide film resistors have a better voltage coefficient and temperature coefficient than carbon film resistors. ... As a matter of fact, metal oxide film resistors work in a wide resistance range and can withstand a higher temperature than the carbon film resistors.
What are metal oxide film resistors used for?
Metal oxide film resistors exceed the performance of metal film and carbon film for the following properties: power rating, voltage rating, overload capabilities, surges and high temperatures. Designers choose often the metal oxide film resistor for high endurance applications.
What is the best type of resistor?
Wirewound resistors are the best choice for noise, followed by metal film, metal oxide, carbon film, and lastly, carbon composition. However, wirewound resistors are not readily available in large resistance values, and are usually inductive, which can cause instability problems in some cases.
What are metal resistors used for?
A resistor is a passive two-terminal electrical component that implements electrical resistance as a circuit element. In electronic circuits, resistors are used to reduce current flow, adjust signal levels, to divide voltages, bias active elements, and terminate transmission lines, among other uses.
What is a metal film resistor?
Metal film resistors have a thin metal layer as resistive element on a non-conducting body. They are amongst the most common types of axial resistors. ... The appearance of metal film resistors is similar to carbon film resistors, but their properties for stability, accuracy and reliability are considerably better.
Current Shunt Resistor Pulse Rating Selection: Sizing for Inrush Energy, TCR Drift, and Kelvin ConnectionsUTMEL12 September 2026326This guide explains how to size low-ohmic current shunt resistors by separating steady-state thermal design from transient pulse survivability. It covers adiabatic inrush energy calculations, manufacturer pulse curves, terminal-temperature derating, composite TCR errors from copper terminations, 4-terminal Kelvin layouts, thermal EMF suppression, ESL-induced spikes, and a dual-checklist verification workflow.
Read More
What are the Differences Between Pull up and Pull down Resistors?UTMEL22 October 202539891Pull up is to clamp an uncertain signal to a high level with a resistor, and the resistor also acts as a current limiter. In the same way, pull down means to clamp the uncertain signal to a low level through a resistor. To pull up is to input current to the device, and the pull-down is to output the current.
Read More
Rheostat Basics: Types, Principle and FunctionsUTMEL25 December 202519450A rheostat is a device that can adjust the size of the resistance and can be connected to the circuit to adjust the size of the current. A general rheostat is composed of a wire with a larger resistance and a device that can change the contact point to adjust the effective length of the resistance wire. Rheostat can limit the current and protect the circuit, and change the voltage distribution in the circuit.
Read More
Basic Introduction to Metal Film ResistorUTMEL28 August 202014344Metal film resistors are a kind of film resistors. Metal film resistors are resistors in which special metals or alloys are used as resistor materials, and the resistor film layer is basically formed on ceramic or glass by vacuum evaporation or sputtering.
Read More
Varistor: Definition, Function, Working and TestingUTMEL03 April 202585353A varistor is a device with a non-linear volt-ampere characteristic. When the voltage applied to the varistor is lower than its threshold value, the current flowing through it is extremely small, which is equivalent to a resistor with infinite resistance, vice versa. The most common varistor is a metal oxide varistor (MOV).
Read More
Subscribe to Utmel !
CC2530F128RHARTexas Instruments
ADL5380ACPZ-R7Analog Devices Inc.
ADF7020BCPZAnalog Devices Inc.
AT86RF215-ZURMicrochip Technology
ATSAMR30G18A-MUTMicrochip Technology
AX5043-1-TW30ON Semiconductor
MICRF112YMMMicrochip Technology
CC2538NF53RTQRTexas Instruments
ADF7012BRUZ-RLAnalog Devices Inc.
CC8520RHARTexas Instruments


Product
Brand
Articles
Tools