Introduction to Flyback Transformer

Flyback transformer / flyback driver
Catalog
| I. Features | 1. Design |
| 2. Circuit | |
| 3. Arc | |
| 4. Winding | |
| II. Working Principle | |
| III. Applications | |
| IV. FAQ | |
A special class in the family of transformers is the flyback transformer. It's essentially a step-up transformer, but with a massive ability to raise the voltage. It is small in size and mobile, as opposed to power transformers. In CRT tube televisions, where a very high voltage in the image tube is necessary, one of the common applications of flyback transformers is. A flyback transformer can achieve an output of up to 20,000 V for an input of 230 V. The capacity of flyback transformers is such. With a low voltage such as 12 V or 5V, it can also run. Building components are distinct from a standard transformer. The early use of the flyback transformer began with the regulation of the electron beam's horizontal movement in a cathode ray tube. With the advent of technology and equipment, with the help of a rectifying circuit consisting of electronic devices such as MOSFET, the new flyback transformer can also be energized with a DC pulse.
Because of the application of flyback transformers in the CRT tunnel, the term flyback was coined. With a very low voltage, a flyback transformer can be energized. When the transformer's primary winding is excited with a low-value sawtooth voltage, due to the existence of the sawtooth waveform, it gets easily energized and de-energized. The beam on the CRT flies back from right to left because of this. The name was coined as a flyback transformer with this unusual property obtained because of the working of the transformer.
I. Features
1. Design
A flyback transformer varies in nature and operation, much like a traditional transformer. The primary has to be fed with an AC voltage in a traditional transformer, which is stepped up or down depending on the number of turns. The traditional transformer's output voltage is small but can be used for different applications.
The primary winding in a flyback transformer does not need to be excited by AC voltage, but can be excited even with a DC pulse input. The low rating of the DC pulse input can be 5 V or 12 V, which can be obtained also from a function generator. With a rectifying circuit, the DC voltage is converted to DC pulses. In a typical transformer, the output voltage is pure AC voltage.
But in the case of a flyback transformer, the arc created is a very high voltage arc. This output voltage can not be transmitted over long distances, but can only be used for SMPS or CRT tube specific applications. The heart of the flyback transformer is similar but compact in size to the standard transformer.
2. Circuit

Flyback Transformer Design
The circuit diagram is shown below for the flyback transformer. As demonstrated, the turns of the windings are L1 and L2. In general, L2 is very broad for flyback transformer than L1, as it is essentially a step-up transformer. To hold the voltage constant, the capacitor on the input side is supplied. For rectifying the input voltage, the switch SW is used.
The diode D is used to maintain the secondary current's unidirectional flow. To maintain the constant output voltage, the capacitor on the secondary side is supplied. Vin is the voltage of the input and Vout is the voltage of the output. For the overall center of the transformer, the dot convention shown in the circuit indicates its series additive equivalent inductance.
3. Arc
The transformer's output voltage is high, even up to 10 to 20 kV. In nature, the high voltage is not sinusoidal but is in the shape of an arc. When two highly conductive bodies are positioned together, an arc is created in the air. The air in between is ionized and created by the arc. Whenever a breaker is energized, the isolator is worked, or the corona phenomenon, the notion is the same.
4. Winding
As compared to primary turns, the secondary turns are very wide in order to achieve a very high voltage on the secondary side. Generally, the windings are made out of copper. And the windings are properly separated from each other, as in a traditional transformer. To provide the insulation, mica insulation is commonly used. Paper insulation is also used in some applications, such as SMPS and converters. No oil is used for insulation or collating purposes, unlike a traditional transformer. Generally, the windings are thin in size, thereby improving the winding loss and efficiency.
II. Working Principle

Flyback Transformer Waveform
Except for its architecture elements, the operating concept of the flyback transformer is the same as the traditional transformer. The primary winding is energized, as seen in the circuit diagram, when the transformer's primary winding is excited with a low voltage sawtooth waveform.
As seen in the waveforms, as shown in the diagram, when the primary winding is energized, the primary inductance produces a ramp current. The flyback waveform produces a high potential when the ramp current hits its peak value. Which is caused on the peripheral side. The diode on the reverse side stops the reverse side of the ramp from flying.
A ramp down follows the secondary current, the moment at which the voltage hits the point of the internal knee. High voltage on the secondary side is obtained at this point. But because it cannot be of the AC in nature, it follows a very high-potential arc-like structure that all guides the electron beam in one specific direction. The second potential is less in applications such as SPMS, but the concept of conversion to transform the secondary AC into switched mode is converted. The operation may also be defined as a continuous or discontinuous mode of operation, depending on the nature of the waveform.
The main winding, secondary winding, and core are involved in the flyback transformer construction. It also consists of a rectifying unit if it is stimulated from a DC supply. In general, there are fewer main winding turns than secondary winding turns. The windings are made of and insulated from each other by copper. As with the traditional transformer, the winding methods are the same.
The windings are positioned over a series of magnetic circuits forming the heart. This helps, at low power specifications, the transformer to tolerate more voltage. On both sides, the core leg has equal dimensions and the winding is encircled around the core. The magnetic circuit is shaped in nature to be additive.
III. Applications
The flyback transformer applications include the following.
CRT Tube
SPMS
DC-DC Power technologies
Battery charging
Telecom
Solar applications
How to Test a Flyback Transformer?
This transformer can be evaluated in different ways. A line-operated potential transformer tester is used to search for the faults to verify whether there is any fault in the winding. The tester would show very high impedance on the winding side in the case of open winding, and the impedance will be relatively low in the case of a short circuit. This is one sign of winding defects. The health of the winding can also be shown in recent testers by a graphical display. It would be a noisy operation to deal with faults in the capacitor. On the display side, a noise such as a tic-tac can appear. This occurs when the condenser opens. In the event of the capacitor shorting, the window will be void. It'll display a blink of strength. The capacitor needs to be replaced in such situations. Shorting windings, splitting in the core, external arcing to field, etc. are other common problems in the transformer. All these issues can be tested by line-operated testers. To test the continuity of the circuit and calculate the voltage at each point, a common multimeter may also be used.
What does a flyback transformer do?
A flyback transformer is a coupled inductor with a gapped core. During each cycle, when the input voltage is applied to the primary winding, energy is stored in the gap of the core. Flyback transformers are used to provide voltage transformation and circuit isolation in flyback converters.
How many volts does a flyback transformer generate?
A flyback transformer, also known as a line output transformer, comprises coupled inductors, making it unique from a typical transformer. It generates voltage from a few kilovolts up to 50 kilovolts with high-frequency currents from 17 kHz to 50 kHz.
How do I know if my flyback transformer is bad?
A sure sign of a bad flyback transformer is when a picture does not display on the monitor. The television continues to produce sounds in conjunction with a picture, but the picture cannot be seen. The flyback transformer is not sending enough high voltage to the monitor in order for a picture to display.
What is a Transformer: Definition, Principle and ApplicationsUTMEL03 November 20218710Hi, fellas. I am Rose. Today I will introduce the transformer to you. The device that increases or decreases the voltage in an AC circuit is known as a transformer. The transformer is an AC voltage converter that works on the mutual inductance concept.
Read More
LVDT - Linear Variable Differential Transformer BasicsUTMEL16 January 20219741LVDT is the abbreviation of linear variable differential transformer, which belongs to linear displacement sensor. It is a movable iron core transformer that consists of a primary coil, two secondary coils, iron core, coil frame, shell and other components.
Read More
Introduction to Flyback TransformerUTMEL29 January 202112181As an energy conversion device that transfers energy from one part of the circuit to the other part at constant power, a flyback transformer can be described. Based on the application, the voltage is stepped up to a very high value in a flyback transformer. It is also called a transformer for line output, as the voltage of the output line is fed to the other part of the circuit. The primary winding of the transformer can be powered by a DC circuit with the assistance of the rectifying circuit.
Read More
Audio Transformer-Types, Functions and WorkingUTMEL05 January 202616045An audio transformer is an electromagnetic system designed to separate an input circuit from an output circuit and produce a signal that passes through it with filtering. A varying electromotive force (voltage) in the secondary winding linked to the other circuit is caused by this changing flux.
Read More
RVDT(Rotary Variable Differential Transformer) BasicsUTMEL02 February 202121156The Rotary Variable Differential Transformer or RVDT is regarded as the transformer that detects the angular displacement of the conductor. That is the kind of electromechanical transducer that gives the angular displacement of the input equal to the linear output.
Read More
Subscribe to Utmel !
H050X044H1TPanduit Corp
110060947Seeed Technology Co., Ltd
1.69508.8100000RAFI USA
SLI-343P8G3FROHM Semiconductor
1203410303Molex
SGNE06C080MT150N25TDK Corporation
1-22279-6TE Application Tooling
H100X044H1T-2Panduit Corp
SLI-343P8C3FROHM Semiconductor
83500000005Littelfuse Inc.


Product
Brand
Articles
Tools