web counter

RVDT(Rotary Variable Differential Transformer) Basics

Published: 02 February 2021 | Last Updated: 02 February 202121127
The Rotary Variable Differential Transformer or RVDT is regarded as the transformer that detects the angular displacement of the conductor. That is the kind of electromechanical transducer that gives the angular displacement of the input equal to the linear output.
In this video, we will learn about the construction and working of RVDT which can be used for measuring rotary displacement.

What is RVDT?

Catalog

Ⅰ Introduction

Ⅱ Construction of RVDT

Ⅲ Working of RVDT

Ⅳ Advantages of RVDT

Ⅴ Disadvantages of RVDT

Ⅵ Applications of RVDT

 

Ⅰ Introduction

RVDT

RVDT

An RVDT (rotary variable differential transformer) is used to calculate the angular displacement of the test circuit. It plays an important role in aircraft (measuring aircraft throttle and flap control systems), in aerospace, in medical sciences, in measuring or varying angular displacement, and in stabilizing the system. The theory of operation is similar to that of LVDT, in which the cam-shaped center rotates with the aid of the shaft between the winding. A brief description of what is the RVDT sensor is explained in this article, its full form, operating theory along with case study and tests, benefits, drawbacks, and real-time implementations.

Ⅱ Construction of RVDT

As seen in the figure below, the circuit diagram for RVDT consists of one main and two secondary windings. The physical parameters and design aspects of the RVDT core are chosen in such a way that angular displacement is produced linearly by the coil with regard to the induced mutual inductance between the primary and individual secondary coils. As it is driven by an external electrical source and transforms angular displacement into electrical signals, it is often considered a passive transducer. An angular location sensor, differential transducer, RVDT transducer, inductive sensor, etc. are other names for RVDT (due to the absence of electronic circuits inside it). The efficiency and longevity of the device is improved by its brushless continuous rotation property.

Ⅲ Working of RVDT

Let us presume that the RVDT transformer's secondary voltage is Es21 and Es22, respectively.

The RVDT Sensitivity is denoted by the parameter 'G'

Theta ( ϴ) determines the shaft's angular displacement and is given by,

θ=G*(Es21-Es22)/(Es21-Es22))

The secondary voltage is calculated with the equation

Es22=Es22±G*θ

The differential output voltage across the secondary side is given by,

∆Es22=2*G*θ

The working theory of the RVDT is similar to that of the LVDT and works on the collective induction principle. A magnetic field is generated within the heart when the RVDT primary windings are exposed to an AC excitation voltage of approximately 5-15V and a frequency range of 50-400Hz. The secondary winding induces a magnetic current equal to the magnetic field that is generated. The distinction between the induced voltage through secondary windings is the net RVDT output voltage.

The output voltage E o is usually equal to,

Eo=Es21-Es22

The RVDT operating theory is divided into three situations with regard to the inner core location, and the RVDT experiment is carried out on the same basis.

RVDT shape, circuit diagram and characteristic curve

RVDT shape, circuit diagram, and characteristic curve

Case 1: When the core is correctly located in the null position (equilibrium state)

In this case, two secondary windings put the core specifically in the middle spot. The flux linkage between secondary windings (S21 and S22) is equal and zero (Eo=Es21-Es22=0) is the net induced EMF. The heart has no displacement and is therefore considered to calculate angular differences as a normal baseline value.

Case 2: In a clockwise direction, core rotation

The RVDT primary coil is attached to an external power source in this state, and an EMF is induced within the circuit. Because of the flux connection around, the center begins to rotate in a clockwise direction.

S21 is superior to S22. This in-turn suggests that the EMF generated is greater than S22 in S21. Therefore, positive Es21-Es22= +ve would be S21>S21 and the complete differential voltage. The primary voltage is in phase, along with the output voltage

Case 3: In an anti-clockwise direction, core rotation

Inside the RVDT circuit, EMF is caused. Due to the fact that the flux linkage through S22 is greater than S21, the core continues to rotate in an anti-clockwise direction. This in-turn suggests that the EMF produced in S22 is greater than that of S21. Es22>Es21 and the overall voltage difference would also be negative Es22-Es21=-ve. The main voltage and output voltage are out of phase at 180 degrees (phase opposition).

Ⅳ Advantages of RVDT

(1). Robust, robust, and suitable for extremely challenging operating environments

With greater product life, RVDT is durable in design. A higher range of operating environments may be reused. Measure angular displacements in applications including vital and ruff wear and tear. It is able to survive harsh conditions, such as strong vibrations, shocks, and overload.

(2). Cost-efficient

If you intend to reduce the cost of calculation, then this is the go-to option of greater importance. The majority of the project is covered by costs, especially if the budget is small. Along with robustness, relative to other sensors, the expense of RVDT is small.

(3). Reduced and quick to handle repairs

With a reduced number of electronic parts, RVDT construction is easier. It is possible to eliminate the need for complicated circuits or specialty auxiliary parts to achieve angular throughput. It also takes down the repair expense to a greater degree with small components.

(4). Compact in volume

In RVDT, the reduction in the number of electronic components scales down the total unit size to a comparatively limited area. To interface with the external devices, a limited space to accommodate the sensor is necessary. The number of applications can also be expanded by this factor.

(5). Construction Contactless

RVDT hinders performance problems related to physical integrity and friction production due to wear and tear within the structure, because there is no mechanical interaction between the components.

Ⅴ Disadvantages of RVDT

The Rotary Variable Differential Transformer drawbacks are described below.

(1). It is restricted to applications where high-precision sensors are required.

(2). To achieve output functions, there is a need for an external AC supply.

(3). Not superior to digital-output applications.

Ⅵ Applications of RVDT

As follows, the Rotary Variable Differential Transformer applications are

For all of these benefits, RVDT applications are more common and commonly preferred to be found in heavy-duty production facilities in the oil and gas, aerospace, and so on industries. As follows, the standard RVDT implementations are,

(1). To test the angular acceleration of control actuators and propeller navigation in aircraft and avionics applications.

(2). In engines to make intelligent fuel control systems

(3). Controllers and cable networks in the cockpit.

(4). To measure angular displacement and extract movements of the hand, legs, and other momentary sections in robotics.

In general, the market research survey on Rotary Variable Differential Transformer applications indicates that the factors pushing the RVDT to the global level are increased automation and the increasing amount of industrial automation. Because of the need for portable research facilities, machine tools, and expanded robotic applications, this need will further increase in the future. In the sequence of RVDT powered devices, let's wait and watch for "what's next."

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1.What are the application of Rvdt?

Woodward's Rotary Variable Differential Transformer (RVDT) position sensors provide unsurpassed reliability and durability for rotary motion-sensing applications. RVDTs are commonly used for flight-critical command and feedback applications such as: Cockpit Controls. Control Surface Feedback.

2.What is the difference between LVDT and Rvdt?

The shape of the LVDT is rectangular whereas the RVDT is cam shaped. The main function of LVDT is to alter the linear motion to an electrical signal, whereas RVDT is used to calculate the angular displacement. The input voltage of LVDT is 1 volt to 24 volts RMS whereas in RVDT will be up to 3V RMS.

3.What is the function of Rvdt?

A Rotary Variable Differential Transformer (RVDT) is an electromechanical transducer that provides a variable alternating current (AC) output voltage that is linearly proportional to the angular displacement of its input shaft.

4.Where is LVDT used?

LVDTs have been widely used in applications such as power turbines, hydraulics, automation, aircraft, satellites, nuclear reactors, and many others. These transducers have low hysteresis and excellent repeatability.
Related Articles

  •  What is a Transformer: Definition, Principle  and Applications
    What is a Transformer: Definition, Principle and Applications
    UTMEL03 November 20218669

    Hi, fellas. I am Rose. Today I will introduce the transformer to you. The device that increases or decreases the voltage in an AC circuit is known as a transformer. The transformer is an AC voltage converter that works on the mutual inductance concept.

    Read More
  • LVDT - Linear Variable Differential Transformer Basics
    LVDT - Linear Variable Differential Transformer Basics
    UTMEL16 January 20219708

    LVDT is the abbreviation of linear variable differential transformer, which belongs to linear displacement sensor. It is a movable iron core transformer that consists of a primary coil, two secondary coils, iron core, coil frame, shell and other components.

    Read More
  • Introduction to Flyback Transformer
    Introduction to Flyback Transformer
    UTMEL29 January 202112154

    As an energy conversion device that transfers energy from one part of the circuit to the other part at constant power, a flyback transformer can be described. Based on the application, the voltage is stepped up to a very high value in a flyback transformer. It is also called a transformer for line output, as the voltage of the output line is fed to the other part of the circuit. The primary winding of the transformer can be powered by a DC circuit with the assistance of the rectifying circuit.

    Read More
  • Audio Transformer-Types, Functions and Working
    Audio Transformer-Types, Functions and Working
    UTMEL05 January 202616003

    An audio transformer is an electromagnetic system designed to separate an input circuit from an output circuit and produce a signal that passes through it with filtering. A varying electromotive force (voltage) in the secondary winding linked to the other circuit is caused by this changing flux.

    Read More
  • RVDT(Rotary Variable Differential Transformer) Basics
    RVDT(Rotary Variable Differential Transformer) Basics
    UTMEL02 February 202121127

    The Rotary Variable Differential Transformer or RVDT is regarded as the transformer that detects the angular displacement of the conductor. That is the kind of electromechanical transducer that gives the angular displacement of the input equal to the linear output.

    Read More

Subscribe to Utmel !

Featured Parts More