web counter
dBm to Watts Calculator

This dBm (decibel milliwatts) Watt Calculator is an online Power conversion tool, which provides you to convert dBm to Watts and calculate Watts from dBm easily. It is more convenient and accurate to use this free RF calculator converting power in dBm to power in watts than converting watts to dBm manually or using Excel table to convert dbm to watts.

dBm to Watts Conversion

Decibel-milliwatt
dBm
To
Watt
W

Power Conversion Formula For dBm TO Watts

Introduction

break down the conversion between Watts and dBm, a key concept in electronics, RF engineering, and communication systems.

dBm to Watt conversion

dBm to Watts Calculator

Use this calculator to convert an absolute power level in dBm to milliwatts or watts, or to convert linear power in watts back to dBm. The conversion is useful for RF, microwave, wireless, optical, and communication-system calculations that span a wide range of power levels.

dBm is referenced to 1 milliwatt. Therefore, 0 dBm equals 1 mW, 10 dBm equals 10 mW, 20 dBm equals 100 mW, and 30 dBm equals 1 W.

How to Use the dBm to Watts Converter

  1. Choose whether the known value is in dBm, milliwatts, or watts.

  2. Enter the known power value.

  3. Run the calculation to display the equivalent power units.

  4. Keep a suitable number of significant digits for the source measurement.

Linear power must be greater than zero when converting watts or milliwatts to dBm because the logarithm of zero is undefined. As power approaches zero, the corresponding dBm value approaches negative infinity.

What Is dBm?

dBm expresses a power level on a base-10 logarithmic scale with a reference power of 1 mW. It is commonly used because a short range of dBm values can represent linear powers ranging from fractions of a picowatt to kilowatts.

The reference is part of the meaning: 0 dBm does not mean zero power. It means that the power equals the 1 mW reference.

What Is a Watt?

The watt, symbol W, is the SI unit of power. One watt equals one joule of energy transferred per second:

1 W = 1 J/s

Common submultiples include the milliwatt, microwatt, nanowatt, and picowatt:

  • 1 mW = 10−3 W

  • 1 µW = 10−6 W

  • 1 nW = 10−9 W

  • 1 pW = 10−12 W

dBm to Watts Formula

Convert dBm to milliwatts with:

PmW = 10PdBm/10

Convert dBm directly to watts with:

PW = 10(PdBm − 30)/10

where PdBm is the power level in dBm, PmW is power in milliwatts, and PW is power in watts.

Example: Convert 20 dBm to Watts

PW = 10(20 − 30)/10 = 10−1 = 0.1 W

Therefore, 20 dBm equals 100 mW or 0.1 W.

Example: Convert 23 dBm to Watts

PW = 10(23 − 30)/10 = 0.199526 W

Therefore, 23 dBm is approximately 199.526 mW.

Example: Convert −85 dBm to Watts

PW = 10(−85 − 30)/10 = 3.16228 × 10−12 W

Therefore, −85 dBm is approximately 3.16228 pW.

Watts to dBm Formula

Convert watts to dBm with:

PdBm = 10 log10(PW/0.001 W)

The equivalent convenient form is:

PdBm = 10 log10(PW) + 30

When power is entered in milliwatts:

PdBm = 10 log10(PmW)

Example: Convert 2 W to dBm

PdBm = 10 log10(2) + 30 = 33.0103 dBm

Example: Convert 50 µW to dBm

First convert 50 µW to 0.05 mW:

PdBm = 10 log10(0.05) = −13.0103 dBm

dBm to Watts Conversion Table

Power LevelPower in WattsConvenient Linear Unit
−120 dBm0.000000000000001 W1 fW
−100 dBm0.0000000000001 W100 fW
−90 dBm0.000000000001 W1 pW
−80 dBm0.00000000001 W10 pW
−70 dBm0.0000000001 W100 pW
−60 dBm0.000000001 W1 nW
−50 dBm0.00000001 W10 nW
−40 dBm0.0000001 W100 nW
−30 dBm0.000001 W1 µW
−20 dBm0.00001 W10 µW
−10 dBm0.0001 W100 µW
0 dBm0.001 W1 mW
1 dBm0.00125893 W1.25893 mW
2 dBm0.00158489 W1.58489 mW
3 dBm0.00199526 W1.99526 mW
4 dBm0.00251189 W2.51189 mW
5 dBm0.00316228 W3.16228 mW
6 dBm0.00398107 W3.98107 mW
7 dBm0.00501187 W5.01187 mW
8 dBm0.00630957 W6.30957 mW
9 dBm0.00794328 W7.94328 mW
10 dBm0.01 W10 mW
13 dBm0.0199526 W19.9526 mW
20 dBm0.1 W100 mW
23 dBm0.199526 W199.526 mW
27 dBm0.501187 W501.187 mW
30 dBm1 W1 W
33 dBm1.99526 W1.99526 W
40 dBm10 W10 W
43 dBm19.9526 W19.9526 W
50 dBm100 W100 W
60 dBm1000 W1 kW

dBm, dB, and dBW

TermMeaningReference
dBmAbsolute logarithmic power level1 mW
dBWAbsolute logarithmic power level1 W
dBLogarithmic ratio between two valuesNo fixed power reference by itself

Because 1 W is 1000 times 1 mW, the relationship is:

PdBm = PdBW + 30

Thus 30 dBm equals 0 dBW, and both represent 1 W.

How a dB Change Affects Power

A power-level difference in dB corresponds to a linear power ratio:

Power ratio = 10ΔdB/10

ChangePower RatioInterpretation
−30 dB0.001One thousandth of the original power
−20 dB0.01One hundredth of the original power
−10 dB0.1One tenth of the original power
−3 dB0.501187Approximately half the power
0 dB1No change
3 dB1.99526Approximately twice the power
6 dB3.98107Approximately four times the power
10 dB10Ten times the power
20 dB100One hundred times the power
30 dB1000One thousand times the power

A 3 dB increase is only an approximation to doubling. An exact factor of two corresponds to approximately 3.0103 dB.

Adding Gains and Power Levels

Add Gain or Loss in dB to a dBm Level

Gains and losses expressed as dB ratios can be added algebraically to an absolute dBm power level. For example:

10 dBm + 20 dB gain − 3 dB loss = 27 dBm

The resulting 27 dBm is approximately 0.501187 W.

Do Not Directly Add Two dBm Values

Two independent power levels must normally be converted to watts or milliwatts, added in linear units, and then converted back to dBm. For two 30 dBm powers:

30 dBm = 1 W; 1 W + 1 W = 2 W; 2 W = 33.0103 dBm

The result is not 60 dBm. When combining coherent signals, phase and the combining network can also affect the measured result, so simple power addition may not describe the complete circuit behavior.

dBm to Voltage Requires an Impedance

dBm describes power, not voltage. To calculate voltage, the load impedance and voltage definition must be known. For power delivered to a purely resistive load:

VRMS = √(PW × R)

For a sine wave only:

Vpeak = √2 × VRMS
   Vpp = 2√2 × VRMS

In a 50 Ω resistive system, 0 dBm corresponds to approximately 0.223607 V RMS and 0.632456 V peak-to-peak for a sine wave. A different impedance produces a different voltage for the same power.

Common Mistakes

  • Treating 0 dBm as zero watts instead of 1 mW.

  • Using 20 rather than 10 as the multiplier for a power ratio in decibels.

  • Forgetting the 30 dB offset between dBm and dBW.

  • Reading 20 dBm as 100 W instead of 100 mW.

  • Adding two dBm power levels directly.

  • Converting dBm to voltage without specifying impedance.

  • Using peak or peak-to-peak voltage where RMS voltage is required.

  • Reporting excessive digits when the measured power has limited accuracy.

dBm Conversion FAQ

How many watts is 0 dBm?

0 dBm equals 1 mW, which is 0.001 W.

How many watts is 10 dBm?

10 dBm equals 10 mW or 0.01 W.

How many watts is 20 dBm?

20 dBm equals 100 mW or 0.1 W.

How many dBm is 1 watt?

1 W equals 1000 mW, so 10 log10(1000) = 30 dBm.

Can dBm be negative?

Yes. A negative dBm value represents a positive power below 1 mW. For example, −30 dBm equals 1 µW. It does not represent negative physical power.

Is dBm a frequency-dependent conversion?

The mathematical conversion between dBm and watts does not depend on frequency. However, the actual delivered or measured power can depend on frequency response, impedance matching, cable loss, calibration, and instrument bandwidth.

Why is 3 dB called a doubling of power?

A 3 dB increase multiplies power by approximately 1.99526, which is close to two. The exact dB value for a factor of two is 10 log10(2), approximately 3.0103 dB.

References

Frequently Asked Questions

What is a dBm signal strength?

dBm stands for decibels per milliwatt. While dB is the expression of a gain and is dimensionless, dBm meaning is a concrete measurement of the power level. It is used to define signal strength in wire and cables at radio and audio frequencies. dBm is measured is very small values.

Can dBm be positive?

Positive dBm means power greater than 1mw and negative means less than 1mw.

Is a higher or lower dBm better?

Strong signal strength results in more reliable connections and higher speeds. Signal strength is represented in -dBm format (0 to -100). This is the power ratio in decibels (dB) of the measured power referenced to one milliwatt. The closer the value is to 0, the stronger the signal.

How much dBm is dangerous?

Phone signal strength shows -51 dBm and 31 asu. I've been looking into this for a while and I have not seen levels this high anywhere else. Thinking somewhere above -65 it gets too excellent and it becomes dangerous, especially on the long term.

Is dBm good or bad?

-80 to -89 dBm, then it's generally considered good signal (3 to 4 bars). -90 to -99 dBm, then it's generally considered average signal (2 to 3 bars). -100 to -109 dBm, then it's generally considered poor signal (1 to 2 bars). -110 to -120 dBm, then it's generally considered very poor signal (0 to 1 bar).

What is a watt equal to?

A unit of measure for power, which measures the rate of energy conversion; equal to one joule per second (or 1/746 horsepower); equivalent to one ampere under a pressure of one volt.

How many watts equal a Volt?

1 watt What Are Volts? A volt, according to BIPM, represents the "potential difference between two points of a conducting wire carrying a constant current of 1 ampere when the power dissipated between these points is equal to 1 watt." The symbol for volt is "V."

Why is Watt A unit of power?

Watt is the unit of power (symbol: W). The watt unit is named after James Watt, the inventor of the steam engine. One watt is defined as the energy consumption rate of one joule per second. One watt is also defined as the current flow of one ampere with voltage of one volt.

What is dBm in terms of watts?

This tool converts power measurements between units of decibel-milliwatts (dBmW) and watts (W). Decibel-milliwatt.

How do you convert dBm to Watts manually?

dbm to watts conversion for radio, radar and microwaves Decibels are used to represent the ratio of two quantities of power: db = 10 log P1/P0 . In the case of dbm the reference power P0 is 1 milliwatt : dbm = 10 log P1/1mw. Inverting this equation gives the power in terms of the reference power: P1= P010db/10.
Hot products

ImagePart NumberManufacturerCategoryPackage/CaseDescriptionPriceQuantityBuy/Quote
BLM18PG121SN1DBLM18PG121SN1DMurata ElectronicsFerrite Beads and Chips0603 (1608 Metric)MURATA - BLM18PG121SN1D - Ferrite Bead, 0603 [1608 Metric], 120 ohm, 2 A, BLM18P Series, 0.05 ohm, ± 25%-

In stock : 355131

Minimum: 1

AD9364BBCZAD9364BBCZAnalog Devices Inc.RF Transceiver ICs144-LFBGA, CSPBGARF Transceiver 1.3V 144-Pin CSP-BGA Tray-

In stock

Minimum: 1

MPZ2012S102AT000MPZ2012S102AT000TDK CorporationFerrite Beads and Chips0805 (2012 Metric)TDK - MPZ2012S102AT000 - FERRITE BEAD, 0.15OHM, 1.5A, 0805-

In stock : 51745

Minimum: 1

SE2537L-RSE2537L-RSkyworks Solutions Inc.RF Amplifiers16-VFQFN Exposed PadRF Amplifier 5GHz Gain 30 dB 3.3Volt -10C 85C-

In stock : 10000

Minimum: 1

CYBL10162-56LQXICYBL10162-56LQXICypress Semiconductor CorpRF Transceiver ICs56-UFQFN Exposed PadMCU 32-Bit CYBL10X6X ARM Cortex M0 RISC 128KB Flash 1.8V/2.5V/3.3V/5V 56-Pin QFN EP Tray-

In stock : 48

Minimum: 1

SKY81294-14-001SKY81294-14-001Skyworks Solutions Inc.PMIC - LED Drivers9-BGA, WLCSPIC LED FLASH DVR 1.2V 9CSP
  • 1:$0.462347
  • 10:$0.436176
  • 100:$0.411487
  • 500:$0.388195

In stock : 1000

Minimum: 1

HSMS-282P-TR1GHSMS-282P-TR1GBroadcom LimitedDiodes - RF6-TSSOP, SC-88, SOT-363Diode Schottky 15V 6-Pin SOT-363 T/R-

In stock

Minimum: 1

80HCPS1432CRM80HCPS1432CRMRenesas Electronics America Inc.Specialized ICs576-BBGA, FCBGAIC SER RAPIDIO SWITCH 576FCBGA-

In stock

Minimum: 1

ALT6702RM45Q7ALT6702RM45Q7Skyworks Solutions Inc.RF Amplifiers-IC RF AMP CELLULAR SMD-

In stock

Minimum: 1

SI8261BBD-C-ISSI8261BBD-C-ISSilicon LabsIsolators - Gate Drivers6-SOIC (0.295, 7.50mm Width)4A Gate Driver Capacitive Coupling 5000Vrms 1 Channel 6-SDIP
  • 1:$7.590526
  • 10:$7.160874
  • 100:$6.755541
  • 500:$6.373152

In stock : 9020

Minimum: 1

SI8261BAD-C-ISSI8261BAD-C-ISSilicon LabsIsolators - Gate Drivers6-SOIC (0.295, 7.50mm Width)Gate Drivers 5kV Opto input Sgl channel 4.0A driver
  • 1:$4.552744
  • 10:$4.295042
  • 100:$4.051926
  • 500:$3.822572

In stock : 100000

Minimum: 1

CSR8510A06-ICXR-RCSR8510A06-ICXR-RQualcommRF Transceiver ICs6-XFBGAIC RF TXRX BLUETOOTH 6XFBGA-

In stock

Minimum: 1

FOD8333FOD8333ON SemiconductorIsolators - Gate Drivers16-SOIC (0.295, 7.50mm Width)Optocoupler AC/DC-IN 1-CH DC-OUT 16-Pin SO Rail
  • 1:$7.111464
  • 10:$6.708928
  • 100:$6.329178
  • 500:$5.970922

In stock : 50

Minimum: 1

FOD8332R2FOD8332R2ON SemiconductorIsolators - Gate Drivers16-SOIC (0.295, 7.50mm Width)OPTOISO 4.243KV GATE DRIVER 16SO-

In stock : 11

Minimum: 1

SP1004U-ULC-04UTGSP1004U-ULC-04UTGLittelfuse Inc.TVS - Diodes10-XFDFNTVS DIODE 9.2V 1004/10DFN-

In stock : 2633

Minimum: 1

ISM303DACTRISM303DACTRSTMicroelectronicsMultifunction-HIGH PERFORMANCELOW POWER COMPAC-

In stock : 4138

Minimum: 1

SLD8S36ASLD8S36ALittelfuse Inc.TVS - DiodesNonstandard SMDTVS DIODE 36.5V 58.1V SMTO-263-

In stock : 20

Minimum: 1

ACPL-302J-500EACPL-302J-500EBroadcom LimitedIsolators - Gate Drivers16-SOIC (0.295, 7.50mm Width)OPTOISO 5KV 1CH GATE DRIVER 16SO
  • 1:$6.881778
  • 10:$6.492243
  • 100:$6.124758
  • 500:$5.778074

In stock : 36800

Minimum: 1

UR020-006-RAUR020-006-RATripp LiteUSB Cables-TRIPP-LITE UR020-006-RACOMPUTER CABLE, USB, 6FT, BLACK-

In stock

Minimum: 1

SFH 4713ASFH 4713AOSRAM Opto Semiconductors Inc.Infrared, UV, Visible Emitters3-SMD, No LeadEMITTER IR 860NM 1A-

In stock : 6000

Minimum: 1