Sort by
What is NAND Flash?04 November 2021
NAND Flash is a better storage device than hard disk drives and is particularly evident in low-volume applications up to 4GB. As the quest continues for lower power consumption, lighter weight, and better performance, NAND is proving to be very attractive. Its development goal is to reduce the cost per bit of storage and increase storage capacity.
What is a Transformer: Definition, Principle and Applications03 November 2021
Hi, fellas. I am Rose. Today I will introduce the transformer to you. The device that increases or decreases the voltage in an AC circuit is known as a transformer. The transformer is an AC voltage converter that works on the mutual inductance concept.
Memory Chip: The Key to Smart Connectivity03 November 2021
In today's post, we talk about memory chips, especially their emerging applications in the AIoT smart interconnect space.
Is there a Limit to the Chip Process Node?02 November 2021
Process node refers to the spacing between circuits within an integrated circuit, specifically, the line width of the gate in the transistor structure, which is the value in the XXnm process. The narrower the width, the lower the power consumption.
What is Resistor?02 November 2021
Hello, I am Rose. Weilcome to the new post today. Today I will introduce resistor to you. Resistor is one of the three main passive components of electronics, along with inductors and capacitors; from an energy standpoint, resistance is an energy-consuming component that turns electrical energy into heat.
What is an LDO (Low Dropout Regulator)?29 October 2021
Hello everyone. Today I would like to introduce you to LDO (low dropout regulator), a low dropout linear regulator. I hope it will help you understand LDO better.
What is VCSEL?28 October 2021
Hello everyone, I am Rose. I welcome you on board, today I will introduce VCSEL to you. The Vertical-Cavity Surface-Emitting Laser (VCSEL, or Vertical-Cavity Surface-Emitting Laser) is a semiconductor whose laser is emitted perpendicular to the top surface. It differs from an edge-fired laser, which emits the laser from the edge.
What are Quantum Sensors?27 October 2021
Today, I will introduce you to the basics of quantum sensors, including theory, concept and status, performance, and applications.
What are the Types of Audio Cables?27 October 2021
Today, I will introduce you to some common audio cables. I hope you will have a new understanding of the cable of the audio equipment.
All You Need to Know about Wireless Access Point26 October 2021
Wireless Access Point (WAP) is a wireless switch used for wireless networks, providing the function of transmitting and receiving wireless signals, and is also the core of wireless networks.
What is Smoke Detector?26 October 2021
Hello everyone, I am Rose. Welcome back to the new post today. The smoke sensor detects whether or not there is smoke in the environment, as well as the concentration of smoke, such as sensing intense smoke during a fire. When the smoke probe comes into contact with smoke or another gas, its internal resistance changes, and an analog value is created to regulate it.
What is Potentiometer?25 October 2021
Hello, I am Rose. Welcome back to the new post today. The potentiometer is a type of electromechanical component that can be found in a variety of instruments and electronic devices. A potentiometer is a resistance that can be adjusted and changed, and it is an electronic component that can be modified. This article mainly introduces structure, classification, electrical parameters and model name and type of potentiometer.


Product
Brand
Articles
Tools