Sort by
An Overview of Bipolar Transistors27 August 2020
Bipolar Transistor, full name bipolar junction transistor(BJT), is an electronic device with three terminals, made of three parts of semiconductors with different levels of doping. The charge flow in the transistor is mainly due to the diffusion and drift movement of carriers at the PN junction.
What is a Piezoelectric Sensor?26 August 2020
A piezoelectric sensor is a sensor based on the piezoelectric effect. It is a self-generating and electromechanical conversion sensor.
How does a Resettable Fuse Work?26 August 2020
A resettable fuse is a kind of over-current electronic protection component. It is made of a high-molecular organic polymer under high pressure, high temperature, and sulfidation reaction. It's mixed with conductive particle materials, and processed by special technology.
Tunnel Diode: Definition, Features and Tunneling Process25 August 2020
Tunnel diode, also known as Ezaki diode, is a crystal diode with tunnel effect current as the main current component. The tunnel diode is a semiconductor diode made of a mixture of gallium arsenide (GaAs) and gallium antimonide (GaSb).
Introduction to Wireless Sensor Networks20 August 2020
The component modules of the wireless sensor are encapsulated in a shell. When it is working, it will be powered by a battery or a vibration generator to form a wireless sensor network node. It consists of randomly distributed micro nodes integrated with sensors, data processing units, and communication modules. The way of self-organizing constitutes a network. The wireless sensor network system usually includes sensor nodes, sink nodes, and management nodes.
An Overview of JFET19 August 2020
JFET is a Junction field-effect transistor. Regular transistor is a current-controlled device that requires biasing power, while JFET is a voltage-controlled device. The JFET is an active electronic component that is one of the electronics industry's workhorses that offers a reasonable compromise between cost and efficiency.
Introduction to Microprocessors18 August 2020
The microprocessor is the central unit of a computer system performing arithmetic and logic operations which typically involve adding, subtracting, moving numbers from one field to another, and comparing two numbers. It's often simply referred to as a processor, a central processing unit, or a logic chip.
How does a Photodiode Work?15 August 2020
A photodiode is a special diode (light-receiving device) that converts optical signals into electrical signals.It has a pn junction, and its shell has a window with glass for light penetration.So how does it work and how do we use it? Read this article to find the answer.
What is a Memory Controller?12 August 2020
The memory controller is an important part of the computer system that controls the memory and is responsible for data exchange between the memory and the CPU. The memory controller determines the maximum memory capacity that the computer system can use, the number of memory banks, memory type and speed, memory particle data depth and data width, and other important parameters. The memory controller determines the memory performance of the computer system and therefore has a greater impact on the overall performance of the computer system.
Rectifier Diode: Function and Circuit12 August 2020
Rectifier Diode is a semiconductor device used to convert alternating current to direct current.It has obvious unidirectional conductivity, and can be made of materials such as semiconductor germanium or silicon. This article gives you a brief introduction to rectifier diodes.
How do Transistors Work?10 August 2020
A transistor is a kind of semiconductor device that controls current. Its function is to amplify the weak signal into an electrical signal with a larger amplitude value, and it is also used as a contactless switch.
An Overview of Common Mode Chokes10 August 2020
Common mode chokes are often used in computer switching power supplies to filter common mode electromagnetic interference signals. This article helps you learn about the Features, Working Principle, Selection Method, Precautions, and Core Material of common mode chokes. Click for more.


Product
Brand
Articles
Tools