Sort by
What is FIR Filter?24 September 2020
FIR (Finite Impulse Response) filter is a finite-length unit impulse response filter, also known as a non-recursive filter, which is the most basic element in a digital signal processing system. It can guarantee arbitrary amplitude-frequency characteristics while having strict linear phase-frequency characteristics, and its unit sampling response is finite, so the filter is a stable system.
Introduction to Potential Transformers21 September 2020
A potential transformer is a device used to transform voltage. The purpose to transform the voltage is mainly for measuring instruments, as the power supply of relays, measure the voltage, power, and energy of the line, or protecting the valuable equipment, motors, and transformers in the line when the line fails.
Solid State Relay Basics: Working, Features and Structure17 September 2020
Solid State Relay (SSR) is a non-contact switch composed of microelectronic circuits, discrete electronic devices, and power electronic power devices. The isolation device is used to realize the isolation between the control end and the load end. The input terminal of the solid state relay uses a tiny control signal to directly drive a large current load.
An Overview of Isolation Transformers17 September 2020
An isolation transformer is a transformer in which the input and output windings are electrically isolated. The isolation transformer is to isolate the current of the primary winding and the secondary winding respectively.
Introduction to Mass Air Flow Sensor15 September 2020
Mass air flow sensor is one of the important sensors of EFI engines. It converts the inhaled air flow into an electric signal and sends it to the electronic control unit (ECU). As one of the basic signals for determining fuel injection, it is a sensor that measures the air flow into the engine.
Basic Understanding of Attenuators15 September 2020
An attenuator is used to introduce a predetermined attenuation within a specified frequency range. It is generally indicated by the decibel of the attenuation introduced and the ohm of its characteristic impedance.
What is a Gyroscope Sensor?11 September 2020
A gyroscope is a device used to sense and maintain direction, designed based on the theory of indestructible angular momentum. The gyroscope sensor is a simple and easy-to-use positioning and control system based on free space movement and gestures.
Introduction to TRIAC and TRIAC Dimmer10 September 2020
TRIAC is developed based on ordinary thyristors. It can not only replace two thyristors connected in parallel with reverse polarity, but also only needs one trigger circuit, which is an ideal AC switching device...
Multivibrator: Circuits, Types and Application08 September 2020
A multivibrator uses deep positive feedback, to turn on and off two electronic devices alternately through the resistance-capacitance coupling, thereby self-excites and generates a square wave output. It's often used as a square wave generator...
What are Programmable Logic Controllers?07 September 2020
Programmable Logic Controller(PLC) is an electronic system operated by digital operations, specially designed for application in an industrial environment. It uses a memory that can be programmed to execute instructions for storing logical operations and sequence control, timing, counting and arithmetic operations.
What is a Radar Sensor?04 September 2020
A radar sensor is a conversion device that can convert microwave echo signals into electrical signals. The radar sensing is a wireless sensing technology that extracts and discovers the target's position, shape, motion characteristics and motion trajectory by analyzing the received target echo characteristics.
Introduction to Voltage Stabilizer03 September 2020
A voltage stabilizer is a device that stabilizes the output voltage. The voltage stabilizer is composed of a voltage stabilizer circuit, a control circuit, and a servo motor. When the input voltage or load changes, the control circuit samples, compares, and amplifies, and then drives the servo motor to rotate to change the position of the carbon brush of the voltage stabilizer. The coil turns ratio is automatically adjusted to keep the output voltage stable.


Product
Brand
Articles
Tools