Sort by
Introduction to Step-down Transformers14 October 2020
The step-down transformer is a transformer that converts the higher voltage at the input terminal into an ideal low voltage output, so as to achieve the purpose of step-down. The step-down transformer is a very important equipment in the power transmission and transformation system. Its normal operation not only relates to its own safety and reliable power supply for users, but also directly affects the stability of the power system...
What is an Electromagnetic Relay?13 October 2020
Electromagnetic relay is an electronic control device. It has a control system (also called an input loop) and a controlled system (also called an output loop). It is usually used in automatic control circuits. It actually a kind of "automatic switch" that uses a smaller current and a lower current to control a larger current and a higher voltage. Therefore, it plays the role of automatic adjustment, safety protection, and conversion circuit in the circuit.
An Overview of Thermal Overload Relays12 October 2020
Thermal overload relays are protective electrical appliances used for overload protection of motors or other electrical equipment and electrical circuits, The thermal overload relay is mainly used for overload protection of asynchronous motors. After the overload current passes through the thermal element, the bimetallic sheet is heated and bent to push the action mechanism to drive the contact...
How do We Select Automotive Relays?30 September 2020
A relay is an automatic control device whose output will have saltatory change when the input (electricity, magnetism, sound, light, heat) reaches a certain value. Automotive relays are relays used in automobiles. Such relays have high switching load power, high shock resistance and vibration resistance. Most power supplies in automobiles use 12V, and most of the coil voltages are designed to be 12V...
What is Field Programmable Gate Array?29 September 2020
Field Programmable Gate Array (FPGA) is a product of further development on the basis of programmable devices such as PAL and GAL. It emerged as a semi-custom circuit in the field of application-specific integrated circuits (ASIC), which not only solves the deficiencies of custom circuits but also overcomes the shortcomings of the limited number of gate circuits of the original programmable devices.
What is Electronic Ballast?28 September 2020
Electronic Ballast is a kind of ballast, which uses electronic technology to drive the electric light source to produce the required lighting. Corresponding to it is the inductive ballast. More and more modern fluorescent lamps use electronic ballasts, which are light and compact, and people can even integrate electronic ballasts with lamps.
Introduction to Silicon Controlled Rectifier25 September 2020
Silicon Controlled Rectifier, abbreviated as SCR, is a high-power electrical component, also known as a thyristor. It has the advantages of small size, high efficiency and long life. In the automatic control system, it can be used as a high-power drive device to realize the control of high-power equipment with low-power controls. It has been widely used in AC and DC motor speed control system, power control system and servo system.
What is FIR Filter?24 September 2020
FIR (Finite Impulse Response) filter is a finite-length unit impulse response filter, also known as a non-recursive filter, which is the most basic element in a digital signal processing system. It can guarantee arbitrary amplitude-frequency characteristics while having strict linear phase-frequency characteristics, and its unit sampling response is finite, so the filter is a stable system.
Introduction to Potential Transformers21 September 2020
A potential transformer is a device used to transform voltage. The purpose to transform the voltage is mainly for measuring instruments, as the power supply of relays, measure the voltage, power, and energy of the line, or protecting the valuable equipment, motors, and transformers in the line when the line fails.
Solid State Relay Basics: Working, Features and Structure17 September 2020
Solid State Relay (SSR) is a non-contact switch composed of microelectronic circuits, discrete electronic devices, and power electronic power devices. The isolation device is used to realize the isolation between the control end and the load end. The input terminal of the solid state relay uses a tiny control signal to directly drive a large current load.
An Overview of Isolation Transformers17 September 2020
An isolation transformer is a transformer in which the input and output windings are electrically isolated. The isolation transformer is to isolate the current of the primary winding and the secondary winding respectively.
Introduction to Mass Air Flow Sensor15 September 2020
Mass air flow sensor is one of the important sensors of EFI engines. It converts the inhaled air flow into an electric signal and sends it to the electronic control unit (ECU). As one of the basic signals for determining fuel injection, it is a sensor that measures the air flow into the engine.


Product
Brand
Articles
Tools