Chip Filters, Piezoelectric Materials and the Piezoelectric Effect

Understanding Piezoelectric effect!
| Topics covered in this article: |
| Ⅰ. Piezo History |
| Ⅱ. Piezoelectric Applications |
| Ⅲ. Piezoelectric Principle |
| Ⅳ. Piezoelectric Equation |
| Ⅴ. Piezoelectric material |
Piezoelectric material, it has a magical effect - the piezoelectric effect. It is this piezoelectric effect that combines electromagnetic waves with sound waves (mechanical waves). So today, let's learn about this magical piezoelectric effect.
Ⅰ. Piezo History

Figure. 1
At the Paris Academy of Sciences in 1880, brothers Pierre and Jacques Curie served as lab assistants. They discovered that pressing crystals like quartz, tourmaline, and Rochelle salt produced an electrical charge on their surfaces. The direct piezoelectric effect is the name given to the mechanism by which mechanical energy is transformed into electrical energy. The Greek word "piezo" means "to press." If one pulls or squeezes along the main axis (of a quartz block), an equal amount of the opposite sign appears at the end of that axis, which is proportional to the force and independent of the size of the quartz. This observation was later summarized by Jacques in his 1889 paper Annales de Chimie et de Physique.

Figure. 2
Gabriel Lippman anticipated the opposite result in 1881 using a mathematical derivation of basic thermodynamic principles, namely that the application of an electric field to these materials would cause internal mechanical strains. Through tests, the Curies swiftly proved this inverse piezoelectric effect.

Figure. 3
In the latter quarter of the 19th century, piezoelectricity emerged as a new field of study, piqued by the scientific community's intense interest in the phenomenon. The result of this investigation was Woldemar Voigt's 1910 textbook Lehrbuch der Kristallphysik, which listed 20 categories of naturally occurring crystals that exhibit piezoelectric properties.

Figure. 4
Although Curie's discovery has sparked interest in the scientific community, it will be some time before the first practical application of piezoelectric materials.
Ⅱ. Piezoelectric Applications
Sonar was created by Paul Langevin and his associates in France during the First World War and was the first practical application. They created an underwater ultrasonic probe that consists of two steel plates sandwiching a sensor and a hydrophone constructed of thin quartz crystals. The hydrophone picks up the return echo when the transducer pulses a high frequency into the water. The depth can be determined by timing the amount of time it takes to hear the echo.

Figure. 5
After the war, the detector design was finally perfected. However, the project's success has generated a lot of interest in piezoelectric technology in industrialized nations. As a result, numerous novel uses for piezoelectric crystals were created during World Wars I and II, including signal filters, microphones, accelerometers, and phonograph pickups.

Figure. 6
The elasticity and viscosity of materials are also measured using upgraded ultrasonic transducers. Research on materials has greatly advanced as a result of this. Additionally, the advancement of time domain reflectometry made it possible to discover flaws in cast metal and stone items that were previously undetectable, increasing structural safety.

Figure. 7
Natural substances like quartz, tourmaline, and Rochelle salts have a negligibly modest piezoelectric effect. The piezoelectric constants of a class of synthetic materials known as ferroelectrics are significantly higher than those of natural materials.

Figure. 8
During World War II, research teams from three nations (the US, Japan, and Russia) independently developed the ferroelectric ceramic substance barium titanate (BaTiO3). Scientists at the Tokyo Institute of Technology created lead zirconate titanate (PZT) in 1952, which has a better sensitivity and operating temperature.

Figure. 9
The United States has made great technological progress in the decades since World War II, but piezoelectric device market development has lagged behind this scientific progress. This is explained by the secrecy surrounding the business operations of the organization where the growth is taking place. This may have been attributed in part to the industry's start during World War II and in part to the idea that patents and exclusive techniques would lead to significant financial gains.

Figure. 10
In contrast, producers in Japan collaborate to quickly resolve technological issues and open up new markets. New families of non-patentable piezoelectric ceramics have also been developed as a result of materials research. Piezoelectric ceramic igniters and signal filters for TV and radio sectors are among the goods created by Japanese producers.

Figure. 11
Ⅲ. Piezoelectric Principle
From the history of the discovery of piezoelectricity, we know that the inverse piezoelectric effect is the process by which materials are deformed by voltage, that is, electrical energy is converted into mechanical energy. The piezoelectric effect is the process by which materials are subjected to pressure to generate voltage, that is, the process of converting mechanical energy into electrical energy. the action of. The piezoelectric effect is schematically depicted in the figure below.

Figure. 12
This results from the uniqueness of the subject matter. Regular crystals are identified by their unit cells, an ordered and repeating structure of atoms connected by bonds.Even if deformation is applied, the overall charge centers of positive and negative ions balance out in the unit cell of non-piezoelectric materials, preventing overall polarization. such as copper, iron, and other metals.

Figure. 13
For piezoelectric materials, the crystal's structure is asymmetrical, but when no external force is applied, the crystal is in a stable state and doesn't display electrical polarity to the outside. However, when an external force is applied, the crystal's atoms will be dispersed and the electricity inside will be dispersed. Electrical polarity is created when the balance shifts. The crystals in a piezoelectric substance similarly expand and compress as you apply a voltage, transforming electrical energy into mechanical energy.

Figure. 14
Ⅳ. Piezoelectric Equation
Through the aforementioned explanation, it is clear that the piezoelectric effect essentially relates to a material's combination of mechanical and electrical capabilities. Hooke's law for elastic materials must be met for the mechanical properties of materials to exist:

Figure. 15
in the formula
S is the strain of the material
T is the pressure
s is the strain factor of the material
For the electrical properties of the material, it can be described by the electrical displacement equation

Figure. 16
in the formula
D is the electrical displacement density
e refers to the relative permittivity of the material
E is the electric field strength
As demonstrated in the following equation, which is the most fundamental equation of the piezoelectric effect, these equations can be combined to construct a piezoelectric coupling equation. The piezoelectric characteristics and piezoelectric coefficients of various piezoelectric materials differ from one another. For instance, the quartz's pressure Lead zirconate titanate (PZT) has a piezoelectric value of 3 10 -10 and an electrical coefficient of 3 10 -12.

Figure. 17
Ⅴ. Piezoelectric material
The Curies investigated the surface charges of numerous substances during the discovery of the piezoelectric effect and discovered that substances like sucrose, tourmaline, quartz, topaz, and Rochelle salt have the piezoelectric effect. They also discovered the characteristics of quartz and Rochelle salt. The greatest effect is the piezoelectric effect. More and more piezoelectric materials are being created as a result of scientists' ongoing research. We categorize them into the following groups.
① Natural Crystals: Quartz, Sucrose, Rochelle Salt, Topaz, Tourmaline, Berlin Stone.
② Artificial crystal: Gallium orthophosphate (GaPO 4 ), Langasite (La 3 Ga 5 SiO 14 )
③ Piezoelectric ceramics: barium titanate (BaTiO 3 ) lead titanate (PbTiO 3 ) lead zirconate titanate (PZT) potassium niobate (KNbO 3 ) lithium niobate (LiNbO 3 ) lithium tantalate (LiTaO 3 ) sodium tungstate (Na 2 WO 4 ) Sodium Potassium Niobate (NaKNb) Bismuth Ferrite (BiFeO 3 ) Sodium Niobate (NaNbO 3 ) Aluminum Nitride ALN Zinc Oxide ZnO
④ Biopiezoelectric materials: tendon wood silk enamel dentin collagen
In the sphere of radio frequency, materials serve as the foundation for technical advancement. The significant advancement in radio frequency design has been facilitated by the use of piezoelectric materials as well as gallium nitride. The majority of those who work in radio frequency lack the necessary material science skills, thus we hope that this article will provide us a basic grasp of piezoelectric materials.
1. What is Piezoelectric Material?
Piezoelectric materials are crystalline materials that develop a voltage across both ends when subjected to pressure. The use of piezoelectric materials can realize the mutual conversion of mechanical vibration (sound wave) and alternating current.
2. How many categories can Piezoelectric materials be divided into?
Divided into 2 categories: 1. Inorganic piezoelectric materials (piezoelectric crystals and piezoelectric ceramics); 2. Organic piezoelectric materials (also known as piezoelectric polymers). (If there is a third category, it is composite piezoelectric materials) .
3. What are the applications of piezoelectric materials?
The application fields of piezoelectric materials can be roughly divided into two categories: vibratory energy and ultrasonic vibration energy-electrical energy transducer applications, including electroacoustic transducers, underwater acoustic transducers and ultrasonic transducers, etc., as well as other sensors and driver applications.
What is a High-pass Filter?UTMEL10 March 202114507A high-pass filter is a combination device of capacitors, inductances, and resistors that allow signal components above a certain frequency to pass, while greatly suppressing signal components below that frequency. The high-pass filter only attenuates the frequency components below a given frequency, and allows the frequency components above the cutoff frequency to pass, and there is no phase shift filtering process. Mainly used to eliminate low-frequency noise, also called low-cut filter.
Read More
Introduction to Pi FilterUTMEL19 February 202115474A Pi filter is a type of filter with a two-port, three-terminal block consisting of three elements with two terminals in each element: the first element is connected to the GND terminal via i/p, the second terminals are connected to the terminals from i/p to o/p and the third element is connected to the terminals from o/p to GND. The circuit model is going to be like a 'Pi' symbol. Capacitors and one inductor are the elements used in the circuit.
Read More
EMI Filter: Introduction, Functions and ApplicationsUTMEL23 December 202013397Electromagnetic interference filter, also known as "EMI filter" is an electronic circuit device used to suppress electromagnetic interference, especially noise in power lines or control signal lines. The EMI filter functions as two low-pass filters: one is to attenuate common mode interference, and the other is to attenuate differential mode interference. It is top choice for electronic equipment design engineers to control conducted electromagnetic interference and radiated electromagnetic interference.
Read More
SAW Filter: Introduction, Features and ApplicationsUTMEL30 December 202010496The Surface Acoustic Wave (SAW) filter is a passive band-pass filter made by using the piezoelectric effect and the physical characteristics of surface acoustic wave propagation. Its role is to filter and delay electrical signals. It has the advantages of small size, stable performance, strong overload capacity, low phase distortion, and no need to adjust, so it is used in televisions, video recorders, wireless data transmission systems and other fields.
Read More
Introduction to Bandstop FilterUTMEL28 January 20219352There are numerous filter types, including high-pass filters, low-pass filters, bandpass filters, and filters for bandstops. The high-pass filter only allows frequencies greater than the cut-off frequency, and the low-pass filter allows frequencies smaller than the cut-off frequencies. A specific band of frequencies will be permitted by the bandpass filter and a band stop filter will reject a specific band of frequencies. An overview of the bandstop filter is discussed in this article.
Read More
Subscribe to Utmel !
CTSL1112F-6R8MCentral
CTLVC6045F-4R7NCentral
PE-0805CD111JTTPulse
74438366010Wurth Electronics
SGIHLP34EBBR10M81SVishay
B66453KX149TDK
SGIHLP34EBTR10M81NVishay
B65811J40A87TDK
LMLP07A7M4R7DTASKYOCERA
IMC1210ER270K35Vishay


Product
Brand
Articles
Tools