Introduction to Centrifugal Switch

Electronic Centrifugal Switches ( SAMUSCO )
Catalog
| I. Working Principle |
| II. Functions |
| III. Applications |
I. Working Principle
A centrifugal switch is an electrical switch commonly used in induction motors and split-phase induction motors for the signal phase. During the 1920s, Royal Lee won a patent for the centrifugal switch. This switch is used to provide the controlled switching operation needed for motors when generating a specified motor speed. Earlier, before the invention of this switch, the motor switches were placed within the motor frame to simplify the construction of the motor switches. This design was quite unsatisfactory because it led to the accumulation of those switches of oil, dust, grease. This in turn rendered the operation of communication unreliable.
A typical centrifugal switch consists of a centrifugal mechanism mounted on a motor shaft and a fixed stationary switch.

Using electrical contacts, the centrifugal device mounted on the motor shaft rotates along with the shaft and is connected to the stationary switch to control the start-winding circuit in the induction motor.
This switch operates on the concept of centrifugal force, as the same implies. This is a fictional force that acts on the spinning bodies.
When a body moves in a circular motion, according to Newton mechanics, a force is produced from the center of the circle that tends to drive the body away from the center. This force is known as the force of centrifuges. It is created due to the inertia of the body. On the body, this force works and pushes it away from the core. In washing machines, this principle is used as well.
A centrifugal switch is a type of switch and an electronic symbol may be used to represent it. An electronic symbol is a pictogram used to describe different electrical and electronic devices or functions, such as wires, batteries, resistors, and transistors, in the schematic diagram of an electrical or electronic circuit.
In electrical engineering, a switch is an electrical function that can disconnect or link the conducting route in an electrical circuit, interrupt or redirect the electrical current from one conductor to another.
A switch that is controlled by shaft rotation is a centrifugal switch. By opening only at increasing speed, it is receptive to velocity or direction.
II. Functions
Centrifugal Switch in Induction Motors
To understand the function of this switch in induction engines, let us first understand the induction engine model. A single stator winding and auxiliary winding consist of induction motors. For the stator winding, a single-phase AC current is applied. But the single winding of the stator does not produce sufficient rotating fields to generate the starting torque. Therefore, it provides an auxiliary winding.
This auxiliary winding produces a field that is out of phase with the stator winding field produced. The resulting field, therefore, induces a starting torque and starts the engine. If the engine is started, a pulsating field that does not include the filed stator is set up by the rotor.
The circuit that energizes the auxiliary winding has to be disconnected when the motor speed exceeds a specified percentage of the synchronous speed. For induction motors, this is where the centrifugal switch comes into the frame. Here, the centrifugal switch helps to open and detach the auxiliary winding circuit.
Functions
Take a look at how in an induction motor the centrifugal switch works. A spring dish with calibrated weights attached to its base, backed by a steel plate, is the centrifugal mechanism mounted on the motor shafts. To provide the auxiliary winding with the necessary power to generate the starting torque, the switch contacts are closed.
The calibrated weights feel centrifugal strength as the rotor rotates. The switch contacts are opened due to the centrifugal force at a certain speed as this force overcomes the spring force of the disc. The weights are shifted away from the rotor shaft here, thereby disconnecting the circuit from the auxiliary winding.
At the critical operating point, three factors can be seen:
- The spring force reduces at a linear rate.
- The centrifugal force increases at a rate proportional to the speed of the rotor.
- The radius of the weights is increased.
How to test:
1. The following criteria should be met by an ideal centrifugal switch:
2. Throughout its life cycle, the process should be uniform. For simplicity of design and low production cost, the number of components of the equipment should be minimal.
3. It should have marginal elements of friction.
4. Cut-out /Cut-in ratio should be changeable quickly without causing any significant design modifications.
The switch is readily accessible as the communication unit of the switch is present on the outside of the motor frame. So, without dismantling the motor assembly, the switch can be tested, washed, and replaced.
III. Applications
This switch is often used in systems where speed detection in systems is necessary for the computer to be safe and operate properly. The following are some of the uses of the centrifugal switch:
1. Defense against Overspeed in motors, generators, etc.
2. Used for DC generators, conveyors, escalators, lifts, etc...
3. These are also used in devices such as blowers, fans as well as conveyors to detect under-speed.
4. Material losses are often used in systems where the loss of speed could lead to device damage.
The centrifugal switch offers good contact reliability compared to the switches used earlier for the same reason. As this switch is not present inside the motor frame, it is separated from dirt, grease, oil, which normally gets through circulating air currents into the motor frame.
What happens if the centrifugal switch does not open?
If the start switch does not open when it is needed, the start winding will overheat and flame out, and the engine will not start next time. If the centrifugal start switch is not closed, the engine will overheat the main winding without any main winding failure.
What is the effect if the centrifugal switch is not disconnected after the motor starts?
The centrifugal switch should be disconnected at about 70 to 80 per cent of the full speed of the engine. If it is not disconnected, a heavy current will continue to flow through the starting winding of the engine, which eventually results in the failure of the starting winding and engine. Also, the speed and the current cannot reach its maximum.
What is the purpose of a centrifugal switch in the end of an open motor?
A centrifugal switch is an electrical switch that operates using the centrifugal force generated by a rotating shaft, most commonly an electric motor or a gasoline engine. Here, the switch is used to disconnect the starting winding of the engine as soon as the engine is approaching its normal operating speed.
Do all single phase motors have a centrifugal switch?
There is no centrifugal switch so that the start winding becomes an auxiliary winding when the engine reaches running speed, making it essentially a two-phase motor. They are considered to be the most reliable single-phase motors because there is no centrifugal starting switch.
Why is the Centrifugal Switch Used in Most Single-Phase Induction Motors?
The centrifugal switches are used along with the additional winding to start the engine in all traditional induction motors used in drill presses, furnaces, table saws, pumps, grinders, washers and dryers. Single-phase induction motors require auxiliary circuits to be started. They can be on the circuit at all times in very small engines, like cooling fans. But energy is wasted and it produces heat. In a small engine, this is tolerable, but it becomes tempting to turn off the starting circuit after the engine is spinning past 1/10hp or so. To do this, a centrifugal switch is used. For the single-phase, the common induction motor does not start on its own, it only sits still and noisy for about 30 seconds and then burns the insulation off the coils. So we've got to start, and that's where the centrifugal switch comes in, along with the extra winding. With an additional winding, the motor starts happily on its own. However, before the full speed is reached, this must be switched off; otherwise the original winding will be burned off, as the subsidiary winding is only scheduled for a few seconds. During engine operation, three factors can be seen. The power of the spring decreases in a linear way. The centrifugal force rises at a rate proportional to the speed of the rotor. The radius will be increased by weight.
The Complete Guide to DPDT Switches: Function, Wiring, and ApplicationsUTMEL23 May 20262869This comprehensive guide explores Double Pole Double Throw (DPDT) switches, explaining their core anatomy, distinct ON-ON and ON-OFF-ON configurations, and essential wiring methods like DC motor polarity reversal and A/B source selection. It also covers various physical designs, selection criteria such as ratings and materials, and effective troubleshooting steps to resolve common circuit failures.
Read More
Long Life Small Volume Detector Switch for Intelligent ApplicationsUTMEL16 March 20224984Hello everyone, I am Rose. Welcome to the new post today. This article will introduce what is a detection switch, how to choose a detection switch and where to use a detection switch.
Read More
Analog Switch: Types and ApplicationUTMEL25 March 202115912The analog switch is mainly to complete the signal switching function in the signal chain. The switching mode of the MOS tube is adopted to realize the switching off or on of the signal link.
Read More
Toggle Switches: Features, Types and ApplicationsUTMEL23 January 202111423Toggle switch adopts integrated circuit technology and SMT appearance device technology to manufacture a new generation of photoelectric switch devices. It has intelligent functions such as delay, expansion, external synchronization, anti-interference, high reliability, stable working area, and self-diagnosis. This novel photoelectric switch is an active photoelectric detection system electronic switch that uses pulse modulation. The cold light source used is infrared light, red light, green light and blue light, etc., which can be quickly and without contact and damage Control the state and action of various solid, liquid, transparent, black, soft, smoke and other substances.
Read More
DIP Switch: Introduction and ClassificationUTMEL20 January 202117499DIP switch is an address switch used for operation control, using the principle of 0/1 binary coding. It is a miniature switch that can be toggled by hand. Dip switches are widely used in data processing, communication, remote control and anti-theft automatic alarm systems and other products that require manual programming.
Read More
Subscribe to Utmel !


Product
Brand
Articles
Tools