Toggle Switches: Features, Types and Applications

Published: 23 January 2021 | Last Updated: 23 January 202111067
Toggle switch adopts integrated circuit technology and SMT appearance device technology to manufacture a new generation of photoelectric switch devices. It has intelligent functions such as delay, expansion, external synchronization, anti-interference, high reliability, stable working area, and self-diagnosis. This novel photoelectric switch is an active photoelectric detection system electronic switch that uses pulse modulation. The cold light source used is infrared light, red light, green light and blue light, etc., which can be quickly and without contact and damage Control the state and action of various solid, liquid, transparent, black, soft, smoke and other substances.
Add a switch easily to any household electronics item or automotive project easily by watching this short video.

How To Add A Toggle Switch

Catalog

I. Features1. Specifications
2. Components
II. Types1. Large current sealed toggle switch
2. One-sided rebound type surface mount toggle switch
3. Long actuator top dial type toggle switch
III. Applications

 

I. Features

A toggle switch is to switch the circuit by turning the switch handle to make the circuit on or off. The commonly used varieties of toggle switches include single-pole double-position, single-pole three-position, double-pole double-position, and double-pole three-position, etc. They are generally used in low-voltage circuits and have the characteristics of flexible slider action and stable and reliable performance. Mainly widely used in: various instruments/meters and equipment, various electric toys, fax machines, audio equipment, medical equipment, beauty equipment, and other electronic products.

1. Specifications

Various aspects of toggle switch performance:

(1) Electrical performance specifications

A. Contact resistance test:

Test under a small current (100mA).

Requirements: Must be less than 30 milliohms.

B. Insulation resistance test:

Input 500V DC voltage for 1 minute and test according to the following contact methods:

Between contact terminals.

Between the rubber seat body and the row feet.

Requirements: It must be more than 100 megohms.

C. Withstand voltage test:

Input AC 500V (50-60Hz) voltage, 1-minute sensitivity current is 0.5mA, test according to the following contact method:

Between rows of feet

Between row feet and shell

Requirements: There is no abnormality such as insulation damage.

(2) Mechanical performance specifications

A. The normal operating force is: 250+_50gf

B. Terminal strength

Increase the force (500gf) on the tip in either direction for 1 minute.

In the row of feet, there is no abnormality such as cracking, movement, etc.

Requirements: Meet the mechanical and electrical performance.

C.Test standard status

The test temperature, humidity, and air pressure are as follows if not specified:

The temperature is 5℃~35℃

Humidity is 45%~85%

The air pressure is 80Kpa~106Kpa

(3) Durability

A. Solderability test

The top of the terminal is immersed in the soldering pool 1 mm deep, the temperature is 230 ± 5 ℃, and the time is 3 ± 0.5 seconds.

note:

- The welding time should be less than 3 seconds

- The welding area must be more than 80%.

B. Solder resistance test

The temperature of the soldering furnace is controlled at 260±5℃, the furnace time is 3±0.5 seconds, and the substrate thickness is 1.0mm

When hand welding, the temperature should be controlled at 320±5℃, and the time is 3±0.5 seconds.

Requirements: Must meet the body without deformation, meet the mechanical and electrical energy.

C. Life test

No load: The operator performs 100,000 no load tests at a frequency of 60 times per minute.

Caution:

- The contact resistance cannot exceed 200mΩ

- Other, satisfy the mechanical and electrical properties.

(4) Heat resistance test

After placing the test at a temperature of 85±2℃ for 96 hours, then place it at normal room temperature for 1 hour to determine.

Requirements: No abnormal appearance, satisfying mechanical and electrical performance.

(5) Cold resistance test

Place at 40±2℃. The relative humidity is 90~96% after 96 hours in an environment,

Then put the sample in a normal environment for 1 hour before testing.

Requirements: No abnormal appearance, satisfying mechanical and electrical performance.

(6) Humidity test

Place at 40±2℃. The relative humidity is 90~96% after 96 hours in an environment,

Then put the sample in a normal environment for 1 hour before testing.

Requirements: No abnormal appearance, satisfying mechanical and electrical performance.

(7) Mechanical specifications:

A. Conventional action force: 250+_50gf

B. Terminal strength: add force (500gf) to the tip in any direction for 1 minute. There is no abnormality such as cracks, scalping, etc. in the row of feet. The requirements of the toggle switch: meet the mechanical and electrical performance.

C. Test standard status: test temperature, humidity,

The air pressure of the toggle switch is as follows:

The humidity is 45%~85%

- The air pressure is 80Kpa~106Kpa

- The temperature is 5℃~35℃

2. Components

A toggle switch is mainly assembled by the following parts through the corresponding process:

1. Iron shell (material: generally iron; treatment process: treated by electroplating nickel or black-burning process to prevent oxidation)

2. Plastic handle (material: generally POM material, if there is a requirement for fire, flame retardant and high temperature resistance, PA nylon material is often used. Processing process: injection molding)

3. Terminal (Material: generally phosphorous copper; Treatment process: silver plating)

4. Insulating bottom plate (Material: Bakelite; Process: Stamping and forming)

5. Contact chip (material: generally phosphor copper; processing technology: silver plating)

6. Round wave beads (material: generally stainless steel; treatment process: nickel plating)

7. Slingshot (Material: Bronze; Processing Technology: Stamping and Forming)

8. Decorative oil (Material: red oil or green oil, a kind of chemical oil, applied to the contact part of the terminal and the bottom plate to play a decorative role. Generally non-toxic and environmentally friendly)

II. Types

Toggle switches are divided into small current toggle switches and large current toggle switches. Small current toggle switches are commonly used in electronic toys and digital communications. Large currents are generally used in electrical appliances, machinery, etc.

 

Large current sealed toggle switch

 

Small current sealed toggle switch

 

1. Large current sealed toggle switch

Its rated current is as high as 5A, and it is sealed with epoxy resin, so it is a large current sealed toggle switch. There are various terminal forms, the contact materials are silver-plated and gold, and the switch functions are diverse. Therefore, there are many types of subdivisions. It is widely used in electrical appliances and machinery. For example, in the 1203A1CQEB (unipolar three-position) model in the 1000 series, the specifications are as follows:

Switch Function: SPDT

Electrical Ratings: 5A @ 120VAC, 28VDC

Electrical Life: 30,000 cycles typical

Contact Resistance: < 10 mΩmax initial @ 2-4VDC, 100mA

Dielectric Strength: 1500Vrms min

Insulation Resistance: > 100MΩ min

Operating Temperature: -40°C to 85°C

Storage Temperature: -40°C to 85°C

2. One-sided rebound type surface mount toggle switch

The operation of the actuator is on the side, and the pin is a patch type, so it is a single-sided rebound type surface mount toggle switch. Widely used in communications, digital audio, and video. Such as the MS1257 model, the specifications are as follows:

Switch FunctionSPDT

Electrical Ratings300mA @ 6VDC

Electrical Life10,000 cycles typical

Contact Resistance< 50 mΩinitial

Dielectric Strength1000Vrms min

Insulation Resistance> 100MΩ min

Operating Temperature-40°C to 85°C

Storage Temperature-40°C to 85°C

3. Long actuator top dial type toggle switch

The actuator is 12mm and is located at the top of the switch, so it is a long actuator top-dip toggle switch. It is widely used in digital audio and video, various instruments/apparatus. Such as the MS2201L12 model, the specific specifications are as follows:

Switch FunctionDPDT

Electrical Ratings200mA @ 30VDC

Electrical Life10,000 cycles typical

Contact Resistance< 50 mΩinitial

Actuation Force200 +/- 100gF

Actuator Travel4.0 mm total

Dielectric Strength1000Vrms min

Insulation Resistance> 100MΩ min

Operating Temperature-40°C to 85°C

Storage Temperature-40°C to 85°C

III. Applications

1. Audio-visual products: MP3, MP4 audio;

2. Digital products: digital cameras, digital video cameras, etc.;

3. Communication products: mobile phones, car phones, telephones, building equipment, PDAs, etc.;

4. Security products: video intercoms, monitors, etc.;

5. Toys: electronic toys, etc.;

6. Computer products: cameras, etc.;

7. Fitness equipment: electronic body fat scale, treadmill, etc.;

8. Medical equipment: sphygmomanometer, clinical thermometer, hospital call system, etc.

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

What is a toggle switch used for?

The toggle switch is a type of electrical switch that is identified by the presence of handle or lever that makes it possible to control the flow of electric current/signal from a power supply to a device or within a device. It is a hinged switch that can assume either of two positions ie. ON or OFF.

How do toggle switches work?

In a toggle switch you have a lever that you turn to one side or to the other to make the current flow to one side or to other, or to not flow at all. There are several types of toggle switches. These are characterized by the pole and the throw. A pole represents a contact.

Which type of toggle switch is called a two way switch?

A 2 Way Switch is also called as a Staircase Switch, as you can control a single load, like a light bulb, from two different places, like either end of a staircase.
Related Articles

  • Long Life Small Volume Detector Switch for Intelligent Applications
    Long Life Small Volume Detector Switch for Intelligent Applications
    UTMEL16 March 20224768

    Hello everyone, I am Rose. Welcome to the new post today. This article will introduce what is a detection switch, how to choose a detection switch and where to use a detection switch.

    Read More
  • Analog Switch: Types and Application
    Analog Switch: Types and Application
    UTMEL25 March 202115014

    The analog switch is mainly to complete the signal switching function in the signal chain. The switching mode of the MOS tube is adopted to realize the switching off or on of the signal link.

    Read More
  • Toggle Switches: Features, Types and Applications
    Toggle Switches: Features, Types and Applications
    UTMEL23 January 202111067

    Toggle switch adopts integrated circuit technology and SMT appearance device technology to manufacture a new generation of photoelectric switch devices. It has intelligent functions such as delay, expansion, external synchronization, anti-interference, high reliability, stable working area, and self-diagnosis. This novel photoelectric switch is an active photoelectric detection system electronic switch that uses pulse modulation. The cold light source used is infrared light, red light, green light and blue light, etc., which can be quickly and without contact and damage Control the state and action of various solid, liquid, transparent, black, soft, smoke and other substances.

    Read More
  • DIP Switch: Introduction and Classification
    DIP Switch: Introduction and Classification
    UTMEL20 January 202116598

    DIP switch is an address switch used for operation control, using the principle of 0/1 binary coding. It is a miniature switch that can be toggled by hand. Dip switches are widely used in data processing, communication, remote control and anti-theft automatic alarm systems and other products that require manual programming.

    Read More
  • Solenoid Switch: Working Principle, Types and Applications
    Solenoid Switch: Working Principle, Types and Applications
    UTMEL03 February 202127266

    A solenoid switch is an electrical switch that is often used where a high current circuit, namely a starter motor circuit, is brought into operation with the aid of a low current switch. This switch switches a durable switch on to connect the vehicle's battery to the starter of the motor. A solenoid switch attaches the drive pinion to the starter until the ignition key is triggered. High performance, reliability, and longevity are the key characteristics of solenoid switches.

    Read More