Advantages of Single-Phase Liquid Immersion Cooling Technology
More technological progress and the widespread use of lithium-ion (Li-ion) batteries for storing electricity will depend on the creation of effective thermal management systems. The demand for quicker charging and discharging rates, higher amp-hour capacities, longer service lives, and higher levels of safety in both fixed battery arrays and electric vehicle batteries is growing.
Better and more secure thermal management systems are essential for all of these. There are efficiency constraints associated with either conventional air cooling or indirect liquid cooling, which are discussed in detail in this article. Recent trials conducted by Engineered Fluids show how effective single-phase liquid immersion cooling (SLIC) technology is for Li-ion battery temperature controls.
Ⅰ. What is air cooling?
By directing cool or room-temperature air through the battery cell or module's outer layer — which may have cooling fins or other ways to make the module's surface area bigger — the heat generated inside can be released into the surrounding air mass.
Ⅱ. Challenges in Air Cooling
Heat capacity of air (Cp) = 1.006 kJ/kg K at standard temperature
Due to the extremely low heat capacity, a significant amount of air is required, especially in situations where there is a small temperature differential between the battery module casing and surrounding air.
Another problem with air cooling is that batteries can only be physically placed in areas with available airflow or where air can be directed since the heat transfer surface of the battery needs to be exposed to air.
This can necessitate adding more infrastructure and volume to the system to guarantee that the entire mass of air required to cool the system is available.
New application requirements for batteries and evolving battery chemistries pose challenges to this technique. The following are some battery application needs that call for more effective thermal management:
1. Quicker cycles of charge and discharge
2. Shorter intervals of rest between cycles
3. Longer lifespan
4. Higher voltages for the batteries
5. Upon discharge and throughout the battery's service life, a more stable, consistent voltage output must be maintained.
These are the requirements for thermal management that modern electric vehicle battery systems impose, which are difficult to accomplish using air cooling.
Ⅲ. What is water cooling?
To reduce the temperature of the battery cells, a water/glycol solution is circulated through a heat sink or "cold plate" located inside the battery or battery module.
Ⅳ. Challenges of Water Cooling
Water/glycol heat capacity (Cp) = 3.777 kJ/kg K at 26.7 °C
Water and glycol coolants are effective in removing heat from the heat sink and have a very high capacity. This efficiency is lessened, though, because heat must be transferred through the fins or the jacket or container's walls.
Also, for the heat sink to properly transfer heat to the cold plate or jacket, it must be thermally attached to the full outermost layer of the battery cell walls and tabs. Any remaining air spaces within the battery cells function as heat insulation, quickly reducing the system's cooling effectiveness.
This is because many battery modules are made up of a lot of pouch or cylindrical cells. So, very precise aluminum frames and cold plates are often used, along with epoxy bonding agents or dielectric thermal grease, to make sure there are no air gaps between the framework and the battery cells' surfaces. Because of the system's total complexity, these systems might have high failure rates, low yield rates, and high fabrication costs.
A lot of manufacturers and users have stressed the fact that in aqueous indirect cooling systems, no aqueous solution gets on the batteries, wiring, or other electrical parts and causes them to short. This could result in thermal runaway in the affected cells or harm to the user because of the high amperage and voltages involved.
Aqueous indirect cooling systems for Li-ion batteries must be reliable so that no aqueous solution comes into contact with the batteries, wiring, or other electrical parts.
The speed at which heat moves from the battery module walls to the water jacket, heat sink framework, and cold plate, which does not conduct electricity, depends on the difference in temperatures and how well the different materials in each layer conduct heat.
Ⅴ. What is direct immersion cooling?
Single-phase liquid immersion cooling (SLIC) refers to the process of cooling battery cells by completely submerging them in a dielectric coolant. In most designs, a pump is used to recirculate the dielectric coolant throughout the system, keeping it in continual contact with the cell walls, tabs, and wiring of the battery module.
Ⅵ. Advantages of Direct Immersion Cooling
The thermal conductivity, density, viscosity, and velocity of the dielectric coolant are the variables that affect how quickly heat is transferred across the walls of the battery cells and the coolant.
Dielectric coolants heat capacity =1.3–1.4 kJ/kg K
For the same volumetric flow rate, heat transfer is much more efficient with dielectric coolants than with air. This is because the boundary layer is smaller and the thermal conductivity of the liquid is higher. Compared to air, a dielectric coolant can have a substantially lower flow rate because of its high heat capacity. Because liquid coolants are more thermally conductive and have a larger heat density than air, they are excellent cooling media.
Direct immersion in liquid single-phase dielectric coolants (SLIC) is supposed to provide the best results among these options in terms of keeping battery cells and modules within the proper temperature range with the least amount of temperature variation, as well as the lowest cost and system complexity.
Since the dielectric liquid coolant comes in direct contact with every part of the system, there is no longer a need for a heat sink framework in the middle, complicated manufacturing processes to keep the cells in place, or thermal bonding.
Dielectric SLIC coolants are safer than other conductive coolants and water glycol in a number of ways. For example, they can be in direct contact with all system parts without increasing the risk of cell thermal runaway, electronic short circuits, or user shock.
Using food-grade, non-toxic, biodegradable dielectric liquid coolants can also help with the safety and environmental problems that come up when dangerous aqueous glycol coolants leak.
Dielectric fluids were not accessible until now with an appropriate combination of properties such as compatibility profile, environmental impact, and fire safety. AmpCool Dielectric Coolants were developed in 2017 as a secure and trustworthy way to enhance and improve the value of today's battery systems.
Direct immersion in a single-phase, nonconductive cooling fluid is the most efficient cooling method for batteries. A comparative analysis of different types of cooling systems was summarized as shown in Fig. 1.

Fig. 1. Comparative analysis of different types of cooling system Source: IEEE Open Journal of Vehicular Technology
Ⅶ. Summarizing the Key Points
● Effective thermal management systems are crucial for optimizing the performance and safety of lithium-ion batteries.
● Conventional air cooling and indirect liquid cooling methods have limitations in meeting the increasing demand for faster charging and discharging rates, higher capacities, longer service lives, and improved safety.
● Single-phase liquid immersion cooling technology offers several advantages over traditional cooling methods, including better temperature control, lower cost, and reduced system complexity.
● The latest advancements in thermal management techniques have the potential to revolutionize battery cooling and improve the overall efficiency and reliability of battery systems.
● The adoption of advanced thermal management systems is essential for the widespread use of lithium-ion batteries in various applications, including electric vehicles, renewable energy storage, and consumer electronics.
Ⅷ. Reference
Sundin, David W., and Sebastian Sponholtz. “Thermal Management of Li-Ion Batteries With Single-Phase Liquid Immersion Cooling.” IEEE Open Journal of Vehicular Technology 1 (2020): 82–92. https://doi.org/10.1109/ojvt.2020.2972541.
Improving the Energy Conversion Efficiency of Triboelectric NanogeneratorsSaumitra Jagdale19 November 20242985There is a huge growth in demand for self-sustaining electronic devices, as the traditional power-generating devices fail in remote and harsh environments due to the periodic requirement of battery changes. Also, these devices are frequency specific; some work only in high frequency and some in low frequency. Triboelectric nanogenerators (TENGs) provide a promising solution by efficiently converting mechanical energy into electricity as they are versatile, compact, and cheap, making them a popular choice.
Read More
Methodologies for Increasing Efficiency of Fuel Stack Technology for Energy GenerationSaumitra Jagdale19 November 20242937Presently, power companies are moving towards renewable energy systems. Conventional energy sources are more expensive because they require a vast network to be maintained and huge human resources. Also, they harm the environment by releasing several harmful gases. As the industry’s focus shifts toward renewable energy sources, energy systems powered by Proton Exchange Membrane Fuel Stacks (PEMFS) are gaining traction.
Read More
VSC Light Meaning, Causes, and Step-by-Step DiagnosticsUTMEL19 May 2026336A VSC (Vehicle Stability Control) light indicates the system is disabled, often as a fail-safe triggered by unrelated engine faults like a loose gas cap. While the stability system prevents lateral skidding, it shuts down when sensor data is unreliable. Proper diagnosis requires an ABS-capable OBD2 scanner. Resolving the root engine code, checking wheel speed sensors, or performing a zero-point calibration usually restores system function.
Read More
Reconfigurable Antennas: Improving Efficiency in Modern CommunicationRakesh Kumar, Ph.D.24 December 20242949This article highlights the limitations of conventional antennas and discusses the advantages of reconfigurable antenna designs. It also explores various reconfiguration techniques, applications, and their potential to enhance efficiency.
Read More
The Ultimate Guide to AI Noise Reduction Translation EarbudsUTMEL01 April 20258280In today’s connected world, talking to others is very important. You’ve likely seen how global business, travel, and learning need easy chats in different languages. This need keeps growing because of new tech like 5G and edge computing. These make fast and smooth connections possible.
Read More
Subscribe to Utmel !
9006450000Weidmüller
CT-2931/STPanduit Corp
36298Wiha
227-1221-9Amphenol RF
47-20249Amphenol RF
0190270172Molex
5012Keystone Electronics
5001Keystone Electronics
0621000700Molex
5008Keystone Electronics


Product
Brand
Articles
Tools