Exploring the Cyber Physical System of Electric Vehicles
| Topics covered in this article: |
| Ⅰ. What makes up an electric vehicle's cyberphysical system? |
| Ⅱ. Physical Layer |
| Ⅲ. Cyber Layer |
| Ⅳ. Summarizing the Key Points |
| Ⅴ. Reference |
The automobile industry is currently undergoing a significant transition with the introduction of electric vehicles (EVs), leading to a shift away from conventional gasoline-fueled vehicles. In the world of electric vehicles, electric vehicle charging stations (EVCSs), and power grids, there exists a web of intricate cyber-physical interdependencies.
The cyber-physical relationship of an electric vehicle is shown in Fig. 1. It is crucial to understand that these interdependencies, and it can also be vulnerable to malicious exploitation, potentially causing harm to the various components involved.

Fig. 1. Cyber-Physical Layer of Electric Vehicle
Ⅰ. What makes up an electric vehicle's cyberphysical system?
The cyber layer describes the communication capabilities and interfaces of the EV that enable linking it with external components, while the physical layer discusses EV components from a power engineering standpoint.
Ⅱ. Physical Layer
As observed by a power engineer, the physical layers of a typical electric vehicle include a power storage unit, a power conditioning unit, a motor, and loads, as shown in Fig. 1.
Power Storage Units (Battery)
EV batteries typically function between 300 and 700 volts and can be charged in a variety of ways, including by plugging into the grid, using an internal combustion engine (ICE), regenerating energy while braking, or some combination of these. Electric vehicles typically include 12 V or 24 V auxiliary batteries for use with auxiliary loads and controllers.
Power Conditioning Units (Chargers)
The electrical grid can charge EV batteries directly via residential or commercial chargers or the on-board charger. The latter technique takes longer to charge the same energy.
The on-board and off-board chargers use an AC/DC power converter to convert AC power from the power grid to DC power for the battery. Chargers also have a power factor corrector (PFC), DC/DC converter, auxiliary AC/DC converter, charging monitor, and controller.
The PFC ensures that the electricity charged to the battery meets harmonic and distortion safety requirements to prevent battery damage and early decay. The battery is connected to four more converters.
The first DC/AC converter is 3-phase and bi-directional, powers the traction motor, and charges the battery during regenerative braking. Second, DC/AC converts power to high-power auxiliary loads like heating, ventilation, and air conditioning systems. The third DC/DC converter serves low-power loads like lights and an auxiliary battery at 12 or 24 V. The fourth AC/DC converter supplies battery power from an ICE.
Motor and Loads
The AC traction motor, commonly a 3-phase permanent magnet synchronous motor (e.g., Nissan Leaf) or induction motor (e.g., Tesla), operates at ≈240 V. High-power auxiliary loads include a 3-phase compressor and air conditioner fans, while low-power (12 or 24 V) include headlights, cabin lights, a radio, power steering, and USB chargers.
If indoor and ambient temperatures are very different, auxiliary loads can lower the EV range by 35%. EV range can be increased by 22% by modifying heating, ventilation, and air conditioning system parameters.
Ⅲ. Cyber Layer
The cyber layer for electric vehicles, which incorporates the in-vehicle and external layers as shown in Fig. 2,

Fig. 2. Cyber Layer of Electric Vehicle
In-Vehicle Layer
There are currently around 125 electronic control units (ECUs) in modern automobiles, and that number is only growing. ECUs make it possible to control the vehicle's essential systems, such as the brakes, batteries, and infotainment systems.
The components of an ECU are a CPU, memory, and input and output ports. As shown in Fig. 2, the Controller Area Network (CAN) bus, Local Interconnect Network (LIN), Media Oriented Systems Transport (MOST), and FlexRay are all used to link the ECUs together.
Because it links the most important ECUs and, if breached, might be used to interfere with the EV charging process, the CAN bus network has been the focus of security discussions. LIN doesn't demand high-speed communication, and it is a low-cost network.
However, MOST is an expensive network utilized in the in-vehicle infotainment (IVI) system that necessitates a high bandwidth transmission, so it is not a suitable choice for most mobile devices. ECUs like the airbag control unit use FlexRay because of the high fault tolerance they demand of their components.
Controller area network (CAN) bus
The CAN bus is built on a peer-to-peer network where all ECUs and peripherals are linked and can communicate with one another as partners. The network functions similarly to a centralized means of communication. There are four main benefits to incorporating this bus standard into EVs.
The first advantage of the CAN bus is that it can process real-time, concurrent commands from numerous ECUs without introducing major communication delays. The CAN bus's centralized design allows for this to happen; an ECU can send a message to all other ECUs with an arbitration identification (ID), and only the intended recipient will get the message.
As a second point, the CAN bus is separated into high-speed and low-speed branches that share a gateway. The heating, ventilation, and air conditioning controller, for example, is hosted on the low-speed CAN bus, while the brake control and battery management, which are time critical units, are connected to the high-speed CAN bus.
Third, the CAN bus allows for centralized ECU diagnostics through the on-board diagnostic (OBD) connector. By using this port, mechanics and regulatory organizations can keep an eye on the carbon emissions and battery health of EVs.
Fourth, the CAN bus is adaptable, making it simple to add or remove electronic control units (ECUs), while also being inexpensive and resistant to electric disturbances and electromagnetic interference that could otherwise disrupt the vital EV functions.
Some electronic control units (ECUs), like the tire pressure monitoring system (TPMS), have their own sensor sub-networks. A radio frequency (RF) connection between battery-powered sensors on the EV tires and the tire pressure control unit creates the TPMS.
The control unit receives sensor data and relays that information through the controller area network (CAN) to the vehicle's operator. Such specialized networks cannot be avoided. To prevent under-inflated tires from causing traffic accidents, TPMS is required by law.
External Layer
This layer includes several criteria, as shown in Fig. 2, which are all described in detail below.
Electric Vehicle Charging Station
EVs use a wired channel to coordinate charging details and preferences with a selected EVCS. The control and protection instructions include ground-fault detection, the required charging current, the current level of charge of the EV battery, and the EV's readiness for charging (using pulse-width modulation (PWM) signals).
Although this connection is often wired, there are times when EVs and EVCSs use their IP addresses to communicate wirelessly. Although widespread adoption of wireless communication is anticipated in the future, a variety of protocols exist for wireless EV-EVCS connections at present.
Physically Accessible Ports
For external connections, EVs feature USB ports, a compact disk CD slot, a secure digital SD card slot, and an on-board diagnostic (OBD) port. Electric vehicle mechanics, EV users, and EV regulatory agencies can monitor EV performance (e.g., carbon emissions), EV speed and traffic patterns, and EV battery state using the OBD port, a standardized interface to the CAN bus.
Internet Service Portals
In most cases, users can have remote access to the EV functions using Internet service portals (such as smartphone applications). Wireless communications between EVs and web-based and smartphone applications make it possible to monitor and control EV charging.
In addition, many EV In-vehicle infotainment (IVI) dashboards include Bluetooth and USB connectors so that smartphones can be linked for media playback and phone access.
Key fobs and other service portals can communicate wirelessly with EVs to allow for keyless entry. While web and smartphone apps use cellular networks and WiFi for long- and medium-range wireless communication, key fobs use short-range RF, or near-field communication (NFC).
Radio Stations
To access the location data being broadcast from a space-based radio station, current EVs require the Global Positioning System (GPS). The EVs, for instance, use the GPS signals to plot a course to the most convenient and economical EVCS or at any other user-specified location. EV infotainment programs use cellular networks to communicate with radio and navigation stations.
Equipment Manufacturer
The EVs use WANs like cellular networks and RF to wirelessly communicate with their manufacturers and OEMs in order to receive regular and ad hoc software updates and security patches. Because of their quick delivery and low costs, OEMs and vendors choose wireless patching techniques over the traditional patching procedures performed via on-site HMI (e.g., USB and Ethernet connections).
Road-Side Infrastructure and Vehicles
Today's EVs are capable of communicating with things like traffic lights and other vehicles on the road over cellular networks, allowing for more efficient and pleasant transportation. These kinds of connections aren't commonly used just yet, but that's expected to change as more and more self-driving and semi-autonomous vehicle technologies enter the market.
Ⅳ. Summarizing the Key Points
● The cyber layer of an electric vehicle's system describes its communication capabilities and interfaces that enable linking it with external components.
● The physical layer of an electric vehicle's system discusses its components from a power engineering standpoint.
● The cyber-physical interdependencies between electric vehicles, charging stations, and power grids are intricate and can be vulnerable to malicious exploitation.
● Understanding these interdependencies is crucial for securing the cyber-physical systems of electric vehicles.
● Solutions for securing the cyber-physical system of electric vehicles include implementing secure communication protocols, developing intrusion detection systems, and establishing secure authentication mechanisms.
Ⅴ. Reference
Acharya, Samrat, Yury Dvorkin, Hrvoje Pandzic, and Ramesh Karri. “Cybersecurity of Smart Electric Vehicle Charging: A Power Grid Perspective.” IEEE Access 8 (2020): 214434–53. https://doi.org/10.1109/access.2020.3041074.
Improving the Energy Conversion Efficiency of Triboelectric NanogeneratorsSaumitra Jagdale19 November 20243398There is a huge growth in demand for self-sustaining electronic devices, as the traditional power-generating devices fail in remote and harsh environments due to the periodic requirement of battery changes. Also, these devices are frequency specific; some work only in high frequency and some in low frequency. Triboelectric nanogenerators (TENGs) provide a promising solution by efficiently converting mechanical energy into electricity as they are versatile, compact, and cheap, making them a popular choice.
Read More
Methodologies for Increasing Efficiency of Fuel Stack Technology for Energy GenerationSaumitra Jagdale19 November 20243230Presently, power companies are moving towards renewable energy systems. Conventional energy sources are more expensive because they require a vast network to be maintained and huge human resources. Also, they harm the environment by releasing several harmful gases. As the industry’s focus shifts toward renewable energy sources, energy systems powered by Proton Exchange Membrane Fuel Stacks (PEMFS) are gaining traction.
Read More
VSC Light Meaning, Causes, and Step-by-Step DiagnosticsUTMEL19 May 20265476A VSC (Vehicle Stability Control) light indicates the system is disabled, often as a fail-safe triggered by unrelated engine faults like a loose gas cap. While the stability system prevents lateral skidding, it shuts down when sensor data is unreliable. Proper diagnosis requires an ABS-capable OBD2 scanner. Resolving the root engine code, checking wheel speed sensors, or performing a zero-point calibration usually restores system function.
Read More
What JEDEC JEP203 and JEP204 Actually Change for SiC Qualification Engineers and Component BuyersUTMEL29 July 2026739Summary: When JEDEC published JEP203 and JEP204 on June 3, 2026[1], most coverage treated them as an announcement. They are better understood as the first shared language the silicon carbide industry has had for two problems that have quietly consumed engineering hours since the first commercial SiC MOSFETs shipped: short-circuit evaluation that produces numbers you can compare across suppliers, and a consolidated reference of stress procedures so qualification engineers stop reinventing test plans from scratch. This article explains what changes on Monday morning and what to ask suppliers for now.
Read More
2nm vs 3nm Chips: What the Latest Process Nodes Mean for PerformanceUTMEL19 August 20262830The shift from 3nm to 2nm process nodes marks a fundamental change in transistor architecture, moving from FinFET to Gate-All-Around (GAA) nanosheets. This transition delivers meaningful improvements in performance, power, and density, but also introduces new challenges like SRAM scaling limits, thermal density, and backside power delivery. The article compares TSMC, Samsung, and Intel approaches, offering a practical decision framework for engineering teams.
Read More
Subscribe to Utmel !
5027Keystone Electronics
0638681100Molex
KC4-6Greenlee Communications
0153-01-INSGreenlee Communications
09990000310HARTING
1212091Phoenix Contact
1205859Phoenix Contact
61030000103HARTING
5126Keystone Electronics
09990000503HARTING


Product
Brand
Articles
Tools