What is a Synchronous Motor?

Working of Synchronous Motor
Catalog
| I. Working Principle | 1. V-shaped curve |
| 2. Starting Method | |
| II. Types | |
| III. Applications | |
A synchronous motor is an AC motor that generates torque by the interaction of the excitation magnetic field supplied by a direct current and the rotating magnetic field of the armature, and rotates at a synchronous speed.) is an AC motor that generates torque by the interaction of the DC-powered excitation magnetic field and the rotating magnetic field of the armature, which rotates at a synchronous speed.
An AC motor in which the rotation of the rotor is the same as the rotation of the stator's rotating magnetic field. The rotor speed n, the number of magnetic pole pairs p, and the power supply frequency f satisfy n=60f/p. The speed n is determined by the power frequency f, so when the power frequency is constant, the speed does not change and has nothing to do with the load. It has the characteristics of high operating stability and large overload capacity. Commonly used in multi-machine synchronous transmission systems, precision speed regulation and speed stabilization systems, and large equipment (such as rolling mills), etc.
Synchronous motors are AC motors, and the stator windings are the same as asynchronous motors. Its rotor rotation speed is the same as the speed of the rotating magnetic field generated by the stator winding, so it is called a synchronous motor. Because of this, the current of the synchronous motor is ahead of the voltage in phase, that is, the synchronous motor is a capacitive load. For this reason, in many cases, synchronous motors are used to improve the power factor of the power supply system.
Because the synchronous motor can run at a leading power factor by adjusting the excitation current, it is beneficial to improve the power factor of the power grid. Therefore, large-scale equipment, such as large-scale blowers, water pumps, ball mills, compressors, rolling mills, etc., are commonly driven by synchronous motors. This advantage is particularly prominent when a synchronous motor is used in large-scale equipment with a low speed. In addition, the speed of the synchronous motor is completely determined by the power frequency. When the frequency is constant, the speed of the motor is also constant, and it does not change with the load. This feature is of great significance in certain transmission systems, especially multi-machine synchronous transmission systems and precision speed regulation and speed stabilization systems. The operating stability of the synchronous motor is also relatively high. Synchronous motors generally run under over-excitation, and their overload capacity is greater than that of corresponding asynchronous motors. The torque of an asynchronous motor is proportional to the square of the voltage, while the torque of a synchronous motor is determined by the product of the voltage and the internal electromotive force generated by the motor's excitation current, that is, it is only proportional to the first power of the voltage. When the grid voltage suddenly drops to about 80% of the rated value, the asynchronous motor torque often drops to about 64% and stops running due to the immobile load; while the synchronous motor torque does not drop much, and it can be forced Excitation to ensure the stable operation of the motor.
I. Working Principle of Synchronous motor
When a symmetrical three-phase alternating current is applied to the stator three-phase winding of a synchronous motor, a rotating magnetic field is generated in the symmetrical three-phase winding. When the excitation winding of the rotor is added to the excitation current, the rotor looks like a "magnet", driven by the rotating magnetic field. Spin. At this time, the speed of the rotor is equal to the synchronous speed of the rotating magnetic field.
Since the torque of the rotor of the synchronous motor is generated by the attraction between the different polarities of the rotating magnetic field and the rotor magnetic field, the rotation speed of the rotor is always equal to the rotation speed of the rotating magnetic field and does not change due to changes in load.
1. V-shaped curve of a synchronous motor
The V-shaped curve of a synchronous motor refers to the relationship curve between the armature current I1 and the excitation current If under the condition that the voltage U and the load TL remain unchanged, that is, I1=ƒ(If). The V-shaped curve can be measured through experiments.
It can be seen from the figure that different loads correspond to a V-shaped curve. For each V-shaped curve, the armature current I1 has a minimum value. The power factor at the lowest point of the curve is cosφ=1, which is the normal excitation point, and this point is the boundary. , The left is under-excitation, and the right is over-excitation; the upper left half of the V-shaped curve, its power factor has exceeded the value corresponding to the stability limit, so it is an unstable zone.
How to adjust the excitation current of the synchronous motor depends on the actual situation of the power grid when the motor is running. If the power factor of the power grid does not meet the requirements and the synchronous motor is required to provide reactive power, the motor should work in an overexcited state (but should use the armature The current does not exceed the rated value limit) in order to increase the power factor of the power grid; if the power factor of the power grid has reached the requirement, the synchronous motor should work in the normal excitation state. At this time, the power factor of the motor is 1, the armature current I1 is the minimum, and the copper loss The smallest and the most efficient.
2. Starting Method of Synchronous motor
Synchronous motors can only produce an average torque at the synchronous speed. If the stator is connected to the power grid immediately and the rotor is excited by DC when starting, the stator rotating magnetic field immediately rotates at a synchronous speed, and the rotor magnetic field is temporarily stationary due to the inertia of the rotor, and the electromagnetic torque generated at this time will be positive or negative. Alternating and its average value are zero, so the motor cannot start by itself. To start a synchronous motor, other methods must be used, mainly the following methods:
(1) Auxiliary motor starting method
The auxiliary motor starting method is to select a small asynchronous motor with the same number of poles as the synchronous motor as the auxiliary motor. When starting, first start the auxiliary motor to drag the synchronous motor to the asynchronous speed, and then put the synchronous motor into the power grid, add excitation, and use the synchronous motor. The torque pulls the synchronous motor rotor into synchronization and cuts off the auxiliary motor power at the same time. This method is suitable for the no-load starting of the synchronous motor.
(2) Frequency conversion starting method
Since the average torque acting on the rotor is zero during constant frequency starting, the motor cannot start by itself. The frequency conversion starting method is to add DC to the rotor before starting, use the frequency conversion power supply to slowly increase the frequency from zero, and the rotating magnetic field pulls the rotor to slowly and synchronously accelerate until the rated speed is reached, and the starting is completed. This method is mostly used for the starting of large synchronous motors.
(3) Asynchronous start method
The asynchronous starting method is to install a starting winding on the rotor, and its structure is like the squirrel cage winding of an asynchronous motor. When starting, do not excite the field winding first, and connect the stator winding of the synchronous motor to the power supply. Through the function of the start winding, starting torque is generated to make the synchronous motor start by itself. When the speed reaches about 95% of the synchronous speed, the excitation winding of the synchronous motor is energized. When DC is applied, the rotor is automatically pulled into synchronization.
II. Types of Synchronous motor
There are roughly two types of synchronous motors in structure:
Excited by direct current
Its rotor is made of salient pole type, and the magnetic field coils mounted on the magnetic pole core are connected in series with alternating opposite polarities, and there are two lead wires connected to the two slip rings mounted on the shaft. . The field coil is excited by a small DC generator or battery. In most synchronous motors, the DC generator is installed on the motor shaft to supply the excitation current of the rotor pole coil.
Because this kind of synchronous motor cannot start automatically, a squirrel cage winding is also installed on the rotor for starting the motor. The squirrel cage winding is placed around the rotor, and the structure is similar to that of an asynchronous motor.
When a three-phase AC power supply is applied to the stator windings, a rotating magnetic field is generated in the motor, and the squirrel cage winding cuts the magnetic lines of force to generate an induced current, which causes the motor to rotate. After the motor rotates, its speed slowly increases to slightly lower than the rotating magnetic field speed. At this time, the rotor field coil is excited by direct current to form certain magnetic poles on the rotor. These magnetic poles try to track the rotating magnetic poles on the stator, thus increasing The speed of the motor rotor until it rotates synchronously with the rotating magnetic field.
Not excited by direct current
Synchronous motors with non-excited rotors can be used on single-phase power supplies, and can also be used on multi-phase power supplies. In this type of motor, there is a stator winding similar to the stator of a split-phase motor or a multi-phase motor, and there is a squirrel cage rotor, and the surface of the rotor is cut into a plane. So it belongs to the salient pole rotor, the rotor pole is made of a kind of magnetized steel, and can always maintain the magnetism. The squirrel cage winding is used to generate the starting torque, and when the motor rotates to a certain speed, the rotor saliency is synchronized with the current frequency of the stator coil. The polarity of the salient pole is induced by the stator, so its number should be equal to the number of poles on the stator. When the motor turns to its proper speed, the squirrel cage winding loses its function. The rotation is maintained by the rotor and the pole. The magnetic poles follow the stator magnetic poles to synchronize them.
III. Applications of Synchronous motor


Synchronous motor for electric motor operation. Because the synchronous motor can be operated under the advanced power factor by dispatching the excitation current, it is beneficial to improve the power factor of the power grid. Therefore, large equipment, such as large blowers, water pumps, ball mills, compactors, rolling mills, etc., are often driven by synchronous motors. This advantage is particularly outstanding when using synchronous motors for large-scale equipment at low speeds. In addition, the rotation speed of the synchronous motor is thoroughly selected based on the power supply frequency. The frequency must be punctual, and the speed of the motor must be, and it does not change with the load. This feature has the primary meaning in some transmission systems, especially the multi-machine synchronous transmission system and the fine speed and steady speed system. The operating stability of synchronous motors is also higher.
Where is synchronous motor used?
Synchronous motors are normally used in applications in which a constant and precise speed is required. Typical applications of these low power motors are positioning machines. They are also used in robot actuators. Synchronous motors are also used in ball mills, watches, record players, and turntables.
What is the main disadvantage of synchronous motors?
Synchronous motors requires dc excitation which must be supplied from external sources. Synchronous motors are inherently not self starting motors and needs some arrangement for its starting and synchronizing. The cost per kW output is generally higher than that of induction motors.
What is difference between synchronous motor and synchronous generator?
The main difference between the two is the sign conventions. Below are the diagrams for a generator on the left and a motor on the right. Each is connected to an infinite bus with voltage Vt (voltage and frequency of an infinite bus are fixed regardless of prime mover power and excitation of the machine.)
What is a Servo Drive?UTMEL16 June 20216039Servo drive, also known as "servo controller" and "servo amplifier", is a kind of controller used to control servo motors. Its function is similar to that of frequency converters acting on ordinary AC motors, and it is part of the servo system. The servo drive is mainly used in high-precision positioning systems. Generally, the servo motor is controlled by three methods of position, speed, and torque to achieve high-precision transmission system positioning.
Read More
What is a Switched Reluctance Motor?UTMEL09 July 20249021Switched reluctance motor is a type of speed-regulating motor developed after DC motor and brushless DC motor. Product power levels range from several watts to hundreds of kilowatts, and are widely used in household appliances, aviation, aerospace, electronics, machinery, and electric vehicles.
Read More
Types, Working, and Selection of DC MotorUTMEL27 March 202518905A direct current motor (DC motor) is an electric motor that operates on direct current. The operation of an electric motor is based on basic electromagnetism. When a current-carrying conductor is put in an external magnetic field, it will feel a force that is equal to the current in the conductor and the frequency of the external magnetic field.
Read More
Linear Induction Motor: Working Principle, Characteristics, and ApplicationsUTMEL02 March 202116346LIM stands for Linear Induction Motor, and it is an improved version of the rotary induction motor that produces linear translational motion instead of rotating motion. Other than rotating torque, this device generates linear movement and force. By cutting a radically shaped cut in the revolving induction and thus leveling the section, the design and functionality of the linear induction motor can be demonstrated in the diagram below.
Read More
Stepper Motor: Types, Working and ApplicationsUTMEL26 December 202511256A brushless, synchronous electric motor that converts digital pulses to mechanical shaft rotation is known as a stepper motor. When operated by a sequentially switched DC power supply, the normal shaft motion is made up of discrete angular motions of approximately uniform magnitude.
Read More
Subscribe to Utmel !
HD-EMB1806-LW32-RPUI Audio, Inc.
HD-EM0802-LW15-RPUI Audio, Inc.
GAM2A6010F0XRK0Sanyo Denki SanMotion Products
GAM2A8075F0XRK0Sanyo Denki SanMotion Products
HD-EM0803-LW20-RPUI Audio, Inc.
HD-EM1204-LW20-RPUI Audio, Inc.
HD-EMB1205-3-SC-RPUI Audio, Inc.
HD-EMC1203-LW20-RPUI Audio, Inc.
HD-EMB1104-LW15-RPUI Audio, Inc.
2331Pololu Corporation


Product
Brand
Articles
Tools