Logic - Translators, Level Shifters: A Semiconductor Device on A Circuit

What is a Level Shifter? | Basic knowledge
Logic level converters, or voltage level converters, are used to convert signals from one logic level to another. Today, most systems operate at 3.3V or 5V. A logic level is simply the high or low voltage level of a particular board or integrated circuit. Knowing this, a logic level converter is needed to create a path between processors, sensors, or boards with different voltage levels.
How Does A Transducer IC Work?
Converter ICs provide an interface between components that operate at different voltage levels. They can convert from low to high voltages and vice versa. Both upward and downward logic level conversion is done by selecting the power supply levels VDD (voltage drain) and VCC (voltage common collector). the VCC level sets the input signal level, while VDD selects the output voltage level.
Types of IC Translators
IC translators are available in various pin counts, translation methods, and package types such as SOIC SOT-23, VSSOP, and different logic levels.
Another type of translator is the I2C (interconnect circuit) translator. These are multi-master to multi-slave two-wire serial bus standards capable of serial communication at multiple-bit rates. the signal of an I2C translator consists of a single data signal with a logical level, verified by a clock signal. Both signals being transmitted are bidirectional.
Common Logic Levels And Usage Times
Currently, the three most common logic levels are 1.8 V, 3.3 V, and 5 V. For logic with a single transistor, such as an EMERGENCY gate, we need to apply a voltage above 0.7 V to the base of that transistor to activate it. Thus, for a single-transistor logic, a voltage above 0.7 V is logic 1 and a voltage below 0.7 V is logic 0.
Now, when one transistor is used to drive another transistor, we have to double the voltage over the single transistor. So the threshold voltage here would be 1.4 V. Another example is DTL (diode transistor logic). A diode has a forward voltage drop of 0.7V, so we need 1.4V to activate the circuit. A good margin is safe, so these circuits retain 1.8V by default.
In order for more transistors to perform a task, a higher voltage level is needed, i.e. 3V or 5V. Therefore, the processor or board has different voltage levels, and all these boards, processors, or sensors must coexist in different applications, which can be achieved by forming logic-level conversion bridges.
Almost all the cards and sensors of the new series operate at a 3.3V logic level. If they are to be connected to a 5V board like the Arduino UNO, voltage conversion is required. However, in some cases, we don't need conversion circuits to connect two boards with different voltage levels.
We all know that from basic electronics, for most boards, most of the time voltage levels above 2V are logic 1 and voltage levels below 0.8V are logic 0. So with this, we can easily apply 3.3V signals to 5V processors/cards without additional circuitry. But of course, it is necessary to check the threshold voltage level in the datasheet of the IC used.
How to Design A 5 V - 3.3 V Conversion Circuit ?
For inverting conversion, a dual-transistor logic is required. Two transistors are connected in series inverting to obtain a non-inverting +5V output. When 3.3V is applied to the first transistor, it saturates and gives an inverted signal to the second transistor, which inverts its level again to give a +5V signal at the output. It should also be understood that a low drop output very close to +5V can be obtained by using an N-channel MOSFET instead of an NPN transistor in Q2, taking into account the voltage drop across resistor R2.
Bidirectional Logic Level Shifter Circuit
A simple bidirectional logic level converter is a very convenient and fast circuit because it is built around a transistor and switching speed is not an issue.

When HIGH (pin) is a logic 1 (i.e., 5 volts at this pin), the drain and source of the MOSFET are pulled high. In this case, the gate voltage is lower than the source voltage, which puts the MOSFET in the cutoff region (i.e., inactive). Therefore, the LOW pin is pulled to 3.3 volts because no current flows through the gate. When High is a logic 0, the gate voltage is greater than the source voltage, resulting in a lower output on the LOW pin.
Similarly, when LOW is a logic 1, Vgs (the gate-to-source voltage) becomes zero, causing the transistor to become inactive, pulling the HIGH pin to +5 volts. When LOW is a logic 0, the gate voltage is again higher than the source voltage, pulling the HIGH pin low.
In this article, we've discussed logic-level converters, looking at why and when they are needed. We've looked at some conversion circuits and a few ICs for multi-line conversion.
Related News
1、Chip Packaging Lead Time Has Grown to 50 Weeks
2、Eight Internet of Things (IoT) Trends for 2022
3、Demand for Automotive Chips Will Surge 300%
4、Volkswagen CFO: Chip Supply Shortage Will Continue Until 2024
5、BMW CEO: The Car Chip Problem Will Not Be Solved Until 2023
6、Shenzhen: This Year Will Focus on Promoting SMIC and CR Micro 12-inch Project
UTMEL 2024 Annual gala: Igniting Passion, Renewing BrillianceUTMEL18 January 20245058As the year comes to an end and the warm sun rises, Utmel Electronics celebrates its 6th anniversary.
Read More
Electronic Components Distributor Utmel to Showcase at 2024 IPC APEX EXPOUTMEL10 April 20246064Utmel, a leading electronic components distributor, is set to make its appearance at the 2024 IPC APEX EXPO.
Read More
UTMEL Showcases One-Stop Electronic Component Sourcing Services at electronica Shanghai 2026UTMEL07 July 2026332SHANGHAI, China, July 7, 2026 - UTMEL, a one-stop electronic components sourcing platform operated by Shenzhen Utmel Intelligent Electronic Co., Ltd., successfully participated in electronica Shanghai 2026, held from July 1 to 3, 2026 at the Shanghai New International Expo Centre.
Read More
Electronic components distributor UTMEL to Showcase at electronica ChinaUTMEL07 June 20244636The three-day 2024 Electronica China will be held at the Shanghai New International Expo Center from July 8th to 10th, 2024.
Read More
Electronic components distributor UTMEL Stands Out at electronica china 2024UTMEL09 July 20245248From July 8th to 10th, the three-day electronica china 2024 kicked off grandly at the Shanghai New International Expo Center.
Read More
Subscribe to Utmel !
TMLM 04115Traco Power
VOF-20B-S12CUI Inc.
RAC10-15SB-ERecom Power
PSK-20B-S12CUI Inc.
YAS1005ECosel USA, Inc.
PBO-3-S3.3CUI Inc.
PBO-3-S15-BCUI Inc.
TUNS300F48Cosel USA, Inc.
TMPS 03-103Traco Power
RAC05-15SKRecom Power


Product
Brand
Articles
Tools