2SC2229 BJT NPN Transistor: Datasheet pdf, Pinout and 2SC2229 Equivalents

UTMEL

Published: 24 December 2021 | Last Updated: 24 December 2021

4316

2SC2229-O(TE6,F,M)

2SC2229-O(TE6,F,M)

Toshiba Semiconductor and Storage

TRANS NPN 50MA 150V TO226-3

Purchase Guide

TRANS NPN 50MA 150V TO226-3

2SC2229 is a BJT NPN transistor available in TO-92L or TO-92MOD package but with some manufacturers, it is also available in the TO-92 package. This article is going to explain details about the 2SC2229 transistor.

DIY 100-Watts Class A Mini Amplifier Extremely Powerful Bass | Super Simple

DIY 100-Watts Class A Mini Amplifier Extremely Powerful Bass | Super Simple

What is 2SC2229?

2SC2229 is a BJT  NPN  transistor available in TO-92L or TO-92MOD  package but with some manufacturers, it is also available in the TO-92 package. It's an NPN triple diffused transistor; they are transistors that are manufactured by diffusing dopants. The transistor has several desirable characteristics, including the ability to operate at high voltage s of up to 150V, a low output capacitance, and a transition frequency of up to 120MHz.

The transistor's collector current maximum is 50mA. To drive a 50mA  load, the maximum voltage required for transistor saturation at its base is merely 0.5V with only 5mA of base current. The output capacitance at the collector is 3.5pF to 5pF, with an 800 mill watt collector dissipation maximum.


2SC2229 Pinout

2sc2229 pinout.jpg

2SC2229 Pinout

2SC2229 CAD Model

2sc2229 footprint.jpg

2SC2229 Footprint

Specifications

Toshiba Semiconductor and Storage 2SC2229-O(TE6,F,M) technical specifications, attributes, parameters and parts with similar specifications to Toshiba Semiconductor and Storage 2SC2229-O(TE6,F,M).
  • Type
    Parameter
  • Mounting Type

    The "Mounting Type" in electronic components refers to the method used to attach or connect a component to a circuit board or other substrate, such as through-hole, surface-mount, or panel mount.

    Through Hole
  • Package / Case

    refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.

    TO-226-3, TO-92-3 Long Body
  • Current-Collector (Ic) (Max)
    50mA
  • Operating Temperature

    The operating temperature is the range of ambient temperature within which a power supply, or any other electrical equipment, operate in. This ranges from a minimum operating temperature, to a peak or maximum operating temperature, outside which, the power supply may fail.

    150°C TJ
  • Packaging

    Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.

    Bulk
  • Published
    2009
  • Part Status

    Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.

    Obsolete
  • Moisture Sensitivity Level (MSL)

    Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures

    1 (Unlimited)
  • Power - Max

    Power - Max is a parameter that specifies the maximum amount of power that an electronic component can handle without being damaged. It is typically measured in watts and indicates the upper limit of power that can be safely supplied to the component. Exceeding the maximum power rating can lead to overheating, malfunction, or permanent damage to the component. It is important to consider the power-max rating when designing circuits or systems to ensure proper operation and longevity of the electronic components.

    800mW
  • Transistor Type

    Transistor type refers to the classification of transistors based on their operation and construction. The two primary types are bipolar junction transistors (BJTs) and field-effect transistors (FETs). BJTs use current to control the flow of current, while FETs utilize voltage to control current flow. Each type has its own subtypes, such as NPN and PNP for BJTs, and MOSFETs and JFETs for FETs, impacting their applications and characteristics in electronic circuits.

    NPN
  • DC Current Gain (hFE) (Min) @ Ic, Vce

    The parameter "DC Current Gain (hFE) (Min) @ Ic, Vce" in electronic components refers to the minimum value of the DC current gain, denoted as hFE, under specific operating conditions of collector current (Ic) and collector-emitter voltage (Vce). The DC current gain hFE represents the ratio of the collector current to the base current in a bipolar junction transistor (BJT), indicating the amplification capability of the transistor. The minimum hFE value at a given Ic and Vce helps determine the transistor's performance and efficiency in amplifying signals within a circuit. Designers use this parameter to ensure proper transistor selection and performance in various electronic applications.

    70 @ 10mA 5V
  • Current - Collector Cutoff (Max)

    The parameter "Current - Collector Cutoff (Max)" refers to the maximum current at which a transistor or other electronic component will cease to conduct current between the collector and emitter terminals. This parameter is important in determining the maximum current that can flow through the component when it is in the cutoff state. Exceeding this maximum cutoff current can lead to malfunction or damage of the component. It is typically specified in the component's datasheet and is crucial for proper circuit design and operation.

    100nA ICBO
  • Vce Saturation (Max) @ Ib, Ic

    The parameter "Vce Saturation (Max) @ Ib, Ic" in electronic components refers to the maximum voltage drop across the collector-emitter junction when the transistor is in saturation mode. This parameter is specified at a certain base current (Ib) and collector current (Ic) levels. It indicates the minimum voltage required to keep the transistor fully conducting in saturation mode, ensuring that the transistor operates efficiently and does not enter the cutoff region. Designers use this parameter to ensure proper transistor operation and to prevent overheating or damage to the component.

    500mV @ 1mA, 10mA
  • Voltage - Collector Emitter Breakdown (Max)

    Voltage - Collector Emitter Breakdown (Max) is a parameter that specifies the maximum voltage that can be applied between the collector and emitter terminals of a transistor or other semiconductor device before it breaks down and allows excessive current to flow. This parameter is crucial for ensuring the safe and reliable operation of the component within its specified limits. Exceeding the maximum breakdown voltage can lead to permanent damage or failure of the device. Designers and engineers must carefully consider this parameter when selecting components for their circuits to prevent potential issues and ensure proper functionality.

    150V
  • Frequency - Transition

    The parameter "Frequency - Transition" in electronic components refers to the maximum frequency at which a signal transition can occur within the component. It is a crucial specification for digital circuits as it determines the speed at which data can be processed and transmitted. A higher frequency transition allows for faster operation and better performance of the electronic component. It is typically measured in hertz (Hz) or megahertz (MHz) and is specified by the manufacturer to ensure proper functioning of the component within a given frequency range.

    120MHz
0 Similar Products Remaining

2SC2229 Features

  • Type: NPN

  • Collector-Emitter Voltage: 150 V

  • Collector-Base Voltage: 200 V

  • Emitter-Base Voltage: 5 V

  • Collector Current: 0.05 A

  • Collector Dissipation: 0.8 W

  • DC Current Gain (hfe): 70 to 240

  • Transition Frequency: 120 MHz

  • Operating and Storage Junction Temperature Range: -55 to +150 °C

  • Package: TO-92MOD 

  • High breakdown voltage  : VCEO = 150 V (min)

  • Low output capacitance: Cob = 5.0 pF (max)

  • High transition frequency  : fT = 120 MHz (typ.)


Equivalents and Replacements for 2SC2229

2SC2310, 2SC3467, 2SC3468, 3DG2229, KSC2310, KTC1026, 2SC3228, BF422, KSC1506, KTC3206

2SC2229 Applications

  • Audio Amplifiers

  • Audio Amplifier Driver Stages

  • High Voltage Applications

  • Radio and  RF  Circuits

  • Switching loads under 50mA 


Where and how to use 2SC2229

The 2SC2229 transistor can be utilized for a wide range of applications. It can be employed in high voltage applications due to its high collector to emitter voltage,  It's also suitable for a wide range of audio amplification and driver circuits. It's also suitable for use in black-and-white video circuits. This transistor.  with a maximum transition frequency of 120MHz, can also be used in  RF circuits below 120MHz, such as AM and FM broadcast and receiving circuits.

 


How to run 2SC2229 circuit safely?

It is recommended that when using the 2SC2229 transistor.  you do not use it to its absolute maximum ratings and instead, stay 20 percent below these maximum ratings. The transistor's maximum collector current is 50mA.  so do not drive loads that draw more than 40mA. The transistor's maximum collector to emitter voltage is 150V, so the load voltage should be under 120V, and the transistor should always be used or stored at temperatures between -55 and +150 degrees Celsius.

2SC2229 Package Outline

2sc2229 package outline.jpg

2SC2229 Package Outline

2SC2229 Manufacturer

Toshiba Semiconductor & Storage offers a broad range of enabling technology solutions that allow OEMs, ODMs, CMs, and fabless chip companies to develop advanced integrated products for computing, networking, and communications, and digital consumer, automotive, and other markets.

Datasheet PDF

Download datasheets and manufacturer documentation for Toshiba Semiconductor and Storage 2SC2229-O(TE6,F,M).
Frequently Asked Questions

What is 2SC2229 used for?

The 2SC2229 is intended for use in general electronics applications (e.g., computers, personal equipment, office equipment, measuring equipment, industrial robots, and home electronics appliances) or for specific applications as expressly stated in this document.

The 2SC2229 is intended for use in general electronics applications (e.g., computers, personal equipment, office equipment, measuring equipment, industrial robots and home electronics appliances) or for specific applications as expressly stated in this document.

Its voltage is 200v. 
2SC2229-O(TE6,F,M)

Toshiba Semiconductor and Storage

In Stock

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe

Related Parts More