Sort by
What is an Instrumentation Amplifier?27 March 2025
One type of IC (integrated circuit), primarily used to amplify a signal, is an instrumentation amplifier. This amplifier belongs to the differential amplifier family since it increases the difference between the two inputs. The primary purpose of this amplifier is to reduce the surplus noise selected by the circuit. Per IC pin known as the CMRRR is familiar with the ability to reject noise (common-mode rejection ratio). Due to its characteristics such as high CMRR, open-loop gain is high, low drift as well as low DC offset, etc, the instrumentation amplifier IC is an integral component in the configuration of the circuit.
Voltage Follower: Purpose, Working, and Circuits27 March 2025
An op-amp circuit is a voltage follower (also called a unity-gain amplifier, a buffer amplifier, and an isolation amplifier). This suggests that the op-amp would not supply the signal with any enhancement. This article addresses the voltage follower description.
What is an Operational Amplifier?27 March 2025
Hello everyone, I am Rose. Today I will introduce operational amplifier to you. An operational amplifier ("op-amp" for short) is a circuit unit with a very high amplification factor. This article includes its symbol, characteristics and parameters.
16 Q&A About the Secrets of Operational Amplifiers27 March 2025
Hello everyone, I am Rose. Last time, I introduce operational amplifier to you. Today, I will answer 16 questions about operational amplifier, let's see whether you have the following questions!
Low-Power Design of Operational Amplifiers27 March 2025
Hello, this is Candy. With the rise in popularity of battery-powered electronics in recent years, analog circuit designers have been increasingly concerned about power usage. This article will cover how to use low-power op amps in system design, as well as low-power op amps with low supply voltage capabilities and their applications, as well as how to read and understand op amp data sheets appropriately. Circuit design with energy-saving technologies for more efficient device choices.
Introduction to Optical Amplifier27 March 2025
An optical amplifier is a subsystem product that can amplify optical signals in optical fiber communication systems. The principle of the optical amplifier is basically based on the stimulated radiation of the laser, which realizes the amplification effect by converting the energy of the pump light into the energy of the signal light.
Introduction to MD8002A Audio Amplifier27 March 2025
The MD8002A is an audio power amplifier that uses a 5V DC power supply to provide 2.0 watts of continuous power to a BTL load with less than 10% distortion. It was created with the aim of providing high-quality o/p control with fewer components. It doesn't use any output coupling capacitors or bootstrap capacitors.
What is a Ground Fault Circuit Interrupter?27 March 2025
A ground fault circuit interrupter(GFCI) is an electrical device installed to protect against severe electric shocks. It can also reduce electrocutions, minimize electrical burns and shock injuries, and detect ground faults, and interrupts the flow of electric current.
Types, Working, and Selection of DC Motor27 March 2025
A direct current motor (DC motor) is an electric motor that operates on direct current. The operation of an electric motor is based on basic electromagnetism. When a current-carrying conductor is put in an external magnetic field, it will feel a force that is equal to the current in the conductor and the frequency of the external magnetic field.
Operational Amplifier Basics: Working Principle and Amplifier Circuit21 March 2025
Operational amplifier (referred to as "op amp") is a circuit unit with very high magnification. In actual circuits, a certain functional module is usually combined with a feedback network. It is an amplifier with a special coupling circuit and feedback. The output signal can be the result of mathematical operations such as addition, subtraction, differentiation, and integration of the input signal. Because of its early application in analog computers to realize mathematical operations, it was named "operational amplifier".
Understanding the Low Noise Amplifier (LNA)20 March 2025
A low noise amplifier is an amplifier with a very low noise figure. It is generally used as a high-frequency or intermediate-frequency preamplifier for various types of radio receivers, as well as amplifying circuits for high-sensitivity electronic detection equipment.
FPGA in Industry and Communication: Key Players, Technologies, and Future Trends07 March 2025
FPGAs (Field Programmable Gate Arrays) have become the core hardware in the industrial and communication fields due to their programmability and parallel processing capabilities.


Product
Brand
Articles
Tools