Voltage Follower: Purpose, Working, and Circuits

Classic Circuits You Should Know: Voltage Follower
Catalog
Ⅰ What is a Voltage Follower?
An op-amp circuit is a voltage follower (also called a unity-gain amplifier, a buffer amplifier, and an isolation amplifier). This suggests that the op-amp would not supply the signal with any enhancement. The explanation that it is called a voltage follower is because the output voltage matches the input voltage directly, which means that the output voltage is the same as the input voltage. So, for instance, if 10V goes in as input into the op-amp, 10V comes out as output. As a buffer, a voltage follower operates, supplying the signal with no distortion or attenuation.
In a voltage follower configuration, operational amplifiers are commonly used. But, in terms of possible damage & capacitive oscillation loading, this is not the finest structure. These loads have an immense influence on applications focused on op-amp stability. To stabilize a regular op-amp, multiple compensation strategies are present. So, the most common ones, used in most situations, will be defined in this application.
Voltage follower can be defined as when the op-amp circuit output directly follows the op-amp input. So, all the voltages of the input and output are the same. There is no amplification given by this circuit. As a consequence, the voltage gain equates to 1. It is also known as the amplifier for unification gain, buffer & isolation. The input impedance of this circuit is high, so it is used in various circuits. The input signal is used by the voltage follower to give effective output isolation. Below, the simple diagram is shown.

Figure1. Voltage Follower Circuit
Ⅱ The Purpose of a Voltage Follower
The primary goal of the voltage follower is to supply the same input voltage as the output voltage. It has a current gain, in other words, but no voltage gain.
The following voltage follower circuit is discussed below for a deeper explanation of this definition. Including a power source and less impedance load, consider the circuit below. Because of the low resistance load, this circuit draws a large amount of current through the attached load. The circuit, thus, uses an immense amount of electricity from the power source which causes large issues within the power source.
After that, we should assume that we are supplying the voltage follower with equivalent control. As this circuit's input impedance is high, less current would be drawn from the above circuit. The output of this circuit is the same as its input due to the absence of resistors for feedback.
Ⅲ Voltage Follower in Voltage Divider Circuits
Otherwise, the voltage in each and every circuit can be shared with the resistance impedance within the circuit of the allied components. Once the operational amplifier is connected, because of a huge impedance, the main voltage element will fall across it. As a result, if we use the voltage follower within the voltage divider circuit, then enough voltage across the given load is allowed.
There are no external components needed by the voltage follower. Refer to Figure 2. But what is the purpose of a voltage follower if it's an amplifier and does not amplify?

Figure 2: A voltage follower has a gain of one, so the output voltage is (theoretically) equal to the input voltage.
Operational amplifiers have a very high input impedance, meaning that the inputs do not suck in a lot of currents (ideally, none). There is also a very low output impedance for Op Amps. In a voltage divider, one application where this is beneficial is. It is possible that the impedance load (Ro) can vary quite a bit in a voltage divisor (as in Figure 3). Because of Ohm's Law (V=IR), it will influence VOUT if Ro varies.

Figure 3: A voltage divider, but as Ro varies, VOUT varies due to Ohm's Law
If Ro differs in Figure 3, so VOUT will differ similarly if you were unable to separate the VOUT of the voltage divider by adding a follower of high impedance voltage between it and Ro, as in Figure 4. The load impedance (Ro) is isolated by adding a voltage follower to the voltage divider circuit so that VOUT is dependent on R1 and R2 (see figure 4), not Ro.

Figure 4: A voltage divider that enables VOUT to stay steady with a voltage follower (unity gain amp)
This is only possible because the op-amp has such a high impedance of input and a low impedance of output; the op-amp functions to preserve this condition! (Remember that an op-amp is a driven device, not a passive device. Op-amp signals seldom suggest the voltage supply to an op-amp, but when you really wire one up, it's still there.)
The voltage follower (Figure 2) helps one to switch and sustain the voltage level from one circuit to another. It retains the signal of the voltage source. That's why it's sometimes called an amplifier for buffer or separation. You can switch from one logic level (e.g. 5V) to another logic level by using a voltage divider circuit (e.g., 3.3V). A cleaner transition is achieved when the voltage divider circuit is added to a voltage follower (buffer amplifier) (Figure 4). To perform the same buffered transition, another way to achieve logic level shifting or translation is to use an IC called a level shifter. The high op-amp impedance allows the voltage follower circuit to avoid the load (Ro) from impacting the output voltage.
The voltage follower, or voltage buffer, provides a way of moving a voltage source signal from one impedance level to another with or without a voltage divider circuit without impacting current. From there, Ohm's Law (V=IR) governs the relationship. Voltage followers are used in other circuits to balance impedance, too. Notice that there is also a current buffer, rather than a voltage signal source, which maintains the current signal source.
As seen in the following circuit, let us address the voltage divider circuit.

Figure 5. Voltage Follower in Voltage Divider
The voltage divider is mounted at the middle of two resistors and the operating amplifier in the following circuit. 10 K Ω -2 are the resistors used in the circuit. 100 megaohms would be the input resistance given by the operating amplifier. So the parallel resistance can be proportional to 10 K Ω|| 100 KΩ. So it is possible to quantify equal parallel resistance as
= 10 X 100/ 10 + 100 => 10 kilo ohm approximately.
It contains two equivalent resistances in the voltage divider circuit that will give half of the voltage inside the power source. Using the voltage divider formula as given below, it can be generated by
Vout = Vin X R2/R1+R2
10X10/10 + 10 = 5Volts
The above voltage would then decrease over the 10K resistance at the top as well as the voltage drop over the 10K resistance at the bottom and the 100 load resistance. So, we know that to get the appropriate voltage from the load, the operating amplifier acts as a buffer. Due to the lack of voltage supply through the load, the above circuit except the voltage follower would not operate properly.
For the most part, this may be applied specifically for two reasons, such as isolating and buffering the output voltage purposes from the circuit in order to achieve the preferred voltage against the attached load.
Ⅳ Reasons for Using a Voltage Follower
The advantages of voltage follower:
It makes a gain of power as well as current power
The output utilizes the lower output impedance of the circuit
Zero current from the i/p is used for this operational amplifier.
It removes loading impact.
It does not increase or decrease the amplitude of the input signal.
It is not practical to strip out high-frequency noise.
It has lower impedance to the output
It has a high impedance of input,
Unity Transmission Gain
The input signal amplitude is not increased or decreased by a voltage follower, and high-frequency noise is not filtered out. Thus, you may be wondering why such a circuit is so helpful. It is true that the amplitude or frequency characteristics of the input signal are not altered intentionally by a voltage follower, but it allows us to enhance impedance relationships.
We have to take the output impedance of the source subcircuit and the input impedance of the load subcircuit into account whenever we send a voltage signal from one subcircuit to another.
A voltage divider forms the output impedance of the source and the input impedance of the load, and consequently, voltage transfer depends on the ratio of input impedance to output impedance. A source circuit with low output impedance and a load circuit with high input impedance require effective voltage transfer.
There is a low output impedance and the extremely high input impedance of a voltage follower, which makes it a simple and efficient solution to problematic impedance relationships. A voltage follower placed between these two subcircuits will ensure that the full voltage is delivered to the load if a high-output-impedance subcircuit has to transfer a signal to a low-input-impedance subcircuit.
Using a resistive voltage divider, a reference voltage (VREF) can be generated, but the output impedance of the circuit will not below, particularly if higher value resistors are used as a way to reduce current consumption. The voltage follower is not negatively affected by the output impedance of the divider, and for other components in the system, it produces a low-output-impedance reference voltage.
Ⅴ Summary
Thus, this is all about the buffer amplifier or voltage follower overview. It is a buffer for non-inverting and unit gain, using a single operational amplifier. These have two characteristics, such as elevated input impedance and low output impedance. By allowing high impedance sources, they reinforce the signal and drive a lower impedance load. This utilizes an operational amplifier where a stable unity-gain should be specified in its design. The creation of a unit gain driver with a high current can be done in its design through the use of external transistors.
A voltage follower is a non-inverting unity-gain buffer that only requires an operational amplifier (and a decoupling capacitor).
Voltage followers have a high impedance of input and low impedance of output; this is the essence of their buffering action. They strengthen a signal and thus allow a low-impedance load to be driven by a high-impedance source.
The "unity-gain stable" op-amp used in a voltage-follower configuration must be specified.
By integrating an external resistor into the voltage-follower setup, a high-current unity-gain driver can be produced.
References
LearningAboutElectronics. (2023). What is a Voltage Follower?. Retrieved from http://www.learningaboutelectronics.com/Articles/Voltage-follower
Jakelectronics. (2024). Voltage Follower: What It Is & How Does It Work?. Retrieved from https://www.jakelectronics.com/blog/voltage-follower
TutorialsPoint. (2022). Voltage Follower Using Operational Amplifier. Retrieved from https://www.tutorialspoint.com/voltage-follower-using-operational-amplifier-definition-circuit-diagram-working-and-applications
1.What do you mean by voltage follower?
A voltage follower (also known as a buffer amplifier, unity-gain amplifier, or isolation amplifier) is an op-amp circuit whose output voltage is equal to the input voltage (it “follows” the input voltage). A voltage follower circuit has a very high input impedance.
2.What is the use of voltage follower?
A voltage follower can be used as a buffer because it draws very little current due to the high input impedance of the amplifier, thus eliminating loading effects while still maintaining the same voltage at the output.
3.What is the purpose of a voltage buffer?
A voltage buffer amplifier is used to transfer a voltage from a first circuit, having a high output impedance level, to a second circuit with a low input impedance level.
4.How much voltage gain is provided by the voltage follower?
In a voltage follower circuit, the output voltage is equal to the input voltage; thus, it has a gain of one (unity) and does not amplify the incoming signal.
5.What is a flipped voltage follower?
The ”flipped voltage follower (FVF)” is an enhanced buffer cell widely employed for low-power and/or low voltage operation. The applications of the FVF and its variations in analog and mixed signal (AMS) circuit design have increased continuously over the last few years.
Introduction to MD8002A Audio AmplifierUTMEL27 March 20259074The MD8002A is an audio power amplifier that uses a 5V DC power supply to provide 2.0 watts of continuous power to a BTL load with less than 10% distortion. It was created with the aim of providing high-quality o/p control with fewer components. It doesn't use any output coupling capacitors or bootstrap capacitors.
Read More
Understanding the Low Noise Amplifier (LNA)UTMEL20 March 202525438A low noise amplifier is an amplifier with a very low noise figure. It is generally used as a high-frequency or intermediate-frequency preamplifier for various types of radio receivers, as well as amplifying circuits for high-sensitivity electronic detection equipment.
Read More
Introduction to Optical AmplifierUTMEL27 March 20259897An optical amplifier is a subsystem product that can amplify optical signals in optical fiber communication systems. The principle of the optical amplifier is basically based on the stimulated radiation of the laser, which realizes the amplification effect by converting the energy of the pump light into the energy of the signal light.
Read More
What is an Inverting Amplifier?UTMEL25 April 202511620An inverting amplifier is a fundamental configuration of operational amplifiers where the output signal has opposite polarity to the input signal. This configuration uses an operational amplifier with its inverting input terminal receiving the input signal, while the non-inverting terminal is typically connected to ground. The primary function of this circuit is to amplify the input signal while inverting its phase by 180 degrees.
Read More
Low-Power Design of Operational AmplifiersUTMEL27 March 20256836Hello, this is Candy. With the rise in popularity of battery-powered electronics in recent years, analog circuit designers have been increasingly concerned about power usage. This article will cover how to use low-power op amps in system design, as well as low-power op amps with low supply voltage capabilities and their applications, as well as how to read and understand op amp data sheets appropriately. Circuit design with energy-saving technologies for more efficient device choices.
Read More
Subscribe to Utmel !
SZESD5Z12T1GON Semiconductor
SM15T100CASTMicroelectronics
ITA25B1RLSTMicroelectronics
SMBJ24CA-TRSTMicroelectronics
USBULC6-2M6STMicroelectronics
SMBJ15ALittelfuse Inc.
ESD202B1CSP01005XTSA1Infineon Technologies
SMBJ6.5CA-13-FDiodes Incorporated
SESDONCAN1LT3GON Semiconductor
ESD8040MUTAGON Semiconductor


Product
Brand
Articles
Tools