What is an Instrumentation Amplifier?

Instrumentation Amplifier Explained (with Derivation)
Catalog
| I. General Introduction | |
| 2. Features | 1. Advantages |
| 2. Difference | |
| III. Applications | |
I. General Introduction of Instrumentation Amplifier
Instrumentation amplifier, an improvement of a differential amplifier, has an input buffer and does not require input impedance matching, making the amplifier suitable for measurement and electronic instruments. Features include very low DC offset, low drift, low noise, very high open-loop gain, very large common-mode rejection ratio, and high input impedance. Instrumentation amplifiers are used in circuits that require very high accuracy and stability.
To reproduce very low-level signals, rejecting noise and interference signals, an instrumentation amplifier is used. Heartbeats, blood pressure, temperature, earthquakes, and so on can be examples. The essential features of a good instrumentation amplifier, therefore, are as follows.
There would be very low signal energy for inputs to the instrumentation amplifiers. The instrumentation amplifier should then have a high degree of gain and should be exact.
By using a single trigger, the gain can be conveniently adjustable.
To avoid loading, it must have High Input Impedance and Low Output Impedance.
The instrumentation amplifier should have a high CMRR because, when broadcast over long wires, the transducer output would normally contain common-mode signals such as noise.
To control sharp rise times of events and have a full undistorted output voltage swing, it must also provide a High Slew Rate.
With the rapid development of electronic technology, operational amplifier circuits have also been widely used. The instrumentation amplifier is a precision differential voltage amplifier, which is derived from the operational amplifier and is better than the operational amplifier. The instrumentation amplifier integrates key components inside the amplifier. Its unique structure makes it have the characteristics of high common-mode rejection ratio, high input impedance, low noise, low linearity error, low offset drift, flexible gain setting, and convenient use. Acquisition, sensor signal amplification, high-speed signal adjustment, medical instruments, and high-end audio equipment are all popular. An instrumentation amplifier is a closed-loop gain component with a differential input and a single-ended output relative to the reference end. It has a differential input and a single-ended output relative to the reference end. The difference from the operational amplifier is that the closed-loop gain of the operational amplifier is determined by the external resistance connected between the inverting input and the output, while the instrumentation amplifier uses an internal feedback resistor network isolated from the input. The input signal is applied to the two differential input terminals of the instrumentation amplifier, and its gain can be preset internally or preset by the user through the internal setting of the pin or through an external gain resistor isolated from the input signal.
Instrumentation Amplifier using Op-Amp
The use of the op-amp circuit instrumentation amplifier is seen below. The non-inverting amplifiers are op-amps 1 & 2 and op-amp 3 is a differential amplifier. Together, these three op-amps form an amplifier for instrumentation. The final value of the Vout instrumentation amplifier is the augmented variance of the input signals added to the op-amp 3 input terminals. Let the op-amp 1 and op-amp 2 outputs be Vo1 and Vo2 respectively.
Vout = (R3/R2) then (Vo1-Vo2)
As seen in the figure below, look at the input stage of the instrumentation amplifier. Below is a discussion of the instrumentation amplifier derivation.
The potential is the input voltage V1 at node A. Hence, from the virtual short definition, the capacity at node B is also V1. The capacity at node G, thus, is also V1.
The potential is the input voltage V2 at node D. The capacity at node C is therefore also V2, from the virtual short. The capacity at node H, thus, is also V2.
Ideally, the current at the input stage op-amps is zero for the operation of the instrumentation amplifier. Therefore, the current I by R1, Rgain, and R1 resistors remain the same.
Applying Ohm's law between nodes E and F,
I = (Vo1-Vo2)/(R1+Rgain+R1) ...(1)
I = (Vo1-Vo2)/(2R1+Rgain)
Since no current flows to the input of the op-amps 1 & 2, it is possible to send the current I between the nodes G and H as:
I = (VG-VH) / Rgain = (V1-V2) / Rgain...(2)
Equating equations 1 and 2,
(Vo1-Vo2)/(2R1+Rgain) = (V1-V2)/Rgain
(Vo1-Vo2) = (2R1+Rgain)(V1-V2)/Rgain ...(3)
The output of the difference amplifier is given as,
Vout = (R3/R2) (Vo1-Vo2)
Therefore, (Vo1 - Vo2) = (R2/R3)Vout
Substituting (Vo1 - Vo2) value in equation 3, we get
(R2/R3)Vout = (2R1+Rgain)(V1-V2)/Rgain
i.e. Vout = (R3/R2){(2R1+Rgain)/Rgain}(V1-V2)
The above equation gives an instrumentation amplifier's output voltage.
The expression (R3/R2){(2R1+Rgain)/Rgain} supplies the total gain of the amplifier.
By changing the value of resistor Rgain, the total voltage gain of an instrumentation amplifier can be regulated.
The differential amplifier supplies the common-mode signal attenuation for the instrumentation amplifier.
II. Features of Instrumentation Amplifier
The instrumentation amplifier is a high-gain, DC-coupled amplifier with differential input, single-ended output, high input impedance, and high common-mode rejection ratio, low noise, low linearity error, low offset voltage and offset voltage drift, and low input bias Features such as current and offset current error.
1. Advantages of Instrumentation Amplifier
(1) High common mode rejection ratio
The instrumentation amplifier has the characteristic that it can eliminate any common-mode signal (the two input terminals have the same potential) and amplify the differential mode signal (the two input terminals have different potentials). In order for the instrumentation amplifier to work properly, it is required to amplify microvolt differential mode signals and at the same time suppress common mode signals of several volts. The instrumentation amplifier that realizes this function must have a high common mode rejection capability. The typical value of the common-mode rejection ratio is 70-100dB. Generally, when the gain is high, the performance of the CMRR will be improved, that is, the CMRR is higher when the gain is high, and lower when the gain is low.
(2) Small linear error
Input offset and scale factor can be corrected by external adjustment, while linear error is an inherent defect of the device and cannot be eliminated by external adjustment. Therefore, the small linear error of the instrumentation amplifier is realized by the manufacturer through the use of advanced production technology and chip structure design. For a high-performance instrumentation amplifier, the linearity error is 0.01%, and some can even reach 0.0001%.
(3) High input impedance
In the actual application circuit, the signal source impedance may be very high or unbalanced. In order to be well-matched, the input impedance of the instrumentation amplifier is not only very high but also has good matching performance. The typical value of the input impedance is 109-1012 ohms.
(4) Low noise
Instrumentation amplifiers are often used in harsh environments to complete the pickup and preprocessing of weaker signals, so it must be a low-noise device, and the signal-to-noise ratio is too low to work. Under normal circumstances, when the frequency of the input signal is 1kHZ, the noise referred to as the input of the instrumentation amplifier should be less than 10nV/Hz. In order to improve the signal-to-noise ratio, it is generally not desirable for the instrumentation amplifier to add its own noise to the signal.
(5) Low offset voltage and low offset voltage drift
The offset voltage drift of an instrumentation amplifier is composed of two parts, input, and output. Each part has an influence on the total gain, but when the gain is increased, the offset drift of the input part will become the main error source, and the influence of the output part can be ignored. The typical values of input and output offsets are 100V and 2mV, respectively. In addition, the instrumentation amplifier has excellent stability. When operating conditions change, its key parameters remain stable. And easy to use, only need to detect the potential difference between the two input terminals. In addition, due to its high degree of integration, the main components are all made inside the chip, and there are few peripheral components.
2. Difference between Operational Amplifier and Instrumentation Amplifier
The foregoing are the main distinctions between the operating amplifier and the instrumentation amplifier.
One type of integrated circuit is an active amplifier (op-amp).
One type of differential amplifier is the instrumentation amplifier.
It is possible to construct instrumentation amplifiers with three operating amplifiers.
A single operating amplifier may be used to build the differential amplifier.
The output voltage of the differential amplifier is impacted by the mismatch of resistors
The instrumentation amplifier produces gain in its primary phase with a single resistor that does not require a corresponding resistor.
III. Applications of Instrumentation Amplifier
The following was used in the instrumentation amplifier implementations:
Such amplifiers specifically include where high differential gain accuracy is needed, power must be maintained in noisy conditions, as well as where there are big common-mode signals. Any of the apps are
Instrumentation amplifiers are used to collect data from small O/P transducers such as thermocouples, strain gauges, Wheatstone bridge scales, etc.
In navigation, pharmacy, radar, etc., these amplifiers are used.
These amplifiers are used in audio applications, such as low-amplitude audio signals, to increase the S/N ratio (signal to noise).
Such amplifiers are used in high-speed signal conditioning for imaging as well as video data acquisition.
In RF cable networks, these amplifiers are used for high-frequency signal amplification.
Reference
Analog Devices. (2019). The Designer's Guide to Instrumentation Amplifiers. https://www.analog.com/media/en/training-seminars/design-handbooks/designers-guide-instrument-amps-complete.pdf
AllecCo Elec. (2024, November 29). Instrumentation Amplifiers: Types, Applications, and Advantages. https://www.allelcoelec.com/blog/Instrumentation-Amplifiers-Types,Applications,and-Advantages.html
Electronics Hub. (n.d.). Instrumentation Amplifier Basics and Applications. https://www.electronicshub.org/instrumentation-amplifier-basics-applications/
Renesas Electronics. (n.d.). Instrumentation Amplifiers. https://www.renesas.com/en/products/analog-products/amplifiers/specialized-amplifiers/instrumentation-amplifiers
Texas Instruments. (2019). What Is an Instrumentation Amplifier?. https://www.ti.com/document-viewer/lit/html/SSZT428
What are the requirements of an instrumentation amplifier?
The instrumentation amplifier is intended for precise, low-level signal amplification where high input resistance, low noise and accurate closed-loop gain is required. Also, low power consumption, high slew rate and high common-mode rejection ratio are desirable for good performance.
Why is CMRR high in instrumentation amplifier?
An instrumentation amplifier (IA) is used to provide a large amount of gain for very low-level signals, often in the presence of high noise levels. The major properties of IAs are high gain, large common-mode rejection ratio (CMRR), and very high input impedance.
Why is instrumentation amplifier needed?
The importance of an instrumentation amplifier is that it can reduce unwanted noise that is picked up by the circuit. The ability to reject noise or unwanted signals common to all IC pins is called the common-mode rejection ratio (CMRR). Instrumentation amplifiers are very useful due to their high CMRR.
Introduction to MD8002A Audio AmplifierUTMEL27 March 20259855The MD8002A is an audio power amplifier that uses a 5V DC power supply to provide 2.0 watts of continuous power to a BTL load with less than 10% distortion. It was created with the aim of providing high-quality o/p control with fewer components. It doesn't use any output coupling capacitors or bootstrap capacitors.
Read More
Understanding the Low Noise Amplifier (LNA)UTMEL20 March 202526562A low noise amplifier is an amplifier with a very low noise figure. It is generally used as a high-frequency or intermediate-frequency preamplifier for various types of radio receivers, as well as amplifying circuits for high-sensitivity electronic detection equipment.
Read More
Introduction to Optical AmplifierUTMEL27 March 202510468An optical amplifier is a subsystem product that can amplify optical signals in optical fiber communication systems. The principle of the optical amplifier is basically based on the stimulated radiation of the laser, which realizes the amplification effect by converting the energy of the pump light into the energy of the signal light.
Read More
What is an Inverting Amplifier?UTMEL25 April 202512407An inverting amplifier is a fundamental configuration of operational amplifiers where the output signal has opposite polarity to the input signal. This configuration uses an operational amplifier with its inverting input terminal receiving the input signal, while the non-inverting terminal is typically connected to ground. The primary function of this circuit is to amplify the input signal while inverting its phase by 180 degrees.
Read More
Low-Power Design of Operational AmplifiersUTMEL27 March 20257744Hello, this is Candy. With the rise in popularity of battery-powered electronics in recent years, analog circuit designers have been increasingly concerned about power usage. This article will cover how to use low-power op amps in system design, as well as low-power op amps with low supply voltage capabilities and their applications, as well as how to read and understand op amp data sheets appropriately. Circuit design with energy-saving technologies for more efficient device choices.
Read More
Subscribe to Utmel !
LT4356IDE-2#TRPBFLinear Technology/Analog Devices
LT4356HDE-1#PBFLinear Technology/Analog Devices
LT4356CMS-1#TRPBFLinear Technology/Analog Devices
LT4356IMS-1#TRPBFLinear Technology/Analog Devices
LT4356CS-1#PBFLinear Technology/Analog Devices
LTC4364IMS-2#TRPBFLinear Technology/Analog Devices
CM2009-02QRON Semiconductor
TPD8S300RUKRTexas Instruments
TL7726IDTexas Instruments
ADG465BRTZ-REEL7Analog Devices Inc.


Product
Brand
Articles
Tools