Sort by
Silicon Carbide (SiC): The Third-generation Semiconductor Material30 August 2021
Silicon carbide (SiC) is the main development direction of the power semiconductor industry. It is the semiconductor material to make power devices. In the foreseeable future, new energy vehicles are the main application for silicon carbide power devices.
What is a USB Data Cable?27 August 2021
The USB data cable is used for the connection and communication of the computer and external devices. It can also be used for the charging of the phone and the external connection. It is popular for transmitting data and charging.
What is Wi-Fi 7?20 August 2021
Following the release of Wi-Fi 6 (802.11ax), new 802.11be (EXTREMELY High Throughput) standards have been proposed. The WiFi Union will name the 802.11be standard Wi-Fi 7.
Network Interface Card: Types, Functions and Buying Guide17 August 2021
Network Interface Card (NIC, also known as a network interface controller) is one of the most basic components in the local area network. It is the hardware device connecting the computer and the network. Whether it is a twisted pair connection, a coaxial cable connection, or an optical fiber connection, data communication must be realized with the help of a network interface card.
Infrared Thermometer: How it Works? How to Use it?12 August 2021
Infrared thermometers are divided into fixed thermometers and hand-held thermometers. They are a kind of thermometer that detects the amount of infrared rays on the surface of an object to achieve temperature measurement.
An Overview of Fiber Optic Cable10 August 2021
A fiber optic cable is a communication cable consisting of two or more glass or plastic optical fiber cores located in a protective coating and covered by a plastic PVC outer sleeve. The signal transmission along with the internal optical fiber generally uses infrared rays.
Understanding of Coaxial Cable06 August 2021
Coaxial cable is a broadband transmission line with low loss and high isolation characteristics. This blog introduces the classification, structure, working principle, parameters, and characteristics of coaxial cables.
Everything You Need to Know about NVMe04 August 2021
NVM Express (NVMe), or Non-Volatile Memory Host Controller Interface Specification, is a logical device interface specification. It is a bus transmission protocol specification based on a device logic interface similar to AHCI.
A User Guide to Automotive Relay30 July 2021
A relay is an automatic control device whose output will change leaps and bounds when the input reaches a certain value. Automotive relays are relays used in automobiles. This type of relay has high switching load power, high shock resistance, and vibration resistance.
Introduction to Wireless Charger27 July 2021
A wireless charger is a gadget that charges by electromagnetic induction. Under the influence of electric power, the transmitting end coil delivers an electromagnetic signal to the outside, and the receiving end coil receives the electromagnetic signal and transforms it into an electric current.
Introduction to UFS (Universal Flash Storage)23 July 2021
UFS (Universal flash storage) is a flash storage specification designed for use in consumer electronic products such as digital cameras and smartphones. Its design goal is to develop a unified flash memory card format. While providing high data transmission speed and stability, it can also reduce consumer confusion about various memory card formats on the market.
What is a Cell Phone Antenna?21 July 2021
Cell phone antennas are devices that receive signals on cell phones. Old cell phones have protruding antennas, and most new cell phones have been hidden in the fuselage.


Product
Brand
Articles
Tools