What is a Server CPU?

Should You Game On a Server CPU?
Catalog |
Server CPU is the CPU (central processing unit) used on the server. The server is an important device in the network. It has to receive access from a few dozens to thousands of people, so it has strict requirements for fast throughput of large data volume, super stability, and long time operation. Therefore, the CPU is the "brain" of the computer and is the primary indicator of server performance.
Ⅰ Classification of server CPU
The CPU of the server is still distinguished by the instruction system of CPU, which is usually divided into two categories: CISC CPU and RISC CPU, and later there is a 64-bit VLIW (Very Long Instruction Word) instruction system CPU.
CISC server CPU
CISC is the abbreviation of "Complex Instruction Set Computing". It refers to the x86 (an Intel CPU naming specification) series CPUs produced by Intel and its compatible CPUs (CISC), which are based on the PC (personal computer) architecture. CISC type CPUs are mainly Intel server CPUs and AMD server CPUs.

Intel server CPU Xeon
Advantages
From the current server development status, the IA architecture (CISC architecture) PC server, which is characterized by "small, compact and stable", has been more widely used due to its reliable performance and low price. In the field of Internet and LAN, they are used for file service, printing service, communication service, Web service, e-mail service, database service, application service, etc.
Disadvantages
The biggest drawback of IA-64 microprocessors is their lack of compatibility with x86, and Intel, in order for IA-64 processors to better run software from both dynasties, has on IA-64 processors (Itanium, Itanium2 ...) An x86-to-IA-64 decoder was introduced so that it could translate x86 instructions to IA-64 instructions. This decoder was not the most efficient decoder, nor was it the best way to run x86 code (the best way was to run x86 code directly on an x86 processor), so Itanium and Itanium2 had very poor performance when running x86 applications. This became the root cause of the creation of X86-64.
One final point worth noting is that although the CPU is one of the most important factors in determining server performance, it cannot perform as well as it should without the support and cooperation of other accessories.
The biggest drawback of IA-64 microprocessors is their lack of compatibility with x86. Intel, on the other hand, introduced x86-to-IA-64 decoders on IA-64 processors such as Itanium and Itanium2 in order for IA-64 processors to better run software from both dynasties. This enables the translation of x86 instructions into IA-64 instructions. This decoder was not the most efficient decoder, nor was it the best way to run x86 code (the best way is to run x86 code directly on an x86 processor), so Itanium and Itanium2 had very poor performance when running x86 applications. This became the root cause of the creation of X86-64.
Although the CPU is one of the most important factors in determining the performance of a server, it cannot perform as well as it should without the support and cooperation of other accessories.
RISC server CPU
RISC is the abbreviation of "Reduced Instruction Set Computing". It is developed on the basis of the CISC (Complex Instruction Set Computer) instruction system, and some people have tested CISC machines to show that the frequency of various instructions is quite disparate. The most frequently used are some relatively simple instructions, which account for only 20% of the total number of instructions, but 80% of the frequency in the program. A complex instruction system is bound to increase the complexity of the microprocessor, making the processor development time long and costly. And complex instructions require complex operations, which will inevitably reduce the speed of the computer.
For these reasons, the RISC CPU was born in the 1980s, which not only streamlined the instruction system compared with the CISC CPU but also adopted a structure called "superscalar and super pipeline", which greatly increased the parallel processing capability. (Parallel processing means that a server has multiple CPUs processing simultaneously. Parallel processing can greatly improve the data processing capability of the server. Department-level and enterprise-level servers should support CPU parallel processing technology.) In other words, the architecture is much higher performance than CPUs with CISC architecture at the same frequency, which is determined by the technical characteristics of CPUs. RISC instruction system is more suitable for UNIX, the operating system of high-grade servers, and Linux is also a UNIX-like operating system.
The main types of CPUs that use RISC instructions in mid- to high- grade servers are as follows.
(1) PowerPC processors
(2) SPARC processors
(3) PA-RISC processors
(4) MIPS processor
(5) Alpha processor
Currently, the two major CPU processor instruction systems, CISC and RISC architectures are both taking advantage of each other's strengths and weaknesses and moving toward convergence. CISC borrows ideas from RISC to optimize the efficiency of the instruction system, while RISC introduces enhanced instructions to improve the efficiency of complex task processing. Therefore, there is no need to be overly concerned about the difference between CISC and RISC, both architectures are very advanced and will evolve over time.
CISC complex instruction set is characterized by a large number of instructions, one instruction performs multiple functions. The advantage is the high efficiency of executing specific functions, such as multimedia processing. The disadvantage is the complex system design and low execution efficiency. Typical architectures include x86.
The RISC reduced instruction set is characterized by fewer instructions, and complex tasks are completed by combining multiple lean instructions. The advantages are high execution efficiency for common tasks and low power consumption. The disadvantage is low processing efficiency for some complex tasks, such as multimedia processing. Typical architectures are ARM, Power, MIPS, Alpha, and SPARC.
VLIW server CPU
VLIW is the abbreviation of "Very Long Instruction Word". VLIW architecture adopts advanced EPIC (Explicit Parallel Instruction) design, we also call this architecture "IA-64 architecture". EPIC processors are mainly Intel's IA-64 (including Intel's Anthem processor) and AMD's x86-64.
Ⅱ Server CPU vs. desktop CPU
1. Different instruction sets
The common CPUs equipped with home or work computers are usually CISC complex instruction sets, which pursue a large and comprehensive instruction set and try to integrate various common functions into one piece, but the calling speed and hit rate are lower compared to server CPUs. The instructions of server CPU are generally RISC (Reduced Instruction Set). The advantage of this design is that it is more targeted and can be optimized specifically for different needs and is more energy-efficient.
2. Different cache
Cache also determines the performance of the CPU. Due to the high computing performance requirements of server CPUs, server CPUs often apply the most advanced processes and technologies and are equipped with one, two, or three caches, running more powerful. Server CPUs have used level 3 cache for a long time. Ordinary CPUs have used cache technology only in recent years.
3. Different interfaces
Server CPU and ordinary CPU interfaces are often different. Server CPU interfaces are mostly Socket 771, Socket 775, LGA 2011, LGA 1150 compared to ordinary CPU interfaces. Server CPU equipped with the motherboard usually no graphics card slot, because the CPU comes with a core graphics card to meet the demand, and its CPU bus bandwidth is higher than the home CPU.
4. Different stability requirements
Server CPUs are designed to work stably for long periods of time and are basically designed to work continuously all year round. Server CPUs are vastly different from home CPUs in terms of stability and reliability, and servers are generally run 365 days a year, with only occasional downtime for maintenance, which requires high stability.
Ordinary CPUs are designed to work continuously for 72 hours.
5. Multi-way interconnection support is different
Multiplexing is a technology used in servers. For example, a server motherboard can have multiple CPU slots at the same time, allowing multiple CPUs to be installed at the same time, which is CPU multi-channel interconnect technology. This technology is only supported by server CPUs, and ordinary home computers, where only one CPU can be installed on a motherboard, do not support multiplexing.
6. Different prices
Multiplexing is a technology used in servers. For example, a server motherboard can have multiple CPU slots at the same time, allowing multiple CPUs to be installed at the same time, which is CPU multi-channel interconnect technology. This technology is only supported by server CPUs, and ordinary home computers, where only one CPU can be installed on a motherboard, do not support multiplexing.
Ⅲ Top 10 Popular Server CPUs
1 Intel Xeon E5-2678 v3
2 AMD Skyline 7763
3 Intel Xeon E5-2680 v2
4 Intel Xeon Silver 4210R
5 Intel Xeon Gold 5218
6 Intel Xeon E5-2650 v2
7 Intel Xeon E5-2680 v4
8 Intel Xeon Silver 4210
9 Intel Xeon Gold 5218R
10 Intel Xeon E5-2670 v2
1. What is a server CPU?
The Central Processing Unit (CPU) in your server, also referred to simply as the processor, is what interprets and executes instructions, processing data and performing tasks like serving web pages, running database queries, and executing other program and computing commands.
2. What CPU is good for a server?
In a nutshell, Intel's Core CPUs are great for mid-level rugged computers and some high-end rugged servers and workstations, but overall, the company's Xeon CPUs are the best choice for servers and workstations running data-intensive applications, especially those of a mission-critical nature.
Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap DevicesSaumitra Jagdale15 March 20243001For a long era, silicon has stood out as the primary material for fabricating electronic devices due to its affordability, moderate efficiency, and performance capabilities. Despite its widespread use, silicon faces several limitations that render it unsuitable for applications involving high power and elevated temperatures. As technological advancements continue and the industry demands enhanced efficiency from devices, these limitations become increasingly vivid. In the quest for electronic devices that are more potent, efficient, and compact, wide bandgap materials are emerging as a dominant player. Their superiority over silicon in crucial aspects such as efficiency, higher junction temperatures, power density, thinner drift regions, and faster switching speeds positions them as the preferred materials for the future of power electronics.
Read More
Applications of FPGAs in Artificial Intelligence: A Comprehensive GuideUTMEL29 August 20255886This comprehensive guide explores FPGAs as powerful AI accelerators that offer distinct advantages over traditional GPUs and CPUs. FPGAs provide reconfigurable hardware that can be customized for specific AI workloads, delivering superior energy efficiency, ultra-low latency, and deterministic performance—particularly valuable for edge AI applications. While GPUs excel at parallel processing for training, FPGAs shine in inference tasks through their adaptability and power optimization. The document covers practical implementation challenges, including development complexity and resource constraints, while highlighting solutions like High-Level Synthesis tools and vendor-specific AI development suites from Intel and AMD/Xilinx. Real-world applications span telecommunications, healthcare, autonomous vehicles, and financial services, demonstrating FPGAs' versatility in mission-critical systems requiring real-time processing and minimal power consumption.
Read More
The 2026 Engineer’s Guide: Choosing the Right MCU for Your Next IoT & New Energy ProjectUTMEL30 April 20262415A comprehensive comparison of 2026's leading MCUs from ST, NXP, and Microchip across power efficiency, processing performance, connectivity, and ecosystems to help engineers select the optimal chip for next-gen IoT and new energy projects.
Read More
AI Server Components: Engineering Next-Gen Data Center Hardware for 100kW RacksUTMEL15 May 20261269The transition from traditional enterprise IT to AI-driven workloads has rendered legacy data center hardware obsolete, forcing infrastructure planners to re-engineer server components for extreme thermal environments.
Read More
The Practical Engineer’s Guide to the NE555N Timer: Pinout, Setup, and TroubleshootingUTMEL29 May 20261159This comprehensive guide explores the NE555N timer, detailing its 8-pin layout, internal architecture, and key datasheet specifications. It compares the bipolar IC to CMOS variants and details setup configurations for astable, monostable, and bistable modes. Additionally, the guide offers practical troubleshooting advice to prevent common breadboard failures, such as floating reset pins and electrical noise issues.
Read More
Subscribe to Utmel !
ACPL-331J-500EBroadcom Limited
PAM8904JPRDiodes Incorporated
AD9961BCPZRLAnalog Devices Inc.
ACPL-332J-000EBroadcom Limited
ACPL-W346-000EBroadcom Limited
SI8261BCC-C-ISRSilicon Labs
ADATE320-1KCPZAnalog Devices Inc.
AT88SC0104CA-SUMicrochip Technology
80HCPS1848CBLGIRenesas Electronics America Inc.
HCS500-I/PMicrochip Technology


Product
Brand
Articles
Tools