FPGA in Industry and Communication: Key Players, Technologies, and Future Trends
FPGA's real-time, high-reliability and multi-interface adaptation capabilities make it widely used in machine vision, motion control and industrial Internet of Things (IIoT). And in the communication field, FPGAs support key scenarios such as 5G base stations and optical transport networks (OTNs) to meet high-speed signal processing and multi-protocol compatibility requirements.
Contents
1. FPGA Header Manufacturer Overview
2. Xilinx: A Leader in Industry and Communications
3. Altera: Pioneers of Innovation and Market Changers in FPGAs
4. Lattice Semiconductor: Market Leader in Low-Power and Miniaturized FPGAs
5. Microchip: Leading mid-range FPGAs with energy efficiency and security
6. How to choose an FPGA vendor?
7. Utmel: One-stop FPGA sourcing and technical support platform
8. Future Trends in FPGA Selection
FPGA Header Manufacturer Overview
Manufacturer | Description |
Xilinx (now part of AMD) | Global market leader, covering both high-performance and mid-to-low-end applications |
Intel PSG (formerly Altera) | Focuses on Stratix series for communications and military applications |
Specializes in low-power FPGAs for consumer electronics and edge computing | |
Entered low-power embedded market through Microsemi acquisition | |
Achronix | Targets AI acceleration and 5G wireless markets with Speedster series |
Xilinx: A Leader in Industry and Communications
Product Matrix & Technology Advantage
Series | Description |
Virtex UltraScale+ | With a logic density as high as millions of logic cells and supporting 112G PAM4 high-speed transceivers, it is specifically designed for 5G base stations and data center acceleration. |
Kintex UltraScale | Balancing performance and power consumption, it is suitable for real-time control and data acquisition in industrial automation. |
Artix-7 | A low-cost solution used in communication edge devices (such as optical modules) and lightweight IIoT terminals. |
Key Features of Xilinx FPGA
Xilinx FPGAs stand out due to their advanced technical specifications and innovative features.
Adaptive Computing Architecture (ACAP): fuses FPGA programmability with AI acceleration to support dynamic reconfiguration.
Hardened IP cores: integrates protocols such as PCIe and Ethernet to reduce development cycles.
Feature | Description |
Logic Cells | Up to 9M logic cells for Virtex UltraScale+ |
DSP Slices | 25 x 18 multipliers for high-speed math |
Transceivers | High-speed serial transceivers up to 32.75Gbps |
Process Technology | 7nm production for the latest process node |
Power Optimization | Low power consumption with 1.2V core voltage |
Packaging | Small form factor wire-bond CSP packaging |
Application Versatility | Used in 5G infrastructure, optical networking, etc. |
These features enable Xilinx FPGAs to deliver high performance while maintaining energy efficiency. For example, the Artix-7 series offers lower power consumption, enhanced thermal management, and a superior performance-per-watt ratio compared to competitors. This makes Xilinx a preferred choice for energy-conscious applications.
Industry Application Cases
Industrial field: Realize microsecond image processing in machine vision; improve production line precision through multi-axis motion control.
Communication field: Supporting 5G pre-transmission/mid-transmission equipment of Huawei, Ericsson and other vendors; realizing flexible protocol conversion in software-defined network (SDN).
Altera: Pioneers of Innovation and Market Changers in FPGAs
Core Product Families and Positioning
Altera's (now Intel Programmable Chip Division) FPGA product line covers the full range of scenarios from low-power to high-performance needs, and mainly includes the following series:
Series | Description |
Agilex series | The flagship product launched by Intel after acquiring Altera, benchmarked against Xilinx UltraScale+ series. It adopts 10nm SuperFin process and 3D heterogeneous packaging (EMIB), integrates quad-core Arm Cortex-A53 processor, and supports PCIe Gen5 and CXL high-speed interconnection (112Gbps transceiver), suitable for data centers, AI acceleration and 5G communications. |
Stratix series | Focusing on the high-performance market. For example, Stratix 10 adopts 14nm trigate technology, integrates quad-core ARM Cortex-A53, supports high bandwidth (58Gbps transceiver) and hard-core virtualization, and is widely used in military, communication base stations and high-speed data processing. |
Arria series | Positioned in the mid-range market, balancing performance and power consumption. For example, the Arria 10 series adopts 20nm process, integrates ARM hard-core processor and supports 28Gbps transceiver, suitable for industrial automation, medical imaging and vehicle-mounted systems. |
Cyclone series | Low-power and low-cost design, such as Cyclone V and Cyclone 10 series, suitable for consumer electronics, Internet of Things terminals and edge computing devices. |
MAX series | Non-volatile FPGA, such as MAX 10, supporting instantaneous startup and analog mixed-signal integration, used in automotive electronics and industrial control. |
Technical Advantages and Innovations
Heterogeneous Integration and High-Speed Interface: The Agilex series realizes heterogeneous packaging of FPGAs with eASIC and HBM through EMIB technology, and supports PCIe Gen5 and CXL protocols, which significantly improves the interconnection efficiency between data centers and AI chips.
Low-power design: Adopting advanced processes (e.g., 20nm/10nm) and dynamic power optimization technologies, the Arria 10 series consumes 20% less power than its predecessor, making it suitable for energy-efficiency-sensitive scenarios.
Secure Architecture: Integrated hardware root of trust (SDM), configurable bitstream encryption, and physical tamper detection to secure industrial control and communication devices.
Development tool ecosystem: Quartus Prime software supports rapid IP core configuration and OpenCL development to shorten the design cycle, while providing rich reference design and documentation resources.
Industry Application Scenarios
Communication: Stratix series is used in 5G base station's pre-transmission/mid-transmission equipment, supporting high-speed signal processing and protocol conversion; Agilex series realizes low-latency data exchange in optical transport network (OTN)210.
Industrial Control: The Arria series is used in machine vision, multi-axis motion control, and Industrial Internet of Things (IIoT), providing real-time response and high reliability.
Data Center and AI: The Agilex series accelerates CPU and FPGA co-computing with CXL technology to improve AI inference and storage efficiency.
Consumer Electronics: Cyclone series for smart home and wearable devices supports low-power edge AI processing.
Lattice Semiconductor: Market Leader in Low-Power and Miniaturized FPGAs
Core Product Lines and Technology Advantages
Nexus family of small FPGA platforms
Nexus™ 2: The latest generation of small FPGAs launched in 2024, utilizing a 16nm FinFET process, with 3x lower power consumption than its predecessor, and a package size of only 9x11mm, is suitable for scenarios such as edge AI and sensor interfaces. Its Certus™-N2 series supports high-speed interfaces (e.g. PCIe Gen4) and low-latency data processing5.
iCE40 series: Known for its ultra-low power consumption (as low as 25μW) and extremely small package (1.4×1.48mm), it is widely used in wearable devices and IoT terminals.
Mid-range FPGA platform Avant series
Aimed at edge intelligence and industrial automation, covering 300k-700k logic cells, supporting AI inference acceleration, multi-protocol interconnect (e.g. Ethernet, USB-C) and real-time control. For example, Avant-E series is optimized for edge AI, while Avant-X series strengthens high-speed connectivity.
Core Technology Highlights
Low-power architecture: Adopting FD-SOI process and dynamic power management technology, the energy efficiency is 10x higher than competitors in scenarios such as video processing.
Security: Integrated hardware root of trust (Secure Boot) and anti-tampering design to meet the high reliability requirements of the industrial and automotive sectors.
Application Scenarios and Industry Layout
Communications and Computing
Used for signal processing and protocol conversion in 5G base stations, supporting AI acceleration and network management functions in data centers.
Industrial and Automotive
Industrial scenarios: machine vision, motion control, predictive maintenance (analyzing equipment status through edge AI).
Automotive scenarios: smart cockpits, sensor preprocessing (e.g., camera data optimization), and in-vehicle network interfaces.
Consumer electronics and edge AI
Sensor interfaces for wearables, real-time response systems for smart homes, and single-chip edge AI solutions (integration of data preprocessing and inference)
Microchip: Leading mid-range FPGAs with energy efficiency and security
Microchip Technology, a key player in the global FPGA market, has established a leading position in the mid-range FPGA field with breakthroughs in energy efficiency, security and reliability in the PolarFire series, especially in scenarios such as industrial IoT, edge computing and real-time control.
Core Technology Advantages
Energy Efficiency Benchmark
PolarFire FPGA series is known for its “50% lower power consumption”. Compared with similar SRAM FPGAs, its low power consumption is suitable for fanless design scenarios, which significantly reduces the system heat dissipation and material costs, and PolarFire SoCs are integrated with RISC-V processors, supporting Linux and real-time applications. PolarFire SoCs also integrate RISC-V processors, support Linux and real-time applications, and lead the industry in energy efficiency.
Military-Grade Security and Reliability
Encryption and Anti-tampering: Supports DPA (Differential Power Analysis) encryption core and defense-grade secure boot to ensure data security.
Reliability Design: Full memory Single Error Correction/Dual Error Detection (SEC-DED), physical memory protection to meet industrial and aerospace requirements.
RISC-V Ecological Innovation
As the only vendor to mass-produce RISC-V SoC FPGAs, Microchip has built a Mi-V ecosystem that unites more than 60 partners (e.g., Wind River, Mentor Graphics), covering development tools, operating systems, and security protocols to accelerate innovation in edge smart devices.
Core Product Lines
PolarFire series: Mid-range mainstay, covering 250K-500K logic cells, supporting 12.7 Gbps transceivers, suitable for industrial vision, communication gateway and other scenarios 1 2.
IGLOO 2/ProASIC 3: Low-density FPGAs, focusing on low power consumption and fast startup, replacing traditional CPLD.
Fusion Mixed-Signal FPGA: integrates analog and digital functions to support sensor fusion and complex control.
How to choose an FPGA vendor?
Performance and scenario matching:
Industrial scenarios need to focus on anti-interference capability (e.g. -40°C~100°C wide temperature support); communication scenarios need to meet high-speed interfaces (e.g. 56G/112G SerDes).
Supply Chain Stability: Head vendor lead times are typically 12+ weeks, while distributor inventory can alleviate emergency demand.
Development threshold: Ceres has a well-established Vivado tool chain ecosystem, but Chinese FPGAs reduce migration costs through hardware compatibility and simplified software tools.
Utmel: One-stop FPGA sourcing and technical support platform
As a professional service provider in the field of electronic components distribution, Utmel offers the following core values to industrial and communication customers:
Genuine Product Guarantee: Authorized cooperation with Ceres, Intel and other head manufacturers to ensure the original quality of chips.
Fast delivery: Covering Virtex, Kintex and other mainstream models, with sufficient inventory and support for 48-hour shipment for urgent projects.
Technical support: provide Vivado/IP core configuration guidance, FAE team to help solve hardware design problems.
Cost Optimization: For small and medium batch requirements, we recommend Chinese alternatives such as Gao Yun and AGM to reduce BOM cost by more than 30%.
Future Trends in FPGA Selection
Technology convergence: Adaptive computing (e.g. Xilinx ACAP) combined with AI edge reasoning to promote industrial equipment intelligence.
Acceleration of Chinese substitution: AGM Micro and other vendors differentiate themselves in the industrial control and AIoT fields through the heterogeneous design of “MCU+FPGA”.
Supply chain resilience: Distributors such as Utmel help customers cope with the complex market environment through its global logistics network and technology empowerment.
Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap DevicesSaumitra Jagdale15 March 20242452For a long era, silicon has stood out as the primary material for fabricating electronic devices due to its affordability, moderate efficiency, and performance capabilities. Despite its widespread use, silicon faces several limitations that render it unsuitable for applications involving high power and elevated temperatures. As technological advancements continue and the industry demands enhanced efficiency from devices, these limitations become increasingly vivid. In the quest for electronic devices that are more potent, efficient, and compact, wide bandgap materials are emerging as a dominant player. Their superiority over silicon in crucial aspects such as efficiency, higher junction temperatures, power density, thinner drift regions, and faster switching speeds positions them as the preferred materials for the future of power electronics.
Read More
A Comprehensive Guide to FPGA Development BoardsUTMEL11 September 202513916This comprehensive guide will take you on a journey through the fascinating world of FPGA development boards. We’ll explore what they are, how they differ from microcontrollers, and most importantly, how to choose the perfect board for your needs. Whether you’re a seasoned engineer or a curious hobbyist, prepare to unlock new possibilities in hardware design and accelerate your projects. We’ll cover everything from budget-friendly options to specialized boards for image processing, delve into popular learning paths, and even provide insights into essential software like Vivado. By the end of this article, you’ll have a clear roadmap to navigate the FPGA landscape and make informed decisions for your next groundbreaking endeavor.
Read More
Applications of FPGAs in Artificial Intelligence: A Comprehensive GuideUTMEL29 August 20253462This comprehensive guide explores FPGAs as powerful AI accelerators that offer distinct advantages over traditional GPUs and CPUs. FPGAs provide reconfigurable hardware that can be customized for specific AI workloads, delivering superior energy efficiency, ultra-low latency, and deterministic performance—particularly valuable for edge AI applications. While GPUs excel at parallel processing for training, FPGAs shine in inference tasks through their adaptability and power optimization. The document covers practical implementation challenges, including development complexity and resource constraints, while highlighting solutions like High-Level Synthesis tools and vendor-specific AI development suites from Intel and AMD/Xilinx. Real-world applications span telecommunications, healthcare, autonomous vehicles, and financial services, demonstrating FPGAs' versatility in mission-critical systems requiring real-time processing and minimal power consumption.
Read More
800G Optical Transceivers: The Guide for AI Data CentersUTMEL24 December 20253439The complete guide to 800G Optical Transceiver standards (QSFP-DD vs. OSFP). Overcome supply shortages and scale your AI data center with Utmel Electronic.
Read More
Xilinx FPGAs: From Getting Started to Advanced Application DevelopmentUTMEL09 September 20254184This guide is your comprehensive roadmap to understanding and mastering the world of Xilinx FPGA technology. From selecting your first board to deploying advanced AI applications, we'll cover everything you need to know to unlock the potential of these remarkable devices. The global FPGA market is on a significant growth trajectory, expected to expand from USD 8.37 billion in 2025 to USD 17.53 billion by 2035. This surge is fueled by the relentless demand for high-performance, adaptable computing in everything from 5G networks and data centers to autonomous vehicles and the Internet of Things (IoT). This guide will walk you through the key concepts, tools, and products in the Xilinx ecosystem, ensuring you're well-equipped to be a part of this technological revolution.
Read More
Subscribe to Utmel !
80HCPS1432CRMRenesas Electronics America Inc.
AT88SC0104CA-SHMicrochip Technology
TPD4S014DSQRTexas Instruments
KSZ8993MIMicrochip Technology
CM2020-00TRON Semiconductor
KSZ8995FQIMicrochip Technology
KSZ8993MMicrochip Technology
KSZ8695PMicrochip Technology
KSZ8995MMicrochip Technology
KSZ8995MIMicrochip Technology


Product
Brand
Articles
Tools