Transfer Learning Method for detailed defect classification in semiconductor manufacturing based on Convolution Neural Network
Defect Inspection and classification are the most crucial parts of manufacturing processes in semiconductor industries. Both these analyses are essential to identify and correct the processing problems to enhance the quality of the final product. A scanning electron microscope is the most widely used tool for process monitoring at production sites.
Defects in varied shapes and textures occur due to the complex manufacturing processes to develop enhanced semiconductors. It was found that when more manual processes were used, the number of defects increased and henceforth Automatic defects classification was developed. This was a function that automatically classifies defect images into predetermined defect classes. After ADC, Deep learning technology brought further essential improvements in defect classification by providing advanced analytical tools for analyzing big data from manufacturing. However, this technique required expensive ground truth labeling which was not always accurate. Based on certain tests, the convolutional neural network(CNN) transfer learning method (a deep learning technology) was considered the best method for defect classification.
Examined Defects
The process of examining defects starts with the engineers identifying the reasons for yield reduction from the results of examining defects. Defect analysis also helps to prevent defects from occurring again by adopting various measures. The main goal based on the analysis is to identify the root cause of commonly occurring defects and develop solutions.
During the course of this analysis of semiconductor manufacturing, defect images are categorized according to the class of defects to suppress yield reduction. Fig 1. showcases the various kinds of defects and Fig 2. shows that the examination of defects falls into three phases: classification of defects, monitoring trends in defects, and detailed analysis of classification. The specific frequency of a defect captured by using a scanning electron microscope (SEM) plays a crucial role to classify the defect type. Such trend monitoring is highly costly, hence deep learning technologies are used for the analysis of the defects.

Fig 1: Example of Defects

Fig 2: Overview of Defect Quality Control
Literature review
Many Scientists and researchers who were working to find a method for defect analysis found CNN (Convolution Neural Network) as the most efficient and effective method. Human-level classification can be achieved by using CNN due to its advanced analytical tools. Surface and fabric defect classification of steel sheets were introduced in the manufacturing sector which impacted globally for manufacturing. It ensures the high quality and performance of the products. Furthermore, effective features were extracted by a CNN-based defect image classification model through silicon processes.
It was commonly observed that supervision was adopted since a large set of data was inaccurately and manually labeled. This supervision approach for the transfer learning method is further explained below in the classification of defects and transfer learning method.
Classification of defects
A model was developed with an input SEM size of 128X128. The convolution factorization method was adopted to lower the computational cost where 1X1 convolutional layers were added before 3X3 convolutional layers to limit the number of input channels. This model consists of 33 convolutional layers with rectified linear activation in each layer. Fully connected layers are added after dropout and convolutional layers with sizes of 256 and defect class and finally, a softmax layer is added for outputting class probability calculation.
Pre-training and fine-tuning methods are the two foremost stages implemented for the model. The CNN model is trained from incorrectly stacked images (tens to thousand) to weakly supervised training in the pre-training stage. In the fine-tuning method, there is an extension of the output layer with randomly initialized weights so as to reduce the loss on the target task with fewer data points.
For evaluating the functioning of the Automatic Defect classification (ADC) method and the given method, water surface defect SEM images were examined from a manufacturing facility. In this experiment, four defect image datasets were assembled and each data set was marked noisy by non-experts and pure data by experts.
Fig 3 shows the comparison of the ADC method and the proposed method which concludes that the deep learning method is more effective than the traditional ADC method. Table III gives an analysis of per-class classification precision, recall, and sample count for every defect of set C.
Fig 3: Comparison of ADC and proposed methods
Transfer Learning Method:
Transfer learning means learning new tasks by relying on the previously learned tasks in a faster and more accurate way with less training data. Therefore, the Transfer Learning Method is used for the Highly accurate classification of defects. Fine-grained defects occur very rarely which is merely impossible to classify by manual classification methods. To classify such problems, a transfer learning strategy is adopted. There are 4 ways to approach this method based on what we want to transfer (1) Examination-based, (2) feature-based, (3) parameter-based, and 4) Relational-based. The domain used for fine-grained defect classification in the third phase is the same as the domain one used for rough defect classification in the first phase for which a feature-based approach is preferred.
Conclusion
The CNN-based transfer learning method is effective in order to avoid inconsistent manual classification and higher costs. The defect analysis task helps in identifying the root cause behind yield reduction and helps in classifying defect images with high accuracy and lowering labor costs. The transfer learning method can be used instead of the deep learning method which requires large labeled training data sets.
When the results were obtained from real semiconductor fabrication data it was concluded that the proposed method is more reliable than others. This method required fewer labeled data sets. Also, there was a significant decrease in the amount of labor required for manual inspection work which is nearly two-thirds of traditional ADC systems.
UTMEL 2024 Annual gala: Igniting Passion, Renewing BrillianceUTMEL18 January 20245153As the year comes to an end and the warm sun rises, Utmel Electronics celebrates its 6th anniversary.
Read More
Electronic Components Distributor Utmel to Showcase at 2024 IPC APEX EXPOUTMEL10 April 20246168Utmel, a leading electronic components distributor, is set to make its appearance at the 2024 IPC APEX EXPO.
Read More
UTMEL Showcases One-Stop Electronic Component Sourcing Services at electronica Shanghai 2026UTMEL07 July 2026499SHANGHAI, China, July 7, 2026 - UTMEL, a one-stop electronic components sourcing platform operated by Shenzhen Utmel Intelligent Electronic Co., Ltd., successfully participated in electronica Shanghai 2026, held from July 1 to 3, 2026 at the Shanghai New International Expo Centre.
Read More
Electronic components distributor UTMEL to Showcase at electronica ChinaUTMEL07 June 20244751The three-day 2024 Electronica China will be held at the Shanghai New International Expo Center from July 8th to 10th, 2024.
Read More
Electronic components distributor UTMEL Stands Out at electronica china 2024UTMEL09 July 20245341From July 8th to 10th, the three-day electronica china 2024 kicked off grandly at the Shanghai New International Expo Center.
Read More
Subscribe to Utmel !
PT15NH06-00839Amphenol
PT15YV18-01169Amphenol
PT15NV18-04631Amphenol
PT15LV18-10305Amphenol
PT6KH-02282Amphenol
PT15NH06-08515Amphenol
PT15WH06-04352Amphenol
PTC10LH01-00545Amphenol
PT15LV18-07074Amphenol
PTC10LV10-00645Amphenol


Product
Brand
Articles
Tools