web counter

EPM240T100C5N CPLD: Features, Applications and Datasheet

Sophie

Published: 27 October 2023 | Last Updated: 27 October 2023

1860

EPM240T100C5N

EPM240T100C5N

Intel

1.5/3.32.5/3.3V 0.5mm PMIC MAX® II Series EPM240 100-TQFP

Purchase Guide

1.5/3.32.5/3.3V 0.5mm PMIC MAX® II Series EPM240 100-TQFP

Intel EPM240T100C5N is a complex programmable logic device (CPLD) that belongs to the MAX II family. This article will introduce its features, applications and datasheet.

EPM240T100C5N Description

The Intel EPM240T100C5N is a complex programmable logic device (CPLD) that belongs to the MAX II family. It has 192 macrocells, 80 I/O pins, and operates at 2.5V or 3.3V. It uses flash memory to store logic functions and can be programmed using the Quartus II software. It comes in a 100-pin TQFP package and can be used for a variety of applications, such as glue logic, interface bridging, power management, and more.

EPM240T100C5N Features

  • It has 192 macrocells and 80 I/O pins that can be configured for various logic functions.

  • It operates at a frequency of up to 201.1 MHz and has a propagation delay of 4.7 ns.

  • It uses flash memory technology and has a total memory of 8192 bits.

  • It supports 2.5 V and 3.3 V supply voltages and has a low power consumption of 55 mA.

  • It comes in a 100-pin TQFP package with a lead-free finish.


Specifications

Intel EPM240T100C5N technical specifications, attributes, parameters and parts with similar specifications to Intel EPM240T100C5N.
  • Type
    Parameter
  • Factory Lead Time
    8 Weeks
  • Mounting Type

    The "Mounting Type" in electronic components refers to the method used to attach or connect a component to a circuit board or other substrate, such as through-hole, surface-mount, or panel mount.

    Surface Mount
  • Package / Case

    refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.

    100-TQFP
  • Surface Mount

    having leads that are designed to be soldered on the side of a circuit board that the body of the component is mounted on.

    YES
  • Number of I/Os
    80
  • Operating Temperature

    The operating temperature is the range of ambient temperature within which a power supply, or any other electrical equipment, operate in. This ranges from a minimum operating temperature, to a peak or maximum operating temperature, outside which, the power supply may fail.

    0°C~85°C TJ
  • Packaging

    Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.

    Tray
  • Series

    In electronic components, the "Series" refers to a group of products that share similar characteristics, designs, or functionalities, often produced by the same manufacturer. These components within a series typically have common specifications but may vary in terms of voltage, power, or packaging to meet different application needs. The series name helps identify and differentiate between various product lines within a manufacturer's catalog.

    MAX® II
  • Published
    2003
  • JESD-609 Code

    The "JESD-609 Code" in electronic components refers to a standardized marking code that indicates the lead-free solder composition and finish of electronic components for compliance with environmental regulations.

    e3
  • Part Status

    Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.

    Active
  • Moisture Sensitivity Level (MSL)

    Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures

    3 (168 Hours)
  • Number of Terminations
    100
  • Terminal Finish

    Terminal Finish refers to the surface treatment applied to the terminals or leads of electronic components to enhance their performance and longevity. It can improve solderability, corrosion resistance, and overall reliability of the connection in electronic assemblies. Common finishes include nickel, gold, and tin, each possessing distinct properties suitable for various applications. The choice of terminal finish can significantly impact the durability and effectiveness of electronic devices.

    Matte Tin (Sn) - annealed
  • Additional Feature

    Any Feature, including a modified Existing Feature, that is not an Existing Feature.

    IT CAN ALSO OPERATE AT 3.3V
  • HTS Code

    HTS (Harmonized Tariff Schedule) codes are product classification codes between 8-1 digits. The first six digits are an HS code, and the countries of import assign the subsequent digits to provide additional classification. U.S. HTS codes are 1 digits and are administered by the U.S. International Trade Commission.

    8542.39.00.01
  • Voltage - Supply

    Voltage - Supply refers to the range of voltage levels that an electronic component or circuit is designed to operate with. It indicates the minimum and maximum supply voltage that can be applied for the device to function properly. Providing supply voltages outside this range can lead to malfunction, damage, or reduced performance. This parameter is critical for ensuring compatibility between different components in a circuit.

    2.5V
  • Terminal Position

    In electronic components, the term "Terminal Position" refers to the physical location of the connection points on the component where external electrical connections can be made. These connection points, known as terminals, are typically used to attach wires, leads, or other components to the main body of the electronic component. The terminal position is important for ensuring proper connectivity and functionality of the component within a circuit. It is often specified in technical datasheets or component specifications to help designers and engineers understand how to properly integrate the component into their circuit designs.

    QUAD
  • Terminal Form

    Occurring at or forming the end of a series, succession, or the like; closing; concluding.

    GULL WING
  • Peak Reflow Temperature (Cel)

    Peak Reflow Temperature (Cel) is a parameter that specifies the maximum temperature at which an electronic component can be exposed during the reflow soldering process. Reflow soldering is a common method used to attach electronic components to a circuit board. The Peak Reflow Temperature is crucial because it ensures that the component is not damaged or degraded during the soldering process. Exceeding the specified Peak Reflow Temperature can lead to issues such as component failure, reduced performance, or even permanent damage to the component. It is important for manufacturers and assemblers to adhere to the recommended Peak Reflow Temperature to ensure the reliability and functionality of the electronic components.

    260
  • Terminal Pitch

    The center distance from one pole to the next.

    0.5mm
  • Time@Peak Reflow Temperature-Max (s)

    Time@Peak Reflow Temperature-Max (s) refers to the maximum duration that an electronic component can be exposed to the peak reflow temperature during the soldering process, which is crucial for ensuring reliable solder joint formation without damaging the component.

    40
  • Base Part Number

    The "Base Part Number" (BPN) in electronic components serves a similar purpose to the "Base Product Number." It refers to the primary identifier for a component that captures the essential characteristics shared by a group of similar components. The BPN provides a fundamental way to reference a family or series of components without specifying all the variations and specific details.

    EPM240
  • JESD-30 Code

    JESD-30 Code refers to a standardized descriptive designation system established by JEDEC for semiconductor-device packages. This system provides a systematic method for generating designators that convey essential information about the package's physical characteristics, such as size and shape, which aids in component identification and selection. By using JESD-30 codes, manufacturers and engineers can ensure consistency and clarity in the specification of semiconductor packages across various applications and industries.

    S-PQFP-G100
  • Qualification Status

    An indicator of formal certification of qualifications.

    Not Qualified
  • Power Supplies

    an electronic circuit that converts the voltage of an alternating current (AC) into a direct current (DC) voltage.?

    1.5/3.32.5/3.3V
  • Supply Voltage-Min (Vsup)

    The parameter "Supply Voltage-Min (Vsup)" in electronic components refers to the minimum voltage level required for the component to operate within its specified performance range. This parameter indicates the lowest voltage that can be safely applied to the component without risking damage or malfunction. It is crucial to ensure that the supply voltage provided to the component meets or exceeds this minimum value to ensure proper functionality and reliability. Failure to adhere to the specified minimum supply voltage may result in erratic behavior, reduced performance, or even permanent damage to the component.

    2.375V
  • Programmable Type

    These include Field Programmable Logic Devices (FPGAs), Complex Programmable Logic Devices (CPLD) and Programmable Logic Devices (PLD, PLA, PAL, GAL). There are also devices that are the analog equivalent of these called field programmable analog arrays.

    In System Programmable
  • Propagation Delay

    the flight time of packets over the transmission link and is limited by the speed of light.

    7.5 ns
  • Output Function

    An output function is a function that an optimization function calls at each iteration of its algorithm. Typically, you use an output function to generate graphical output, record the history of the data the algorithm generates, or halt the algorithm based on the data at the current iteration.

    MACROCELL
  • Number of Macro Cells
    192
  • JTAG BST

    JTAG BST stands for Joint Test Action Group Boundary Scan Test. It is a testing technique used in electronic components to verify the functionality of integrated circuits on a printed circuit board. The JTAG BST method allows for testing of individual components without the need for physical access to the pins of the component, making it a valuable tool for debugging and testing complex electronic systems. By using a standardized test access port and a set of test logic, JTAG BST can help identify faults, shorts, and other issues in electronic components quickly and efficiently.

    YES
  • Voltage Supply - Internal

    Voltage Supply - Internal is a parameter in electronic components that refers to the internal voltage supply required for the proper functioning of the component. This voltage supply is typically generated within the component itself and is used to power its internal circuitry. It is important for the component to receive the correct internal voltage supply to ensure reliable operation and performance. The specified voltage supply range for a component must be adhered to in order to prevent damage or malfunction. Manufacturers provide this information in the component's datasheet to guide users in proper integration and usage.

    2.5V 3.3V
  • Voltage - Supply (Max)

    Voltage - Supply (Max) is a parameter in electronic components that specifies the maximum voltage that can be safely applied to the component for proper operation. This parameter is crucial for ensuring the component's longevity and preventing damage due to overvoltage conditions. Exceeding the maximum supply voltage can lead to component failure, reduced performance, or even permanent damage. Designers must carefully consider this parameter when selecting components and designing circuits to ensure reliable and safe operation within the specified voltage limits.

    2.625V
  • Delay Time tpd(1) Max

    The parameter "Delay Time tpd(1) Max" in electronic components refers to the maximum time delay between the input signal changing and the output signal responding. It represents the longest time it takes for the output to change after a change in the input signal. This parameter is crucial in determining the speed and performance of the component in various electronic circuits. A longer delay time can result in slower response times and potentially impact the overall functionality of the circuit. It is important to consider this parameter when designing or selecting electronic components to ensure proper operation and timing requirements are met.

    4.7ns
  • Number of Logic Elements/Blocks
    240
  • Length
    14mm
  • Height Seated (Max)

    Height Seated (Max) is a parameter in electronic components that refers to the maximum allowable height of the component when it is properly seated or installed on a circuit board or within an enclosure. This specification is crucial for ensuring proper fit and alignment within the overall system design. Exceeding the maximum seated height can lead to mechanical interference, electrical shorts, or other issues that may impact the performance and reliability of the electronic device. Manufacturers provide this information to help designers and engineers select components that will fit within the designated space and function correctly in the intended application.

    1.2mm
  • Width
    14mm
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    RoHS Compliant
0 Similar Products Remaining

EPM240T100C5N CAD Model

Symbol

image.png

Footprint

image.png

3D Model

image.png

EPM240T100C5N Applications

Intel EPM240T100C5N is a versatile and powerful CPLD that can be used for various applications, such as:

  • Digital signal processing: The device can perform high-speed arithmetic operations, filtering, and data manipulation using its fast input registers, flash memory, and multi-volt I/Os. For example, it can be used to implement a digital filter for audio or video signals, or a digital modulator/demodulator for wireless communication.

  • Embedded system design: The device can act as a glue logic or a microcontroller interface for embedded systems, such as sensors, actuators, displays, or keyboards. It can also implement custom logic functions, such as timers, counters, state machines, or serial protocols. For example, it can be used to control a robotic arm, a smart home device, or a gaming console.

  • Prototyping and testing: The device can be used to prototype and test new designs or concepts quickly and easily, using its real-time ISP and JTAG features. It can also be used to debug and verify existing designs or systems, using its boundary-scan and JTAG translator features. For example, it can be used to emulate a missing component, a faulty circuit, or a new functionality.


EPM240T100C5N Manufacturer

Intel is a multinational corporation and technology company that develops and manufactures microprocessors, chipsets, graphics cards, memory, storage, software, and other products. Intel is one of the world’s largest and most influential semiconductor companies, and a leader in data center solutions, Internet of Things (IoT), and personal computing innovation. Intel was founded in 1968 by Robert Noyce and Gordon Moore, and is headquartered in Santa Clara, California. Intel’s mission is to create world-changing technology that enriches the lives of every person on earth.


Parts with Similar Specs

Frequently Asked Questions

What is Intel EPM240T100C5N?

Intel EPM240T100C5N is a complex programmable logic device (CPLD) that belongs to the MAX II family. It has 192 macrocells and 80 I/O pins that can be configured for various logic functions. It uses flash memory technology and supports 2.5 V and 3.3 V supply voltages.

How to program Intel EPM240T100C5N?

 Intel EPM240T100C5N can be programmed using the Quartus II software tools from Intel. The software tools allow you to design, simulate, synthesize, place and route, and download your logic design to the device. You can also use the JTAG interface or the in-system programmability (ISP) feature to program the device.

How to buy Intel EPM240T100C5N?

You can buy Intel EPM240T100C5N from various online distributors, such as Utmel Electronics or Digi-Key Electronics. You can also contact Intel directly or visit their website for more information on how to order their products.
EPM240T100C5N

Intel

In Stock: 1962

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe