web counter
555 Timer Calculator

555 Timer Calculator, namely 555 Astable Calculator and 555 Monostable Calculator, is designed to determine the pulse width of the output based on the resistance and capacitance values entered for 555 timer chip circuit(NE555, LM555).

555 Timer Calculator

R1 RESISTOR VALUE
C1 CAPACITANCE VALUE
OUTPUT PULSE DURATION

FORMULA

_____ MILLISECONDS V cc R 2 R 1 S 1 C 1 C 2 8 (VCC)4 (RESET)7 (DISCHARGE)6 (THRESHOLD)2 (TRIGGER)3 (OUT)5 (CTRL V)1 (GND)TRIGGER PULSE(S1)OUTPUT PULSE

FORMULAS

_____ MILLISECONDS_____ MILLISECONDS V cc V cc R 1 R 2 C 1 8 (VCC)4 (RESET)7 (DISCHARGE)6 (THRESHOLD)3 (OUTPUT)2 (TRIGGER)1 (GND)TIME LOWTIME HIGH
Introduction

555 Astable calculations. Worked examples of how to calculate T, R, and C.

555 Astable Calculations

555 Timer Calculator Overview

The 555 Timer Calculator helps calculate timing values for common 555 timer circuits. It supports both astable mode, where the 555 generates a continuous pulse train, and monostable mode, where the 555 produces one output pulse after a trigger event.

Use this calculator to estimate output high time, output low time, total period, frequency, duty cycle, and monostable pulse width from the resistor and capacitor values used around a 555 timer IC such as the NE555 or LM555.

555 Astable Calculator

In astable mode, the 555 timer has no stable output state. The timing capacitor repeatedly charges and discharges between internal threshold levels, producing a rectangular waveform at the output pin.

555 timer astable circuit diagram

In the standard astable circuit, the capacitor charges through R1 + R2 and discharges through R2. This is why the output high time and low time are different unless the circuit is modified.

555 timer output waveform showing high and low time

Astable Mode Formulas

For the common 555 astable circuit:

Time high = 0.693 × (R1 + R2) × C

Time low = 0.693 × R2 × C

Period = Time high + Time low = 0.693 × (R1 + 2R2) × C

Frequency = 1 / Period

Duty cycle = Time high / Period × 100%

SymbolMeaningUnit
R1Charging resistor from VCC to discharge pin.Ω, kΩ, or MΩ
R2Timing resistor between discharge pin and timing capacitor.Ω, kΩ, or MΩ
CTiming capacitor connected to the trigger and threshold node.F, µF, nF, or pF
0.693Approximation of ln(2), used because the capacitor charges and discharges between 1/3 VCC and 2/3 VCC.unitless

Astable Example Calculation

Suppose R1 = 10 kΩ, R2 = 47 kΩ, and C = 10 nF.

Time high = 0.693 × (10,000 + 47,000) × 0.00000001 ≈ 0.000395 s

Time low = 0.693 × 47,000 × 0.00000001 ≈ 0.000326 s

Period ≈ 0.000721 s

Frequency ≈ 1 / 0.000721 ≈ 1.39 kHz

Duty cycle ≈ 0.000395 / 0.000721 × 100% ≈ 54.8%

555 Monostable Calculator

In monostable mode, the 555 timer works as a one-shot pulse generator. A trigger pulse on pin 2 starts a timing interval, and the output stays high until the timing capacitor reaches the threshold level.

The monostable pulse width is set mainly by one timing resistor and one timing capacitor:

Pulse width = 1.1 × R × C

InputMeaningUnit
RTiming resistor used to charge the capacitor.Ω, kΩ, or MΩ
CTiming capacitor.F, µF, nF, or pF
1.1Approximation of ln(3), used because the capacitor charges toward VCC until it reaches about 2/3 VCC.unitless

Monostable Example Calculation

Suppose R = 100 kΩ and C = 10 µF.

Pulse width = 1.1 × 100,000 × 0.00001 = 1.1 s

This means the output will stay high for about 1.1 seconds after a valid trigger. The actual pulse width can vary because resistor tolerance, capacitor tolerance, leakage current, trigger shape, supply voltage, and temperature all affect real timing.

What Is a 555 Timer IC?

A 555 timer is an integrated timing circuit used for pulse generation, time delay, oscillation, waveform generation, LED flashing, missing-pulse detection, pulse-width modulation, and simple timing control. Classic bipolar versions include the NE555 and LM555. CMOS versions are also available and can offer lower supply current and different operating limits.

Internally, a 555 timer uses a voltage divider, two comparators, a flip-flop, a discharge transistor, and an output stage. In the usual configuration, the trigger comparator responds near 1/3 VCC, and the threshold comparator responds near 2/3 VCC. The control voltage pin can shift these thresholds when needed.

555 Timer Pinout

555 timer pinout diagram

PinNameFunctionDesign Note
1GNDGround reference.All voltages are measured with respect to this pin.
2TRIGTrigger input.A voltage below about 1/3 VCC starts the timing interval or sets the output high.
3OUTTimer output.Can drive a load within the output current and voltage limits of the selected device.
4RESETActive-low reset input.Connect to VCC if reset control is not used.
5CTRLControl voltage input.Often bypassed to ground with a small capacitor to reduce noise sensitivity.
6THRThreshold input.When this node rises above about 2/3 VCC, the timer resets and the output goes low.
7DISDischarge transistor output.Discharges the timing capacitor during the low portion of the timing cycle.
8VCCPositive supply input.Use the voltage range specified in the datasheet for the exact 555 variant.

Astable vs Monostable Mode

ModeOutput BehaviorMain FormulaTypical Use
AstableContinuous rectangular waveform.f = 1 / [0.693 × (R1 + 2R2) × C]LED flasher, clock pulse, tone generator, simple oscillator.
MonostableOne pulse after each valid trigger.T = 1.1 × R × COne-shot delay, pulse stretching, debounce timing, trigger shaping.

Choosing R and C Values

For best practical results, avoid values that are too extreme. Very large resistors can make the timing node sensitive to leakage current, noise, and PCB contamination. Very large electrolytic capacitors often have wide tolerance and leakage. Very small capacitors can be strongly affected by stray capacitance from wiring, breadboards, sockets, and probes.

When accurate timing is important, use stable capacitors, choose resistors with suitable tolerance, keep the timing node clean and short, and verify the circuit over temperature and supply-voltage range. For precise long delays, a microcontroller, crystal-based timer, or dedicated timing IC may be more appropriate than a basic 555 RC circuit.

Practical Accuracy Limits

FactorEffect on Timing
Resistor toleranceA 5% resistor can shift the calculated time by about the same order of magnitude.
Capacitor toleranceElectrolytic capacitors can vary widely from the marked value.
Leakage currentLeakage changes the effective charge and discharge current, especially with large resistors.
Supply noiseNoise on VCC or the control pin can shift trigger and threshold behavior.
Load currentHeavy loads can change output levels, increase heating, or require a driver transistor.
Device variantBipolar and CMOS 555 timers have different supply current, output drive, leakage, and voltage limits.

Common Applications

ApplicationPreferred ModeReason
LED flasherAstableGenerates a repeating on-off waveform.
Clock pulse generatorAstableProvides a periodic timing signal for simple digital circuits.
One-shot delayMonostableProduces one pulse with a defined width after a trigger.
Switch debounceMonostableConverts a noisy mechanical transition into a clean pulse.
Pulse-width modulationModified 555 circuitUses the timing network or control pin to vary pulse width.

Common Mistakes to Avoid

MistakeWhy It Causes Trouble
Leaving RESET floatingThe output may reset unexpectedly. Tie RESET to VCC when unused.
Ignoring capacitor leakageLong timing intervals can be very inaccurate with leaky capacitors.
Using a breadboard for high-frequency timingStray capacitance and inductance can distort the waveform.
Driving a large load directlyThe 555 may overheat or the output voltage may sag. Use a transistor or MOSFET driver when needed.
Assuming duty cycle can reach exactly 50% in the basic astable circuitThe standard two-resistor astable circuit charges through R1 + R2 and discharges through R2, so duty cycle is normally above 50% unless modified.

Video Reference

How the 555 Timer Works.

FAQ

Why does the 555 use 1/3 VCC and 2/3 VCC thresholds?

The classic 555 uses an internal resistor divider to create reference levels near 1/3 and 2/3 of the supply voltage. The trigger and threshold comparators use these levels to set and reset the internal latch.

Can a 555 timer make an exact 50% duty-cycle waveform?

The basic astable circuit normally produces a duty cycle above 50%. A near-50% duty cycle can be achieved with circuit modifications, such as steering charge and discharge paths with diodes or using a different oscillator arrangement.

Why is my measured timing different from the calculator?

The calculator uses ideal formulas. Real timing changes with resistor tolerance, capacitor tolerance, leakage, supply voltage, temperature, trigger shape, wiring capacitance, and the selected 555 variant.

Can I use a 555 timer for very long delays?

It is possible, but accuracy can become poor because large resistor and capacitor values are sensitive to leakage and tolerance. For reliable long delays, consider a digital timer, microcontroller, RTC, or crystal-based circuit.

Related 555 Timer Parts and Datasheets

NE555P - classic bipolar 555 timer from Texas Instruments.

NE555N - NE555 timer IC option from STMicroelectronics.

NE555PWR Datasheet - datasheet reference for a TI NE555 variant.

Related Online Calculation Tools

SMD Resistor Code Calculator - decodes 3-digit, 4-digit, and EIA-96 SMD resistor markings.

Resistor Color Code Calculator - calculates through-hole resistor values from color bands.

Capacitor Energy and Time Constant Calculator - calculates capacitor energy and RC time constants.

Ohm's Law Calculator - calculates voltage, current, resistance, and power.

Frequently Asked Questions

1.How does a 555 timer work in astable mode?

We can also connect the 555 timer IC in an Astable mode to produce a very stable 555 Oscillator circuit for generating highly accurate free running waveforms whose output frequency can be adjusted by means of an externally connected RC tank circuit consisting of just two resistors and a capacitor.

2.What is the astable mode of operation?

In astable mode, the 555 timer acts as an oscillator that generates a square wave. The frequency of the wave can be adjusted by changing the values of two resistors and a capacitor connected to the chip.

3.What is the purpose of a 555 timer?

A Monostable 555 Timer is required to produce a time delay within a circuit. If a 10uF timing capacitor is used, calculate the value of the resistor required to produce a minimum output time delay of 500ms.

4.How accurate is a 555 timer?

For less than 1% accuracy, the 555 timer is an ideal choice. For an accuracy better than 0.1%, consider digital or crystal techniques. Occasionally the 555 will suffer from jitter problems on its output if the supply- voltage variations are rapid with respect to the timing cycle.

5.What is the maximum frequency of a 555 timer?

500-kHz to 2-MHz  The Max frequency range of the 555 timer IC in astable mode is from 500-kHz to 2-MHz. Astable Multivibrator mode of 555 timer IC is also called Free running or self-triggering mode.

6.What is the difference between monostable mode and astable mode in 555 timer circuits?

Astable multivibrator, in which the circuit is not stable in either state —it continually switches from one state to the other. Monostable multivibrator, in which one of the states is stable, but the other state is unstable (transient). A trigger pulse causes the circuit to enter an unstable state.

7.What does a monostable circuit do?

Monostable circuits are used as timers, pulse generators, waveform generators, and sweep generators for CRTs (cathode ray tubes) such as the ones found in some television (TV) receivers, older computer displays, oscilloscopes, and spectrum analyzers.

8.How do you trigger a 555 monostable?

Usually, the timer IC 555 is triggered by applying a negative going pulse to its trigger pin 2. This timer is triggered through a positive pulse in its reset pin. In the monostable mode IC 555 starts timing cycle when a negative pulse is applied to its trigger pin 2.

9.What are the applications of 555 timer?

PWM (Pulse Width Modulation) & PPM (Pulse Position Modulation)  Duty Cycle Oscillator.  Lamp Dimmer.  To provide Accurate time delays.  As a flip-flop element.  Digital logic probes.  Analog frequency meters.  Quad Timer applications.

10.What are the operating modes of 555 timer?

The 555 IC has the following operating modes:  Astable (free-running) mode – the 555 can operate as an electronic oscillator.  Monostable (one-shot) mode – in this mode, the 555 functions as a "one-shot" pulse generator.  Bistable (flip-flop) mode – the 555 operates as an SR flip-flop.
Hot products

ImagePart NumberManufacturerCategoryPackage/CaseDescriptionPriceQuantityBuy/Quote
BLM18PG121SN1DBLM18PG121SN1DMurata ElectronicsFerrite Beads and Chips0603 (1608 Metric)MURATA - BLM18PG121SN1D - Ferrite Bead, 0603 [1608 Metric], 120 ohm, 2 A, BLM18P Series, 0.05 ohm, ± 25%-

In stock : 355131

Minimum: 1

AD9364BBCZAD9364BBCZAnalog Devices Inc.RF Transceiver ICs144-LFBGA, CSPBGARF Transceiver 1.3V 144-Pin CSP-BGA Tray-

In stock

Minimum: 1

MPZ2012S102AT000MPZ2012S102AT000TDK CorporationFerrite Beads and Chips0805 (2012 Metric)TDK - MPZ2012S102AT000 - FERRITE BEAD, 0.15OHM, 1.5A, 0805-

In stock : 51745

Minimum: 1

SE2537L-RSE2537L-RSkyworks Solutions Inc.RF Amplifiers16-VFQFN Exposed PadRF Amplifier 5GHz Gain 30 dB 3.3Volt -10C 85C-

In stock

Minimum: 1

CYBL10162-56LQXICYBL10162-56LQXICypress Semiconductor CorpRF Transceiver ICs56-UFQFN Exposed PadMCU 32-Bit CYBL10X6X ARM Cortex M0 RISC 128KB Flash 1.8V/2.5V/3.3V/5V 56-Pin QFN EP Tray-

In stock : 48

Minimum: 1

SKY81294-14-001SKY81294-14-001Skyworks Solutions Inc.PMIC - LED Drivers9-BGA, WLCSPIC LED FLASH DVR 1.2V 9CSP-

In stock

Minimum: 1

HSMS-282P-TR1GHSMS-282P-TR1GBroadcom LimitedDiodes - RF6-TSSOP, SC-88, SOT-363Diode Schottky 15V 6-Pin SOT-363 T/R-

In stock

Minimum: 1

80HCPS1432CRM80HCPS1432CRMRenesas Electronics America Inc.Specialized ICs576-BBGA, FCBGAIC SER RAPIDIO SWITCH 576FCBGA-

In stock

Minimum: 1

ALT6702RM45Q7ALT6702RM45Q7Skyworks Solutions Inc.RF Amplifiers-IC RF AMP CELLULAR SMD-

In stock

Minimum: 1

SI8261BBD-C-ISSI8261BBD-C-ISSilicon LabsIsolators - Gate Drivers6-SOIC (0.295, 7.50mm Width)4A Gate Driver Capacitive Coupling 5000Vrms 1 Channel 6-SDIP-

In stock

Minimum: 1

SI8261BAD-C-ISSI8261BAD-C-ISSilicon LabsIsolators - Gate Drivers6-SOIC (0.295, 7.50mm Width)Gate Drivers 5kV Opto input Sgl channel 4.0A driver-

In stock

Minimum: 1

CSR8510A06-ICXR-RCSR8510A06-ICXR-RQualcommRF Transceiver ICs6-XFBGAIC RF TXRX BLUETOOTH 6XFBGA-

In stock

Minimum: 1

FOD8333FOD8333ON SemiconductorIsolators - Gate Drivers16-SOIC (0.295, 7.50mm Width)Optocoupler AC/DC-IN 1-CH DC-OUT 16-Pin SO Rail-

In stock

Minimum: 1

FOD8332R2FOD8332R2ON SemiconductorIsolators - Gate Drivers16-SOIC (0.295, 7.50mm Width)OPTOISO 4.243KV GATE DRIVER 16SO-

In stock

Minimum: 1

SP1004U-ULC-04UTGSP1004U-ULC-04UTGLittelfuse Inc.TVS - Diodes10-XFDFNTVS DIODE 9.2V 1004/10DFN-

In stock : 2633

Minimum: 1

ISM303DACTRISM303DACTRSTMicroelectronicsMultifunction-HIGH PERFORMANCELOW POWER COMPAC-

In stock

Minimum: 1

SLD8S36ASLD8S36ALittelfuse Inc.TVS - DiodesNonstandard SMDTVS DIODE 36.5V 58.1V SMTO-263-

In stock : 20

Minimum: 1

ACPL-302J-500EACPL-302J-500EBroadcom LimitedIsolators - Gate Drivers16-SOIC (0.295, 7.50mm Width)OPTOISO 5KV 1CH GATE DRIVER 16SO-

In stock

Minimum: 1

UR020-006-RAUR020-006-RATripp LiteUSB Cables-TRIPP-LITE UR020-006-RACOMPUTER CABLE, USB, 6FT, BLACK-

In stock

Minimum: 1

SFH 4713ASFH 4713AOSRAM Opto Semiconductors Inc.Infrared, UV, Visible Emitters3-SMD, No LeadEMITTER IR 860NM 1A-

In stock

Minimum: 1