web counter
Ohms Law Calculator

Use the Ohms Law calculator to quickly calculate resistance, current, voltage, and power. Ohm's Law Calculator online tool represents the relationship between voltage, current, and resistance in an electrical circuit. Enter any two known values and click calculate to get the remaining values. Reset after each calculation.

Ohms Law Calculator

Voltage (V)
V
Current (I)
A
Resistance (R)
Ω
Power (P)
W
Formula
ohm law
Introduction

A basic introduction to ohm's law.  It explains how to apply ohm's law in a series circuit and in a parallel circuit.

Ohm's Law

Ohm's Law Calculator Overview

The Ohm's Law Calculator quickly calculates voltage, current, resistance, and power in a simple electrical circuit. Enter any two known values and the calculator returns the remaining values using Ohm's law and electric power formulas.

Ohm's law is most useful for resistive circuits where voltage, current, and resistance have a predictable relationship. It is commonly used when choosing resistors, checking current draw, estimating power dissipation, sizing LED resistors, and troubleshooting basic DC circuits.

What Is Ohm's Law?

Ohm's law describes the relationship between voltage, current, and resistance in an ohmic conductor. If temperature and other physical conditions remain approximately constant, the current through the conductor is proportional to the voltage across it.

The basic formula is:

V = I × R

where V is voltage in volts, I is current in amperes, and R is resistance in ohms.

Ohm's Law Formulas

FindFormulaUse When You Know
VoltageV = I × RCurrent and resistance
CurrentI = V / RVoltage and resistance
ResistanceR = V / IVoltage and current

Ohm's law triangle

Power Formulas

Electrical power is the rate at which electrical energy is converted to heat, light, motion, or another form of energy. In DC resistive circuits:

P = V × I

Combining this with Ohm's law gives:

FindFormulaUse When You Know
PowerP = V × IVoltage and current
PowerP = I² × RCurrent and resistance
PowerP = V² / RVoltage and resistance
CurrentI = P / VPower and voltage
VoltageV = P / IPower and current

Ohm's law power formula wheel

Electrical Units

QuantitySymbolUnitMeaning
VoltageVvoltElectrical potential difference between two points.
CurrentIampereRate of electric charge flow.
ResistanceRohmOpposition to current flow.
PowerPwattRate of energy conversion or dissipation.

How to Use the Ohm's Law Calculator

Choose the value you want to calculate, then enter any two known values. For example, if you know voltage and resistance, the calculator can find current and power. If you know current and resistance, it can find voltage and power.

Always enter values in compatible units. Convert milliamps to amps, kilohms to ohms, and milliwatts to watts before comparing or calculating unless the calculator provides unit selectors.

Ohm's law equation variations

Example Calculations

Find Current

A circuit has a 12 V supply and a 6 Ω resistor.

I = V / R = 12 / 6 = 2 A

The power dissipated by the resistor is:

P = V × I = 12 × 2 = 24 W

Find Resistance

A lamp operates from 120 V and draws 0.625 A.

R = V / I = 120 / 0.625 = 192 Ω

The lamp power is:

P = V × I = 120 × 0.625 = 75 W

Ohmic and Non-Ohmic Devices

Ohm's law works directly for ohmic materials and devices whose resistance stays approximately constant over the operating range. Many metal-film resistors are close to ohmic under normal conditions.

Some devices are not ohmic. LEDs, diodes, transistors, thermistors, lamps, varistors, batteries, and many semiconductor devices do not have a constant resistance over all voltages and currents. For those parts, use the datasheet curves and the correct circuit model instead of treating them as fixed resistors.

DC and AC Use

For DC resistive circuits, use:

V = I × R

For AC circuits with impedance, the comparable relationship is:

V = I × Z

where Z is impedance in ohms. In AC circuits, impedance can include resistance, inductive reactance, and capacitive reactance. Voltage and current may also have phase difference, so RMS values and power factor may be required for accurate power calculations.

Common Mistakes to Avoid

MistakeCorrect Approach
Using milliamps as amps without conversion.Convert 20 mA to 0.02 A before using the formula.
Ignoring resistor power rating.Calculate power and choose a resistor with suitable wattage margin.
Applying fixed-resistance math to LEDs directly.Use LED forward voltage and current to calculate a series resistor.
Assuming resistance never changes.Temperature, material, tolerance, and self-heating can change resistance.
Using DC formulas for reactive AC loads.Use impedance, RMS values, and power factor for AC circuits.

Practical Design Notes

In real circuits, resistor tolerance and temperature coefficient affect the actual value. A resistor marked 1 kΩ may not be exactly 1000 Ω, and its resistance can drift as it warms. For precision circuits, choose components with suitable tolerance, temperature coefficient, voltage rating, and power rating.

When calculating current draw from a power supply, include every load and check startup current, inrush current, and transient conditions. A steady-state Ohm's law calculation may not capture short peaks that matter for fuses, switches, connectors, and power supplies.

Video Reference

How to Calculate Ohm's Law.

FAQ

What two values do I need for the calculator?

Any two values among voltage, current, resistance, and power are usually enough to calculate the others for a simple resistive DC circuit.

Why is power important in Ohm's law calculations?

Power tells you how much energy is being dissipated. If a resistor dissipates more power than it is rated for, it can overheat or fail.

Does Ohm's law apply to LEDs?

Not directly as a fixed resistance. LEDs are nonlinear devices. Use the LED forward voltage and target current to choose a current-limiting resistor.

What is the difference between resistance and impedance?

Resistance is the real opposition to current flow. Impedance includes resistance plus AC effects from inductance and capacitance.

Related Online Calculation Tools

Voltage Divider Calculator - calculates output voltage and resistor values for voltage divider circuits.

LED Series Resistor Calculator - calculates a current-limiting resistor for LED circuits.

Parallel and Series Resistor Calculator - calculates equivalent resistance for resistor networks.

dBm to Watts Calculator - converts RF power between dBm and watts.

Frequently Asked Questions

1.What are the 3 forms of Ohm's law?

A circle diagram to help in memorizing the Ohm's Law formulas V = IR, I = V/R, and R= V/I. The V is always at the top. 

2.What is the current formula?

Current is usually denoted by the symbol I. Ohm's law relates the current flowing through a conductor to the voltage V and resistance R; that is, V = IR. An alternative statement of Ohm's law is I = V/R.

3.What is Ohm's law in simple terms?

A law in electricity: the strength of a direct current is directly proportional to the potential difference and inversely proportional to the resistance of the circuit.

4.How many ohms is 100 watts?

For example, a 100 watt light bulb operating on 120 volts AC will have 144 ohms of resistance and will draw 0.833 Amps.

5.How can you mean by 1 ohm?

1 Ohm is defined as the resistance of a conductor with a potential difference of 1 volt applied to the ends through which 1-ampere current flows.

6.What is the wattage formula?

The formula for calculating wattage is: W (joules per second) = V (joules per coulomb) x A (coulombs per second) where W is watts, V is volts, and A is amperes of current. In practical terms, wattage is the power produced or used per second. For example, a 60-watt light bulb uses 60 joules per second.

7.What is the relation between current and resistance?

The relationship between current, voltage, and resistance is expressed by Ohm's Law. This states that the current flowing in a circuit is directly proportional to the applied voltage and inversely proportional to the resistance of the circuit, provided the temperature remains constant.

8.What are the types of current?

There are two kinds of current electricity: direct current (DC) and alternating current (AC). With direct current, electrons move in one direction. Batteries produce direct current. In alternating current, electrons flow in both directions.

9.How many ohms is 40 watts?

40 watts divided by 20 amps squared. The 20 amps squared is 400, so we have 40 watts divided by 400, giving us an answer of . 1 ohms or 100 milliohms.  10.How many watts is a 2-ohm speaker?

10.How many watts is a 2-ohm speaker?

With a 2 ohm speaker, the maximum output power will be 550 watts.
Hot products

ImagePart NumberManufacturerCategoryPackage/CaseDescriptionPriceQuantityBuy/Quote
BLM18PG121SN1DBLM18PG121SN1DMurata ElectronicsFerrite Beads and Chips0603 (1608 Metric)MURATA - BLM18PG121SN1D - Ferrite Bead, 0603 [1608 Metric], 120 ohm, 2 A, BLM18P Series, 0.05 ohm, ± 25%-

In stock : 355131

Minimum: 1

TP3420AV309TP3420AV309Texas InstrumentsInterface - Telecom20-LCC (J-Lead)IC TELECOM INTERFACE 20PLCC-

In stock

Minimum: 1

19-217/R6C-AL1M2VY/3T19-217/R6C-AL1M2VY/3TEverlight Electronics Co LtdLED Indication - Discrete0603 (1608 Metric)LED RED CLEAR 2SMD-

In stock : 6070

Minimum: 1

MPZ2012S102AT000MPZ2012S102AT000TDK CorporationFerrite Beads and Chips0805 (2012 Metric)TDK - MPZ2012S102AT000 - FERRITE BEAD, 0.15OHM, 1.5A, 0805-

In stock : 51745

Minimum: 1

SE2537L-RSE2537L-RSkyworks Solutions Inc.RF Amplifiers16-VFQFN Exposed PadRF Amplifier 5GHz Gain 30 dB 3.3Volt -10C 85C-

In stock

Minimum: 1

SKY81294-14-001SKY81294-14-001Skyworks Solutions Inc.PMIC - LED Drivers9-BGA, WLCSPIC LED FLASH DVR 1.2V 9CSP-

In stock

Minimum: 1

HMC588LC4BTRHMC588LC4BTRAnalog Devices Inc.RF Misc ICs and Modules24-TFQFN Exposed PadIC OSC VCO WIDEBAND 24SMD-

In stock

Minimum: 1

80HCPS1432CRM80HCPS1432CRMRenesas Electronics America Inc.Specialized ICs576-BBGA, FCBGAIC SER RAPIDIO SWITCH 576FCBGA-

In stock

Minimum: 1

DS21Q48NDS21Q48NMaxim IntegratedInterface - Telecom144-BBGAIC LIU E1/T1/J1 4X 5V LONG144BGA-

In stock

Minimum: 1

ALT6702RM45Q7ALT6702RM45Q7Skyworks Solutions Inc.RF Amplifiers-IC RF AMP CELLULAR SMD-

In stock

Minimum: 1

EEF-CS1E150REEF-CS1E150RPanasonic Electronic ComponentsAluminum - Polymer Capacitors2917 (7343 Metric)Aluminum Organic Polymer Capacitors 15uF 25volt-

In stock

Minimum: 1

AFBR-2418TZAFBR-2418TZBroadcom LimitedFiber Optics - Receivers-Fiber Optic Transmitters, Receivers, Transceivers RX DC-50MBd ML 820nm ST Thrd-

In stock

Minimum: 1

SFH 4713ASFH 4713AOSRAM Opto Semiconductors Inc.Infrared, UV, Visible Emitters3-SMD, No LeadEMITTER IR 860NM 1A-

In stock

Minimum: 1

TZY2Z060AC01R00TZY2Z060AC01R00Murata ElectronicsTrimmers, Variable Capacitors-2.5 ~ 6pF Trimmer Capacitor 25V Top Adjustment-

In stock

Minimum: 1

SML-S13RTT86SML-S13RTT86ROHM SemiconductorInfrared, UV, Visible Emitters1206 (3216 Metric)EMITTER IR 850NM 30MA 1206-

In stock : 1

Minimum: 1

TZY2Z100AC01R00TZY2Z100AC01R00Murata ElectronicsTrimmers, Variable Capacitors-3 ~ 10pF Trimmer Capacitor 25V Top Adjustment-

In stock

Minimum: 1

DGD2136S28-13DGD2136S28-13Diodes IncorporatedPMIC - Gate Drivers28-SOIC (0.295, 7.50mm Width)HV GATE DRIVER SO-28-

In stock

Minimum: 1

TEN-HS5TEN-HS5Traco PowerAccessoriesAluminumTRACOPOWER TEN-HS5 Power Supply Accessory, Heat Sink, DC/DC Converter, TEN25, TEN25WI Series
  • 1:$3.817981
  • 10:$3.601869
  • 100:$3.397990
  • 500:$3.205651

In stock : 255

Minimum: 1

HEF4044BT,652HEF4044BT,652NXP USA Inc.Logic - Latches16-SOIC (0.154, 3.90mm Width)IC R/S LATCH 3-STATE QUAD 16SOIC-

In stock

Minimum: 1

T9GV5L14-22T9GV5L14-22TE ConnectivityRelays-Power Relays, Standard, Monostable, DC, 900 mW Coil Power Rating DC, 538 Ω Coil Resistance, UL Coil Insulation Class F, Potter & Brumfield T9G-

In stock

Minimum: 1