Sort by
Emerging Storage Technologies: MRAM, RRAM, and PCRAM08 January 2026
The semiconductor industry is turning to emerging memories that offer higher storage performance, lower cost, and the ability to move toward process miniaturization. Three of these memories stand out -- MRAM, RRAM, and PCRAM.
What is an ASIC Chip?07 January 2026
ASIC (Application Specific Integrated Circuit) is a special-purpose integrated circuit, which is an integrated circuit designed and manufactured in response to specific user requirements and the needs of a specific electronic system.
How a CPU is made? [HD Graphics]07 January 2026
Hello everyone, I am Rose. Welcome back to the new post today. The CPU, sometimes known as a "microprocessor," is the heart of modern computers. The specs and frequencies of the CPU are frequently regarded as crucial indicators of a computer's performance in PCs.
What are Resonators?07 January 2026
A resonator is an electronic component that can generate a resonant frequency. It has the characteristics of stability and good anti-interference performance. Like the low-frequency circuit, the resonator is also the basic component of the radio frequency circuit. It is widely used in filters, oscillators, frequency meters and adjustable In circuits such as amplifiers. The commonly used RF/MW resonators are basically transmission line resonators.
Basic Introduction to Color Sensor07 January 2026
The color sensor is also called a color recognition sensor. It is a sensor that compares the object color with the previously taught reference color to detect the color.
How to Generate Negative Voltage: 5V to -5V Circuit Analysis & Schemes05 January 2026
Hello everyone, I am Rose. Welcome to the new post today. Today I will introduce negative voltage to you. Including its definition, how it was generated and its meaning.
Audio Transformer-Types, Functions and Working05 January 2026
An audio transformer is an electromagnetic system designed to separate an input circuit from an output circuit and produce a signal that passes through it with filtering. A varying electromotive force (voltage) in the secondary winding linked to the other circuit is caused by this changing flux.
What is LCD? Working Principle, Features, and Future Trends05 January 2026
LCD is a liquid crystal display. The LCD structure is to place a liquid crystal cell between two parallel glass substrates. LCD has replaced CRT as the mainstream, and the price has dropped a lot, and it has become fully popular.
What is DDR5 SDRAM? The Ultimate Guide to Specs, Architecture, and Market Trends05 January 2026
DDR5 is a computer memory specification. In July 2020, the JEDEC Association officially announced the DDR5 standard, starting at 4800MHz and reaching 6400MHz in the future.
Stepper Motor: Types, Working and Applications26 December 2025
A brushless, synchronous electric motor that converts digital pulses to mechanical shaft rotation is known as a stepper motor. When operated by a sequentially switched DC power supply, the normal shaft motion is made up of discrete angular motions of approximately uniform magnitude.
What is FPC (Flexible Printed Circuit)?26 December 2025
Flexible Printed Circuit (FPC) is a highly reliable and excellent flexible printed circuit board made of polyimide or polyester film. It has the characteristics of high wiring density, lightweight, thin thickness, and good bendability.
Switching Power Supply Debugging: 10 Most Common Problems26 December 2025
Hello everyone, I am Rose. Today I will introduce 10 common problems about SMPS debugging to you. Switch Mode Power Supply (SMPS for short), also known as switching power supply, switching converter, is a high-frequency power conversion device and a type of power supply.


Product
Brand
Articles
Tools