Sort by
What are Wire Wound Resistors?19 January 2026
Wire wound resistors are a type of fixed resistors. Wire-wound resistors are constructed with resistance wires wound on an insulating frame. The resistance wire is generally made of nickel-chromium, manganese-copper alloys with a certain resistivity.
What is Chip: Definition, Classification and Design Process17 January 2026
Hi fellas. I am Rose. Today I will introduce the process of designing chips for you. Chips, also known as integrated circuits or VLSIs, are electronic circuits made up of thousands, millions, or even billions of transistors, resistors, and capacitors.
What are the Applications of Filters?17 January 2026
Filtering is a basic and important technique in signal processing. Using filtering techniques, the desired signal can be extracted from various signals and unwanted interference signals can be filtered out. A filter is an important component in the frequency domain analysis of a signal.
The Comprehensive Guide to MOSFETs: Principles, Types, and Parameters (2026 Edition)16 January 2026
Hello everyone, I am Rose. Today I will introduce MOSFET to you. Metal-Oxide Semiconductor Field Effect Transistor (MOSFET) is a field effect transistor that can be widely used in analog circuits and digital circuits
Introduction to Types of Oscillator Circuits14 January 2026
The oscillator operates on the theory of the oscillation and it is a mechanical or electronic unit. The periodic difference between the two items is dependent on the variations in the electricity. The oscillations are used in the watches, clocks, metal detectors and in many other applications use the oscillators.
Everything You Need to Know about RF Chip14 January 2026
RF chip is one of the most important cores of cell phone terminals. The RF chip is responsible for RF transceiver, frequency synthesis, and power amplification.
Basic Introduction to Power Amplifier09 January 2026
Power amplifier refers to an amplifier that can generate the maximum power output to drive a certain load (such as a speaker) under a given distortion rate. The power amplifier plays a pivotal role of "organization and coordination" in the entire audio system, and to a certain extent dominates whether the entire system can provide good sound quality output.
Diode Basis: Symbol, Types and Applications09 January 2026
Hello everyone, I am Rose. Today I will introduce diode to you. A diode is an electronic device made of semiconductor materials (silicon, selenium, germanium, etc.). It has unidirectional conductivity, that is, when a forward voltage is applied to the anode and cathode of the diode, the diode conducts. When a reverse voltage is applied to the anode and cathode, the diode is turned off.
What is a Voltage Controlled Oscillator?09 January 2026
Voltage controlled oscillator (VCO) refers to an oscillator circuit whose output frequency corresponds to the input control voltage. The operating state of the oscillator or the component parameters of the oscillation circuit are controlled by the input control voltage. The frequency of the VCO has a linear relationship with the control voltage. It is an important part of PLL.
What is a Knock Sensor?08 January 2026
Hello everyone, I am Rose. Welcome back to the new post today. I will introduce Knock Sensor to you. The knock sensor is a small "listening" device in or on the engine that detects abnormal vibrations and sounds coming from the engine block.
Introduction to EPROM and EEPROM08 January 2026
EPROM (Erasable Programmable Read-Only Memory) is a kind of ROM memory with erasable function and can be reprogrammed after erasing. Before writing, the contents inside must be irradiated with ultraviolet rays on the transparent window on its IC card to clear it. EEPROM (Electrically Erasable Programmable Read-Only Memory), a memory chip that does not lose data after power failure. EEPROM can erase the existing information and reprogram it on the computer or special equipment.
What is a Digital Potentiometer?08 January 2026
Digital potentiometer, also known as CNC programmable resistor, is a new CMOS digital and analog mixed signal processing integrated circuit that replaces traditional mechanical potentiometer (analog potentiometer). The digital potentiometer is controlled by a digital input and produces an analog output. Depending on the digital potentiometer, the maximum tap current can range from a few hundred microamps to a few milliamperes.


Product
Brand
Articles
Tools