Sort by
Introduction to MSP430 Microcontroller26 December 2025
MSP430 microcontroller is a 16-bit ultra-low power, RISC mixed-signal processor marketed by Texas Instruments (TI) in 1996.
What is a Motor Starter?26 December 2025
A motor starter is an electrical system used to safely start and stop a motor. Like a relay, the motor starter turns power on/off, which offers low voltage and overcurrent safety, as opposed to a relay.
Rheostat Basics: Types, Principle and Functions25 December 2025
A rheostat is a device that can adjust the size of the resistance and can be connected to the circuit to adjust the size of the current. A general rheostat is composed of a wire with a larger resistance and a device that can change the contact point to adjust the effective length of the resistance wire. Rheostat can limit the current and protect the circuit, and change the voltage distribution in the circuit.
Surge Protection Devices (SPD): The Complete 2025 Guide25 December 2025
A surge protection device (SPD), also called a surge protector, is an electronic device that provides safety protection for various electronic equipment, instruments, and communication lines. When a spike current or voltage is suddenly generated in the electrical circuit or communication circuit due to external interference, the surge protection device can conduct and shunt in a very short time, so as to prevent the surge from damaging other equipment in the circuit.
What is Time Delay Relay?18 December 2025
Hello everyone, I am Rose. Today I will introduce Time Relay to you. A Time Relay is an electrical component that is used on a circuit with a lower voltage or lower current to turn on or off a circuit with a higher voltage and bigger current or to regulate a higher voltage or larger power. This article will introduce some basic knowledge of Time Relay.
An Overview of Development Board18 December 2025
The development board is a circuit board used for embedded system development. Development boards are generally customized by embedded system developers according to development needs.
What is GND in a Circuit?18 December 2025
In this article, you will learn the classification of GND and its working principle. GND is an abbreviation for the ground. GND represents the ground wire or the 0 wire. This ground is not a real ground, it is a ground assumed for the purpose of application. For the power supply, it is the negative pole of a power supply.
Top 10 OSAT (Outsourced Semiconductor Assembly and Test) Companies18 December 2025
This article introduces the flow of semiconductor assembly and test, global packaging and testing vendor revenue from 2020-2021, and an overview of the top 10 OSAT companies.
Ultimate Guide to KVM Switches: Definition, Usage, and 2025 Trends18 December 2025
Hello, I am Rose. Welcome back to the new post today. KVM stands for keyboard, video and mouse. The so-called KVM is also called a multi-computer controller, and the official name is a multi-computer switch. A KVM switch is a hardware device that allows users to control 2, 4, 8, 16, or even more than 4096 computer hosts through a set of keyboards, video monitors, and mice.
Thermistor: Characteristics, Classification, Symbol and Applications10 December 2025
Thermistors are a class of sensitive components. They are divided into positive temperature coefficient thermistors (PTC) and negative temperature coefficient thermistors (NTC) according to different temperature coefficients.
Global Ceramic Capacitors Market In-Depth Analysis to 202510 December 2025
This article provides an in-depth analysis of the global ceramic capacitors market in 2025.
The Evolution History of Storage Devices26 November 2025
Some people say that "most technology products are destined to be open for only a short period of time." Today, I intend to talk about the evolutionary history of storage devices in the age of technology.


Product
Brand
Articles
Tools